Icon Legend Definitions
Compatible
The form, fit and function of such products permit them to be used in combination or as part of a single solution. Compatibility may require a specific product configuration and firmware or software revisions/updates. Compatibility does not refer to third party interfaces and technologies that are not under RA's control.
Clicking on the Compatibility Green Check will take you to additional information in Knowledgebase.
Clicking on the Compatibility Green Check will take you to additional information in Knowledgebase.
Not Compatible
Has known limitations which will restrict the functionality available to the end user.
Clicking the link may take you to document(s) with more information.
Clicking the link may take you to document(s) with more information.
No known issues or dependencies
No known issues or dependencies
May be Compatible
Has known limitations which may restrict the functionality available to the end user that can be overcome by following specific configuration, setup, or additional programming.
Clicking the icon may take you to a Knowledge Base article about the specific situation.
Clicking the icon may take you to a Knowledge Base article about the specific situation.
Known Anomaly
The anomaly exists in the associated version of the product
Corrected Anomaly
The anomaly was corrected in the associated version of the product
Documentation Download Available
Release note for the selected version. Can be in PDF or HTML format. Some release notes can be viewed across a range of versions.
Click the icon to begin or select available downloads.
Click the icon to begin or select available downloads.
Software/Firmware Download Available
Free downloads available for a particular product version.
Click the icon to begin or select available downloads.
Click the icon to begin or select available downloads.
Important Notice
Means a product version has one of the following advisories available for viewing: 'Product Safety Advisory', 'Product Security Advisory', or 'Product Notice'
View Incompatible Products
Check for not compatible or may be compatible products
Active (Applies to Latest Offering)
Most current offering within a product category.
Active Mature
Product is fully supported, but a newer product or family exists. Gain value by migrating.
LifeCycle Details
You will see this icon when a product represents multiple product lifecycles. Click the icon for the respective product to view the full listing of lifecycles.
End of Life
Discontinued date announced - actively execute migrations and last time buys. Product generally orderable until the discontinued date. Outages on specific items may occur prior to the Discontinued date.
Discontinued
New product no longer manufactured or procured. Limited stock may be available in run-out mode, regionally. Repair/exchange services may be available.
Disabled by default
Port disabled by default; configurable
Enabled by default
Port enabled by default; configurable
Essential; nonconfigurable
Essential port is always enabled; not configurable