Icon Legend Definitions
     Icon
     Legend 
      Compatible   Not Compatible
      No known issues or dependencies    May be Compatible
      Known Anomaly    Corrected Anomaly
      Documentation Download Available    Software/Firmware Download Available
      Important Notice    View Incompatible Products
      Active (Applies to Latest Offering)    Active Mature
      LifeCycle Details    End of Life
      Discontinued    Disabled by default
      Enabled by default    Essential; nonconfigurable
     A blank or empty cell indicates that there are no known issues or dependencies.
     Click on an icon for a more detailed definition.
    Compatible
    The form, fit and function of such products permit them to be used in combination or as part of a single solution. Compatibility may require a specific product configuration and firmware or software revisions/updates. Compatibility does not refer to third party interfaces and technologies that are not under RA's control.

    Clicking on the Compatibility Green Check will take you to additional information in Knowledgebase.
    Not Compatible
    Has known limitations which will restrict the functionality available to the end user.

    Clicking the link may take you to document(s) with more information.
    No known issues or dependencies
    No known issues or dependencies

    May be Compatible
    Has known limitations which may restrict the functionality available to the end user that can be overcome by following specific configuration, setup, or additional programming.

    Clicking the icon may take you to a Knowledge Base article about the specific situation.
    Known Anomaly
    The anomaly exists in the associated version of the product

    Corrected Anomaly
    The anomaly was corrected in the associated version of the product

    Documentation Download Available
    Release note for the selected version. Can be in PDF or HTML format. Some release notes can be viewed across a range of versions.

    Click the icon to begin or select available downloads.
    Software/Firmware Download Available
    Free downloads available for a particular product version.

    Click the icon to begin or select available downloads.
    Important Notice
    Means a product version has one of the following advisories available for viewing: 'Product Safety Advisory', 'Product Security Advisory', or 'Product Notice'

    View Incompatible Products
    Check for not compatible or may be compatible products

    Active (Applies to Latest Offering)
    Most current offering within a product category.

    Active Mature
    Product is fully supported, but a newer product or family exists. Gain value by migrating.

    LifeCycle Details
    You will see this icon when a product represents multiple product lifecycles. Click the icon for the respective product to view the full listing of lifecycles.

    End of Life
    Discontinued date announced - actively execute migrations and last time buys. Product generally orderable until the discontinued date. Outages on specific items may occur prior to the Discontinued date.

    Discontinued
    New product no longer manufactured or procured. Limited stock may be available in run-out mode, regionally. Repair/exchange services may be available.

    Disabled by default
    Port disabled by default; configurable

    Enabled by default
    Port enabled by default; configurable

    Essential; nonconfigurable
    Essential port is always enabled; not configurable