Series 
 Version 
PanelView Plus 700-1500
series
5.10.16UP
5069-L320ER
series A
30.011
   Compatibility
   Release Notes
   Features
  General
Controller Message to Self
Device Level Ring (DLR)
Dual Configurable Ethernet Ports
Electronic Data Sheet AOP
Embedded EDS Files
Embedded Real Time Clock (RTC)
EtherNet/IP Support
Extended Tag Properties
HMI Connectivity and Performance Improvements
Improved Controller Capacity Calculation
Improved Messaging Performance
Improved Power Supply Design
Improved Security
Instruction-based Alarm Support
IO Event Task
Logix Tree, Enhancements to Finding-Adding Devices
Logix Tree, Module Discovery
Module Discovery on Logix Tree
Precision Time Protocol (PTP)
Project Documentation Stored in Controller
Quality of Service
SD Card Read/Write
String Literals
Support for PanelView 5000 Button Control
USB Network Access Port
  Add On Instructions
Add-On Instructions, Attributes
Add-On Instructions, False Execution
Add-On Instructions, High-Integrity
Add-On Instructions, Improved False Execution Time
Add-On Instructions, Safety
Add-On Instructions, User Defined
Add-on-Profiles (AOP's)
High-integrity Add-On Instructons Unique Signature ID
Pre-scan of Add-On Instruction Behavior
  Alarms and Events
Alarm Shelving support for Logix device-based Alarms
ALMA and ALMD Instructions
FactoryTalk Alarms and Events Features
Full ISA 18.2 Alarm State Standard Adoption
  Communications DeviceNet Network
DeviceNet I/O communication
  Communications EtherNetIP Network
Ability to Unicast on EtherNet/IP
Dual IP Address
Duplicate IP Address Detection
Embedded Switch Technology
Enhanced Embedded Web Pages
Expanded Socket Connections Support
Open Socket capability
Support for CIP Sync
Support for Precision Time Protocol
Support for Sockets and Increased Packet Size
Unicast IO with EtherNetIP Networks
Unicast Produce/Consume Standard
Use of Dynamic Host Configuration Protocol
  Communications General
Class 1 Messaging (I/O)
Class 3 Messaging (MSG)
  Firmware Management
Digitally Signed
Increased Firmware Upgrade Stability
Logix5000 Firmware Supervisor
  Integrated Motion On EtherNetIP
CIP Motion Using EtherNet/IP Networks
Kinetix 5500 CIP-Motion Servo Drives
Kinetix 5500 CIP-Safety Drives Supported
Load Observer CIP Motion
Motor Test and Commutation Angle Test
PowerFlex Support
Third Party Motor Support
  Motion Coordinated
Updated Motion Coordinate Linear Move Instruction Merge All Functionality
  Motion General
Automatic Device Configuration for Drives (ADC)
Drive Multiplexing Provides Support for Multiple Coarse Update Rates
Kinematic Geometries
Kinematic Transformations Instructions Added
MCD and MCCD Motion Instructions Enhancements
  Motion SERCOS
Kinetix 6000M Integrated Drive-Motor Systems
  Programming
Event Task
FactoryTalk Alarms and Events (Logix-Based Alarms)
PhaseManager
Runtime Detection of Controller Modifications
  Redundancy
Hold Output State During Fault Mode
Hold Output State During Program Mode
Hot Backup
  Safety
EtherNetIP and ControlNet CIP Safety
GuardLogix Safety Instructions
Safety Add-On Instructions
Support for Remote Safety Modules
  Security
Change Detection Audit Value
Data Access Control
License-Based Source Protection
Security Authority for Authentication and Authorization
   PanelView Plus Run-time
  General
MER File V3.2
MER File V4.0
MER File V5.0
MER File V5.1
MER File V6.0
MER File V6.10
MER File V7.00
MER File v8.00
MER File v8.10
MER File V8.20
MER File V9.00
  Domain Authentication
Windows 2000 Domain
Windows 2003 Domain, Mixed-mode
Windows 2003 Domain, Native-mode
Windows 2008 Domain
Windows 2012 Domain
   Networks and Communications
  KEPServer Enterprise
KEPServer Enterprise V4.0
KEPServer Enterprise V4.5
KEPServer Enterprise V5.03
KEPServer Enterprise V5.07
   Anomaly
  General
1756-IB16D Module Can Become Non-operable
A String Length of a Large Number or Negative Value Can Cause a Controller MNRF
After power cycling, the controller SFC routines do not execute properly (00229202)
Cannot Modify Armor PowerFlex Configuration While Online
CIP™ Axis Velocity Loop Causes Controller To MNRF/Assert
CompactLogix 5380 Controller in Dual-IP Mode Takes a Long Time to Connect to I/O
Connected UnCached Messages Fail (00173896)
Controller Asserts When Ethernet Gateway Address Matches IP Address
Controller Can Assert During The I/O Module Configuration Process
Controller Can Assert When Motion Instruction Accel And/Or Decel Operands Are Out of Range
Controller Can MNRF When Executing CPS Instruction with Specific Data Types
Download Can Fail
Dual Feedback position error jumps (00232347, 00232504)
Editing of UDTs and AOIs Online May Affect Online Behavior
Embedded Ethernet port can cause excessive position error faults in Kinetix drives
Invoking the same MSG in both the Prescan and Logic Routines of an AOI causes a MNRF
IP Route Table Web Page Shows the Mask in Reverse Order
Misconfigured Produced/Consumed Tags Can Cause a Controller MNRF/Assert
MSF Instruction Clears the .DriveEnableStatus Bit after the .DN is Set
Multicast Connections with Network Disruptions Can Cause a Controller MNRF/Assert
Multiple Online Sessions of Logix Designer on the Same Controller Can Cause a MNRF
Nested SFC with Selection Branch execution on first transition may be incorrect (00227908)
Online editing of existing LBL or additions of LBL instructions could result in missing code in routines
PCMD Returns Incorrect Error Code
PortPhysicalAddressInfo GSV Does Not Populate After Controller Power Cycle
Removing the SD Card While the Controller Accesses It Can Cause a MNRF
Running Trends Can Cause a MNRF on the Controller
Sent Bytes Per Second Displays a Larger Incorrect Value
Socket application code can cause the controller to MNRF (00227905)
Socket Object Does Not Receive Multicast Traffic
Third-party HMI Communication Drivers can Cause a MNRF
Time in CompactLogix 5380, CompactLogix 5480, and ControlLogix 5580 Alarms is Reported Differently Than in CompactLogix 5370 and
Unable To Change Port A2 IP Configuration After Switch To Dual-IP Mode
Value That Is Outside the Supported WallClockTime Range
When Executing Multiple RTOS Instructions A MNRF/Assert Can Occur
  Motion General
MAR and MAW Instructions Do Not Execute Properly After Controller Power Is Cycled
   Requirements
Compatible Software for Controller Firmware Revision 29
   Application Notes
Equipment Phases Not Supported
New Firmware File Format
New Firmware Updates Can Impact the Performance of Message Rate Capacity HMI/MSG (Class 3) Data
PXRQ Instruction Can Cause a Controller MNRF/Assert
   Security
Change Detection
ControlLogix 5580 and CompactLogix 5380 Programmable Automation Controller Denial of Service
Denial-of-Service Vulnerability That Affects Logix 5000™ Controllers
GoAhead Web Server Vulnerabilities – Logix 5000® Controllers
System and Device-Level Security
VxWorks vulnerabilities that affect Logix 5000™ controllers (00225605, 00225606 and 00225607)