Release Notes

FactoryTalk® Linx high performance communications software optimized for Logix5000 controllers. (included with FTSP)
Version 6.60.00 (released 9/2025)

Catalog Number FactoryTalk Linx (aka RSLinx Enterprise) 

These release notes describe version information for FactoryTalk Linx (aka RSLinx Enterprise), version 6.60.00 (released 9/2025).

Requirements

This release has the following requirements.

FactoryTalk Linx version 6.60.00 (CPR 9 SR 16)
FactoryTalk Linx works within the system requirements of all Rockwell Automation® software products.
For the latest compatibility and driver support information, refer to the Product Compatibility and Download Center.
Hardware requirements
FactoryTalk Linx recommends the following hardware for applications with typical data acquisition needs:
Lower level x86-based CPUs will also work in standalone configurations with reduced data acquisition needs.
For small applications, the following configuration was also evaluated:
It is recommended to run a performance validation test on the planned computer hardware to ensure that the desired capacity and performance can be achieved.
Software requirements
The following operating systems are supported and recommended*:
*The recommended operating systems have priority for Microsoft Patch Qualifications with Rockwell Automation® software.
**Windows Server Datacenter editions are supported. The key difference between Windows Server Standard and Datacenter edition is how Microsoft licenses the operating system. Windows Server Standard includes licensing for up to two virtual machines per core license, making it suitable for lightly virtualized environments. Datacenter edition allows unlimited virtual machines per core license, offering better value for highly virtualized or cloud-scale deployments.
***Windows 11 IoT Enterprise LTSC and Windows 11 Enterprise LTSC are binary equivalents but are licensed differently. Windows 10 IoT Enterprise LTSC and Windows 10 Enterprise LTSC are binary equivalents but are licensed differently.
Rockwell Automation's software installation policy is based on the lifecycle information of Microsoft operating systems. If an operating system's lifecycle state is approaching its end, you may encounter a warning message when trying to install Rockwell Automation software on it.
Microsoft lifecycle policy
Rockwell Automation installation warning policy
Rockwell Automation installation prevention policy
Fixed
Present a warning message during installation on Microsoft operating systems that are 18 months before Microsoft's extended end date.
Prevent installation on Microsoft operating systems that are six months past Microsoft's extended end date.
Modern
Present a warning message during installation on Microsoft operating systems that are 18 months before Microsoft's retirement date.
Prevent installation on Microsoft operating systems that are six months past Microsoft's retirement date.
The following table illustrates how the installation policy is applied using the current operating systems. For the latest compatibility information, refer to the Microsoft Lifecycle Policy and Product Compatibility and Download Center.
Operating system
Microsoft lifecycle policy
Extended end date
Retirement date
Installation warning
Installation prevented
Windows 11 Enterprise and Professional editions
Modern
None
None
None
None
Windows 10 Enterprise and Professional editions
Modern
None
October 14, 2025
April 14, 2024
April 14, 2026
Windows Server 2025 Standard and Datacenter editions
Fixed
October 10, 2034
None
April 10, 2033
April 10, 2035
Windows Server 2022 Standard and Datacenter editions
Fixed
October 14, 2031
None
April 14, 2030
April 14, 2032
Windows Server 2019 Standard and Datacenter editions
Fixed
January 9, 2029
None
July 9, 2027
July 9, 2029
Windows Server 2016 Standard and Datacenter editions
Fixed
January 12, 2027
None
July 12, 2025
July 12, 2027
For requirements specific to running FactoryTalk Linx within FactoryTalk View Studio, refer to the System requirements topic in the FactoryTalk View SE and FactoryTalk View ME Release Notes.
FactoryTalk Linx version 6.60.00 is compatible with these Rockwell Automation products:
Firmware requirements
To use the ControlNet communication feature with FactoryTalk Linx, the minimum requirements are:
To use the DeviceNet communication feature with FactoryTalk Linx, the minimum requirements are:
High Resolution Display Support
Windows 10 v1809 or later is the recommended operating system if running this software with a 2K High Resolution Display with scaling up to 125% and 4K with 150%.
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Supported browsers
The following web browsers have been tested and are supported for use with this release:
Security Requirements
To learn about designing a secure networking environment, review this publication:
To learn about implementing application-level security using FactoryTalk Security, review this publication:
To learn about designing and implementing an architecture with device-level security using CIP Security, review these publications:

Features

This release includes the following system features.

FactoryTalk Linx version 6.60.00 has the following new features:

Corrected Anomalies in This Release

This release corrects the following anomalies.

The list identifies the anomalies corrected in FactoryTalk Linx version 6.60.00.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk Linx version 6.60.00 has no changes in functionality since the last release.

Application Notes

This release has the following application notes.

These are the application notes for FactoryTalk Linx version 6.60.00.
ASCII string convert modifier: SC##
The upper limit of the length of C style strings specifier (SC##) supported in FactoryTalk Linx is 400 bytes. The default upper limit value is SC30, and you can increase the upper limit manually.
Backup and restore
When restoring FactoryTalk Linx configuration in FactoryTalk Administration Console, the existing drivers will be removed and new divers will be restored. The running shortcuts will be affected.
To avoid this issue, reconfigure the shortcuts after the restore process completed or use FactoryTalk Linx Configuration Import Export Tool to make a backup in advance.
Certificates
The following certificates are installed while installing Rockwell Automation software.
  • Use Microsoft Management Console (MMC) to view the certificates in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
    • 2016-Rockwell-Driver-SHA1.cer
    • 2016-Rockwell-SHA256.cer
    • DriverCodeSigning2012-1.cer
    • Drivers-10-10-2018.cer
    • Drivers-11-03-2017.cer
    • Drivers-12-06-2016.cer
    • DriversSHA1-10-10-2018.cer
    • Drivers-SHA1-11-27-2017.cer
    • Logix-11-04-2016.cer
    • Rockwell_2013.cer
    • Rockwell_2014.cer
    • Rockwell_2015.cer
    • rockwellcert2010.cer
    • rockwellcert2013.cer
    • VeriSign Class 3 Public Primary Certification Authority -G5 2036.cer
  • Use Microsoft Management Console (MMC) to view the certificates in Console Root > Certificates (Local Computer) > Trusted Publishers > Certificates.
    • MicRooCerAut2011_2011_03_22.cer
    • RA - Enterprise Root Certification Authority.cer
    • VeriSign Universal Root Certification Authority.cer
CIP connections
If you must limit connections usage in your application, refer to Rockwell Automation Knowledgebase Document ID: QA4294 - CIP connections with RSLinx Enterprise (Reducing PanelView Plus connections) for more information on FactoryTalk Linx connection usage.
CIP Security
On a FactoryTalk Linx workstation where multiple IP addresses exist, only one of them can be configured with CIP security in FactoryTalk Policy Manager.
When FactoryTalk Linx is included in a CIP Security zone, it is required that FactoryTalk Linx retain the IP address of the computer when the FactoryTalk Policy Manager deploys the CIP Security configuration. To accomplish this, the computer either must be configured to use a static or fixed IP address, or the network BOOTP or DHCP server must always provide the computer with the same IP address. If the computer’s IP address is changed after CIP Security is deployed, FactoryTalk Linx will not be permitted to establish a connection to controllers or devices using CIP Security.
Communication Setup editor
Considerations for importing configuration files to version 6.40.00 or earlier
FactoryTalk Linx version 6.50.00 introduced a new parameter, Switch to Windows Default, which is included as an additional column in the exported CSV file. Previous versions do not support this parameter.
To import a new configuration file into version 6.40.00 or earlier, ensure that the column with the header “Param Switch To Windows Default” is deleted from the CSV file.
For more information on importing shortcuts or drivers, see FactoryTalk Linx Help.
ControlNet I/O and DeviceNet I/O
ControlFLASH
FactoryTalk Linx version 6.00.00 cannot be used as the communication software if you are using ControlFLASH version 14.00.00.
To avoid this problem, upgrade ControlFLASH to version 15.00.00 and try again, or use RSLinx Classic as the communication software.
Data access and tag browsing
Device Description File Installation Tool
Starting from FactoryTalk Linx version 6.40.00, the EDS Hardware Installation Tool is renamed to Device Description File Installation Tool.
DH+ limitations
EtherNet/IP compliance
This version of FactoryTalk Linx maintains compliance with the EtherNet/IP standard of Open DeviceNet Vendor Association, Inc. (OVDA).
FactoryTalk Alarms and Events
FactoryTalk Diagnostics
The term "Meta Data" or "metadata" refers to Logix extended tag properties and tag descriptions.
Fast User Switching
FactoryTalk Linx does not support the Fast User Switching feature in Windows operating systems.
File Transfer Utility
In FactoryTalk View Studio, you cannot use the File Transfer Utility to upload/download FactoryTalk View ME (*.mer) files from/to a network location. Although the upload/download appears to complete (via the disappearance of the upload/download progress bar), a follow-up dialog box notifies you that the operation did not complete.
Uploading/downloading FactoryTalk View ME (*.mer) files from/to your local computer works properly. If you want to download a file, copy it from the network location to your local hard drive. If you want to upload a file, upload to a local hard drive and then copy it to the network location.
Firmware Upgrade Wizard
The operation of the Firmware Upgrade Wizard over the Serial-DF1 port is not supported.
To avoid this problem, we recommend that you create a Firmware Upgrade Package on an external compact flash and use it as a means to upgrade your terminal.
Hardware and operating system
Memory related counters and predefined tags are not displayed correctly for L8x controllers. This information is normally obtained from the controller. However, the Logix L8 (ControlLogix 5580 and CompactLogix 5480) series of controllers do not provide this information because of architectural changes within the controller firmware.

Impact of Microsoft deprecating VBScript

Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
IMPORTANT: Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Network Browser
Networks, drivers, and devices
Pass-through description
If an alias tag is created with its base tag's data type as ALARM_ANALOG and ALARM_DIGITAL, FactoryTalk Linx doesn't provide pass-through descriptions for this alias tag. Manually input descriptions if needed.
Predefined items
Starting with version 6.10.00, the FactoryTalk Linx "@RedundancyMode" pre-defined tag was removed and is no longer supported. If an application attempts to access the data value for this tag, it will only receive the default value "0" and the reference will show as a wireframe in FactoryTalk View. To avoid this problem, remove references to this tag from the application.
Remote I/O
Requestor’s subscription rate recommendation
In a FactoryTalk system, data moves from a source like a controller connected to FactoryTalk Linx to a software client when a data item’s value has changed. Once changes are detected, the data values are transferred between multiple components or services. The services use the subscription rate from the requestor to initiate a processing thread to transfer the data to its next destination in the system. Small processing delays by components, network delivery time, a high number of values changing at once, or a heavily loaded system can cause data to be processed and delivered slower than the requested rate. If the source data value changes faster than twice the subscription rate, a newer data value could likely overwrite a previous data value as it travels between the services.
In some cases, sampling at a rate faster than half of the speed of the value changes can help to ensure that data value changes are detected by the requester. Also, balancing the data subscriptions across multiple computers and services can reduce processing and delivery delays.
Security considerations
For information on the security considerations when using Rockwell Automation products, including:
Server Status display
If the FactoryTalk Linx server service is explicitly stopped using the Windows Services control panel, the service will automatically restart to respond to client requests. If using redundant servers, stopping the service will cause a switchover to the secondary server.
In both situations, a standalone server and a redundant server configuration, if the Server Status dialog box is open when the service is stopped the status of the server displays Ready to provide service instead of Active.
Closing the Server Status dialog box and reopening it updates the status displayed accordingly.
Shortcuts
System sizing recommendations
When you design and set up a FactoryTalk system, we recommend using the following guidelines. If you find that your system must expand beyond these guidelines, contact your Rockwell Automation sales or distributor representative to discuss your application design.
Component
Recommended guidelines
FactoryTalk Alarms and Events
 
FactoryTalk Alarms and Events servers per application
10 non-redundant servers or 10 redundant server pairs
FactoryTalk tag-based alarms per server
20,0001
Logix device-based alarms per server
10,0002
Total alarms per application
100,0003
FactoryTalk Linx
 
FactoryTalk Linx data servers per application
10 non-redundant servers or 10 redundant server pairs
Total device tags per application
1,000,0004
Tags per FactoryTalk Linx data server
100,0004
FactoryTalk View SE
 
HMI servers
10 non-redundant servers or 10 redundant server pairs
HMI tags per HMI Server
40,0005
Total data logged tags per HMI server (1-second scan rate)
5,000
FactoryTalk View SE client sessions simultaneously connected to the application
1204
FactoryTalk ViewPoint SE servers per application
4
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
50
  1. The number of alarm backing tags influences the maximum number of available alarms because they increase the resource requirements of the alarm server. When using backing tags for status and control, a good rule of thumb is to multiply the total number of backing tags by the total number of alarms, and ensure that the result is less than 20,000. PlantPAx® users should refer to the PlantPAx Reference Manual PROCES-RM001 for alarm server sizing guidance for a PlantPAx application.
  2. This number is the sum of both instruction alarms and Logix tag-based alarms across all the controller shortcuts in each FactoryTalk Linx server.
  3. The total number of alarms per application includes all FactoryTalk Alarms and Events tag-based and device-based alarms in the application.
  4. Refer to Rockwell Automation Answer ID 1070902 to determine system scalability using this option.
  5. The maximum number of HMI tags that can be created on a single HMI server is 175,000. Extensive use of HMI tags has a significant performance impact on an HMI server, so Rockwell Automation recommends minimizing their use, and instead using direct-reference tags as much as possible.
 
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Installation Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows errors or restart messages.
When using this parameter, the installation will stop and display a prompt if there are errors or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/Product="value"
Specifies which product will be installed.
When installing FactoryTalk Services, the value must be one of the following:
  • FactoryTalk Services Server
  • FactoryTalk Services Client
FactoryTalk Services Custom Installation For example, /Product="FactoryTalk Services Server". This parameter is required.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file. When applied, the installation process automatically creates a recording file <Product>.REC that is stored in this path: %USERPROFILE%\Desktop.
This parameter is optional.
/Playback="value"
Plays back a recording file to specify the installation options. The value is the full path of the REC file to be used. For example, /Playback="C:\Users\<Username>\Documents\<Product>.REC".
This parameter is optional.
/SetupLanguage="value"
Specifies which language will be displayed during the install process. The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
For example, /SetupLanguage="ENU".
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/IISCommPort="value"
Specifies the IIS server communication port for HTTPS. The default port for HTTPS is 443. The range is from 1025 through 49151.
If the HTTPS port was previously configured using FactoryTalk Services Platform, like port 4356, then the existing HTTPS port setting is retained.
This parameter is optional.
/ftsp-scope="value"
Specifies the FactoryTalk Directory scope. The "global", "local", and "both" directory scopes are supported. If you do not configure this parameter during installation, both "global" and "local" scopes will be specified.
This parameter is only available when installing FactoryTalk Services Server or FactoryTalk Services Custom Installation. This parameter is optional.
/ftsp-s="value"
Specifies the FactoryTalk Directory scope for restore. Only "global" and "local" directory scopes are supported. The NETWORK_SECURE.BAK backup file provided by Rockwell Automation is only supported for the "global" scope.
This parameter is only available when restoring FactoryTalk Services Server or FactoryTalk Services Custom Installation. This parameter is optional.
/ftsp-bak="value"
Restores the backup file and specifies where the restore file can be found.
Rockwell Automation provides a NETWORK_SECURE.BAK backup file containing pre-configured access control lists which limit user access. The pre-configured access control lists follow Rockwell Automation recommended best practice.
To implement the access control, restore the NETWORK_SECURE.BAK backup file located in the FactoryTalk Services Platform installation package, Redist\FTSPSecureBak. The BAK file is only supported for the "global" scope, which can be specified with ftsp-s.
This parameter is only available when restoring FactoryTalk Services Server or FactoryTalk Services Custom Installation. This parameter is optional.
IMPORTANT: Applying a BAK file during installation will overwrite an existing FactoryTalk Directory contents, use with caution when applying this parameter.
/ftsp-pp="value"
Specifies the plaintext password used to decrypt the backup file.
This parameter is only available when restoring FactoryTalk Services Server or FactoryTalk Services Custom Installation. This parameter is optional.
/ftsp-value="value"
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether a client computer account must exist in the directory to log in. Only "enable" and "disable" are supported.
This parameter is optional.
/FTSPWebAuth="value"
Specifies that the installation includes the FactoryTalk Web Authentication Server. The FactoryTalk Web Authentication Server will be installed by default with FactoryTalk Services Server.
This parameter is only available when installing FactoryTalk Services Custom Installation. This parameter is optional.
The value must be one of the following:
  • Yes
    If the value is Yes, the FactoryTalk Web Authentication Server will be installed. The FactoryTalk Reverse Proxy will also be installed as it is required for operation of the FactoryTalk Web Authentication Server.
  • No
    If the value is No, the FactoryTalk Web Authentication Server will not be installed, but Internet Information Services (IIS) will be enabled.
/ReverseProxy="value"
Specifies that the installation includes the FactoryTalk Reverse Proxy. The FactoryTalk Reverse Proxy will be installed by default with FactoryTalk Services Server.
This parameter is only available when installing FactoryTalk Services Custom Installation. This parameter is optional.
The value must be one of the following:
  • Yes
    If the value is Yes, the FactoryTalk Reverse Proxy will be installed.
  • No
    If the value is No, the FactoryTalk Reverse Proxy will not be installed, but Internet Information Services (IIS) will be enabled.
/FTSPWebEventServer="value"
Specifies that the installation includes the FactoryTalk Web Event Server. The FactoryTalk Web Event Server will be installed by default with FactoryTalk Services Server.
This parameter is only available when installing FactoryTalk Services Custom Installation. This parameter is optional.
The value must be one of the following:
  • Yes
    If the value is Yes, the FactoryTalk Web Event Server will be installed. The FactoryTalk Reverse Proxy will also be installed as it is required for operation of the FactoryTalk Web Authentication Server.
  • No
    If the value is No, the FactoryTalk Web Event Server will not be installed, but Internet Information Services (IIS) will be enabled.
/SystemStatusPortal="value"
Specifies that the installation includes the FactoryTalk System Status Portal. The FactoryTalk Web Authentication Server and FactoryTalk Reverse Proxy will be installed by default with the FactoryTalk System Status Portal.
This parameter is only available when installing FactoryTalk Services Server or FactoryTalk Services Custom Installation. This parameter is optional.
The value must be one of the following:
  • Yes
    If the value is Yes, the FactoryTalk System Status Portal will be installed. The FactoryTalk Reverse Proxy and FactoryTalk Web Authentication Server will also be installed as it is required for operation of the FactoryTalk System Status Portal.
  • No
    If the value is No, the FactoryTalk System Status Portal will not be installed, but Internet Information Services (IIS) will be enabled.
/DirectoryServer="value"
Specifies the directory server name.
This parameter is only available when installing FactoryTalk Services Client or FactoryTalk Services Custom Installation. This parameter is required when you specify a remote directory server.
/NoHTTPS
Specifies that the setup turns off HTTPS.
This parameter is only available when installing FactoryTalk Services Server or FactoryTalk Services Custom Installation.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/Repair
Runs a repair operation on the installed products. This parameter is optional.
/InstallLocation="value"
Specifies the install location.
For example, InstallLocation="D:\Program Files (x86)\Rockwell Software".
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/InstallDrive="value"
Specifies the install drive.
For example, /InstallDrive="D:".
Some information and files will still be installed to the system volume (typically C:) even when a different target volume is specified. For example, registry entries.
This parameter is optional. If this parameter is not used, the default install drive is C:.
/Uninstall
Use to uninstall the product.
This parameter is optional.
Examples
The following examples show how to use the installation commands.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was canceled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A restart is required to continue the installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restarting, the product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart is pending. Restart the computer to continue the installation.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.
Update Rate
The FactoryTalk Live Data server has the following update rate settings:
When a client application sets an update rate different from the FactoryTalk Live Data server settings, the FactoryTalk Live Data server will update the tag using the closest update rate. For example, the client application sets a 70 msc update rate, the FactoryTalk Live Data server will use 50 msc instead. If the client application update rate is configured as 1000 msc or larger, the FactoryTalk Live Data server will use the integer seconds. For example, the client application sets a 1600 msc update rate, the FactoryTalk Live Data server will use 2000 msc instead. If the client update rate is set as 0 msc, the FactoryTalk Live Data server will use 10,000 msc instead.
There are many factors that can impact the resulting speed that data can be accessed (controller or network communications bandwidth, computer processing capacity, other operations being performed on the computer running FactoryTalk Linx), because of this, requested data values may/will be missed, particularly for the faster rates. Verify the system operation to ensure it handles the resulting effective rate and handles cases where periodic values are not delivered.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.