Release Notes

The TotalFORCE Medium Voltage Drive to control all non-regen applications for Induction and Permanent Magnet Motors
Version 10.002 (released 11/2024)

Catalog Number PowerFlex 6000T (series A)

These release notes describe version information for PowerFlex 6000T, version 10.002 (released 11/2024).

Requirements

This release has the following requirements.

Firmware Revision Control

 

7.xxx is the first firmware package for PowerFlex 6000T drives. The number “7” before the decimal denotes the major revision.

Earlier firmware revisions (1.xxx, 2.xxx, 3.xxx, 4.xxx, 5.xxx, and 6.xxx) apply to PowerFlex Medium Voltage Drive configurations that are built with a different control hardware architecture and a different firmware database.

Updating from those firmware revisions is an intensive process. Contact your Rockwell Sales Office or Technical Support for enquiries.

Features

This release includes the following system features.

Enhanced Transformer Predictive Maintenance

Feature first identified as of Firmware Revision 10.002

Bulletin Number: 6000T


This firmware revision enhances the Transformer Predictive Maintenance feature to normalize the measured AC Line Current with the calculated RMS value before using it in the Predictive Maintenance algorithm.

Improved Logic for Turning on Control Pod Fans

Feature first identified as of Firmware Revision 10.002

Bulletin Number: 6000T


This firmware revision improves the logic to turn on the Control Pod fans based on temperature thresholds for both the SFIB Board and the MPU.

Corrected Anomalies in This Release

This release corrects the following anomalies.

Incorrect Estimated Transformer Life in Dual Transformer Configuration

Corrected Anomaly as of Firmware Revision 10.002

Bulletin Numbers: 6000T


This firmware revision resolves the anomaly where the predictive estimation of the life of each transformer in dual transformer configuration was incorrect.

False Fiber Offline Faults when Drive is in Standby Mode

Corrected Anomaly as of Firmware Revision 10.002

Bulletin Numbers: 6000T


This firmware revision resolves the anomaly where false Fiber Offline faults are reported when the drive is in Standby mode.

Indefinite Precharge Cycles When no Medium Voltage Applied to Main Input Device

Corrected Anomaly as of Firmware Revision 10.002

Bulletin Numbers: 6000T


This firmware revision resolves the anomaly in Secondary Precharge testing, where indefinite Precharge cycles can occur when no Medium Voltage is applied to the Main Input Device.

Incorrect Internal Temperature Readings

Corrected Anomaly as of Firmware Revision 10.002

Bulletin Numbers: 6000T


This firmware revision resolves the anomaly where incorrect internal temperature readings are reported due to synchronization errors between internal clocks.

Frame A Drives – Remaining Fans in the Group Stop Operating After One Fan Fails

Corrected Anomaly as of Firmware Revision 10.002

Bulletin Numbers: 6000T


This anomaly occurs in the Group Fan Control for Non-Redudant Fan configuration for Frame A drives, where one fan failure causes the remaining fans to stop operating.

This firmware revision resolves this anomaly and confirms that the remaining fans are in continuous operation after the failure of one fan.

Known Anomalies in This Release

This release has the following known anomalies.

Predictive Maintenance Page does not Display upon Initial Connection to Connected Components Workbench Software

Known Anomaly first identified as of Firmware Revision 10.002

Bulletin Numbers: 6000T


When the Predictive Maintenance feature is enabled, occasionally the Predictive Maintenance page does not display its contents upon initial connection to Connected Components Workbench™ software.

You can cycle control power to restore the display.

Application Notes

This release has the following application notes.

Application Notes first identified as of Firmware Revision 10.002

Bulletin Number: 6000T

 

  1. Firmware Update

The firmware revision can be verified in the Overview screen in Connected Components Workbench™ software version 22 or later, or Studio 5000 Logix Designer® application.

If the firmware revision is earlier than 10.002 (for example 9.001), updating to firmware revision 10.002 or later is required to get all features that are available with the 10.002 release.

This firmware revision may also require additional hardware such as sensors for options such as predictive maintenance alerts.

graphic

For more information on updating the firmware revision, see the PowerFlex 6000T Drives Programming Manual, publication 6000-PM100.


Before You Begin a Firmware Update

Download the file from PCDC (Product Compatibility and Download Center).

Select the file for firmware revision 10.002.

 

 IMPORTANT
ControlFLASH™ is NOT supported for PowerFlex 6000T main control board firmware updates. Only use ControlFLASH Plus.

 

We recommend that you download and use the latest version of Connected Components Workbench™ software version 22 or later, and Studio 5000 Logix Designer® application.


Update from firmware revision 9.001 to 10.002

  1. Launch Connected Components Workbench software and connect to the drive.
  2. Power down the control bucket.
    If you are updating from firmware revision 7.001, you must also remove all option cards.
  3. Power up the control bucket and connect to the drive using Connected Components Workbench software. Accept the new configuration.
  4. Update the drive to firmware revision 10.002 using the ControlFLASH Plus software.
  5. Connect to the drive using Connected Components Workbench software.
  6. Power down the control bucket.
    If you are updating from firmware revision 7.011, you must also reinstall all option cards.
  7. Power up the control bucket and connect to the drive using the Connected Components Workbench software. Accept the new configuration.

 

  1. eHIM Application Update

Prerequisite: You must download and install version 1.03 for eHIM from the Rockwell Automation PCDC website.

Update to firmware revision 10.002 for the PowerFlex 6000T drive.

The firmware revision file, a *.dmk file, can be downloaded from the Rockwell Automation PCDC website. ControlFLASH Plus™ software is the recommended application to update your firmware when using a *.dmk file,

  1. Power down the eHIM module.
  2. Remove the eHIM module’s Ethernet connection from the product.
  3. Connect the Ethernet connection to a network with internet connection. If required, change the IP address settings. Before doing so, record the existing settings so that they can be set back at the end of the procedure.
  4. Download the latest version of the “Enhanced HIM” software from the “Rockwell Automation Download Center” to the local “Download” folder on your computer.
  5. Once downloaded, power down the eHIM module and remove the Ethernet connection from the network with internet connection.
  6. Power up the eHIM module.
  7. Go to the “Download” folder and double-click on the file “EnhancedHIM.Installer.Bootstrapper.exe”.
  8. Follow the on-screen installation instructions to complete the Enhanced HIM software update installation.
  9. Connect the Ethernet

 

  1. Predictive Maintenance Dashboard in Connected Components Workbench software and Studio 5000 Logix Designer application

To view the option for the Predictive Maintenance dashboard in the explorer tree, download and use the following software from PCDC (Product Compatibility and Download Center).


The following dashboard example is visible from the explorer tree and shows the predicted life of the fans in the drive.

graphic

  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.