This release has the following requirements.
The following are the system requirements for FactoryTalk View SE version 15.00.00 (CPR 9 SR 15).
Hardware requirements
The hardware required with FactoryTalk View SE depends on the demands that an application places on the system. Factors that affect the demands include whether a computer hosts application servers such as FactoryTalk View SE server, FactoryTalk Alarms and Events, FactoryTalk Linx, and FactoryTalk Directory, the number of tags logging at the same time, the number of display clients and related components. The greater the demand, the more powerful the system is required. In any application, faster processors and more memory will result in better performance. In addition, you should specify a hard drive that has enough disk space to provide virtual memory that is at least twice the size of the physical RAM.
The following is a sample specification of computer hardware to run FactoryTalk View SE applications aligned with the hardware used in product development testing.
|
Type
|
Description
|
Hardware
Requirements
|
|
Operator
Workstation
|
FactoryTalk View SE Client
or
FactoryTalk View SE Station
|
Minimum
Recommended
|
|
Engineering
Workstation
|
FactoryTalk View Studio Enterprise
FactoryTalk Linx
Studio 5000
|
Minimum
Recommended
|
|
Application Server
|
FactoryTalk View SE server
FactoryTalk View Studio Enterprise
FactoryTalk Alarms and Events tag-based server
FactoryTalk Linx data server with FactoryTalk Alarms
and Events enabled
|
Smaller systems:
Minimum
Recommended
|
| Medium to larger
systems:
Minimum
Recommended
|
Software requirements
Operating systems
The following operating systems are supported and recommended*:
*The recommended operating systems have priority for Microsoft Patch Qualifications with Rockwell Automation software.
**For more information, see Rockwell Automation Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.
Rockwell Automation's software installation policy is based on the lifecycle information of Microsoft operating systems. If an operating system's lifecycle state is approaching the end, you may encounter a warning message when trying to install Rockwell Automation software on it.
|
Microsoft lifecycle policy |
Rockwell Automation installation warning policy |
Rockwell Automation installation prevention policy |
|
Fixed |
Present a warning message during installation on Microsoft
operating systems that are six months past Microsoft's mainstream date. |
Prevent installation on Microsoft operating systems that are six
months past Microsoft's extended end date. |
|
Modern |
Present a warning message during installation on Microsoft
operating systems that are 18 months ahead of Microsoft's retirement date. |
Prevent installation on Microsoft operating systems that are six
months past Microsoft's retirement date. |
Rockwell Automation will provide a notice about the lifecycle information of the following operating systems.
|
Operating system |
Microsoft lifecycle policy |
Start date |
Mainstream date |
Extended end date |
Retirement date |
Installation warning |
Installation prevented |
|
Windows Server 2019 Standard and Datacenter editions |
Fixed |
November 13, 2018 |
January 9, 2024 |
January 9, 2029 |
None |
August 1, 2024 |
August 1, 2029 |
|
Windows Server 2016 Standard and Datacenter editions |
Fixed |
October 15, 2016 |
January 11, 2022 |
January 12, 2027 |
None |
August 1, 2022 |
August 1, 2027 |
|
Windows 10 Enterprise and Professional editions |
Modern |
July 29, 2015 |
None |
None |
October 14, 2025 |
May 1, 2024 |
May 1, 2026 |
For the latest compatibility information, refer to the Microsoft Lifecycle Policy and Product
Compatibility and Download Center.
Domain controller requirements
The following operating systems are supported for use as domain controllers for FactoryTalk View SE client computers. Using a domain is recommended for applications that include more than 10 computers. If your application includes 10 or fewer computers, they can be organized in a workgroup.
High-resolution display support
If running this software with a 2K or 4K high-resolution display with scaling up to 125%, you can expect acceptable results. For optimal user experiences, use the Windows recommended scaling rate for 2K, 4K, or 8K displays.
Rockwell Automation test environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Supported browsers
The following web browsers are supported for use with this release:
Security requirements
To learn about designing a secure networking environment, review this publication:
To learn about implementing application-level security using FactoryTalk Security, review this publication:
To learn about designing and implementing an architecture with device-level security using CIP Security, review these publications:
This release includes the following system features.
FactoryTalk View SE version 15.00.00 has the following new and enhanced features.
New features
Rockwell Automation has tested and officially supports the following InfluxDB editions: InfluxDB OSS 2.7 and InfluxDB Cloud Serverless.
Enhanced features
This release corrects the following anomalies.
To avoid this issue, import global object displays first.
The following list identifies the anomalies corrected in FactoryTalk View SE version 15.00.00.
This release has the following known anomalies.
These anomalies are from previous releases but are still known in this release.
Datalogoff <name of datalog> and then the command
Datalogon <name of datalog>.Pause 5 command between the launch of each SE client file. This will allow the start of each SE client to be offset from each other.HKEY_USERS\.DEFAULT\Software\Rockwell Software\RSView Enterprise\Data Log
HKEY_USERS\S-1-5-18\Software\Rockwell Software\RSView Enterprise\Data Log
To avoid this issue, do not insert such string tags in a button toggle action's remark.
There is no workaround for this issue.
There is no workaround for this issue.
To view the annotation, right-click and select Annotation from the context menu.
To resolve this issue, set the Live Data policy to TCP/IP.
To resolve this issue, after performing any of those actions, restart your computer.
To avoid this issue, use other login types to log in.
First identified in FactoryTalk Service Platform version 6.40.00. [Jira 3289981]
These documents are renamed with the latest version of FactoryTalk Services Platform, and the older version of FactoryTalk View is hard-coded to previous names. You can view these documents in C:\Program Files (x86)\Common File\Rockwell\Help:
You can also view the FactoryTalk Services Platform Help and Release Notes from the FactoryTalk Administration Console Help menu.
This issue occurs due to the unintended handling of temporary files created when displays are opened in either FactoryTalk View SE client or FactoryTalk View Studio, especially within the Windows Remote Desktop Server (RDS) environment. For specific causes and associated solutions, see Knowledgebase Document ID: BF27588 - FactoryTalk View SE - No longer able to open displays in FactoryTalk View Studio or FactoryTalk View SE Client.
This release has the following functional changes from the previous release.
FactoryTalk View SE version 15.00.00 has the following changes in functionality since the last release.
Require SSL
If HTTPS is enabled during the installation, the RSViewSE site's Require SSL setting is also enabled in Internet Information Services (IIS), which deactivates the HTTP protocol (with the default port 80).
Upgraded VBA version
Microsoft Visual Basic for Applications (VBA) is upgraded to version 7.1.
This release has the following application notes.
The following are the application notes for FactoryTalk View SE version 15.00.00.
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk View SE versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
System sizing recommendations
When you design and set up a FactoryTalk system, we recommend using the following guidelines. If you find that your system needs to expand beyond these guidelines, contact your Rockwell Automation sales or distributor representative to discuss your application design.
|
Component
|
Recommended guidelines
|
|
FactoryTalk Alarms and Events
|
|
|
FactoryTalk Alarms and
Events servers
per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs*
(1)
|
|
FactoryTalk tag-based alarms per
server
|
20,000* (2)
|
|
Logix device-based alarms per server
|
10,000* (3)
|
|
Total alarms
per FactoryTalk Directory
|
100,000* (4)
|
|
FactoryTalk Linx
|
|
|
FactoryTalk Linx data servers
per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs*
(1)
|
|
Total device tags
per FactoryTalk Directory
|
1,000,000* (5)
|
|
Tags per FactoryTalk Linx data
server
|
100,000* (5)
|
|
FactoryTalk View SE
|
|
|
HMI servers
per FactoryTalk Directory
|
10 non-redundant servers or 10 redundant server pairs*
(1)
|
|
HMI tags per HMI server
|
40,000* (6)
|
|
Total data logged tags per HMI
server (1 second scan rate)
|
DataLogPro 50,000 or data log model 5,000
Note: If you want to run both DataLogPro and data log
model on the same HMI server, reduce the number of
tags because the greater the number, the more powerful
the system is required.
|
|
FactoryTalk View SE client sessions
simultaneously connected to the
application
|
120
|
|
FactoryTalk ViewPoint SE servers
per application
|
4
|
|
FactoryTalk ViewPoint SE
concurrent clients per ViewPoint
server
|
50
|
| |
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
Important:
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Unattended installation
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software
installation using an IT tool or script, and don’t expect any error or
restart messages. When using this parameter, check the error codes,
and respond as needed. For example, if the installation returns error
code 1641, then the IT tool or script should restart the computer and
relaunch the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows
progress through the UI, it does not accept any input but still shows
error or restart messages.
When using this parameter, the installation will stop and display a
prompt if there are error or restart messages. For example, if an
immediate restart is required to complete the install, a restart message
will be displayed to confirm the restart. Installation resumes
automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete.
Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used, silent install
(/Q) will return either error code 1641 or 3010 if a restart is required,
and unattended install (/QS) will result in a confirmation prompt that
must be agreed to before the installation is completed.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during the install process.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default
language is the current user or operating system user interface
language.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a
warning occurs.
|
|
/Product="value"
|
Specifies which subproducts will be installed.
This parameter is required.
For FactoryTalk View ME, the value must be one of the following:
For FactoryTalk View SE, the value must be one of the following:
|
|
/DirectoryServer="value"
|
Specifies the FactoryTalk network directory if you are using a
distributed system.
This parameter is optional. If it is not specified, the software will use its
current computer as the FactoryTalk Directory server.
The value must be the host name of the FactoryTalk Directory server.
|
|
/SystemStatusPortal="value"
|
Specifies that the installation includes the FactoryTalk System Status
Portal.
This parameter is optional.
The value must be one of the following:
The FactoryTalk System Status Portal will be installed.
The FactoryTalk System Status Portal will not be installed.
|
|
/NoHTTPS
|
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on
HTTPS for communication, and a certificate must be configured after
installation.
|
|
/IISCommPort
|
Specifies the IIS server communication port for HTTPS. The default port
for HTTPS is 443.
If the HTTPS port was previously configured using FactoryTalk Services
Platform, like port 4356, then the existing HTTPS port setting is
retained.
This parameter is optional.
|
|
/HMIFolder="value"
|
Specifies the folder to store the HMI projects.
This parameter is optional. If you specify a folder that doesn’t exist yet,
it will create a folder for you.
The larger the size of HMI projects, the longer it takes to set up the
folder. Thus, if the size of HMI projects is large, we recommend that
you use the HMI Projects Folder Path Config Utility to configure the
new HMI projects folder after the installation.
|
|
/Uninstall
|
Uninstalls the product.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/InstallDrive="value"
|
Specifies the installation drive.
This parameter is optional. If this parameter is not used, the default
install drive is C:.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used
to activate the software during installation.
This parameter is optional. If it is not specified, the software must be
activated manually after installation if activation is required.
Some software does not require activation. If activation is not required,
this parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during
installation.
This parameter is optional. If it is not specified, the software must be
activated manually after installation if activation is required.
Some software does not require activation. If activation is not required,
this parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate, which corresponds to
the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified, the installer will use the
most recent product version available.
Some software does not require activation. If activation is not required,
this parameter is not available.
|
|
/RemoveApp
|
Deletes the application files when uninstalling the product.
|
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt.
Contact your support personnel.
|
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a restart. After restart, the
installation will continue.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation.
After restart, the product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart the computer for the
installation to continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products
are already installed.
|
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the
installation log file for details. To complete the
installation, restart the computer.
|
HTTPS enabled by default
If you install Studio Enterprise, Site Edition Server, or FactoryTalk ViewPoint SE on a computer with no FactoryTalk View component installed, the installation enables HTTPS by default. In Internet Information Services (IIS), the RSViewSE site's Require SSL setting is also enabled, deactivating the HTTP protocol (with the default port 80).
If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk View SE components. For details on configuring a TLS certificate, see FactoryTalk View Site Edition Installation Guide.
Security requirements
For information on the security considerations when using Rockwell Automation products, including
CIS Benchmarks test results
Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.
For more information about the guidelines, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).
FactoryTalk View SE version 15.00.00 has been tested on CIS Microsoft Windows 10 (Release 22H2) Benchmark v3.0.0, CIS Microsoft Windows 11 (Release 23H2) Benchmark v3.0.0, CIS Microsoft Windows Server 2019 MS Benchmark v3.0.1, and CIS Microsoft Windows Server 2022 MS Benchmark v3.0.0.
Exceptions settings for FactoryTalk View SE version 15.00.00 are listed.
CIS Microsoft Windows 10 (Release 22H2) Benchmark v3.0.0
CIS Microsoft Windows 11 (Release 23H2) Benchmark v3.0.0
CIS Microsoft Windows Server 2019 MS Benchmark v3.0.1
CIS Microsoft Windows Server 2022 MS Benchmark v3.0.0
UAC support
Turning off User Account Control (UAC) is not recommended.
|
Action and Utility
|
Prompts for authentication or confirmation before running
this program
|
|
Configuring Internet Information
Services (IIS)
|
RSViewWebManager.exe CustomWebSite.exe
|
|
Updating Samples application
directory information
|
RefreshSampleApplication.exe
|
|
Ending processes
|
VSClean.exe
|
|
DeskLock
|
DeskLock2000.exe
|
|
Legacy Tag Database Conversion
|
LegacyTagDBConvertTool.exe
|
|
HMI Projects Folder Path Config
Utility
|
HMIProjectsFolderPathConfigUtility.exe
|
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Memory usage by InfluxDB
To help prevent excessive memory usage by the Influxd.exe process, consider balancing the number of tags being queried and the querying frequency, and adjusting your data retention period (storage duration) to optimize system performance.
Ensuring InfluxDB access during administrator upgrade
If FactoryTalk View SE is upgraded by a different administrator, access to InfluxDB may be restricted because the upgrading administrator lacks permissions to the InfluxDB database.
To ensure uninterrupted access to InfluxDB, do either of the following before upgrading:
However, if the upgrade is completed without any precautions beforehand, you can still restore the InfluxDB access. In addition to either of the operations as described above, you must also reset InfluxDB. To do so, go to C:\Program Files (x86)\Rockwell Software\RSView Enterprise, and then run the SetupInfluxDB.exe /r command to reset InfluxDB.
Restoring data log models within different FactoryTalk Directory
Starting from FactoryTalk View SE version 14.00, the data log configuration for the ODBC database is bound with a specific FactoryTalk Directory. As a result, when importing data log MDF files or restoring an HMI server with data logs within a different FactoryTalk Directory, you must enter a username and password on the Setup tab of the Data Log Models editor to connect to the ODBC database.
KEPServer
If you are using KEPServer Enterprise as an OPC server with FactoryTalk View version 9.00.00 or later and using an HMI tag to connect to a third-party device, you will not be able to access the tag value. The cause is that the security enhancements in FactoryTalk View version 9.00.00 or later affect the communications with third-party devices. To access the tag value, the additional Distributed Component Object Model (DCOM) configuration is required for KEPServer Enterprise on the computers.
For more information about the configuration, see Set DCOM configuration for KEPServer Enterprise in Help.
Considerations for application server host computers
In a network application, it is possible for a single-server computer that meets the recommended requirements to host all of the following components:
If a network application requires multiple HMI servers, data servers, or alarm servers, to distribute the load, it is recommended that you install the necessary software and run the servers on multiple host computers.
For information about setting up redundant FactoryTalk View SE servers, see FactoryTalk View Site Edition User’s Guide.
TrendPro objects
Clicking on the X-axis or Y-axis takes it into the free layout mode. In this case, anything done to the canvas is how you want it and it does not resize. The free mode does not persist scale and removes tags from the trend. Avoid using the free mode in the trend.
FactoryTalk Batch View HMI controls
Using EChartsWidget .NET control and earlier versions of FactoryTalk Batch View HMI controls in the same FactoryTalk View SE application may have compatibility problems. To avoid such problems, we recommend that you use the built-in version of Batch View HMI controls included in the FactoryTalk View installation package. For example, EChartsWidget of FactoryTalk View version 14.00 and Batch View HMI controls version 2.02 or earlier cannot be used in the same application. To fix this problem, upgrade Batch View HMI controls to version 3.00.