This release has the following requirements.
FactoryTalk View ME version 15.00.00 (CPR 9 SR 15)
|
Microsoft lifecycle policy
|
Rockwell Automation installation warning policy
|
Rockwell Automation installation prevention
policy
|
|
Fixed
|
Present a warning message during installation on
Microsoft operating
systems that are six months past Microsoft's
mainstream date.
|
Prevent installation on Microsoft operating systems
that are six
months past Microsoft's extended end date.
|
|
Modern
|
Present a warning message during installation on
Microsoft operating
systems that are 18 months ahead of Microsoft's
retirement date.
|
Prevent installation on Microsoft operating systems
that are six
months past Microsoft's retirement date.
|
Rockwell Automation will provide a notice about the lifecycle information of the following operating systems.
|
Operating
system
|
Microsoft
lifecycle
policy
|
Start date
|
Mainstream
date
|
Extended end
date
|
Retirement date
|
Installation
warning
|
Installation
prevented
|
|
Windows
Server 2019
Standard and
Datacenter
editions
|
Fixed
|
November 13,
2018
|
January 9, 2024
|
January 9, 2029
|
None
|
August 1, 2024
|
August 1, 2029
|
|
Windows Server
2016 Standard
and
Datacenter
editions
|
Fixed
|
October 15, 2016
|
January 11, 2022
|
January 12, 2027
|
None
|
August 1, 2022
|
August 1, 2027
|
|
Windows
10
Enterprise
and
Professional
editions
|
Modern
|
July 29, 2015
|
None
|
None
|
October 14, 2025
|
May 1, 2024
|
May 1, 2026
|
FactoryTalk View ME version 15.00.00 supports SQL Server 2022 Express LocalDB as HMI tag databases.
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
This release includes the following system features.
Add Component Tool
Support adding ME components to an application through command lines without using FactoryTalk View Studio.
HMI Projects Folder Path Config Utility
A new utility that supports customizing the HMI projects folder location.
Global Objects folder enhancement
Support creating up to two levels of logical folders for systematic organization of global graphic display components, while maintaining global object references. It also facilitates the drag-and-drop capabilities between different FactoryTalk View Studio instances, and between FactoryTalk View Studio and the Windows Explorer.
FactoryTalk View Studio enhancement
Introduce new menu options to enhance usability:
ME Recipe ActiveX control enhancement
Add ME Recipe 4 ActiveX control to support 1000 floating tags.
Performance enhancement
Enhance the speed of testing an application and creating a runtime application (*.mer) to expedite development workflows and elevate user experience.
This release corrects the following anomalies.
Corrected in FactoryTalk View version 15.00.00.
These anomalies are from previous releases but are still known in this release.
First identified in FactoryTalk Service Platform version 6.40.00. [Jira 3289981]
These documents are renamed with the latest version of FactoryTalk Services Platform, and the older version of FactoryTalk View is hard-coded to previous names. You can view these documents in C:\Program Files (x86)\Common File\Rockwell\Help:
You can also view the FactoryTalk Services Platform Help and Release Notes from the FactoryTalk Administration Console Help menu.
To resolve this problem, reload the runtime application in FactoryTalk View ME Station.
To avoid this problem, you can use the PNG files provided in
Knowledgebase Document ID: BF17144 - Transparency is not working
correctly on the PanelView Plus 6/7 terminals for Symbol Factory objects.
There is currently no workaround for this anomaly.
To avoid this problem, go to Control Panel > Regional and Language Options, and select the appropriate language to match the desired language.
To avoid this problem, enter a valid value in the expression setting for the animation property of the base object first.
To avoid this problem, re-configure the project window size in the Project Settings window.
To successfully register or unregister an ActiveX Control object, do one of the following before the operation:
For more information about UAC, see Application notes.
To avoid this problem, put the Recipe ActiveX control object on a Replace display.
There is currently no workaround for this anomaly.
To avoid this problem, follow the steps below:
C:\Program Files (x86)\Common Files\Rockwell\ on 64-bit operating systems
C:\Program Files\Common Files\Rockwell\ on 32-bit operating systems
where C: is the drive to which Rockwell Automation applications are installed.
regsvr32 RnaSecurityInterfaces.dllThere is currently no workaround for this anomaly.
|
Loading a web page every number of
seconds (s)
|
Approximate memory leak increase
by the number of kilobytes (KB)
|
Approximate cumulative memory
leak over a 600-second duration
|
|
30 s
|
56 KB
|
1,120 KB
|
|
60 s
|
58 KB
|
580 KB
|
|
300 s
|
133 KB
|
266 KB
|
There is currently no workaround for this anomaly.
To show the Chinese characters, link the Tahoma, Arial, and Courier New fonts with Arial Unicode MS.
To link a font with Arial Unicode MS
To ensure that the global connection for remote navigation works, close ME Custom String Popup Keyboard.
To avoid this problem, remove the parameter from the global object.
To avoid this problem, use a tag for the Data_Source connection instead of a tag placeholder.
To avoid this problem, use a mouse and right-click the component to open the menu.
Parameters can be resolved in the test run or runtime mode.
There is currently no workaround for this anomaly.
To unlock the user account in FactoryTalk ViewPoint, reload the application on the PanelView Plus family terminal.
To avoid this problem, run the Microsoft Hotfix KB3201845 outlined in https://support.microsoft.com/en-us/kb/3201845.
Alternatively, you can run Windows 10 v1703 or other supported operating systems where this issue is not present.
For more information about Windows 10 operating system support, see Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.
For more information about Windows Server 2016 operating system support, see Knowledgebase Document ID: IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.
To avoid this problem, configure the data source name and target table. Then other changes can be saved on the ODBC Database tab.
This release has the following functional changes from the previous release.
ME program launcher ActiveX control security enhancement
When adding an ME program launcher ActiveX control to a graphic display, a security confirmation will be displayed. At runtime, a diagnostic message will be logged to identify the program executed.
This release has the following application notes.
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t
expect any error or restart messages. When using this parameter, check the error codes, and respond as
needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the
computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept
any input but still shows error or
restart messages. |
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used when a restart is required to
complete the installation.
This parameter is optional. If this parameter is not used, silent install (/Q) will return either error code 1641 or
3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be
agreed to before the installation is completed.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/HMIFolder="value"
|
Specifies the folder to store the HMI projects.
This parameter is optional. If you specify a folder that doesn’t exist yet, it will create a folder for you.
The larger the size of HMI projects, the longer it takes to set up the folder. Thus, if the size of HMI projects is
large, we recommend that you use the HMI Projects Folder Path Config Utility to configure the new HMI
projects folder after the installation.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/Uninstall
|
Uninstalls the product.
|
|
/RemoveApp
|
Deletes the application files when uninstalling the product.
This parameter is optional.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during the
install process. The value must be the one of the
following:
This parameter is optional. If this parameter is not used, the default language is the current user or operating
system user interface language.
|
|
/Product="value"
|
Specifies which sub-products will be
installed. This parameter is required.
For FactoryTalk View ME, the value must be one of the following:
For FactoryTalk View SE, the value must be one of the following:
|
|
/InstallDrive="value"
|
Specifies the installation drive.
This parameter is optional. If this parameter is not used, the default install drive is C:.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to activate the software during
installation.
This parameter is optional. If it is not specified, the software must be activated manually after installation
if activation is required. Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified, the software must be activated manually after installation
if activation is required. Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate, which corresponds to the product version associated with the
SerialNumber and ProductKey. This parameter is optional. If it is not specified, the installer will use the most
recent product version available.
Some software does not require activation. If activation is not required, this parameter is not available.
|
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support
personnel.
|
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a restart. After restart, the installation
will continue.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restart,
the product is
successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart the computer for the installation to
continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the
installation log file for
details. To complete the installation, restart the computer.
|
Examples
Setup.exe /Q /IAcceptAllLicenseTerms /Product="Machine Edition Station for Windows"Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /Product="Studio for MachineEdition" /InstallDrive=D: /SerialNumber=12345ABCDE /ProductKey=ABCD2-34KDC /Version=13.00.00Setup.exe /Q /Repair /Product="Studio for Machine Edition"If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.
RSNetWorx v21.00 or later is also available in Studio Professional v21.00 or later. If you are not under a current technical support contract, you may purchase an update for RSNetWorx by contacting Rockwell Automation sales.
If you are installing PanelBuilder 1400e and FactoryTalk View Studio on the same computer, install PanelBuilder 1400e first. If you install FactoryTalk View Studio first, the PanelBuilder software will open, but you cannot create applications or open existing applications.
For the latest network security considerations when using Rockwell Automation products, visit the Rockwell Automation Knowledgebase. For information about:
Tip: If your computer is running a 64-bit operating system, the files are in \Program Files (x86), instead of \Program Files.
|
This action
|
Prompts for authentication or confirmation before running this
program
|
|
Setting or changing settings related to DeskLock
|
DeskLock2000.exe
|
|
Creating an application by importing a PanelBuilder application (*.pba) or
a PanelView terminal file (*.pva)
|
VStudio.exe
|
|
In the Networks and Communications dialog box, double-clicking
FactoryTalk Linx
Communications
|
MERuntime.exe
|
|
In the FactoryTalk Linx Configuration dialog box, clicking Close
|
MERuntime.exe
|
|
In the Application Settings dialog box, double-clicking Device
Shortcuts
|
MERuntime.exe
|
|
In the ShortCuts dialog box, clicking Close
|
MERuntime.exe
|
|
Clicking OK in the FactoryTalk View ME Station Startup dialog box
|
MERuntime.exe
|
|
Installing the FactoryTalk View software
|
Setup.exe
|
|
Installing the SQL Server Express 2008 R2 SP2 instance for FactoryTalk
View
|
SQLServerInstall.exe
|
|
Uninstalling the FactoryTalk View software
|
UninstallAllFTView.exe
|
Constraints when using FactoryTalk View version 6.10.00 or later
|
FactoryTalk View ME version
|
Tag database
|
|
6.0 and earlier
|
Watcom
|
|
6.10, 7.0, 8.0, 8.10, 8.20, and 9.0
|
Microsoft SQL Server 2008 R2 Express
|
|
10.0, 11.0, and 12.0
|
Microsoft SQL Server 2014 Express LocalDB
|
|
13.0
|
Microsoft SQL Server 2019 Express LocalDB
|
|
14.0 and later
|
Microsoft SQL Server 2022 Express LocalDB
|
For more information about constraints with creating and running MER on a 64-bit Windows operating system, review Appendix D, "Constraints when using FactoryTalk View version 6.10.00 or later" in FactoryTalk View ME Installation Guide for details.
The names for the following FactoryTalk View Studio components do not support extended ASCII characters or UNICODE characters:
Firmware Upgrade Package
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk View Machine Edition versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.