Release Notes

Connected Components Workbench (CCW) Standard Edition (free) single software to program, simulate, configure, and visualize.
Version 22.00.00 (released 11/2023)

Catalog Number Connected Components Workbench 

These release notes describe version information for Connected Components Workbench, version 22.00.00 (released 11/2023).

Features

This release includes the following system features.

Virtual Network Computing (VNC) support

Feature First Identified as of Firmware Revision 8.012

Catalog Numbers:                                   


The Virtual Network Computing (VNC) feature is now supported for PanelView 800™ terminals that shipped with firmware revision 8.011.

For information on how to use the VNC feature, see the PanelView 800 Terminals User Manual, publication 2711R-UM001.


For older series of PanelView 800 terminals with firmware revision 4.011…7.011

There is no change to the functionality of the current VNC feature and does not affect your PanelView 800 applications.

Corrected Anomalies in This Release

This release corrects the following anomalies.

Get Identity command sent frequently by PanelView 800 terminal to Micro800 controller

Corrected Anomaly as of Firmware Revision 8.012

Known Anomaly First Identified as of Firmware Revision 8.011

Catalog Numbers:                                   


The PanelView™ 800 terminal sends the Get Identity command to the Micro800™ controller repeatedly over short intervals.

This anomaly occurs due to a damaged configuration file, which prevents the terminal from reading the timeout information that is configured.

(APBCCCWART-6495)

Unable to restore, download, and upload recipe table if ingredients are referenced in multiple tables

Corrected Anomaly as of Firmware Revision 8.012

Known Anomaly First Identified as of Firmware Revision 8.011

Catalog Numbers:                                   


If an ingredient is referenced in multiple recipe tables, the application cannot restore, download, or upload the recipe table.

(APBCPV800-422)

Data loss occurs over CIP Serial communication with a Micro800 controller

Corrected Anomaly as of Firmware Revision 8.012

Known Anomaly First Identified as of Firmware Revision 8.011

Catalog Numbers:                                   


Data loss occurs when communicating with a Micro800™ controller over a CIP™ Serial connection.

This anomaly occurs when communicating with the following Micro800 controllers.

(APBCMC800N-8462)

Unable to read custom STRING data from a CompactLogix L3 controller

Corrected Anomaly as of Firmware Revision 8.012

Known Anomaly First Identified as of Firmware Revision 8.011

Catalog Numbers:                                   


Unable to read a custom STRING data type (six-character length) from a CompactLogix™ L3 controller.

(APBCPV800-434)

Functional Changes

This release has the following functional changes from the previous release.

Communication protocols and devices support in PanelView 800 firmware revision 8.012 or later 

Feature set
2711R-T4T series B,
2711R-T7T series A,
2711R-T10T series A,
Firmware revision 7.011 or earlier,
Controller type
2711R-T4T series C,
2711R-T7T series B,
2711R-T10T series B,
Firmware revision 8.012 or later,
Controller type
Updates planned in the future
Virtual Network Computing (VNC) server
Supported
Supported
No
Serial communication
DF1
MicroLogix™, SLC™, and PLC-5® controllers
MicroLogix controllers
No
DH-485
MicroLogix and SLC controllers
Not supported
No
Modbus
Modbus and third-party device listing – Elliott, Magnetek, Omni, Daniel S500, and Dynamic Fluid
Modbus
No
Modbus ASCII
Modbus ASCII, Flow Controller, and
Flow Automation
Not supported
No
Modbus Unsolicited
Modbus
Modbus
No
Ethernet communication
Allen-Bradley® CIP
Supported
Supported
No
Allen-Bradley CIP CompactLogix™
Supported
Supported
No
Allen-Bradley MicroLogix™/ENI
MicroLogix 1400, MicroLogix 1100,
ENI: MicroLogix, ENI: SLC 500 Fixed I/O,
ENI: SLC 500 Modular I/O, and
ENI: PLC-5 and Enumeration_Model_17
MicroLogix 1400 controllers
No
Allen-Bradley SLC/PLC
SLC and PLC-5 controllers
Not supported
No
Modbus
Modbus, Mailbox, Instromet, Roxar RFM, and Fluenta FGM
Modbus
No


Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.