This release has the following requirements.
The following are the system requirements for FactoryTalk Transaction Manager version 14.00.00.
FactoryTalk Transaction Manager works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
FactoryTalk Transaction Manager requires the following hardware:
|
Item
|
Description
|
|
Processor
|
Processor type:
Processor speed:
|
|
Memory
|
|
|
Disk space
|
|
|
Graphics
|
Resolution:
|
|
Peripherals
|
A DVD drive.
|
|
TCP/IP
communication
|
FactoryTalk Transaction Manager services connect to one another via TCP/IP
sockets. To allow FactoryTalk Transaction Manager to operate as a single
system even when services are not distributed over multiple computers in a
network (and FactoryTalk Transaction Manager is only used on a single
computer), ensure that the default networking services are used.
|
Software requirements
FactoryTalk Transaction Manager has been tested on the following operating systems:
Software compatibility
FactoryTalk Transaction Manager is compatible with these Rockwell Automation products:
If using FactoryTalk Transaction Manager with FactoryTalk Metrics, install FactoryTalk Transaction Manager from the FactoryTalk Metrics media. Other versions of FactoryTalk Transaction Manager may be incompatible.
Database installation
FactoryTalk Transaction Manager does not install or configure a database. Therefore, a database must be accessible to your FactoryTalk Transaction Manager application.
If a database has already been installed at your site, your database administrator should handle the administration necessary to connect to the database and provide connection information (user name and password).
See the FactoryTalk Metrics Administration Guide for detailed instructions on how to create a Microsoft® SQL Server® database for use with RSBizWare or FactoryTalk Transaction Manager.
Supported databases
FactoryTalk Transaction Manager supports the following versions of Microsoft SQL Server and Oracle® databases:
FactoryTalk Transaction Manager interfaces with these databases via the following systems:
ODBC (Microsoft SQL Server and Oracle)
It is an industry standard supported by most major database vendors in the industry, including Oracle, Sybase, and Informix. However, different versions of ODBC drivers can impact compatibility.
OLE DB (Microsoft SQL Server only)
It is implemented in Microsoft SQL Server and provides another method for accessing SQL Server. The versions of Microsoft SQL Server supported by OLE DB are the same as for the ODBC driver.
You can convert an existing ODBC connector to OLE DB, or build a new OLE DB connector from scratch.
OCI (Oracle only)
It is implemented for Oracle only. Different versions of OCI drivers can impact compatibility.
For known issues related to specific databases, refer to the technical notes in the Rockwell Automation Knowledgebase.
Microsoft SQL Server
SQL Server ODBC driver and SQL Server Native Client 11.0 ODBC Driver are the supported ODBC drivers for Microsoft SQL Server databases. The version required is dependent on the operating system that you are using.
|
Operating system
|
SQL Server ODBC driver
version
|
SQL Server Native Client ODBC
Driver
|
|
Microsoft Windows
Server 2016
|
SQLSRV32.dll
File and product
version:10.00.7134.010
|
SQLNCLI11.dll
File and product version:
2011.110.654.00.00
|
For OLE DB drivers, use the version listed for the Microsoft SQL Server Native Client ODBC drivers.
Oracle
For Oracle databases, both ODBC and OCI drivers are supported. Regardless of the type of driver used, you must have a net client included to facilitate the connection.
|
Database
|
ODBC driver
|
OCI driver
|
|
Oracle 19c
|
SQORA32.dll
File version:11.2.0.1
Product
version:11.2.0.1.0
|
Oracle database 19c release 2 client for Microsoft
Windows 32 bit
|
|
Oracle 21c
|
SQORA32.dll
File version:12.2.0.1
Product
version:12.2.0.1.0
|
Oracle database 21c release 2 client for Microsoft
Windows 32 bit
|
Software requirements for connectors
Control connectors
The control connector services manage the interaction between the industrial control system and the FactoryTalk Transaction Manager service in the FactoryTalk Transaction Manager.
|
This connector:
|
Requires:
|
|
Generic OPC control
connector
|
An OPC server in either of the following versions:
|
|
FactoryTalk® Live Data
control connector
|
FactoryTalk Services Platform, FactoryTalk® View Site Edition (SE),
RSLinx® Classic, and FactoryTalk Linx in the supported versions.
|
Enterprise database connectors
The enterprise database connector services manage FactoryTalk Transaction Manager interaction between a database and the Transaction Control Manager service or FactoryTalk Transaction Manager service.
|
This connector:
|
Requires:
|
|
Oracle OCI enterprise connector
(Oracle Only)
|
Oracle 19c or 21c.
|
|
OLE DB enterprise connector
(Microsoft SQL Server Only)
|
A Microsoft OLE DB driver, available with any of the
following versions of Microsoft SQL Server:
|
|
ODBC enterprise connector
(Microsoft SQL Server and Oracle)
|
A database-specific ODBC driver that is compliant with the
ODBC specification version 2.0 or later.
|
Language settings
All languages are supported, but the system needs to have the English language added and set as default.
Other software
Microsoft Data Access Components (MDAC) 2.8 is updated during the FactoryTalk Transaction Manager installation.
This release includes the following system features.
FactoryTalk Transaction Manager version 14.00.00 has the following new and enhanced features.
New features
Enhanced features
This release corrects the following anomalies.
Importing an XML file that binds tags to the column name with the number 8 fails
If a SQL Server table column name includes the number 8, when importing an XML file that binds tags to the column name to FactoryTalk Transaction Manager, an error occurs. First identified in FactoryTalk Transaction Manager version 10.20.00. [Jira 461309]
To avoid this issue, do not include the number 8 in column names.
Corrected in FactoryTalk Transaction Manager version 14.00.00.
FactoryTalk Transaction Manager OCI Connector service stops responding on restart if the service is stopped using Toad
If the FactoryTalk Transaction Manager OCI Connector service is stopped using Toad, when you restart the service, it stops responding on restart. First identified in FactoryTalk Transaction Manager version 12.10.00. [Jira 461322]
To avoid this issue, do not use Toad to stop the FactoryTalk Transaction Manager OCI Connector service. Instead, use Microsoft Management Console to do so.
Corrected in FactoryTalk Transaction Manager version 14.00.00.
This release has the following functional changes from the previous release.
FactoryTalk Transaction Manager version 14.00.00 has the following changes in functionality since the last release:
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32 bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64 bit).
Change in enterprise database connector support
Beginning in this release, FactoryTalk Transaction Manager doesn't support the Time-Series Data Compression connector.
This release has the following application notes.
The following are the application notes for FactoryTalk Transaction Manager version 14.00.00.
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
IMPORTANT: Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
SQL Server Management Studio version 2019 and SQL Server Reporting Services version 2019
Starting in FactoryTalk Report Expert version 13.00.00, SQL Server Management Studio version 2019 and SQL Server Reporting Services version 2019 are not included in the installation package. Go to the following links to download these two components:
SQL Server Management Studio
SQL Server Reporting Services version 2019
https://www.microsoft.com/en-us/download/details.aspx?id=100122
Upgrade
For details on upgrading FactoryTalk Transaction Manager to the current version, see FactoryTalk Transaction Manager User Guide. The manual is available on the FactoryTalk Transaction Manager installation media and on the Rockwell Automation Literature Library page.
Activation options
NOTE: For up-to-date information on activation options for FactoryTalk Transaction Manager, consult the Rockwell Automation Knowledgebase article number QA56641.
Activating FactoryTalk Transaction Manager software is determined by the following factors:
Keep the following in mind about the FactoryTalk Transaction Manager activation:
CIS Benchmarks test results
Rockwell Automation conducts tests using the computer configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.
For more information about the guidelines, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).
FactoryTalk Transaction Manager version 14.00.00 has been tested on CIS Microsoft Windows Server 2019 Benchmark v1.3.0.
Exceptions settings for FactoryTalk Transaction Manager version 14.00.00 are listed.
CIS Microsoft Windows Server 2019 Benchmark v1.3.0
Known issues