Release Notes

( 9324-RLDx ) Studio 5000 programming software. All you need for discrete, process, batch, motion, safety etc.
Version 36.00.00 (released 11/2023)

Catalog Number Studio 5000 Logix Designer 

These release notes describe version information for Studio 5000 Logix Designer, version 36.00.00 (released 11/2023).

Requirements

This release has the following requirements.

System requirements for Studio 5000 Logix Designer version v36.00.02

For optimal performance of the Logix Designer application, the personal computer should meet or exceed these hardware and software requirements.

graphic
Tip: The Logix Designer application can be installed on a personal computer that meets the operating system minimum requirements but may not meet performance expectations when used in a production system.
Hardware requirements
Software requirements
graphic
This release is not intended to run on a 32-bit operating system. All operating systems listed are the 64-bit variant.
IMPORTANT
Keep these operating system considerations in mind:
  • Universal C Runtime (CRT) is a Windows operating system component that enables core functionality on the Windows operating system. It was introduced in Windows 10 and distributed to most computers running earlier supported operating systems. This component is present on computers that have been kept up to date.
When installing the Logix Designer application on computers that have not been updated, a prompt displays to install Universal C Runtime or to update the computer to at least the Microsoft April 2014 update roll-up.
  • While the Windows 8.1 and later operating systems run on many touch-enabled devices, various features of the Logix Designer application may not be touch-enabled. Most functions are expected to work with touch, but the software has only been tested with a keyboard and mouse.
  • Logix Designer was tested with UAC set to the most restrictive level (Always notify). This version of the Logix Designer application is also expected to operate correctly when UAC is configured for any less restrictive setting.
  
Preferred operating systems

Preferred operating systems are prioritized for support, testing, and post-release patch qualifications. These operating systems are preferred for this release:

High Resolution Display support

If running this software with a 2K or 4K High Resolution Display with scaling up to 125% you can expect acceptable results.

FactoryTalk Updater version 4.10.00 installation

Install one or more functionalities for FactoryTalk Updater:

Agent

FactoryTalk Updater Agent collects information and activation license data from the Rockwell Automation software installed on the computer. Install the FactoryTalk Updater Agent on each computer that requires data collection. This is the default functionality installed with most Rockwell Automation software.

Server

FactoryTalk Updater Server:

graphic
Tip: To avoid issues, limit FactoryTalk Updater Server installations to one instance per intranet.
Client

FactoryTalk Updater Client is the user interface that displays information collected by the FactoryTalk Updater Server. Install FactoryTalk Updater Client to display information from the intranet.

Firmware requirements
graphic
Tip: Most modules use Flash-ROM for the storage of firmware. If a module requires a firmware change, use the ControlFLASH™ tool or the ControlFLASH Plus® tool to perform the update to the Flash-ROM. These tools are contained in the downloaded image or on a DVD-ROM shipped with the Logix Designer application. Another option is to update the firmware automatically as part of the project download.
For additional information and assistance in performing a Flash-ROM update, review the ControlFLASH Firmware Upgrade Software User Manual, publication 1756-UM105, or the ControlFLASH Plus Quick Start Guide, publication CFP-QS001.

Rockwell Automation test environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Features

This release includes the following system features.

System features for Logix Designer v36.00

Logix Designer application version v36.00 has these new and enhanced features.

New features
In this version of the Logix Designer application, Axis Test Mode allows a Logix Motion Application developer to develop and test an application program without controller network connections to a complete set of physical CIP Motion drives, motors, or machine components. Axis Test Mode works in conjunction with FactoryTalk Logix Echo, so you can test application programs on an emulated setup. With a simple change of target, you can expect that same logic to work on the real hardware.
In this version of the Logix Designer application, the safety signature is a hierarchy of multiple safety signature elements. For example, the safety task, programs, and routines are examples of safety signature elements. Use imitated safety element signatures during impact analysis to help identify the individual changes within a controller project. It might reduce your certification effort if your validation plan does not require re-validation of unchanged elements. To view all safety signature elements for a project, run the Safety Signature report in the Logix Designer application.
This version of Logix Designer application adds the OPC Unified Architecture (OPC UA) at the controller level. You can configure ControlLogix 5580 and CompactLogix 5380 controllers to work as an OPC server or as a client. Use message instructions to configure OPC UA.
Select this link to browse to a Knowledgebase article that describes OPC UA access.
Enhanced features
This version of the Logix Designer application allows you to cut, copy, and paste multiple devices. Cut or copy once and paste the devices multiple times. Import and export multiple devices simultaneously.
In this version of the Logix Designer application, you can use ID number reference for the axis or coordinate system parameter in motion instructions. Using ID number references can help simplify your  code and improve system performance and memory utilization.
In this version of the Logix Designer application, you can select Export all and Import all to export and import all of the EDS files, IO-Link IODD files, and HART DD files between workstations.
In the Logix Designer application version 36.00 you can use these instructions in safety routines on CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers. All standard operators are now also available in safety routines.
  • ACOS
  • IsNAN
  • ASIN
  • LFL
  • ATAN
  • LFU
  • AVE
  • LN
  • BSL
  • LOG
  • BSR
  • RAD
  • COS
  • SIN
  • DEG
  • STD
  • FFL
  • TAN
  • FFU
  • TO_BCD
  • BCD_TO
  • TRUNC
  • IsINF
  • XPY
In this version of the Logix Designer application, the mnemonics for these instructions have been updated to align with IEC 61131-3 and PLCopen standards.
Instruction
Mnemonic in versions v35 and earlier
Mnemonic in versions v36 and later
Arc Cosine
ACS
ACOS
Arc Sine
ASN
ASIN
Arc Tangent
ATN
ATAN
Convert to BCD
TOD
TO_BCD
Convert to Integer
FRD
BCD_TO
Equal To
EQU
EQ
Greater Than
GRT
GT
Greater Than or Equal To
GEQ
GE
Less Than or Equal To
LEQ
LE
Less Than
LES
LT
Limit
LIM
LIMIT
Move
MOV
MOVE
Not Equal To
NEQ
NE
Square Root
SQR
SQRT
Truncate
TRN
TRUNC
X to the Power of Y
XPY
EXPT



New devices supported

This table lists new hardware supported in this release.

Catalog Number
Description
Vendor Name
1756-L85ES
GuardLogix 1756-L85ES Series A controller
Rockwell Automation

Electronic Data Sheets

The version of FactoryTalk Linx software provided with this version of the Logix Designer application includes an updated set of electronic data sheet (EDS) files for Rockwell Automation products. Installing this software ensures that FactoryTalk Linx software and RSNetWorx software will be able to work with the new revisions of firmware. To download and install the latest EDS file, access the Rockwell Automation Services & Support website (http://www.rockwellautomation.com/global/support/downloads.page?).


  

Corrected Anomalies in This Release

This release corrects the following anomalies.

DataExchange fails AML and RDF imports and exports due to incorrect catalog number (1427806)

DataExchange AML and RDF imports and exports fail because the catalog number 5059-HSC2xOB4 is incorrectly listed as 5059-HSC2XOB4 in ModuleType and CatalogServices.

This anomaly corrected in version 36.00.

This anomaly first identified in version 34.00.

PFO Advanced dialog box Clamping limits input range (1585324)

The PFO instruction Advanced dialog box Clamping limits do not update to match the Minimum and Maximum values.

This anomaly only applies to projects using the CompactLogix 5380P and ControlLogix 5580P controllers.

This anomaly corrected in version 36.00.

This anomaly first identified in version 33.00.

Displayed alarm fields may not update when modified programmatically (1541337)

Alarm behavior functions properly with the programmatically modified value; however, the Alarm List and Alarm Properties dialogs box might display values that existed before the programmatic modification.

Saving the file, uploading tags, and reopening the dialogs updates the Alarm List and Alarm Properties to the current value.

This anomaly first identified in version 32.03.

This anomaly corrected in version 36.00.

Logix Designer application Tag-based Alarm extended properties do not auto-populate completely (1957929)

The Logix Designer application tag-based alarm extended property @Alarms does not auto-populate completely in Sequential Function Chart (SFC) or Structured Text (ST) routines. You must manually type out the text in its entirety to access all extended properties.

For example, if your alarm is named MyAlarm, and the input tag is named AlarmInput, you must type:

AlarmInput.@Alarms.MyAlarm.

When you enter the last period, you can select from the list of available extended properties in a dialog box.

This anomaly first identified in version 35.00.

Motion Coordinated Linear Move (MCLM) Instruction Show ??'s for V_X, V_Y, V_Z Axes Positions (2069950)

In the Motion Coordinated Linear Move (MCLM) instruction, if the Position operand is defined with an array tag and the array pointer is set at element 1 or greater, axes V_X, V_Y, V_Z appear as question marks “??” instead of their respective positions.

This anomaly only occurs with direct array references. This will not occur with indirect addressing of the array tag.

This is a display anomaly that does not affect the instruction’s functionality.

This anomaly corrected in version 36.00.

This anomaly first identified in version 33.00.

Changes to a user-defined data type sometimes causes the Logix Designer application to become unresponsive (1170213, 1170044)

Changing user-defined data type (UDT) members when a routine is open, accessing the UDT being changed causes the Logix Designer application to become unresponsive.

This anomaly first identified in version 32.00.

This anomaly corrected in version 36.00.

Upload error: Logic reconstruction data may be corrupted (2180963)
Converting a file to a newer revision that includes structured text application code in a routine or Add-On Instruction with #Region defining the beginning of a collapsible outline segment but omitting the #EndRegion defining the ending results in the verified and downloaded file generating the error Logic reconstruction data may be corrupted during upload.
Issues within the application code can be identified by:
  1. Exporting the file as L5K or L5X.
  2. Importing the file.
  3. Building the file after the import identifies the missing #EndRegion instances with errors.

This anomaly first identified in version 33.00.

Message datatype cannot compile after upload from controller (1785828, 1789626)

The Logix Designer application cannot compile the ACD file after uploading a program-scoped MSG backing\control tag that is used as an InOut parameter in an Add On Instruction (AOI) to a new ACD file.

This anomaly corrected in versions 33.02, 35.00, and 36.00.

This anomaly first identified in version 34.00.


Failure to import Add-On Instructions with partially matching signature history (2239482, 2239491, 2239489)

An error occurs when attempting to import and overwrite an Add-On Instruction that has a signature history with at least one overlapping entry, and a matching active signature status. The import fails with one of several error messages.

This anomaly corrected in version 33.03, 34.03, 35.01.

This anomaly first identified in version 32.00.

Logix Designer application Tag-based Alarm extended properties do not auto-populate completely (1957929, 1957940)

The Logix Designer application tag-based alarm extended property @Alarms does not auto-populate completely in Sequential Function Chart (SFC) or Structured Text (ST) routines. You must manually type out the text in its entirety to access all extended properties.

For example, if your alarm is named MyAlarm, and the input tag is named AlarmInput, you must type:

AlarmInput.@Alarms.MyAlarm.

When you enter the last period, you can select from the list of available extended properties in a dialog box.

This anomaly corrected in versions 35.01 and 36.00.

This anomaly first identified in version 35.00.

AlarmSet attribute sometimes displays erroneous value (3109190)

The AlarmSet attribute sometimes displays an erroneous value. However, the display issue does not affect the logic execution.

This anomaly corrected in version 36.00.

This anomaly first identified in version 34.00.

Changing nested UDT to main UDT removes defined alarms from the nested UDT (2339160, 2339163, 2339161)

Changing a nested UDT structure of a tag removes alarms set for the other tags that contain a similar UDT structure.

This anomaly corrected in version 34.05, 35.05.

This anomaly first identified in version 31.00.

Dialogs undocked, split, or set to auto-hide provide unpredictable results for F4 key (2335181)

When dialogs in the Logix Designer application are undocked, split, or set to auto-hide, the F4 key produces unexpected results.

This anomaly first identified in version 31.00.

This anomaly corrected in version 36.00.

Structured text block comment can cause crash on upload (2209737)

When you create a comment inside #region and #endregion constructs in a Structured Text routine, the Logix Designer application sometimes crashes when you upload the project from a controller to a new project or into a current project.

This anomaly first identified in version 32.00.

This anomaly corrected in version 36.00.

Cfg_SPRampMaxDev range incorrect on PPID dialog box (2193171)

On the PPID instruction dialog box, the Cfg_SPRampMaxDev parameter allowed values that are outside the correct range.

This anomaly first identified in version 35.00.

This anomaly corrected in version 36.00.

Studio 5000 Logix Designer Ladder Diagram routines may stop execution after download (2047296)

Studio 5000 Logix Designer ladder diagram routines may stop execution after download to ControlLogix 5580, GuardLogix 5580, CompactLogix 5380, 5480 and Compact GuardLogix 5380 controllers. See Product Notice ID: PN1620 for the specific sequence of events to experience this anomaly.

This anomaly first identified in version 31.00.

This anomaly corrected in version 36.00.


  

Fatal Error 0x80042001 when creating an Add-On Defined output parameter in a routine (1731323)

Fatal error 0x80042001 could occur when creating a new control tag for an Add-On Instruction (AOI) and setting the control tag as an output program parameter.

This fatal error will occur when the tag is created directly from the instruction within the routine. 

This fatal error will not occur if the tag is created from the tag data tables.  

Reference technote BF29394 for additional information.

This anomaly first identified in version 31.00.

This anomaly corrected in version 36.00.

Failed to import file occurs during AOI import (2239485)

When an Add On Instruction (AOI) with the same name and one or more matching signature entries is imported with Overwrite option an error occurs. NOTE: The error occurs with signed and unsigned AOIs.

Error message in popup window:  Failed to import file ‘C:\….L5x.’ The import was canceled due to errors.  No changes were made to the project.  See Output Window Errors tab for details.

Error message in Output Window Errors tab:  Error:  Unable to import “AOI name here”, The Import was cancelled due to a name collision (Name=' ').

Workarounds:

Unsigned AOIs: clear the signature history on the AOI that already exists in the ACD file.

Signed AOIs: remove the signature from the AOI that already exists in the ACD file.

This anomaly first identified in version 32.00.

This anomaly corrected in version 36.00 and 36.01.

 

IO safety online module property functions may not work using USB path (2327701)

Using the USB path to perform online safety IO property functions may show a pop up dialog containing this text:

Path specified invalid or module not responding.

See Knowledgebase BF29682 for a workaround to this issue.

This anomaly corrected in version 36.00.

This anomaly first identified in version 35.00.

 

Fatal Error 0xe06d7363 Adding Devices to the I/O Configuration (2159635)

This anomaly affects European-based Windows Operating Systems.

An anomaly exists in Add-on Profiles that could cause a fatal error to occur when adding certain devices to the I/O configuration or when opening these device profiles in an existing project.

This anomaly was corrected in the Add-on profiles released with the Logix Designer application v36.00, v35.01, v34.03, v33.03.

This anomaly was first identified with the Add-on profiles that were released with the Logix Designer application v35.00, V34.02, and v33.02. For additional information, please reference ID: QA65946.

  

Incorrect help topic opens In Alarm and Alarm Definition properties dialog boxes (2372006, 2125791)

Selecting the Help button in the New Alarm dialog box incorrectly opens the New Alarm dialog box help topic instead of the correct Alarm Properties dialog box help topic.

Selecting the Help button in the New Alarm Definition dialog box incorrectly opens the New Alarm Definition dialog box help topic instead of the correct Alarm Properties dialog box help topic.

This anomaly first identified in version 33.02.

This anomaly corrected in version 36.00.

Known Anomalies in This Release

This release has the following known anomalies.

Safety IO modules incorrectly appear as selectable in standard controller projects in LogixDesigner version 36 (3679519, 3835539)
In Logix Designer version 36, Safety IO modules incorrectly appear as selectable in standard controller projects. This anomaly does not occur in version 37 or 38.
This anomaly first identified in version 36.00.
Partial AOI import sometimes fails to create Alarm (3115573, 2223611)

The Logix Designer application sometimes fails to create an alarm when you do a partial import for an Add-On Instruction (AOI) that contains the alarm. To work around this issue, export and then import the affected project.
This anomaly first identified in version 31.00.
Cannot update value for tag member in DT and LDT data types (2363908)

You can expand and display the bit members for tags using the DT and LDT data types, but you cannot change the values for the bit members. This is expected behavior.
This anomaly first identified in version 36.00.
Attempting to access a controller through a blocked path can freeze the interface (2362117)

When CIP Security is configured, you can access the controller only through the Ethernet port. When you attempt to access the controller through a path blocked by CIP security, the Logix Designer application appears to freeze.
To work around this issue, hover your cursor over the application icon in the taskbar and close the hidden dialog. This anomaly first identified in version 36.00.

Selecting Go to Cross Ref prompts Save All (3064189)

When you open a project in the Logix Designer application, select Go to Cross Reference for a tag, and then close the project, the Logix Designer application asks you to save changes even though the project has not changed.

There is no workaround for this issue.

This anomaly corrected in version 37.00.

This anomaly first identified in version 34.00.

Opening Extended Properties for new UDT can freeze Logix Designer (3121716)

The Logix Designer application sometimes locks up when you create a new data type and select graphic for one of the properties. To work around this issue, hover your cursor over the application icon in the taskbar and close the empty dialog.
This anomaly first identified in version 36.00.
Logix Designer version 36.00 installer fails to install AOP Core when GuardLink EIP Scanner AOP is already installed (3185534)
When a Guardlink EIP Scanner 432ES AOP version 1.00.34 is already installed on your Logix Designer workstation and you attempt to install version 36, installation errors occur and the installer fails to install AOP core files.
To work around this issue, uninstall the GuardLink EIP Scanner AOP from your Logix Designer application before installing version 36.00. For more information, see this Knowledgebase article.
This anomaly first identified in version 36.00. This anomaly corrected in version 38.00.

Partial AOI import sometimes fails to create Alarm (3115573, 2223611, 2223616)

The Logix Designer application sometimes fails to create an alarm when you do a partial import for an Add- On Instruction (AOI) that contains the alarm.
To work around the issue, export and then import the affected project. This anomaly corrected in version 33.04.

This anomaly first identified in version 33.00.

FactoryTalk Directory clients are losing communication with the FactoryTalk Directory Server (4180731)
  
To resolve this problem, do one of the following:
  1. Stop and disable the Rockwell Alarm History Archiver service, FTAEArchiver.exe.
  2. On March 1, re-enable the Rockwell Alarm History Archiver service, FTAEArchiver.exe.
This anomaly first identified in version 36.00.
Opening Extended Properties for new UDT can freeze Logix Designer (3121716)

The Logix Designer application sometimes locks up when you create a new data type and select graphic for one of the properties. To work around this issue, hover your cursor over the application icon in the taskbar and close the empty dialog.
This anomaly first identified in version 36.00.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Trends display steps instead of linear line (1093987)

Trends show steps instead of linear line while executing quantums larger than 10ms. Part of trends use physical time instead of virtual time. This anomaly first identified in version 33.00.
Unable to upload project from PLC (1489327)
The Logix Designer application stops performing with attempting to upload a project from the controller on a sequence diagram. For details about this issue, see Tech Note BF28540.
This anomaly first identified in version 34.00.

Can create safety I/O module successfully when Safety Modify Component set to deny (1787414)

You can successfully create an Add-On Profile based safety I/O module without errors when FactoryTalk Security user privileges's Safety Modify Component is set to Deny.

This anomaly first identified in version 35.00.

Can create a 5015-AENFTXT under the 1756-EN2TSC I/O configuration (1882887)
When creating a module under 1756-EN2TSC, 5015-AENFTXT is listed in available modules and can be created successfully. 5015-AENFTXT should only appear under adapters that support concurrent connections, such as 1756-EN4TR major revision 4. Communication between 1756-EN2TSC and 5015-AENFTXT is not supported and will not function.
First reported in version 35.00 and AOP version 28.04.

Direct Add-on-Profile-to-Device Communication Could Result in Time Out Errors or Communication Routing to the Wrong Device (1927272)

Direct Add-on-Profile-to-device communication could result in time out errors or routing the communication to the wrong device in circumstances where all of the following conditions are met:

This applies to configuration data that goes through unconnected communication to the target I/O device (for instance, uploading/downloading device parameters).

This does not apply to I/O data.

This does not apply to commands from the controller (for instance, inhibiting/uninhibiting a device).

Please see technote BF28941 for additional details.

This anomaly first identified in version 20.00.

Removed KNOptimassMfc400 profile (2106380)

The KN profile no longer has a license in the Logix Designer application.

This anomaly first identified in version 32.02.

Some Catalog numbers not displaying correctly in Module Discovery (2001084)

After creating a new L85E v35 project with a 5032 I/O-Link bridge device connected to the Ethernet bus and enabling at least one channel for the I/O-Link, connect Siemens-K20-4DI IO-Link device with the 5032 I/O-Link bridge module, and download the project. Launching Module Discovery from the I/O-Link bus shows some Catalog numbers do not display correctly.

This anomaly first identified in version 35.00.

I/O-Link Module Discovery displays 17.00 (100,1.1001) (1848106)

When creating an L85E project and adding a 5032-Master, after configuring some channels to I/O-Link and downloading the project, launch Module Discovery from the I/O-Link bus. The Revision column shows 17.000 for the I/O-Link devices instead of the expected 1.1 or 1.0.

This anomaly first identified in version 35.00.

L5K file with I/O Device cannot be imported (2047005)

When creating an L85E project using a 5032 master profile on the Ethernet bus and adding the I/O-Link device 42AF-R1MAB1-xx[209] with default setting on the I/O-Link bus, the error Unexpected end of file encountered occurs and the import is not successful.

This anomaly first identified in version 35.00.

Mismatching display resolution and scaling may result in overlapping SFC elements (2122642)

Editing a Sequential Function Chart (SFC)) using a display with a given resolution (for example, 1920 x 1200) and Windows scale setting (for example, 100%), closing the ACD, and then opening the same ACD in another resolution (for example, 3840 x 2160) and Windows scale setting (for example, 150%) may result in overlapping SFC elements.

Studio 5000 Logix Designer Ladder Diagram routines may stop execution after download (2047296)

Studio 5000 Logix Designer ladder diagram routines may stop execution after download to ControlLogix 5580, GuardLogix 5580, CompactLogix 5380, 5480 and Compact GuardLogix 5380 controllers. See Product Notice ID: PN1620 for the specific sequence of events to experience this anomaly.

This anomaly first identified in version 31.00.

Upload failure (1024944)

When attempting to upload a project, the Logix Designer application generates these errors and the upload fails:

Failed to upload project. Reverting to the last saved copy of [location and file name]

To work around this issue, remove long names from the project.

This anomaly first identified in version 32.00.

Tag based alarm does not create on import (1093641)

If Logix based alarms are not verified or created when importing a User-defined Data Type (UDT) that references them, users will experience a controller major non-recoverable fault (MNRF) after download.

This anomaly first identified in version 33.00.

The Logix Designer stops responding when copying motion axes (1170662)

When copying and pasting motion axes between motion groups, the Logix Designer stops responding.

This anomaly first identified in version 32.00.

Public parameter imports as a local tag (910972, Lgx00231568, Lgx00231638, Lgx00231000)

When importing and exporting programs or routines with Public program parameters between projects, the program or routine causes the parameter to appear undefined.

This anomaly first identified in version 32.02.
Tag Browser may disappear when the Watch view is in Auto Hide mode (Lgx00216392)

The Tag Browser may disappear behind the Watch view preventing the user from selecting a tag. This can happen when the Watch view is in Auto Hide mode, the user opens the Tag Browser from the Watch view, and the Tag Browser appears outside the Watch view.

This anomaly first identified in version 32.00.

Use one of these steps to work around the issue:

Size the Watch view so the Tag Browser fits inside the Watch view.

Hyperlinks in Vendor Sample Projects.pdf file may not work (Lgx00215047)

Some browsers (particularly the Microsoft Edge browser) may not launch the hyperlinks in the Sample Projects.pdf file when the hyperlinks are configured to open PDF files.   

This anomaly first identified in version 32.00

To work around this issue, open the PDF file with Adobe Acrobat Reader:

Logix Designer application runs out of memory with Accelerate 3D Graphics selected in VMware (Lgx00216060)

The Accelerate 3D Graphics setting in VMware sometimes causes the Logix Designer application to run out of memory.

This anomaly first identified in version 32.00.

Use one of these steps to work around this issue:

Selecting all consumed tags causes the Logix Designer application to freeze (Lgx00217420, Lgx00217421, Lgx00217422, Lgx00217118)

In the Tag Editor with Show: Consumed tags displayed, selecting all the consumed tags can cause the Logic Designer application to freeze.

This anomaly first identified in version 32.00.

Multiple routines left open for over two days while online with the controller can cause the Logix Designer application to crash (Lgx00217902, Lgx00217946)

Leaving multiple routines open for over two days while online with the controller can cause the Logix Designer application to crash.

This anomaly first identified in version 32.00.

Subroutine called by locked routine through JSR instruction might not show energized power rail (Lgx00218331)

When a locked routine uses a JSR instruction to call a subroutine, Logix Designer sometimes fails to display the power rails in the subroutine as energized. The problem is limited to the incorrect display; the execution flow in the controller is still correct.

This anomaly first identified in version 32.00.

Labels are cut off and dislocated in BOOTP-DHCP Server applications (Lgx00152848)

When the font size in Windows 7 is set to 125%, the labels in the Network Settings and DHCP properties of BOOTP-DHCP Server application are cut off, making them unreadable. They are also dislocated, where they do not match with the proper input fields.

This anomaly first identified in version 23.00.

In 5094-IF8IH Modules, fault input does not indicate a fault on some channels (1313229)
In 5094-IF8IH Modules, during network cable breaks or MP power loss, a fault input does not indicate a fault on some channels. This anomaly first identified in version 34.00.
Input controller tag value after cable break varies (1494865, 1494862, 1494859)
The input controller tag values after a cable break varies based on the channel value at the last inhibition and uninhibition action. This anomaly first identified in version 33.00.

Error in the content of Studio 5000 Logix Designer application generated reports (1421415)

"ACD filename - Label does not exist" appears at the top of the page instead of "ACD filename - Controller Organizer Listing" when using the Generate Report menu option. 

This anomaly first identified in version 33.00.

Fatal error when converting a project to a newer major revision (1476922)]]]
A fatal error sometimes occurs when converting a project to a newer major revision where issues exist in the ChangeLog.
To work around this issue, export from the older project to a .L5K or .L5X file and import the project to a newer major revision to avoid the fatal error.
This anomaly first identified in version 16.00.

Editing Operand Description sometimes results in unexpected display behavior (1354684)

When the same tag description exists on many branches that span an area that extends beyond what is visible on a display and the tag description is edited, the content on the display sometimes jumps upon acceptance of the tag description edit. 

Using the left or right arrow keys causes the screen to focus on the tag description that was just edited.

The anomaly does not occur when the tag description is edited for the rung where the contacts are unique because the tag description only exists in one location.

This anomaly first identified in version 20.00.

Storing Firmware Supervisor files from PowerFlex 755T causes the <ST5LD>  application to stop responding (1518416)

Attempting to store Firmware Supervision files for PowerFlex 755T devices causes the <ST5LD> application to stop responding. The application must be closed using Task Manager.

This anomaly was first identified in version 33.00.

Error when attempting to run a trend (1435208)
The Logix Designer application is unable to run a trend in v29 or earlier after switching communication software from RSLinx Classic to FactoryTalk Linx in another instance of the Logix Designer application v31 and later on the same workstation.
Once a trend is run in the Logix Designer application v31 and later, using FactoryTalk Linx as the communication software, you will receive this error message if you then attempt to run a trend in the Logix Designer application v29 or earlier on the same workstation:
Error: <trend name> - : Can’t open the specified RSLinx driver. For more information, refer to the technical note BF23206.
This anomaly first identified in version 20.00.
This anomaly resolved in version 38.00.
Removed KNOptimassMfc400 Add-on profile (2106380)

The KNOptimassMfc400 device Add-on profile is no longer included with the Logix Designer application. This anomaly first identified in version 32.02.

Using specific set of characters in structured text outlining comment, will cause an upload failure into a blank project ACD file (2207451)

Using the ** set of characters with a single-line comment (//) (that is, //**) in a structured text outlining comment (#region\#endregion) causes an upload error into a blank ACD file. The ** characters are used for multi-line comments and using the ** characters with a single-line comment causes this anomaly to occur. 

To work around this issue, put double quotes around the ** characters, such as “**”.

This anomaly first identified in version 31.00.

 

Fatal Error 0xc0000005 on Import from L5X (3161896)

If an application was generated in an XML editor and a move instruction (MOV/MOVE) was created with an empty/missing operand, a Fatal Error occurs on import of the L5X file.

Example of text that would cause the Fatal Error on import:

Example of text that would not cause the Fatal Error on import:

NOTE: The fatal error does not occur when importing L5X created with Logix Designer because the software inserts a “?” in place of the missing operand.

This anomaly corrected in version 37.00.

This anomaly first identified in version 34.00.

Fatal Error 0xe0434352 when creating, opening, or interacting with a module’s properties after installing a later version of the Studio 5000 Logix Designer application or after installing a new Add-on Profile (3219935)

Fatal Error 0xe0434352 occurs on creating, opening, or viewing of profiles updated with a web-based interface, including 1756 Ethernet modules, 5069 Ethernet Adapters, 5094 Ethernet adapters, 1734 Ethernet Adapters, and 1756 I/O.

This fatal error could occur after an installation of the Studio 5000 Logix Designer application or a stand-alone Add-On Profile (AOP), which causes an upgrade to all module profiles.

The fix for this anomaly is available in the Add-on Profiles update for the 1756 Analog Modules, v40.14.70. The Add-on Profiles can be downloaded from the Product Compatibility and Download Center. For more information on this anomaly and the solution, please see technote ID BF30201. 

This anomaly first identified in v20.05.

Public parameter imports as a local tag (910972, Lgx00231568, Lgx00231638, Lgx00231000)
When importing and exporting programs or routines with Public program parameters between projects, the program or routine causes the parameter to appear undefined.
This anomaly first identified in version 32.02.

Functional Changes

This release has the following functional changes from the previous release.

Functional changes for Logix Designer v36.00

Logix Designer version 36.00 has these changes in functionality since the last release.

No write access to Alarm status flag bits

The Logix Designer application no longer allows programmatic write access to Alarm status flag bits.

Maximum days value for TIME and LTIME data types

The maximum days value that you can enter for the TIME and LTIME data types is 106750d.

Tools menu option change

The EDS Hardware Installation Tool option accessed from the Tools menu is now the Device Description Registration Tool option. Use the Device Description Registration Tool option to export and import EDS files, IO-Link IODD files, and HART DD files between workstations.

EDS AOP uses data types defined in EDS AOP file without conversion

EDS AOP will now take advantage of the additional datatype support in Logix Designer. Adding a device using an EDS AOP now uses the data types as defined in the EDS AOP file without conversion. This is a workstation install that updates versions 34 and later for ControlLogix 5580, 5480, and 5380 projects.

Updated mnemonics are automatically changed during project import and conversion

In this version of the Logix Designer application, the mnemonics for these instructions have been updated to align with IEC 61131-3 and PLCopen standards. Mnemonics for specific instructions are automatically updated on import and project conversion. The updated mnemonics are:

Instruction
Mnemonic in versions v35 and earlier
Mnemonic in versions v36 and later
Arc Cosine
ACS
ACOS
Arc Sine
ASN
ASIN
Arc Tangent
ATN
ATAN
Convert to BCD
TOD
TO_BCD
Convert to Integer
FRD
BCD_TO
Equal To
EQU
EQ
Greater Than
GRT
GT
Greater Than or Equal To
GEQ
GE
Less Than or Equal To
LEQ
LE
Less Than
LES
LT
Limit
LIM
LIMIT
Move
MOV
MOVE
Not Equal To
NEQ
NE
Square Root
SQR
SQRT
Truncate
TRN
TRUNC
X to the Power of Y
XPY
EXPT

Import/Export

The Import/Export version number for this version of Logix Designer application is 2.27. The table lists the Import/Export versions for previous releases.

Release Version
Import/Export Version
36.xx
2.27
35.xx
2.26
34.xx
2.25
33.xx
2.24
32.xx
2.23
31.xx
2.22
30.xx
2.21
29.xx
2.20
28.xx
2.19
27.xx
2.18
26.xx
2.17
24.xx
2.15
23.xx
2.14
21.xx
2.12
20.xx
2.11
19.xx
2.10
18.xx
2.09
17.xx
2.08
16.xx
2.07
15.xx
2.06
14.xx
2.05
13.xx
2.04
12.xx
2.03
11.xx
2.02
10.xx
2.01
9.00
2.00
5.02
1.02
2.xx, 6.xx, 7.xx, 8.xx
1.01
1.21, 1.23
1.00
1.10, 1.11
0.04


  

Application Notes

This release has the following application notes.

The Module Info tab within Module Properties will not return module information when utilizing FactoryTalk Linx

Viewing the Module Info tab of any device in the I/O configuration results in the following error:

Internal direct communications error. Call Technical Support.

This error will occur even when the module is connected and successfully communicating with the controller. The error will only occur when utilizing FactoryTalk Linx as the communication software package for Logix Designer.

This is not an anomaly in Logix Designer.

This anomaly in FactoryTalk Linx was addressed in a Patch Update for FactoryTalk Linx. See technote BF28781 for additional details.

Application notes for Logix Designer v36.00

Logix Designer SDK Installation Error when Installing Studio 5000 Logix Designer PRO Edition

The following installation error could occur when installing Logix Designer SDK on an Operating System with language settings set to any language other than English.

An error occurred while applying security settings. Users is not a valid user or group. This could be a problem with the package, or a problem connecting to a domain controller on the network. Check your network connection and select Retry or Cancel to end the install.

To work around the error:

  1. In Windows Start, search for and open the Computer Management app.
  1. Select Local Users and Groups > Groups.
  2. Add a local Windows group and name the group Users.
  3. Add the logged in user to that Windows group.
  4. Reboot your computer and reattempt the install.

Logix Designer SDK v1.00 is included in the Studio 5000 Logix Designer Professional Edition installer for v35.00. This is not a Studio 5000 Logix Designer anomaly. But you can experience this issue when installing Studio 5000 Logix Designer and selecting the option to install the Logix Designer SDK.

CIS Benchmarks test results

Studio 5000 Logix Designer v35.00 has been tested on CIS Microsoft Windows 10 Enterprise (Release 21H2) Benchmark v1.12.0 (L1).

Exceptions settings for Studio 5000 Logix Designer v35.00 are listed.

Reference: Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks)

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Rung comments lost when going online with a controller

When going online with the controller with the Download Project Documentation and Extended Properties option cleared, online edits did not save after making online edits to Ladder Logic routines, saving and copying the project, going offline, and then going online with the copied project. (Lgx00230263, Lgx00230366, Lgx00230369, Product Safety Advisory 2017-10-002)

Motion Import Tool version 3.0 required for importing CMF

You must upgrade to version 3.0 of the Motion Import Tool to import a Custom Motor File (CMF). Version 3.0 is required so that CMF/Motor Data can be imported into the MotionDB in the new admin location.

Security requirements

To help meet secure system design requirements, review these publications:

To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products (publication SECURE-AT001).

Supported Logix controllers

While the programming software continues to extend its functionality with each new release, the physical controllers that it supports will vary. New controllers are added, and in some cases, support for existing controllers may be removed. While a specific controller may not be supported by the current release, the side-by-side installation of multiple versions of the software will, in most cases, provide a means to support the older hardware. If migrating from one controller to another, a project created for one controller can be easily converted to another controller using the Controller Properties configuration dialog box within the software.

If opening a project that is configured for a controller that is no longer supported and the older version of software is not installed, the software will provide an appropriate warning and will automatically provide the option to convert the project to one of the controllers supported by the release.

The table provides a breakdown of the various Logix 5000 controllers and the initial or minimum version of Logix Designer application that is required to support the controller.

 Controller Catalog Number
Minimum Major Software Version
ControlLogix 1756-L71 Series B
20.00
ControlLogix 1756-L71S Series B
20.01
ControlLogix 1756-L72 Series A
19.00
ControlLogix 1756-L72 Series B
20.00
GuardLogix 1756-L72S Series B
20.00
ControlLogix 1756-L73 Series A
18.00
ControlLogix 1756-L73 Series B
20.00
ControlLogix 1756-L73XT Series B
20.00
GuardLogix 1756-L73S Series B
20.00
GuardLogix 1756-L73SXT Series B
20.00
GuardLogix 1756-L81ES Series A
31.00
GuardLogix 1756-L82ES Series A
31.00
GuardLogix 1756-L83ES Series A
31.00
GuardLogix 1756-L84ES Series A
31.00
GuardLogix 1756-L85ES Series A
31.00
GuardLogix 1756-L8SP Series A
31.00
ControlLogix 1756-L74 Series A
19.00
ControlLogix 1756-L74 Series B
20.00
ControlLogix 1756-L75 Series A
18.00
ControlLogix 1756-L75 Series B
20.00
ControlLogix 1756-L81E Series B
29.00
ControlLogix 1756-L81E-NSE
33.00
ControlLogix 1756-L81EP
33.00
ControlLogix 1756-L82E Series B
29.00
ControlLogix 1756-L82E-NSE
33.00
ControlLogix 1756-L83E Series B
28.00
ControlLogix 1756-L83E-NSE
33.00
ControlLogix 1756-L83EP
33.00
ControlLogix 1756-L84E Series B
29.00
ControlLogix 1756-L84E-NSE
33.00
ControlLogix 1756-L85E Series B
28.00
ControlLogix 1756-L85E-NSE
33.00
ControlLogix 1756-L85EP
33.00
CompactLogix 1769-L16ER-BB1B Series A
20.00
CompactLogix 1769-L16ER-BB1B Series B
20.00
CompactLogix 1769-L18ER-BB1B Series A
20.00
CompactLogix 1769-L18ER-BB1B Series B
20.00
CompactLogix 1769-L18ERM-BB1B Series A
20.00
CompactLogix 1769-L18ERM-BB1B Series B
20.00
CompactLogix 1769-L19ER-BB1B
28.00
CompactLogix 1769-L24ER-QB1B
20.00
CompactLogix 1769-L24ER-QBFC1B
20.00
CompactLogix 1769-L27ERM-QBFC1B
20.00
CompactLogix 1769-L30ER
20.00
CompactLogix 1769-L30ER-NSE
20.00
CompactLogix 1769-L30ERM
20.00
CompactLogix 1769-L33ER
20.00
CompactLogix 1769-L33ERM
20.00
CompactLogix 1769-L37ERM
31.00
CompactLogix 1769-L38ERM
31.00
CompactLogix GuardLogix 1769-L30ERMS
28.00
CompactLogix GuardLogix 1769-L33ERMS
28.00
CompactLogix GuardLogix 1769-L36ERMS
28.00
CompactLogix GuardLogix 1769-L37ERMS
31.00
CompactLogix GuardLogix 1769-L37ERMOS
30.00
CompactLogix GuardLogix 1769-L38ERMS
31.00
CompactLogix 1769-L36ERM
20.00
CompactLogix 1769-L37ERMO
30.00
CompactLogix 5069-L306ER
29.00
CompactLogix 5069-L306ERM
29.00
CompactLogix 5069-L306ERMS3
32.00
CompactLogix 5069-L310ER
29.00
CompactLogix 5069-L310ERM
29.00
CompactLogix 5069-L310ERM-NSE
29.00
CompactLogix 5069-L310ERMS3
32.00
CompactLogix 5069-L3100ERM
30.00
CompactLogix 5069-L3100ERMS3
32.00
CompactLogix 5069-L320ER
28.00
CompactLogix 5069-L320ERMS3
29.00
CompactLogix 5069-L320ERM
32.00
CompactLogix 5069-L320ERP
33.00
CompactLogix 5069-L330ER
29.00
CompactLogix 5069-L330ERM
29.00
CompactLogix 5069-L330ERMS3
32.00
CompactLogix 5069-L340ER
29.00
CompactLogix 5069-L340ERM
28.00
CompactLogix 5069-L340ERMS3
32.00
CompactLogix 5069-L340ERP
33.00
CompactLogix 5069-L350ERM
30.00
CompactLogix 5069-L350ERMS3
32.00
CompactLogix 5069-L360ERMS3
32.00
CompactLogix 5069-L380ERM
30.00
CompactLogix 5069-L4100ERMW
32.00
CompactLogix 5069-L4200ERMW
32.00
CompactLogix 5069-L430ERMW
32.00
CompactLogix 5069-L450ERMW
32.00
CompactLogix 5069-L46ERMW
30.00
Compact GuardLogix 5069-L306ERMS2
31.00
Compact GuardLogix 5069-L306ERMS3
32.00
Compact GuardLogix 5069-L310ERMS2
31.00
Compact GuardLogix 5069-L320ERMS2
31.00
Compact GuardLogix 5069-L330ERMS2
31.00
Compact GuardLogix 5069-L340ERMS2
31.00
Compact GuardLogix 5069-L350ERMS2
31.00
Compact GuardLogix 5069-L380ERMS2
31.00
Compact GuardLogix 5069-L3100ERMS2
31.00
Compact GuardLogix 5069-L306ERS2
31.00
Compact GuardLogix 5069-L310ERS2
31.00
Compact GuardLogix 5069-L320ERS2
31.00
Compact GuardLogix 5069-L330ERS2
31.00
Compact GuardLogix 5069-L340ERS2
31.00
Compact GuardLogix 5069-L350ERS2
31.00
Compact GuardLogix 5069-L380ERS2
31.00
Compact GuardLogix 5069-L3100ERS2
31.00

Launching with Ctrl + Shift does not reset Controller Organizer

One method to restore or reset Workstation Options is to hold Ctrl + Shift, launch the Logix Designer application, and continue to hold Ctrl + Shift until the application is fully launched.

However, when this restore method is used and the Windows User Account Control (UAC) setting is set at a level higher than Never notify, a UAC dialog box sometimes appears containing the following message:

Do you want to allow this app to make changes to your device?

Clicking Yes on the dialog box while continuing to hold Ctrl + Shift, the Workstation Options are not reset.

To reset Workstation Options, use one of these workarounds:

FactoryTalk Linx compatibility

Some device properties, online functions, communication drivers, and FactoryTalk Security authentication with Studio 5000 Logix Designer are not supported with FactoryTalk Linx. Use the following table as a guide for the recommended communication software to use with select modules.

Product
Communication software
ArmorStart Ethernet (28xe)
RSLinx Classic
ArmorStart LT (29xe)
RSLinx Classic
Drives Profiles
  • PowerFlex Drives
  • 1305
  • 1336
  • FactoryTalk Linx
  • RSLinx Classic
  • RSLinx Classic
GuardMaster and GuardLink (440C-CR30-22BBB)
  • RSLinx Classic (v3.0100 and earlier)
  • FactoryTalk Linx (v3.02.00 and later)
HIPROM
  • 1788-EN2PAR
  • 1788-CN2PAR
  • 1788-EN2FFR
  • 1788-CN2FFR
  • RSLinx Classic
  • RSLinx Classic
  • RSLinx Classic
  • RSLinx Classic
IO-Link Block (1732E-8IOLM12R IO Link)
FactoryTalk Linx
IO-Link Point (1734-4IOL)
FactoryTalk Linx
Default font type and size for Structured Text Editor

Starting with version 31.00 of Logix Designer application, the default font type size for the Structured Text Editor changed from Courier New size 8 to Consolas size 10. Since the Sequential Function Chart (SFC) Action uses structured text to execute assignments and instructions, this change makes the SFC Action larger causing the overlap of the SFC elements in projects converted from version 30.00 and earlier to version 31.00 and later. 

To get the same SFC layout as in v30.00 and earlier:

  1. Select Tools > Options.
  1. In the Workstation Option, select Structured Text Editor > Font/Color.
  2. In Font, choose Courier New.
  3. In Size, choose 8. 
Converting a project with Function Block Diagram text boxes from version 11 of the RSLogix 5000 software to version 21.00 and later

To convert a project with a Function Block Diagram routine with text boxes from version 11 of RSLogix 5000 software to version 21.00 and later, use one of these steps:

Resize multiple large SFC routines using Fit to Width command

The Logix Designer application may exceed memory when multiple large Sequential Function Chart (SFC) routines are opened and resized to fit the full window using the View>Zoom>Fit to Window command. To work around this issue, use the View>Zoom>Fit to Width command to set the zoom of the selected routines so that the entire width of the routine fits within the routine windows. 

Trend server sometimes fails for multiple versions of the Logix Designer application

When versions 30.00 and 31.00 of the Logix Designer application are both installed on the same computer, and trending has never been run in the version 31.00 Logix Designer application, trending fails to run in the version 30.00 Logix Designer application. RSLinx Classic is the default communication software for Trend Server, which causes this behavior. After switching between FactoryTalk Linx and RSLinx Classic, the trend will not work for version 30.00. (Lgx00203589)

Add-On Instruction module references

Starting with version 24.00 of the Logix Designer application, modules can be accessed via module references. Because of this, program-scoped tags with the same names as modules ignore those modules in terms of logic references. For version 24.00 and later, when attempting to access modules via module reference from within the Logix Designer application, a warning message opens. If converting from a version earlier than version 24.00, the application returns a verification error.

Uninstalling the CodeMeter® kit causes Logix Designer uninstall to fail

If uninstalling the CodeMeter kit, which is installed with the FactoryTalk® Activation Manager, the Logix Designer application fails to uninstall. To restore the CodeMeter kit, uninstall the FactoryTalk Activation Manager and then reinstall it.

SequenceManager not available on Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers

The SequenceManager feature is not available for Compact GuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers in this release of the Logix Designer application.

However, SequenceManager is available on these Process controllers:

Non-alphanumeric characters in a STRING need an escape carriage

When editing existing standard STRINGs or entering a new STRING, if there is a non-alphanumeric character in the STRING, such as a space, period or apostrophe, add an escape carriage.

Microsoft® .NET Framework 4.6 may cause failure in earlier versions of the Logix Designer application

For installations of version 32.00 of Logix Designer, Microsoft .NET Framework 4.6 is installed automatically. However, .NET Framework 4.6 can cause these issues:

Follow one of these steps to work around the issue:
Signatures break for Add-On Instructions from earlier releases

When using version 29.00 or later to open a project from a release earlier than version 29.00, the signature breaks for any Add-On Instruction included in the project. In the same way, when importing an Add-On Instruction from a project created in a release earlier than version 29.00, the signature breaks for that Add-On Instruction. Un-seal and then re-seal each Add-On Instruction to get a new signature.

Kinetix® Encoder Emulator RPI must match the Motion Task update rate

The Requested Packet Interval (RPI) setting for the Kinetix Encoder Emulator must match the Motion Group Base Update period. If the RPI setting and the Motion Group Base Update period do not match, output can fail from the Encoder Emulator.

Drive safety instructions Boolean members

Some Boolean members of the AxisSafetyFaults attribute were renamed and some were added to support the drive safety instructions. If a member of the AxisSafetyFaults is used in logic, the logic will not compile until the old axis Boolean attribute is replaced with the new name.

Versions 18.00 and later require updates to Custom Motion Database

When using a Custom RSLogix 5000 Motion Database in RSLogix 5000 software versions 12.00 through 17.00, update the motion database to work with versions 18.00 or later. The table lists the motion database revisions that are used with these application versions.

 

Version of Application
Motion Database Revision
36.00
14.50.00 [ Motion.mdb format ]
35.01
14.50.00 [ Motion.mdb format ]
35.00
14.43.00 [ Motion.mdb format ]
34.02 / 34.03
14.45.00 [ Motion.mdb format ]
34.00 / 34.01
14.39.00 [ Motion.mdb format ]
33.02 / 33.03 / 33.04
14.50.00 [ Motion.mdb format ]
33.01
14.31.00 [ Motion.mdb format ]
33.00 / 33.00.02
14.24.00 [ Motion.mdb format ]
32.00 / 32.01 / 32.02 / 32.03 / 32.04
13.04.00 [ Motion.mdb format ]
31.00/ 31.02
12.02.00 [ Motion.mdb format ]
30.00
11.06.00 [ Motion.mdb format ]
29.00
11.05.00 [ Motion.mdb format ]
28.00
10.05.00 [ Motion.mdb format ]
27.00
10.03.00 [ Motion.mdb format ]
26.01
10.03.00 [ Motion.mdb format ]
24.00
9.24.00 [ Motion.mdb format ]
23.00
9.22.00 [ Motion.mdb format ]
21.03
9.15.00 [ Motion.mdb format ]
21.00
9.08.00 [ Motion.mdb format ]
20.01
8.12.00 [ Motion.mdb format ]
20.00
8.09.00 [ Motion.mdb format ]
19.01 / 19.00
7.05.00 [ Motion.mdb format ]
18.02 / 18.01 / 18.00
6.09.00 [ Motion.mdb format ]
17.01/ 17.00
5.03.00 [ *Motion.md format ]
16.04 / 16.03 / 16.00
4.02.00 [ *Motion.md format ]
15.03 / 15.02/ 15.01 / 15.00
3.24.00 [ *Motion.md format ]
14.01 / 14.00
3.12.00 [ *Motion.md format ]
13.04 / 13.03/ 13.02 / 13.01 / 13.00
3.12.00 [ *Motion.md format ]
12.06 / 12.05 / 12.04 / 12.03 / 12.02 / 12.01 / 12.00
3.03.00 [ *Motion.md format ]

* Before a Custom Motor can be used in version 18.00 or later, any Custom Motor currently in a motion database file at revision 5.00 or earlier (Motion.db format) must be converted to the newer Motion.mdb format.

To initiate the process of getting the database updated, please email the request to raeptechsupport@ra.rockwell.com. Please include any prior tech support case number if the current database includes non-Rockwell motors.

Locked routines from earlier releases must be unlocked and re-locked before download

When using version 32.00 to open a project from a release earlier than version 32.00, any routines that are locked in the project will not download to a controller. Before downloading the project, open the project in version 32.00, unlock the routines, and then re-lock them. Download the project with the re-locked routines to the controller.

MSXML 4.0

This version of Studio 5000 Logix Designer application does not install or use MSXML 4.0. MSXML 4.0 has security risks associated with it and is no longer supported by Microsoft. For more information about MSXML and its availability, see the MSXML Roadmap. When installing products or components made by other vendors that use MSXML 4.0, contact the vendor for questions about the security risk associated with MSXML 4.0.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation command-line parameters

Use command Setup.exe /? to display the usage options for installation parameters. Command-line parameters are case-insensitive. If a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Examples

These examples show how to use the installation commands.

Setup.exe /Q /IAcceptAllLicenseTerms
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /InstallDrive=D:
Error codes

This table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A reboot is required to continue the installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_REBOOT_PENDING
3012
A restart is pending and is required before the installation can continue.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.


Delay when opening a 1756-EN4TR Add-on Profile when configured as adapter pair

The 1756-EN4TR Add-on Profile takes 10-15 seconds to fully load content while online with a controller if all of the following conditions are true.

 
 1

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.