This release has the following requirements.
This release includes the following system features.
This release corrects the following anomalies.
This release has the following known anomalies.
These anomalies are from previous releases but are still known in this release.
Invalid IP address blocks ability to change properties, turn controller off, or modify SD Card (1894909)
When you create an emulated controller using an ACD file or by restoring or importing a snapshot, and the IP address for the emulated controller is not valid, you cannot apply changes to some controller properties, and you cannot turn the controller off or modify the SD Card. The symptom of this anomaly is that, after you change a controller property on the controller with an invalid IP Address, the Apply button is disabled.
This error appears when you attempt to turn the controller off, attach or detach the SD card from the controller property screen, or toggle the controller on or off from the device status panel:
Modify controller failed. An error occurred when communicating with the FactoryTalk Logix Echo service. If this error occurs often, contact Rockwell Automation technical support.
However, there is no error to indicate that the IP address is not valid.
To work around this issue, enter a valid IP address for the emulated controller.
This anomaly first identified in FactoryTalk Logix Echo v1.00.
Emulated controllers sometimes shut down when program contains a motion axis (1833982)
When the program for an emulated controller contains a motion axis, the emulated controller might shut down suddenly during startup.
To work around this issue, try starting the emulated controller again.
This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.
IP address and network mask are not restored from the SD card (1708087)
When you save an emulated controller configuration to the emulated controller SD card, change the IP address and network mask, and then restore the configuration from the SD card, the IP address and network mask are not restored to the original configuration.
To work around this issue, use a snapshot to restore a configuration.
This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.
Controllers stop responding during snapshot creation (1767371)
One or more controllers might stop responding during Snapshot creation. The message Controller is not responding appears on the Device Status panel in the Dashboard for those controllers.
To work around this issue, turn the controller off and then on again, re-download the project, and attempt snapshot creation again.
This issue first identified in FactoryTalk Logix Echo version 2.01.
Delayed changes fault sometimes occurs for produced and consumed tags (1076648, 1172801)
When the Requested Packet Interval (RPI) is set to 200 ms or less for produced and consumed tags, a fault sometimes occurs that indicates a data change delay.
There is no workaround for this issue.
This anomaly first identified in the FactoryTalk Logix Echo application, version 1.00.00.
Trends display steps instead of a linear line (1093987)
Trends show steps instead of linear line while executing quantums larger than 10ms. Furthermore, some trends use physical time instead of virtual time.
This anomaly first identified in the FactoryTalk Logix Echo application, version 1.00.00.
This release has the following functional changes from the previous release.
This release has the following application notes.
Tip: If you do not have RemoteSigned permission in PowerShell, enter this PowerShell command:
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software
installation using an IT tool or script, and don’t expect any error or
restart messages. When using this parameter, check the error codes,
and respond as needed. For example, if the installation returns error
code
1641, then the IT tool or script should restart the computer and relaunch
the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows
progress through the UI, it does not accept any input but still shows error
or restart messages.
When using this parameter, the installation will stop and display a prompt
if there are error or restart messages. For example, if an immediate
restart is required to complete the install, a restart message will be
displayed to confirm the restart. Installation resumes automatically from
the point of interruption after restart.
This parameter is required if /Q is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete.
Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q)
will return either error code 1641 or 3010 if a restart is required, and
unattended install (/QS) will result in a
confirmation prompt that must be agreed to before the installation is
completed.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback="value"
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/SetupLanguage="value"
|
Specifies which language is displayed during
install process. The value must be the one of
these:
|
|
|
This parameter is optional. If this parameter is not used, the default
language is the current user or operating system user interface
language.
|
|
/Product="value"
|
Specifies which sub-products will be installed.
Only required if sub-products are included with the install package.
If the software does not include sub-products this parameter is not
available.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a
warning occurs.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used
to activate the software during installation.
This parameter is optional. If it is not specified the software must be
activated manually after installation if activation is required.
Some software does not require activation. If activation is not required
this parameter is not
available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be
activated manually after installation if activation is required.
Some software does not require activation. If activation is not required
this parameter is not
available.
|
|
/Version="value"
|
Specifies the version of the software to activate which corresponds to the
product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer uses the most
recent product version available.
Some software does not require activation. If activation is not required
this parameter is not
available.
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was cancelled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is
corrupt. Contact
your support personnel.
|
|
ERROR_REBOOT_CONTINUE
|
1641
|
A restart is required to continue to installation.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation.
After restart
the product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
A restart is pending and is required before the
installation can
continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the
products are
already installed.
|