Release Notes

Studio 5000 Logix Emulate software works with the Rockwell Automation Logix platforms: ControlLogix® etc.
Version 36.00.00 (released 11/2023)

Catalog Number Studio 5000 Logix Emulate 

These release notes describe version information for Studio 5000 Logix Emulate, version 36.00.00 (released 11/2023).

Requirements

This release has the following requirements.

 
System requirements for Studio 5000 Logix Emulate Release Notes version 36.00

For optimal performance of the Studio 5000 Logix Emulate application, your personal computer should meet or exceed the following hardware and software requirements. Studio 5000 Logix Emulate can be installed on a personal computer that meets the operating system minimum requirements.

Hardware Requirements
Software Requirements
graphic
Note: This release is not intended to run on a 32-bit operating system. All operating systems listed are the 64-bit variant.
IMPORTANT
Keep these operating system considerations in mind:
  • Universal C Runtime (CRT) is a Windows operating system component that enables core functionality on the Windows operating system. It was introduced in Windows 10 and distributed to most computers running earlier supported operating systems. This component is present on computers that have been kept up to date.
When installing the Logix Designer application on computers that have not been updated, a prompt displays to install Universal C Runtime or to update the computer to at least the Microsoft April 2014 update roll-up.
  • While the Windows 8.1 and later operating systems run on many touch-enabled devices, various features of the Logix Designer application may not be touch-enabled. Most functions are expected to work with touch, but the software has only been tested with a keyboard and mouse.
  • Logix Designer was tested with UAC set to the most restrictive level (Always notify). This version of the Logix Designer application is also expected to operate correctly when UAC is configured for any less restrictive setting.
  

Features

This release includes the following system features.

System features for Studio 5000 Logix Emulate Release Notes version 36.00

In this release of the Studio 5000 Logix Emulate application, product improvements have been made to increase product resiliency to potentially disruptive activities. These enhancements have been verified not to affect product safety, performance, expected life, configuration, or operation of the product. Rockwell Automation recommends that you follow good Industrial Control System (ICS) security practices that include regular product updates. To maintain authenticity, obtain product updates and new releases directly from Rockwell Automation.


Known Anomalies in This Release

This release has the following known anomalies.

Emulate API test sometimes fails on Windows 2022 Server OS (3164278)

The Emulate API test RA_GetTagInfo returns an incorrect error value when attempting to get tag info from a controller that is not present in the virtual rack.  This only occurs for Windows Server 2022.

There is no workaround for this issue.

This anomaly first identified in Studio 5000 Logix Emulate version 36.00.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Anomalies for Studio 5000 Logix Emulate version 33.00

The following list identifies the anomalies corrected in Studio 5000 Logix Emulate version 33.00 and the known anomalies found during testing for this release. Use the identification information provided in the brackets [] to track the anomaly in future releases or contact Customer Support for assistance with a related issue.

Corrected anomalies
Known anomalies

Avoid using RET with SFC subroutines (Lgx00155841)
An anomaly exists in Studio 5000 Logix Emulate controllers when using the Jump to Subroutine (JSR) instruction with Return (RET) instruction parameters in the Sequential Function Chart [SFC] programming language.
To resolve this issue, avoid using RET with SFC subroutines. Use alternate languages such as Ladder, Structured Text, or Function Block.
Result of ADD instruction in SFC is different than other languages (Lgx00156771)
The result of the ADD instruction in SFC is different than the other languages. It is also different from a physical controller.
To resolve this issue, avoid using ADD instructions with SFC subroutines. Use alternate languages such as Ladder, Structured Text, or Function Block.
Avoid configuring a low Watchdog value for tasks (Lgx00219641)
Rockwell Automation recommends not configuring a low Watchdog value for tasks in Emulate because Windows system tasks may preempt user tasks in the Emulate controller. When preemption occurs for a specified duration, a Watchdog fault occurs. Improved watchdog timing does not prevent a watchdog fault for low watchdog values. 

Functional Changes

This release has the following functional changes from the previous release.

Functional changes for Studio 5000 Logix Emulate Release Notes version 36.00

These are the functional changes for Studio 5000 Logix Emulate version 36.00.

Application Notes

This release has the following application notes.

Application notes for Studio 5000 Logix Emulate Release Notes version 36.00

The following are the application notes for Studio 5000 Logix Emulate version 36.00.

Limitations
Performance
Studio 5000 Logix Emulate controller restrictions
Enable remote connections

Studio 5000 Logix Emulate requires an upgrade to RSLinx Classic Gateway version 4.20 or later. If RSLinx Classic Lite is installed, uninstall RSLinx Classic Lite and install RSLinx Classic Gateway version 4.20 or later. Remote connections are disabled when both FactoryTalk Linx and RSLinx Classic version 4.20 or later are installed. Beginning with Studio 5000 Logix Emulate version 35.00, you can also create remote connections with FactoryTalk Linx version 6.31 or later.

To enable remote connections when using RSLinx Classic version 4.20 or later:

  1. Ensure that FactoryTalk Linx is not running. If FactoryTalk Linx is running as a service, stop the service and mark the service for manual startup.
  2. In RSLinx Classic Gateway, select View > Options and select Accept UDP messages on Ethernet port.
  3. Restart RSLinx Classic.
  4. Under Communications, verify that Configure Gateway… is selected.
  5. Restart RSLinx Classic.
graphic
Tip: After configuring RSLinx Classic, FactoryTalk Linx may be enabled. RSLinx Classic will enable remote connections.
  1. In Logix Designer, select Communications > Communications Software > RSLinx Classic.

To enable remote connections when using FactoryTalk Linx version 6.31 or later on the server side:

  1. Install FactoryTalk Gateway Server OPC UA and DA on the server side of the connection.
  1. Open FactoryTalk Linx Gateway Configuration. Select Remote Proxy Service. Make sure Enable Remote Proxy Server is selected. Make sure all NIC cards are enabled on which the proxy service should listen.
  2. Open FTLinx Network Browser and configure the driver to listen to Ethernet/IP encapsulation ports on the intended interface. Verify that Configure Driver > Ethernet > Advanced > Listen on Ethernet/IP encapsulation ports is selected.
  3. Make sure RSLinx Classic is not running.

To enable remote connections when using FactoryTalk Linx version 6.31 or later on the client side:

  1. Open FTLinx Network Browser. Make sure that Advanced Settings > General > Enable Communications to Remote Proxy is selected.
  1. Add a new Remote Device via Proxy Server driver, specifying the IP address of the server and the name of the remote driver.
  2. In the Logix Designer application, select Communications > Communications Software > FactoryTalk Linx.


  
 
3

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.