Release Notes

( 9301-OPCx , 9301M-KSETx) KEPServer Enterprise connects 3rd Party HW / SW, from plant control systems to enterprise information systems
Version 14.00.00 (released 11/2023)

Catalog Number KepServer Enterprise 

These release notes describe version information for KepServer Enterprise, version 14.00.00 (released 11/2023).

Requirements

This release has the following requirements.

KEPServer Enterprise works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
KEPServer Enterprise requires the following hardware:
Software requirements
KEPServer Enterprise has been tested on the following operating systems:

Features

This release includes the following system features.

KEPServer Enterprise version 14.00.00 has the following new and enhanced features:
New features
Server
Fanuc Focas Ethernet Driver
Modbus Ethernet Driver
Torque Tool Ethernet Driver
Enhanced features
Server
Memory Based Driver
ODBC Client Driver
Omron FINS Ethernet Driver
OPC UA Client Driver
Torque Tool Ethernet Driver
User Configurable (U-CON®) Driver

Corrected Anomalies in This Release

This release corrects the following anomalies.

The list identifies the anomalies corrected in the KEPServer Enterprise version 14.00.00.
Server
Fanuc Focas Ethernet Driver
GE Ethernet Driver
Mitsubishi Ethernet Driver
Modbus Ethernet Driver
Modbus Serial Driver

Functional Changes

This release has the following functional changes from the previous release.

KEPServer Enterprise version 14.00.00 has the following changes in functionality since the last release:

Application Notes

This release has the following application notes.

The following are the application notes for KEPServer Enterprise version 14.00.00.
Known limitations of KEPServer Enterprise
  • Multiple failed attempts to authenticate usernames or passwords will now result in a ten-minute lock-out period.
  • KEPServer Enterprise is only able to browse tags using nested structures within four levels deep. 
  • Hilscher Universal Driver
  • Deprecates this driver. Existing OPF project files have loaded, but the channels present an error in the event log. Existing JSON project files are unable to load.

Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
IMPORTANT: Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID:  IN39461 - Microsoft DCOM Hardening Information TOC.
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Set DCOM authentication level of KEPServer Enterprise
When using KEPServer Enterprise, change the authentication level through the following:
  1. Open Component Services.
  2. Double-click Console Root > Component Services > Computers > My Computer > DCOM Config.
    graphic
  1. Right-click KEPServerEnterprise x.xx and select Properties.
    graphic
  1. On the General tab, select the authentication level in Authentication Level
    .graphic
  2. Click OK and restart KEPServer Enterprise.
In addition to DCOM configuration, you must configure the following setting:
  1. From the notification area, right-click KEPServerEnterprise and select Settings.
    graphic
  2. In the Settings - KEPServerEnterprise dialog box, select Runtime Options > Use DCOM configuration settings.
    graphic
  1. Click OK.
Supported Drivers
The PC edition of KEPServer Enterprise version 14.00.00 supports these drivers:
 Driver List
                               
Advanced Simulator
GE SNP
Omron NJ Ethernet
Themo Westronics Serial
Allen-Bradley Bulletin 1609
GE SNPX
Omron Process Suite
TIWAY Host Adapter
Allen-Bradley Bulletin 900
Honeywell HC900 Ethernet
Omron Toolbus
Torque Tool Ethernet
Analog Devices
Honeywell UDC Ethernet
OPC DA Client
Toshiba Ethernet
Aromat Ethernet
Honeywell UDC Serial
OPC UA Client
Toshiba Serial
Aromat Serial
IA Super SEL
OPC XML-DA Client
Toyopuc® PC2 Serial
AutomationDirect DirectNET
Idec Serial
Optimation OptiLogix
Toyopuc PC3/PC2 Ethernet
AutomationDirect EBC
IOtech PointScan 100
Opto 22 Ethernet
User Configurable (U-CON)
AutomationDirect ECOM
Keyence KV Ethernet
Partlow ASCII
Wago Ethernet
AutomationDirect K Sequence
KraussMaffei MC4 Ethernet
Philips P8/PC20
Wonderware InTouch Client
AutomationDirect Productivity Series Ethernet
Memory Based
SattBus Ethernet
Yaskawa Memobus Plus (SA85)
BACnet™ /IP
Mettler Toledo Serial
SattBus Serial
Yaskawa MP Series Ethernet
Beckhoff® TwinCAT®
Micro-DCI™
Scanivalve Ethernet
Yaskawa MP Series Serial
Busware Ethernet
Mitsubishi® CNC Ethernet
Siemens® S5 (3964R)
Yokogawa Controller
CODESYS®
Mitsubishi Ethernet
Siemens S5 (AS511)
Yokogawa CX Ethernet
Contrex® M-Series
Mitsubishi FX
Siemens S7 MPI
Yokogawa Darwin Ethernet
Contrex Serial
Mitsubishi FX Net
Siemens S7-200
Yokogawa Darwin Serial
Cutler-Hammer D50/D300
Mitsubishi Serial
Siemens TCP/IP Ethernet
Yokogawa DX Ethernet
Cutler-Hammer ELC Ethernet
Modbus® ASCII Serial
Siemens TCP/IP Slave Ethernet
Yokogawa DX Serial
Cutler-Hammer ELC Serial
Modbus Plus
Simatic/TI 505 Ethernet
Yokogawa DXP Ethernet
Dataforth® isoLynx®
Modbus RTU Serial
Simatic/TI 505 Serial
Yokogawa HR2400 Serial
DDE Client
Modbus Slave RTU Serial
Simulator
Yokogawa MW Ethernet
Fanuc Focas Ethernet
Modbus TCP/IP Ethernet
SIXNET EtherTRAK®
Yokogawa MX Ethernet
Fanuc Focas HSSB
MTConnect® Client
SIXNET UDR
Yokogawa SMARTDAC+ GX, GP, and GM
Fuji Flex
ODBC Client
SquareD Serial
Yokogawa YS100 Serial
GE® CCM
Omron FINS Ethernet
System Monitor
 
GE Ethernet
Omron FINS Serial
Telemecanique Uni-Telway Slave
 
GE Ethernet Global Data
Omron Host Link
Thermo Westronics Ethernet
 

KEPServer Enterprise versions
This table displays the versions of KEPServer Enterprise and the related or equivalent versions for the following software:
KEPServer Enterprise version
KEPServerEX equivalent version
FactoryTalk View SE and ME
Station
PanelViewPlus
MobileView
5.00.00
4.5
5.00.00
5.00.00 to 5.10.00
Not applicable
8.00.00
5.13.235
8.00.00
8.00.00 to 8.20.00
Not applicable
9.00.00
5.19.476
9.00.00
9.00.00
Optional installation
10.00.00
5.21.158
10.00.00
11.00.00 (requires patch)
10.00.00 to 12.00.00
11.00.00 to 12.00.00
11.00.00
6.6.504
11.00.00
Not supported
Not supported
12.00.00
6.9.572
12.00.00
Not supported
Not supported
12.01.00
6.9.636
12.00.00
Not supported
Not supported
13.00.00
6.11.725
13.00.00
Not supported
Not supported
13.01.00
6.12.325
13.00.00
Not supported
Not supported
14.00.00
6.14.263
14.00.00
Not supported
Not supported

graphicTip: FactoryTalk View SE and ME Station versions 10.00.00 and 11.00.00 require this patch to use KEPServer Enterpriseversion 10.00.00: https:// rockwellautomation.custhelp.com/app/answers/answer_view/a_id/1083527.
For more information, see KEPServer Enterprise User Manual (publication KSE–UM001).
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.