Release Notes

( 9358-Bx ) Provides efficient, predictable batch processing, consistency between batches, and generation of event info. FTB
Version 16.00.00 (released 11/2023)

Catalog Number FactoryTalk Batch 

These release notes describe version information for FactoryTalk Batch, version 16.00.00 (released 11/2023).

Requirements

This release has the following requirements.

System requirements for FactoryTalk Batch v16.00

Review these minimum and recommended system requirements for installing, configuring, and running FactoryTalk Batch v16.00. Unless noted, these requirements assume that no other applications are installed on the computer. Preferred operating systems and software applications are prioritized for support, testing, and post-release patch qualifications.

Hardware requirements
Supported operating systems
graphic
Tip: The installer software inhibits installation of FactoryTalk software on all Windows 7 and 32-bit operating systems, including Windows 10 (32 bit).
Supported database applications

(for storing recipes, materials, reports, and journal archives)

Web browsers

(for FactoryTalk Batch View only)

Logix firmware requirements

(for FactoryTalk Batch only)

Logix Designer Application requirements

(for FactoryTalk Batch only)

FactoryTalk View SE requirements

(for integration of FactoryTalk Batch View HMI Controls and legacy FactoryTalk Batch ActiveX controls only)

FactoryTalk Services requirements
Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Warranty

The warranty does not cover systems that do not meet the minimum requirements for the version of software.

IMPORTANT
FactoryTalk Batch v16.00 supports only the U.S. English versions of operating systems. For more information about supported operating systems and other Rockwell Software product version support, refer to the Product Compatibility and Download Center (PCDC).
IMPORTANT
FactoryTalk Batch v16.00 components do not support touch screen technology.

Features

This release includes the following system features.

System features for FactoryTalk Batch v16.00

FactoryTalk Batch v16.00 has these new, enhanced, and deprecated features:

New features

Deferred Material Parameters

FactoryTalk Batch Server v16.00 adds the ability to defer material parameters to a higher-level recipe, allowing customers to apply modular programming practices and take advantage of formulations when developing material-based recipes.

Support of UTC time stamp in the Event Journal files

The UTC time stamp of batch events is now recorded at the time of the event to prevent displaying ambiguous values from the BatchHistoryEx database after transitioning out of daylight savings.

In FactoryTalk Batch v16.00 a new journal file format has been added.  The new file format is based on JSON Lines format and uses a new file extension (*.evtj).The new format also includes a new data field for storing the GMT time for a record, making integration of data between multiple systems easier and more accurate.  The batch server can be configured to use either the legacy file format (tab-delimited EVT) or the new format.

Enhanced features

Improved Logging

FactoryTalk Batch v16.00 improves logging of server information, warning, and error messages. Messages that were previously sent to the Windows Application log are now sent to the FactoryTalk Diagnostics logs. This feature also includes new messages for Runtime Area Model Updates, Warm and Warm All restarts, and changes in communication status between the Material Server and Batch Server. This feature aligns diagnostics messages for the FactoryTalk Batch system with other FactoryTalk software and makes troubleshooting system issues easier.

Installation and Migration Improvements

The FactoryTalk Batch v16.00 installer includes improved migration of existing Batch Archive databases.

Deprecated features

Legacy Event Journal Format

The tab delimited event journal format (EVT) will not be updated or enhanced. It has been replaced by the enhanced JSON Lines based format (EVTJ) and the option to use legacy EVT format will be removed in a future release. We recommend systems using FactoryTalk Batch v16.00 or later move to the new EVTJ format.

Legacy client applications

The FactoryTalk eProcedure Client, legacy FactoryTalk Batch View Client, and the FactoryTalk Batch ActiveX Controls are not included nor supported by FactoryTalk Batch v15.00 and later. If your production system has dependencies on these products, transition to the modern FactoryTalk Batch View and FactoryTalk Batch View HMI Controls before upgrading to FactoryTalk Batch v16.00.

Corrected Anomalies in This Release

This release corrects the following anomalies.

Pop-up notifications are persistent (519919, 519912)

For example: When an invalid login is used, a pop-up notification is displayed, indicating that the login is invalid. The notification is not cleared even after a successful login is completed.

Corrected in FactoryTalk Batch View v2.01.

First identified in FactoryTalk Batch View v2.00.

To work around this issue, the user must close the notification.

Known Anomalies in This Release

This release has the following known anomalies.

Upgrade to FactoryTalk Batch v16.00 from v15.00 without uninstalling v15.00 caused failed installation (2355688)
When upgrading to FactoryTalk Batch version 16.00 from version 15.00, the upgrade reports a failure when all components are not upgraded at the same time or the service user name is changed.
This issue is resolved by re-running the installer, which ensures that all of the installed components for the existing installation are selected and that the user name is the same as the one used for the existing installation.
Anomaly first identified in FactoryTalk Batch version 16.00.00.
Anomaly corrected in FactoryTalk Batch version 18.00.00.
Problem installing FactoryTalk View Studio Enterprise with FactoryTalk Batch v16.00 already installed (2313853)
Installing FactoryTalk Batch version 16.00 with FactoryTalk Batch View HMI Controls, restarting the computer after the installation is complete, and customizing the installation of FactoryTalk View Studio Enterprise version 13.00 by clearing the HTTPs option, generates the error Install could not locate the FactoryTalk Directory to change the Network Distributed sample application HMI server computer names. Start FactoryTalk View Studio, open the Network Distributed sample applications and change all the HMI server computer names to the correct computer names. To work around this issue, selecting OK on the error dialog box allowed the installation to continue and all the components to install successfully.
This issue is resolved because FactoryTalk View no longer distributes the FactoryTalk Batch View HMI Controls.
Anomaly first identified in FactoryTalk Batch version 16.00.00.
Anomaly corrected in FactoryTalk Batch version 18.00.00.
Material parameters cannot be deferred (3135145)
Inaccurate text in FactoryTalk Batch Recipe Editor User Manual, publication BATCH-UM006: These material parameters cannot be deferred: MATERIAL, LOT, LABEL, or MATERIAL CLASS.
In FactoryTalk Batch version 16.00 and later only, the Material_Class cannot be deferred.
Anomaly first identified in FactoryTalk Batch version 16.00.00.

Creating a material-based batch fails when no binding units are satisfied (3153921)

Creating a batch from a material-based recipe that uses “By Configuration” binding and Material Class, may fail to be created in the following scenario: The material that is selected during batch creation for the Material Class was created in the material database after the batch server was started.  In this case, the batch server will not have the new material in the Materials enumeration. 

To work around the issue, perform an online area model deploy using the same area model that the server is currently using. This will cause the Batch Server to read in the new material from the Material Database.

First identified in v16.00

FactoryTalk Event Archiver

Installing FactoryTalk Batch v14.00 updates FactoryTalk Services Platform to v6.20. There is a known anomaly in FactoryTalk Services Platform 6.11 and 6.20 that impacts FactoryTalk Event Archiver components. When FactoryTalk Diagnostics v6.11 or 6.20 and Microsoft SQL Server Reporting Services 2017 or 2019 are installed on the same computer, Microsoft SQL Server Reporting Services fails to work. This anomaly was first identified in FactoryTalk Services Platform v6.11.00. (#00369202)

To avoid this problem, change the default port used by Microsoft SQL Server Reporting Services from 8082 to another port.
For steps to address the issue after installation is complete, see Knowledgebase Document ID: BF25929 - SQL Server Reporting Services stops working after installing FactoryTalk Diagnostics.

Cross Invocation for User Controls (3106639)
In the FactoryTalk Batch Administrator's User Manual, publication BATCH-UM003, the text inaccurately states that Cross Invocation is supported by the current view or User Controls.
Cross Invocation is not supported by the current view or User Controls.
Anomaly first identified in FactoryTalk Batch version 16.00.00.
FactoryTalk View Tag browser is inoperative (3146132)
When FactoryTalk Batch version 16.00 is installed after FactoryTalk View version 14.00, the tag browser in FactoryTalk View is inoperative.
The post-installation tasks in the FactoryTalk Batch Components Installation Instructions, publication BATCH-IN002 now include an optional task to Reboot after installing multiple products.
If you are installing multiple Rockwell Automation products in succession, such as both FactoryTalk View and FactoryTalk Batch, Rockwell Automation recommends that you restart your computer after completing the final installation to avoid this issue.
Anomaly first identified in FactoryTalk Batch version 16.00.00.
Anomaly corrected in FactoryTalk Batch version 18.00.00.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

FactoryTalk Event Archiver

Installing FactoryTalk Batch version 14.00 and later updates FactoryTalk Services Platform to version 6.20 [00369202]

There is a known anomaly in FactoryTalk Services Platform 6.11 and 6.20 that impacts FactoryTalk Event Archiver components. When FactoryTalk Diagnostics version 6.11 or 6.20 and Microsoft SQL Server Reporting Services 2017 or 2019 are installed on the same computer, Microsoft SQL Server Reporting Services fails to work. This anomaly was first identified in FactoryTalk Services Platform version 6.11.00.

To avoid this problem, change the default port used by Microsoft SQL Server Reporting Services from 8082 to another port.
For steps to address the issue after installation is complete, see Knowledgebase Document ID: BF25929 - SQL Server Reporting Services stops working after installing FactoryTalk Diagnostics.

FactoryTalk Batch Material Manager

Material Editor cannot access the material database after upgrading FactoryTalk Batch [929120]

The MTUser account is not in the correct database. Anomaly first identified in FactoryTalk Batch 14.00.

To work around this issue use these steps:

  1. Open the SQL Server Management Console.
  2. Navigate to the database Logins and delete the MachineName\MTUser login.
  3. Navigate to the material database and open the list of users: delete the user account MTUser.
  4. Run the script MaterialTrack_DBSecurity.sql on the material database. This will recreate the MTUser user account under the database.
    The script is located in the C:\Program Files(x86)\Rockwell Software\Batch\Scripts folder.
    Access to the material database should now be restored.

FactoryTalk eProcedure

Cannot create HMI Server on a computer with FactoryTalk eProcedure and FactoryTalk View SE [00369237]

After adding eProcedure to a FactoryTalk Batch and FactoryTalk View SE install, an HMI Server cannot be created.

To work around this issue, restart the computer after installing eProcedure, then create the HMI Server. 

 FactoryTalk Batch View 2.00

Pop-up notifications are persistent [519919, 519912]

For example: When an invalid login is used, a pop-up notification is displayed, indicating that the login is invalid. The notification is not cleared even after a successful login is completed.

Anomaly first identified in FactoryTalk Batch View 2.00.

To work around this issue, the user must close the notification.

Unintended actions from Arbitration Summary page [98187]

On the Arbitration Summary page, when the More menu graphic is open and a user selects Enter, the first item in the More menu is executed, resulting in possible unintended actions.

Anomaly first identified in FactoryTalk Batch View 2.00.

To avoid this issue, in FactoryTalk Security, enable confirmation messages, which prompt to confirm before actions are performed in FactoryTalk Batch View.

Spurious "No master recipes are released to production" message [263925]

When adding a batch to the batch list, the client may display a "No master recipes are released to production" message while the system is gathering the control recipe data.

Anomaly first identified in FactoryTalk Batch View 2.00.

To work around this issue, wait for the recipes to load. The message disappears after the recipes are loaded.

Spurious client reports of control recipe removal [471548]

During the runtime area model update, the control recipe may be inaccessible to the client, causing the client to report that the control recipe has been removed.

Anomaly first identified in FactoryTalk Batch View 2.00.

The control recipe is not actually removed, so you can ignore this message

Filters not functioning on Arbitration Summary page [760902]

On the Arbitration Summary page, when performing a warm restart or applying a run-time area model update, applied filters may not function as expected.

Anomaly first identified in FactoryTalk Batch View 2.00.

To work around this issue, reapply filters.

Filter values are not cleared automatically [98193]

When a user sets filter values on a phase while on the Equipment page and then restarts the FactoryTalk Batch View Server, the filter values are not cleared automatically.

Anomaly first identified in FactoryTalk Batch View 2.00.

To work around this issue, after restarting the FactoryTalk Batch View Server, manually clear the filter values.

FactoryTalk Batch View HMI Controls 1.00

FactoryTalk View SE Client process lock [360350]

When a Display Client is closed while running a FactoryTalk View SE display that contains the FactoryTalk Batch HMI Controls, the Display Client process keeps running as a background process. This may prevent the ability to launch subsequent instances of the Display Client.

Anomaly first identified in FactoryTalk Batch View HMI Controls 1.00

To work around this issue, reboot the machine on which the FactoryTalk View SE Display Client is executing.

FactoryTalk View Batch server authorization changes only reflected in FactoryTalk View SE user interface only after login [362225]

If a change is made to the FactoryTalk Batch View authorization policies when a FactoryTalk View SE display containing an HMI Control is in runtime, the change is not reflected in the user interface.

The user is required to log out and then login with valid credentials for the new authorization policy changes to be reflected in the user interface.

Removed BaseFilter batch remains on batch list [CLM 4578]

If a BaseFilter batch state is applied (such as State:Running) and the state changes for a currently visible batch on the Batch List, the batch is visibly removed from the list and the message: Control Recipe <name> has been removed appears.

Even though the applied BaseFilter removes visibility to the batch, the batch is actually still on the batch list and can be viewed from other clients or HMI Controls that do not filter based on the batch state.

FactoryTalk eProcedure

Videos are not displayed correctly in manual instruction content served from Batch View Server (1503087)

In FactoryTalk Batch version 15.00, a new folder named customercontent was added to the FactoryTalk Batch View Server. During installation, you can choose to have your custom images, videos, and scripts migrated to this folder to support existing instructions. Absolute paths in the scripts files and manual instructions to the customer content are updated correctly to point to the new content location. However, if you are using relative paths, the content paths in the scripts files and manual instructions are not correctly updated by the installation. Video and script files must include eProcedure/ at the beginning of the relative path.
The src attributes for the instructions need to be updated as follows:
After updating the attributes, the videos should display as expected.
Anomaly first identified in FactoryTalk Batch View version 2.01.00.

Functional Changes

This release has the following functional changes from the previous release.

Functional changes for FactoryTalk Batch v16.00

FactoryTalk Batch v16.00 has no function changes.

Application Notes

This release has the following application notes.

Application notes for FactoryTalk Batch v16.00

The FactoryTalk Batch v16.00 release has the following application notes.

Impact of Microsoft deprecating VBScript

Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.

FactoryTalk Batch versions 18.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.

To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.

Preserve Basefilter property between releases

When upgrading the User Controls between releases, the controls are rewritten and must be deleted and reinstalled. After the install, you must reconfigure the properties on the controls.

If the control is 2.x or later, FactoryTalk View SE applies the properties to the new control. You do not have to reconfigure the properties.

The COM ClassID verifies the new control is compatible. If it is not compatible, the control must be deleted and reinstalled.

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Upgrade
  1. Open the FactoryTalk Administration Console and then navigate to FactoryTalk Linx.
  2. Create FactoryTalk Linx shortcuts to the controllers that have the Phase Manager phases or Sequence Manager sequences.
  3. Open the area model in the Equipment Editor and navigate to the Data Servers. 
  4. Edit each Data Server that is the type Logix5000 CIP, changing the FactoryTalk Linx Controller Shortcut to shortcuts created in step 2.
FactoryTalk Batch
graphic
Tip: For more information, see the FactoryTalk Linx Help topic What's FactoryTalk Linx instance02 service?
Command-line parameters

Use command-line parameters to perform an unattended or silent installation of the software.

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Common Rockwell Automation parameters

These parameters are applicable for all Rockwell Automation software that are available in the installation package.

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes,
and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/Product="value"
Specifies which sub-products will be installed.
Only required if sub-products are included with the install package.
If the software does not include sub-products this parameter is not available.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Or
/InstallDrive="value"
Specifies the install location or install drive respectively.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.
FactoryTalk Batch-specific command line parameters

The command-line install of FactoryTalk Batch performs a full install of FactoryTalk Batch. To install FactoryTalk Batch, FactoryTalk <EA>, FactoryTalk Batch Material Manager, or FactoryTalk Batch View HMI Controls separately use the installation wizard instead of the command-line.

These options are specific to installing FactoryTalk Batch software:

Parameter
Description
BatchServerName
Required for Batch. Machine name where the Batch server is installed.
eProcedureServerName
Required for eProcedure. Machine name where the eProcedure Server is installed.
MaterialManagerServerName
Required for Material Manager. Machine name where Material Manager Server  is installed.
FirstInSystem
Optional. Set to "No" to add a Batch or Material Manager install to an existing system.
If omitted, the default is "Yes"
DomainWorkgroup
Optional. Set to "WORKGROUP" to indicate for a Batch, eProcedure, or Material Manager install that the machine is not connected to a domain.
If omitted, the default is "DOMAIN"
BatchDomain
Required for Batch, eProcedure, and Material Manager.
Specifies the domain name of the machine where the product is being installed. Value should be set to the local machine name when installing in a workgroup.
BatchUserName
Required for Batch, eProcedure, and Material Manager.
BatchPassword
Required for Batch, eProcedure, and Material Manager.
RecipesInSQL
Optional. Set to "Yes" to indicate for a Batch or Material Manager install that recipes should be stored in SQL.
If omitted, the default is "No"
FTDirectory
Optional. Set to "Local" to indicate for a Batch or eProcedure install that FTSP should use the Local directory.
If omitted, the default is "Network"
MaterialJournaling
Optional. Set to "Yes" for a Material Manager install to record activity to the MaterialBasedRecipe_MAJ database.
If omitted, the default is "No"
ArchiverSqlAuth
Optional. Set to "Yes" to indicate for an Event Archiver Database install to use SQL authentication with the user and password values passed in /ArchiverSqlUser and/ArchiverSqlPass.
If omitted, the default is "No"
ArchiverSqlUser
Optional for Event Archiver Database Feature.
ArchiverSqlPass
Optional for Event Archiver Database Feature.
ArchiverDbAction
Required for Event Archiver Database Feature.
"Migrate" updates pre-Batch 12 DB schema to current format
"Upgrade" updates only stored procedures and reports
"Create" generates a new DB, overwriting an existing one
ArchiverServerName
Required for Event Archiver Database Feature.
ArchiverInstanceName
Optional for Event Archiver Database Feature.
ArchiverDataSourceName
Required for Event Archiver Database Feature.
ArchiverWithReports
Optional. For an Event Archiver Database install, set to:
"Yes" to use a BatchHistoryEx database with reporting
"No" to use a BatchHistory database without reporting
If omitted, the default is "Yes"
HTTPS_PORT_USER
Optional for BatchView Server.
If omitted, the default value is 443.
To define a custom port, specify the value of the desired port (port value must follow the validation rules for port number assignment).
CopyCustomerContentSelected
Optional for BatchView Server.
If omitted, the default is "No".
Example

The following example shows how to use the installation commands.

Setup.exe /Q /IAcceptAllLicenseTerms /DomainWorkgroup=Domain /BatchDomain=MyDomain /BatchUserName=User1 /BatchPassword=s3cretp@ssw0rd! /Product=FTBatch /BatchServerName=BatchServer1 /HTTPS_PORT_USER=8443 /CopyCustomerContentSelected=Yes
Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_SUCCESS_RELAUNCH_REQUIRED
3011
Restart of setup needed before installation can continue.
FactoryTalk Batch Material Manager
FactoryTalk Batch Enterprise Integration Server
The FactoryTalk Batch EI Server.msi file is in the EIServer folder of your FactoryTalk Batch v15.00 installation media.
CIS Benchmarks test results recommendations
The following CIS Benchmarks recommendations for Windows 11 with FactoryTalk Batch and eProcedure are exceptions that are set contrary to the recommendation:
2.2.3 (L1) Ensure 'Act as part of the operating system' is set to 'No One'
2.2.4 (L1) Ensure 'Adjust memory quotas for a process' is set to 'Administrators, LOCAL SERVICE,
NETWORK SERVICE'
2.2.11 (L1) Ensure 'Create a token object' is set to 'No One'
2.2.13 (L1) Ensure 'Create permanent shared objects' is set to 'No One'
2.2.25 (L1) Ensure 'Increase scheduling priority' is set to 'Administrators, Window Manager\Window
Manager Group'
2.2.36 (L1) Ensure 'Replace a process level token' is set to 'LOCAL SERVICE, NETWORK SERVICE'
2.3.10.8 (L1) Ensure 'Network access: Remotely accessible registry paths and sub-paths' is configured
2.3.17.1 (L1) Ensure 'User Account Control: Admin Approval Mode for the Built-in Administrator
account' is set to 'Enabled'
2.3.17.2 (L1) Ensure 'User Account Control: Behavior of the elevation prompt for administrators in
Admin Approval Mode' is set to 'Prompt for consent on the secure desktop' or higher Fail
2.3.17.3 (L1) Ensure 'User Account Control: Behavior of the elevation prompt for standard users' is set to
'Automatically deny elevation requests'
2.3.17.6 (L1) Ensure 'User Account Control: Run all administrators in Admin Approval Mode' is set to
'Enabled'
The following CIS Benchmark Recommendations for Server2022 with all FactoryTalk Batch components installed
are exceptions which are set contrary to the recommendation:
2.2.4 (L1) Ensure 'Act as part of the operating system' is set to 'No One'
2.2.6 (L1) Ensure 'Adjust memory quotas for a process' is set to 'Administrators, LOCAL SERVICE,
NETWORK SERVICE'
2.2.14 (L1) Ensure 'Create a token object' is set to 'No One'
2.2.16 (L1) Ensure 'Create permanent shared objects' is set to 'No One'
2.2.33 (L1) Ensure 'Increase scheduling priority' is set to 'Administrators, Window Manager\Window
Manager Group'
2.2.44 (L1) Ensure 'Replace a process level token' is set to 'LOCAL SERVICE, NETWORK SERVICE'
2.3.10.9 (L1) Configure 'Network access: Remotely accessible registry paths and sub-paths' is configured
FactoryTalk Batch View

When adding a batch using FactoryTalk Batch version 16.00, if a control recipe has an equipment bind, you must select the equipment in the Unit Bindings area. By default, the equipment is not selected.

In previous versions, the default selection was the first candidate in the Unit Bindings list.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.