Release Notes

FactoryTalk AssetCentre Server provides you with a set of asset focused tools to securely/centrally manage your facility and process automation.
Version 13.00.00 (released 6/2023)

Catalog Number FactoryTalk AssetCentre Server 

These release notes describe version information for FactoryTalk AssetCentre Server, version 13.00.00 (released 6/2023).

Requirements

This release has the following requirements.

FactoryTalk AssetCentre version 13.00.00 (CPR 9 SR 14)

FactoryTalk AssetCentre works within the system requirements of all Rockwell Automation® software products.

Hardware requirements

System size

FactoryTalk AssetCentre is tested based on these system sizes.

Types
Components
System architecture
Small systems
Server
AssetCentre Server, Microsoft SQL Server®, and FactoryTalk Directory Server are co-located.
Agent
1-5
Desktop Client
10
Web Client
25
Medium systems
Server
AssetCentre Server and Microsoft SQL Server are co-located. FactoryTalk Directory Server is on a separate computer.
Agent
6-25
Desktop Client
60
Web Client
100
Large systems
Server
AssetCentre Server, Microsoft SQL Server, and FactoryTalk Directory Server are hosted on separate computers.
Agent
26-50
Desktop Client
100-150
Web Client
200


Product compatibility

FactoryTalk AssetCentre version 13.00.00 is compatible with the following Rockwell Automation products. For the latest compatibility information, refer to the Rockwell Automation Product Compatibility and Download Center.

FactoryTalk AssetCentre Desktop Client

For more information about the specific drives that FactoryTalk AssetCentre is compatible with, see Knowledgebase Document ID: QA47141 - FactoryTalk AssetCentre RA Motor Control or PowerFlex Drive Device Support.

FactoryTalk AssetCentre Agent


Operating systems

The following tables introduce FactoryTalk AssetCentre’s compatibility with different 64-bit operating systems.

IMPORTANT:
Category
Descriptions
Compatible
The installation is allowed and recommended. Rockwell Automation tested the FactoryTalk AssetCentre’s operation with this operating system.
May be compatible
A pop-up alert will show but the installation is allowed to continue. FactoryTalk AssetCentre is expected to run on these operating systems, but they are not tested with, and you will install on them at your own risk.
Not compatible
A pop-up alert will show, and the installation is prevented.

 

Operating System
FactoryTalk AssetCentre Server
FactoryTalk AssetCentre Agent, Client, and Web Client
Windows Server 2022
Compatible
Compatible
Windows Server 2019
Compatible
Compatible
Windows Server 2016
Compatible
Compatible
Windows Server 2012 R2
May be compatible
May be compatible
Windows Server 2012
May be compatible
May be compatible
Windows Server 2008 R2 SP1
May be compatible
May be compatible
Windows Server 2008 R2
May be compatible
May be compatible
Windows Server 2008 SP1
Not compatible
Not compatible
Windows Server 2008 SP2
Not compatible
Not compatible
Windows Server 2003
Not compatible
Not compatible
Windows 11 (v21H2 and v22H2)
Not compatible
Compatible
Windows 10 (v21H2 and v22H2)
Not compatible
Compatible
Windows 10 IoT Enterprise 2021 Long-Term Servicing Channel (LTSC)
Not compatible
Compatible
Windows 10 IoT Enterprise 2019 Long-Term Servicing Channel (LTSC)
Not compatible
Compatible
Window 10 (v20H2 and v21H1)
Not compatible
May be compatible
Windows 10 v2004 or earlier
Not compatible
May be compatible
Windows 8 and 8.1
Not compatible
Not compatible
Windows 7
Not compatible
Not compatible
Windows XP
Not compatible
Not compatible


Software requirements

SQL Server database

The following is the SQL Server supported by FactoryTalk AssetCentre.

FactoryTalk AssetCentre Agent

The following are minimum software requirements for FactoryTalk AssetCentre Agent.

FactoryTalk AssetCentre Client

The following are minimum software requirements for FactoryTalk AssetCentre Client.

Supported browsers

The following web browsers have been tested and are supported for FactoryTalk AssetCentre Web Client and FactoryTalk AssetCentre Help with this release:

High Resolution Display Support

Windows 10 v1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Security requirements

To help meet secure system design requirements, review these publications:

Features

This release includes the following system features.

FactoryTalk AssetCentre version 13.00.00 has the following new and enhanced features:

New features

Enhanced features

Corrected Anomalies in This Release

This release corrects the following anomalies.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk AssetCentre version 13.00.00 has the following changes in functionality since the last release.

Remove Agent Service Logon Configuration tool

Beginning with FactoryTalk AssetCentre version 13.00.00, the Agent Service Logon Configuration tool is removed. From FactoryTalk AssetCentre version 13.00.00, you can use the FactoryTalk AssetCentre Agent Controller Launch Control Panel to grant the necessary permissions for Disaster Recovery operations.

Folder location change

FactoryTalk AssetCentre version 13.00 changes the following folder location:

Change in Address Book

Beginning with FactoryTalk AssetCentre version 13.00.00, personally identifiable information, such as phone number and street address, has been removed from the Address Book. When upgrading FactoryTalk AssetCentre to version 13.00.00, any personally identifiable information entered will be cleared in its entirety.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk AssetCentre version 13.00.00.

Impact of Microsoft deprecating VBScript

Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation. 

FactoryTalk AssetCentre versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.

To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.

Disaster Recovery schedule tasks fail with Device Not Found recorded in the FactoryTalk AssetCentre Event log

When a Logix controller asset’s Addressing property is configured using RSLinx Classic, Disaster Recovery schedule tasks may start failing with Device Not Found recorded in the FactoryTalk AssetCentre Event log. Rebooting the FactoryTalk AssetCentre Agent(s) will temporarily address the error, however, the task failures will eventually return. This behavior is addressed in an RSLinx Classic patch. See technote BF27867 for additional details.

Full OS backup

Rockwell Automation does not test any third-party software to perform the full Windows operating system backup, for example, Veritas Backup Exec. When performing a computer backup on a running virtualized system, it is recommended the system is stopped before performing a backup.

CIS Benchmarks test results

Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.

For more information about the guidelines, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).

FactoryTalk AssetCentre version 13.00.00 has been assessed against CIS Microsoft Windows 10 Enterprise Benchmark v2.0.0 (L1), CIS Microsoft Windows Server 2019 Benchmark v2.0.0 (L1), CIS Microsoft Windows 11 Enterprise Benchmark v2.0.0 (L1), and CIS Microsoft Windows Server 2022 Benchmark v2.0.0 (L1).

The exceptions for FactoryTalk AssetCentre version 13.00.00 are listed.

CIS Microsoft Windows 10 Enterprise Benchmark v2.0.0 (L1)

CIS Microsoft Windows Server 2019 Benchmark v2.0.0 (L1)

CIS Microsoft Windows 11 Enterprise Benchmark v2.0.0 (L1)

CIS Microsoft Windows Server 2022 Benchmark v2.0.0 (L1)

Secure communication with TLS and SSL protocols

Windows implements SSL and TLS through S-channel Security Support Provider (SSP). The S-channel SSP implementation of the TLS and SSL protocols uses algorithms from a cipher suite to create keys and encryption information. Starting from FactoryTalk AssetCentre version 9.00, the operating system's capability is used to automatically filter out the unsecure ciphers.

Configure certificates for a remote FactoryTalk Network Directory when TLS is enabled

If your FactoryTalk Network Directory server and FactoryTalk AssetCentre server are installed on different computers and secure communications (TLS) are being used, the FactoryTalk Network Directory Web Authentication server requires a certificate for authenticating the FactoryTalk AssetCentre web client. You must configure a certificate authority (CA) issued, or a self-signed, certificate for the FactoryTalk Network Directory server so that the FactoryTalk AssetCentre web client can be used successfully. 

For instructions related to using a certificate authority (CA) issued certificate on the FactoryTalk Network Directory server, see the FactoryTalk AssetCentre Installation Guide:

-Configure the TLS protocol for FactoryTalk AssetCentre

For instructions related to using a self-signed certificate on the FactoryTalk Network Directory server, see the following topics in the FactoryTalk AssetCentre Installation Guide:

-Create a self-signed TLS certificate on the SQL Server or FactoryTalk Network Directory computer

-Configure the HTTPS site binding

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

IMPORTANT: When installing or upgrading FactoryTalk AssetCentre to version 11.00.00 or later with SQL Server Authentication, you must use silent or unattended setup to install it.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter

Description

/?

Displays the usage options for installation parameters.

/Q

Silent Install, install runs in a quiet mode without any user interface.

This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.

This parameter is required if /QS or /Record is not specified.

/QS

Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.

When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.

This parameter is required if /Q or /Record is not specified.

/IAcceptAllLicenseTerms

Acknowledges acceptance of the license terms.

This parameter is required for /Q or /QS parameters.

/AutoRestart

Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.

This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.

/SetupLanguage="value"

Specifies which language will be displayed during install process.

The value must be the one of the following:

  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB

This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.

/Record

Records the installation options chosen to a recording file.

This parameter is optional.

/Playback

Plays back a recording file to specify the installation options.

This parameter is optional.

/IgnoreWarning

Specifies that the setup ignores warnings and continues.

This parameter is optional. If it is not specified, the setup exits when a warning occurs.

/Product="value"

Specifies which sub-products will be installed.

The product name must be one of followings:

  • AssetCentre Server

  • AssetCentre Client

  • AssetCentre Agent

  • AssetCentre Custom Installation

/Uninstall

Uninstalls the product.

This parameter is optional.

/ProductLanguage="value"

Specifies the language version of the software being installed.

The value must be the one of the following:

  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB

This parameter is optional. If this parameter is not used, the default language is the same as the setup language.

If the software does not support multiple languages this parameter is not available.

/SerialNumber="value"

Specifies the serial number of the software being installed. This is used to activate the software during installation.

This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.

Some software does not require activation. If activation is not required this parameter is not available.

/ProductKey="value"

Specifies the product key used to get activation keys during installation.

This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.

Some software does not require activation. If activation is not required this parameter is not available.

/Version="value"

Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.

This parameter is optional. If it is not specified the installer will use the most recent product version available.

Some software does not require activation. If activation is not required this parameter is not available.

/InstallDrive="value"

Specifies the install drive.

This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".

Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.

/ftsp-value="value"

Specifies the FactoryTalk security policy value.

This parameter is optional.

Use the enable or disable value to change the state of RequireComputerAccounts during installation.

/IISCommPort

Specifies the IIS server communication port for HTTPS. The default port for HTTPS is 443.

If the HTTPS port was previously configured using FactoryTalk Services Platform, like port 4356, then the existing HTTPS port setting is retained.

This parameter is optional.

/ftsp-s

Specifies the FactoryTalk Directory scope for restore. Only "Global" and "Local" scopes are supported.

The SECURE.BAK backup file provided by Rockwell Automation is only supported for the “Global” scope.

This parameter is optional.

/ftsp-bak

Restores the backup file and specifies where the restore file can be found.

Rockwell Automation provides a SECURE.BAK backup file containing pre-configured access control lists which limit user access. The pre-configured access control lists follow Rockwell Automation recommended best practice.

The SECURE.BAK backup file is located in the FactoryTalk Services Platform installation package, Redist\FTSPSecureBak.

This parameter is optional.

/ftsp-pp

Specifies the plain text used to decrypt the backup file.

This parameter is optional.

/FTSPWebAuth="value"

Specifies that the installation includes the FactoryTalk Web Authentication Server.

This parameter is optional.

The value must be one of the following:

  • Yes
  • If the value is Yes, the FactoryTalk Web Authentication Server will be installed. The FactoryTalk Reverse Proxy will also be installed as it is required for operation of the FactoryTalk Web Authentication Server.

  • No
  • If the value is No, the FactoryTalk Web Authentication Server will not be installed.

/ReverseProxy="value"

Specifies that the installation includes the FactoryTalk Reverse Proxy.

This parameter is optional.

The value must be one of the following:

  • Yes
  • If the value is Yes, the FactoryTalk Reverse Proxy will be installed.

  • No
  • If the value is No, the FactoryTalk Reverse Proxy will not be installed.

/FTSPWebEventServer="value"

Specifies that the installation includes the FactoryTalk Web Event Server.

This parameter is optional.

The value must be one of the following:

  • Yes
  • If the value is Yes, the FactoryTalk Web Event Server will be installed.

  • No
  • If the value is No, the FactoryTalk Web Event Server will not be installed.

/SystemStatusPortal="value"

Specifies that the installation includes the FactoryTalk System Status Portal.

This parameter is optional.

The value must be one of the following:

  • Yes
  • If the value is Yes, the FactoryTalk System Status Portal will be installed. The FactoryTalk Reverse Proxy and FactoryTalk Web Authentication Server will also be installed as it is required for operation of the FactoryTalk System Status Portal.

  • No
  • If the value is No, the FactoryTalk System Status Portal will not be installed.

/noHTTPS

Specifies that the setup turns off HTTPS and continues.

This parameter is optional.

/SqlServer="value"

Specifies FactoryTalk AssetCentre database server (Microsoft SQL Server) location.

This parameter is required when installing the FactoryTalk AssetCentre server software.

/MSA="value"

Specifies the Group Managed Service Account (gMSA) or Managed Service Account (MSA) that will be used by FactoryTalk AssetCentre Server to access the Microsoft SQL Server database when using Windows Authentication.
  • The parameter is required when the Microsoft SQL Server is hosted on a different computer than the FactoryTalk AssetCentre Server.
  • The parameter is optional when the Microsoft SQL and FactoryTalk AssetCentre Servers are hosted on the same computer.

/sql

Uses SQL Authentication between the FactoryTalk AssetCentre and Microsoft SQL Servers. The use of SQL Authentication is discouraged due to security concerns.

This parameter is required if SQL authentication will be used over MSA.

/sa="value"

Uses SQL Authentication for SQL Server Logins. If you use SQL Server Authentication to perform silent or unattended installation, the parameters /SqlAdmin, and /SqlAdminPwd are required.

/SqlAdmin="value"

Specifies the Microsoft SQL Server administrator account name.

/SqlAdminPwd="value"

Specifies the Microsoft SQL Server administrator account password.

/DirectoryServer="value"

Specifies the FactoryTalk network directory if you are using a distributed system.

This parameter is optional. If it is not specified, the software will use its current computer as the FactoryTalk Directory server.

The value must be the host name of the FactoryTalk Directory server.

/ThirdPartyConnectorAccount="value"

Specifies a Windows user account with standard user permissions that you want to use to run the Agent Controller.

This parameter is required if you want to use Siemens or Mitsubishi connectors in your system.

The format for the "value" is domain\username.

Note: After you specify the username, the Agent Controller mode will be run as an application.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code

Value

Description

ERROR_SUCCESS

0

The installation completed successfully.

ERROR_INVALID_PARAMETER

87

One of the parameters was invalid.

ERROR_INSTALL_USEREXIT

1602

The installation was cancelled by the user.

ERROR_INSTALL_FAILURE

1603

A fatal error occurred during installation or the software component to be installed already exists on the computer.

ERROR_BAD_CONFIGURATION

1610

The configuration data for this product is corrupt. Contact your support personnel.

ERROR_REBOOT_CONTINUE

1641

A reboot is required to continue to installation.

ERROR_SUCCESS_REBOOT_REQUIRED

3010

A restart is required to complete the installation. After restart the product is successfully installed.

ERROR_REBOOT_PENDING

3012

A restart is pending and is required before the installation can continue.

ERROR_SUCCESS_NOT_APPLICABLE

3013

The installation cannot proceed because the products are already installed.

ERROR_SUCCESS_WARNING_REBOOT

3014

Install succeed with warnings. Check installation logs for details. A restart is required to complete the installation.


FactoryTalk AssetCentre Client

FactoryTalk AssetCentre Agent

The number of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system

The following is the number of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system at the same time. More clients, agents, or agent groups running will impact the system performance. The system cannot exceed 50 agents total. For example, a system could have 50 agent groups each with one agent member.

Ensuring consistent domain credentials for FactoryTalk AssetCentre desktop and web clients

In a Windows domain environment, signing in to the FactoryTalk AssetCentre desktop and web clients using the Windows domain user account without the domain name can result in file check-in failures on the web client, even though file check-out on desktop clients works. This happens because the web client handles authentication requests remotely. When the domain name is omitted, Windows automatically selects an authentication method, recognizing the user as a local account rather than a domain account. This causes authentication inconsistencies between the desktop and web clients.

To avoid this problem, sign in using domain\username on both desktop and web clients.

Considerations for generating large PDF reports

Generating very large PDF reports may result in generation failures, incomplete report content, or reports that cannot be opened. Common factors that can affect large PDF report generation include:

To help avoid problems when generating large PDF reports:

Synchronizing lifecycle information with the Rockwell Automation lifecycle website

Lifecycle information can be used to develop hardware device migration plans, or to find devices that require firmware updates. To retrieve the lifecycle information of your Rockwell Automation devices from the Product Compatibility and Download Center (PCDC), perform one of the following methods:

Use a Forward Proxy Server

It is recommended to use a forward proxy server to communicate lifecycle information between the FactoryTalk AssetCentre Server and the PCDC because it provides a more secure connection than configuring firewall access. The forward proxy server must be accessible from the iDMZ and from the FactoryTalk AssetCentre server to access the PCDC.

In the FactoryTalk AssetCentre Server, configure the forward proxy for device lifecycle using FactoryTalk AssetCentre Server Settings. Enter a FactoryTalk administrator's credentials to log in.

In FactoryTalk AssetCentre Server Settings, to enable the forward proxy server, select the checkbox next to Use the forward proxy. In the dialogs, enter the IP address and port number used by your forward proxy server to communicate lifecycle information between the FactoryTalk AssetCentre server and the PCDC. Once this information is entered, select OK. Be sure to restart your computer to ensure the settings take effect.

For the forward proxy server, there are many types and styles of software available. Each proxy server will have different methods and settings. Ensure that the forward proxy server has the web domain https://api.rockwellautomation.com added to the allowed web domain list.

Configure firewall access

Use the following information to configure firewall access to retrieve the lifecycle statuses from the PCDC.

One size does not fit all when it comes to risk tolerance. Please refer to Rockwell Automation's Converged Plantwide Ethernet document for more information about configuring a scalable plant-wide security architecture.

Database mirroring fails when the communication between FactoryTalk AssetCentre and Microsoft SQL Server is encrypted using TLS

FactoryTalk AssetCentre supports database mirroring through the FactoryTalk AssetCentre Data Source Configuration Wizard to improve SQL Server availability.

If both Secure communications using TLS and Enable SQL Mirroring are selected, the FactoryTalk AssetCentre desktop client and web clients cannot connect to the mirrored database after a failover from the principal database.

To ensure the database mirroring function works properly, install Patch: Web client cannot show asset tree, FactoryTalk AssetCentre 12.0, 13.0, 15.0, 16.0, and then disable the TLS encryption. Follow the steps:

  1. On the computer hosting SQL Server:

    1. Open SQL Server Configuration Manager, and then expand SQL Server Network Configuration.

    2. Right-click Protocols for <InstanceName>, and then select Properties.

    3. On Flags, set Force Encryption to Off, and then select OK.

    4. On SQL Server Configuration Manager, select SQL Server Services.

    5. Right-click SQL Server <InstanceName>, and then select Restart.

  2. On the computer hosting the FactoryTalk AssetCentre server:

    1. Open FactoryTalk AssetCentre Data Source Configuration.

    2. On Database User Configuration, clear Secure communications using TLS.

    3. On FactoryTalk AssetCentre SQL Server Mirror, ensure Enable SQL Mirroring is selected.

    4. Complete the remaining configurations and save the changes.

Allen-Bradley Stratix Switch MAC address correction

For an Allen-Bradley Stratix Switch device, its actual MAC address scanned using CIP might differ from the MAC address shown on its switch management page. Each physical interface on a switch has its own unique MAC address that derives from a base MAC address. Additionally, logical ports, such as management ports, might have different MAC addresses. Therefore, the MAC address displayed on the switch management page of Stratix Switch serves only for management purposes. The actual MAC address is in its asset property or the RAAI file.

Use FactoryTalk Linx to browse Logix 5000 controllers of firmware revision 38.00 or later

Beginning with the version 38.00 firmware release, Logix 5000 controllers running firmware revision 38.00 or later can only be browsed using FactoryTalk Linx. RSLinx Classic cannot be used to browse controllers with these newer revisions in Studio 5000 Logix Designer nor FactoryTalk AssetCentre. The following table illustrates communication software support:

Design Software Version RSLinx Classic FactoryTalk Linx
RSLogix 5000 18-20 Supported Not supported
Studio 5000 Logix Designer 21-30 Supported Not supported
Studio 5000 Logix Designer 31-37 Supported Supported
Studio 5000 Logix Designer 38 or later Not supported Supported

After upgrading an existing FactoryTalk AssetCentre system from an earlier version to version 16.00 and later, scheduled backup, backup and compare, and source code validation tasks will fail when:

To resolve this problem, follow the steps to configure FactoryTalk Linx to browse Logix 5000 controllers:

  1. In FactoryTalk AssetCentre Client, select Design.

  2. In the asset tree, right-click the Allen-Bradley Logix 5000 Controller asset, and then select Properties.

  3. In the Addressing Info box, select the browse button.

  4. In the Network Browser list, select FactoryTalk Linx.

  5. Find and select your device from the device list.

  6. Select OK.

Run disaster recovery tasks for controller projects developed with RSLogix 5000 version 16.00 in FactoryTalk AssetCentre version 13.00 or later

FactoryTalk AssetCentre version 13.00 or later includes Logix Designer Compare Tool version 10.00 or later by default in its installation package. However, these versions of the Logix Designer Compare Tool are no longer compatible with RSLogix 5000 version 16.00. As a result, FactoryTalk AssetCentre version 13.00 or later cannot run disaster recovery tasks on controller projects developed with RSLogix 5000 version 16.00 when using the bundled Logix Designer Compare Tool.

To resolve this problem, do the following:

Part 1: Ensure FactoryTalk AssetCentre agent compatibility with RSLogix 5000 version 16.00

On the FactoryTalk AssetCentre agent computer version 13.00 or later, choose one of the following options. This is only required on agent computers that will be used to service Logix controllers running firmware revision 16.00.

Part 2: Create agent groups for FactoryTalk AssetCentre agents that are compatible with the RSLogix 5000 version 16.00

On the FactoryTalk AssetCentre desktop client computer:

  1. Open FactoryTalk AssetCentre desktop client, and then enter the Design mode.

  2. Create an agent group to include agents that will run tasks for controller projects developed with RSLogix 5000 version 16.00.

    1. On the Menu bar, select View > Agent Groups.

    2. On the Agent Group Creation and Agent Assignment toolbar, select the Add Agent Group button, configure the settings for the agent group, and then select OK.

    3. Select the created agent group, and then select Add Agent Computer to add agents.

    4. Configure the settings for the agent computers, and then select OK.

  3. Exit the Design mode.

Part 3: Assign controller assets to FactoryTalk AssetCentre agent groups that are compatible with the RSLogix 5000 version 16.00

On the FactoryTalk AssetCentre desktop client computer:

  1. Open FactoryTalk AssetCentre desktop client, and then enter the Design mode.

  2. Configure all Allen-Bradley Logix 5000 Controller assets running firmware with major revision 16 to use the newly created agent group.

    1. Select an Allen-Bradley Logix 5000 Controller asset in the asset catalog and add it to the asset tree.

    2. On asset properties, select the Agent Group field, find the created agent group, and then select OK.

    3. Configure other properties as desired, and then select OK.

      Repeat steps a-c for all controller assets running firmware with major revision 16.

  3. Exit the Design mode.

  4. Create disaster recovery tasks as needed.

    For more information, see Agent Groups and Schedules in the FactoryTalk AssetCentre Desktop Client Help. 

FactoryTalk Directory asset compare

Differences are always found between two FactoryTalk Directory backup files after a Backup and Compare schedule, even though no changes are made to the FactoryTalk Directory. This is because the BAK files include timestamp information, which is detected as a difference during the binary compare of the backup files.

Event Log Attachment Extractor

The Event Log Attachment Extractor utility cannot properly extract event log attachments in the following two cases:

Install product updates

For the latest Product Updates and Patch information, refer to Knowledgebase Document ID: QA15600 - FactoryTalk AssetCentre Patch Roll-up for 3.0 and later.

You can subscribe to be notified when new product updates, or patches are released via the Knowledgebase by clicking graphicbelow the Knowledgebase answer title.

To download software or firmware updates, and patch roll-ups, go to Product Compatibility and Download Center.

Security requirements

For information on the security considerations when using Rockwell Automation products, including:

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.