Release Notes

E300 EtherNet/IP Communication Module
Version 7.200 (released 7/2023)

Catalog Number 193-ECM-ETR (E300) (series B)

These release notes describe version information for 193-ECM-ETR (E300), version 7.200 (released 7/2023).

Features

This release includes the following system features.



E300 ENET System Revision

Feature First Identified as of Firmware Revision 7.200

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


Changes highlighted in green.

graphic



193-EIO Application

Feature First Identified as of Firmware Revision 7.000

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


Changes highlighted in green.


graphic

v7.006

v7.008


Corrected Anomalies in This Release

This release corrects the following anomalies.


ADC Does Not Complete After Reset

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.180

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


Automatic Device Configuration does not complete after 8-8-8 reset of E300 Series B module with custom DeviceLogix™ program.

 


E3 Emulation Mode Input Not Changing States

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.182

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


Input is not changing states on the DIO when in E3 Emulation Mode and using a 2In2Out GP control module.



GUID Does Not Reset

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.182

Catalog Numbers 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


In an E300 Series B module, GUID does not change or reset if DeviceLogix™ program changes.



Lost EtherNet/IP Connection

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.180

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


MS LED Blinking Red when EtherNet/IP™ connection is lost.



NVS Data Cleared

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.180

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


When a large file size is loaded/restored into the product, some NVS data might have been cleared.



Buffer Overflow Issue

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware 7.198

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


E300 Control Module Series B, the buffer in ac_ShowSelTimeEnt overflows. The correction prevents the overflow from occurring.



Unsigned Integer Overflow

Corrected Anomaly with Firmware Revision 7.200

Known Anomaly First Identified as of Firmware Revision 7.198

Catalog Numbers: 193-EIO-xx-xxx, 193-EIOGP-xx-xxx


E300 Control Module Series B, the unsigned integer overflow buffer in Timer0IntHandler overflows. The correction prevents the overflow from occurring.



  

  Rockwell Automation Company 'Internal'

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.