This release has the following requirements.
The setup.exe supports the following command-line parameters (e.g. C:\Patches-Aug.2022\Setup.exe /Q). The parameters are not case-sensitive.
|
Parameter
|
Description
|
|
One of /Q and
/QS is required
|
Silent Install, installs the patch in the silent mode without any user
interface.
It’s recommended if you are deploying the installation using an IT tool
or script, and don’t expect to see any error or restart messages.
With this parameter, IT tool or script should check the error codes,
and take action accordingly.
|
| /QS
One of /Q and
/QS is required
|
Unattended Install, installs the patch in the unattended mode without
user interaction during installation, and shows the progress, errors, or
complete messages on the user interface.
With this parameter, you will not have to check the error codes, and
the installation will prompt you if there are error or restart messages.
|
|
Default (or /I) Optional.
|
Installs the patch.
|
| /Uninstall (or /X)
Optional.
|
Uninstalls the patch.
|
| /Repair
Optional.
|
Repairs the patch.
|
Error Codes
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed
successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The user cancels installation.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during
installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this PIM
is corrupt. Contact your support
personnel.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete
the installation. This message is
indicative of a success.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
There is nothing to do, or already
installed
|
This release corrects the following anomalies.
Product Anomalies in Patch Roll-up CPR9 SRx January 2023
This release corrects these product anomalies:
FactoryTalk Live Data, version 6.20.00
FactoryTalk Live Data, version 6.21.00
FactoryTalk Live Data, version 6.30.00
FactoryTalk Batch, version 14.00.00
FactoryTalk Linx OPC UA Connector, version 6.21.00
FactoryTalk Linx OPC UA Connector, version 6.30.00
FactoryTalk AssetCentre, version 11.00.00
FactoryTalk Linx, version 6.30.00
FactoryTalk Linx, version 6.31.00
FactoryTalk Alarms & Events, version 6.20.00
FactoryTalk Alarms & Events, version 6.21.00
FactoryTalk Alarms & Events, version 6.30.00
FactoryTalk Alarms & Events, version 6.31.00
FactoryTalk AssetCentre, version 11.00.00
FactoryTalk Services Platform, version 6.30.00
FactoryTalk Services Platform, version 6.31.00
FactoryTalk Live Data, version 6.21.00
FactoryTalk Live Data, version 6.30.00
FactoryTalk Live Data, version 6.31.00
FactoryTalk View, version 12.00.00
FactoryTalk View, version 13.00.00
FactoryTalk Linx, version 6.30.00
FactoryTalk View ME, version 13.00.00
FactoryTalk Services Platform, version 6.10.00
FactoryTalk Services Platform, version 6.11.00
FactoryTalk Services Platform, version 6.20.00
FactoryTalk Services Platform, version 6.21.00
FactoryTalk Services Platform, version 6.30.00
FactoryTalk Services Platform, version 6.31.00
FactoryTalk Linx, version 6.31.00
This release has the following application notes.
Patch a distributed system in the following order:
To run the roll-up on these operating systems, you must first disable User Account Control (UAC).