Release Notes

FactoryTalk Logix Echo Single Node
Version 2.01.00 (released 12/2022)

Catalog Number FactoryTalk Logix Echo Single Node 

These release notes describe version information for FactoryTalk Logix Echo Single Node, version 2.01.00 (released 12/2022).

Requirements

This release has the following requirements.

System requirements for FactoryTalk Logix Echo version 2.01.00

FactoryTalk Logix Echo works within the system requirements of all Rockwell Automation® software products.

Hardware requirements

FactoryTalk Logix Echo has these minimum hardware requirements:

graphic
Tip: Downloading projects simultaneously to many controllers while the system is under heavy load can cause errors. To improve simultaneous download performance, reduce the number of controllers or downloads, or add additional logical cores to the system.
graphic
Tip: For best performance when using FactoryTalk Logix Echo in a virtual machine, take advantage of Intel® Virtualization Technologies.
Software requirements

FactoryTalk Logix Echo requires the following software on the host computer:

FactoryTalk Logix Echo is tested on operating systems installed from original Microsoft® media only. FactoryTalk Logix Echo runs on the 64-bit versions of the following Windows® operating systems:

When you install FactoryTalk Logix Echo, these components are installed:

This component is installed if you select it on the installer:

This software is also available to install based on what is installed on the host computer:


Features

This release includes the following system features.

System features for FactoryTalk Logix Echo version 2.01

FactoryTalk® Logix Echo™ version 2.01.00 introduces these features:


Known Anomalies in This Release

This release has the following known anomalies.

Deleting controllers during snapshot save can block creation of snapshots (1693247)
When the FactoryTalk Logix Echo application saves or restores a snapshot, it puts the emulated controllers in the snapshot in co-simulation mode. If you restart or delete emulated controllers during saving or restoration of a snapshot, the controllers in the snapshot are stuck in co-simulation mode, and you cannot create or restore a snapshot using those controllers.
To work around this issue, delete the controllers in the snapshot and re-add them in the FactoryTalk Logix Echo application. This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.
This anomaly corrected in the FactoryTalk Logix Echo application, version 3.00.

Emulated controllers sometimes shut down when program contains a motion axis (1833982)

When the program for an emulated controller contains a motion axis, the emulated controller might shut down suddenly during startup.

To work around this issue, try starting the emulated controller again.

This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.


IP address and network mask are not restored from the SD card (1708087)

When you save an emulated controller configuration to the emulated controller SD card, change the IP address and network mask, and then restore the configuration from the SD card, the IP address and network mask are not restored to the original configuration.

To work around this issue, use a snapshot to restore a configuration.

This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.


Controllers stop responding during snapshot creation (1767371)

One or more controllers might stop responding during Snapshot creation. The message Controller is not responding appears on the Device Status panel in the Dashboard for those controllers.

To work around this issue, turn the controller off and then on again, re-download the project, and attempt snapshot creation again.

This issue first identified in FactoryTalk Logix Echo version 2.01.


API GetDataTypeInfo API method can result in an exception (2098043)
Using API GetDataTypeInfo API method to access tags associated with Input or Output module tags results in an error. This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.
This anomaly corrected in the FactoryTalk Logix Echo application, version 3.00.00.
Download fails when ACD includes 5094-72IS or -IRT8S (2317915)
It is not possible to successfully download an ACD file containing a 5094-G2IS(XT) or 5094-IRT8S(XT) module to a FactoryTalk Logix Echo controller. During the download the Echo controller asserts and becomes non-responsive. To recover the Echo controller to operation it must be turned off and back on.
This anomaly first identified in the FactoryTalk Logix Echo application, version 2.01.00.
This anomaly corrected in the FactoryTalk Logix Echo application, version 3.00.00.


  
Timer structure API set unexpected results in CoSim mode (2253703)
​​Timer accumulate value does not increment from restored value when the timer structure is written to using the API when the Echo controller is in CoSim mode.
Example: Timer ACC = 1000 prior to API write to time r structure with ACC = 500. When the next one second CoSim quantum is completed the timer ACC = 2000 instead of expected 1500.
​To work around this issue, write directly to Timer ACC, which results in expected behavior in CoSim mode quantum execution.
This anomaly first identified in the FactoryTalk Logix Echo application, version 1.00.00.

 

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Invalid IP address blocks ability to change properties, turn controller off, or modify SD Card (1894909)

When you create an emulated controller using an ACD file or by restoring or importing a snapshot, and the IP address for the emulated controller is not valid, you cannot apply changes to some controller properties, and you cannot turn the controller off or modify the SD Card. The symptom of this anomaly is that, after you change a controller property on the controller with an invalid IP Address, the Apply button is disabled.

This error appears when you attempt to turn the controller off, attach or detach the SD card from the controller property screen, or toggle the controller on or off from the device status panel:

Modify controller failed. An error occurred when communicating with the FactoryTalk Logix Echo service. If this error occurs often, contact Rockwell Automation technical support.

However, there is no error to indicate that the IP address is not valid.

To work around this issue, enter a valid IP address for the emulated controller.

This anomaly first identified in FactoryTalk Logix Echo v1.00.


Delayed changes fault sometimes occurs for produced and consumed tags (1076648, 1172801)

When the Requested Packet Interval (RPI) is set to 200 ms or less for produced and consumed tags, a fault sometimes occurs that indicates a data change delay.

There is no workaround for this issue.

This anomaly first identified in the FactoryTalk Logix Echo application, version 1.00.00.


Trends display steps instead of a linear line (1093987)

Trends show steps instead of linear line while executing quantums larger than 10ms. Furthermore, some trends use physical time instead of virtual time.

This anomaly first identified in the FactoryTalk Logix Echo application, version 1.00.00.


Functional Changes

This release has the following functional changes from the previous release.

Functional changes for FactoryTalk Logix Echo version 2.01

These are the functional changes for FactoryTalk® Logix Echo™ version 2.01.00.


Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.