This release has the following requirements.
Compatible Software for Controller Firmware Revision 35.011
System Requirements as of Revision 35.011 for these catalog numbers:
This table identifies the minimum software versions that are compatible with firmware revision 35.011:
|
Software
|
Version
|
|
|
Studio 5000 Logix Designer®
|
35.00.00
|
|
|
RSLinx® Classic
|
4.30.00
|
|
|
FactoryTalk® Linx
|
6.31.00
|
|
|
ControlFLASH™
|
15.06.00
|
|
|
ControlFLASH Plus™
|
5.00.00
|
|
These anomalies are from previous releases but are still known in this release.
PI Function Block (Lgx00070832)
Known Anomaly First Identified as of:
For more information regarding the PI instruction, see the Logix5000™ Controllers Advanced Process Control and Drives Instructions User Manual, publication 1756-RM006.
Accept Edits (Lgx00122528, Lgx00122622)
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
When you accept edits in LD, ST, and FBD, the controller will log an 'Online Edit' entry in the controller log. Accepting edits in a SFC routine is done by performing a partial import, resulting in a 'Transaction Commit' entry in the controller log. This is confusing because you can select to mask both entries separately. Selecting only Online edits would cause the Audit Value to change only when FBD, ST, and LD edits are made. SFC online edits would change the Audit Value only if the 'Partial Import Online Transaction Completed' bit was set.
Arithmetic State Flags (Lgx00122480)
Known Anomaly First Identified as of Firmware Revision 20.011
Catalog Numbers:
Logix CPU Security Tool
Known Anomaly First Identified as of Firmware Revision 20.011
RSLogix 5000™ Version 20.00
Studio 5000 Logix Designer™ First Identified as of Version 21.00
Catalog numbers:
Browse via RSLinx Classic over the USB Port (Lgx00128816, Lgx00128101)
Known Anomaly First Identified As Of Firmware Revision 20.012
Catalog Numbers
- 5370 CompactLogix L2
- 5370 CompactLogix L3
Communication with 1769 I/O Modules
Anomaly
Logix Firmware/RSLogix 5000 Software 20.011
Catalog Numbers 1769-L24ER-QB1B, 1769-24ER-QBFC1B, 1769-L27ERM-QBFC1B, 1769-L30ER, 1769-L30ERM, 1769-L30ER-NSE, 1769-L33ER, 1769-L33ERM, 1769-L36ERM
Connection via USB Cable (Lgx00122143)
Known Anomaly First Identified As Of Firmware Revision 20.011
Catalog Numbers:
- 5370 CompactLogix L1
- 5370 CompactLogix L2
- 5370 CompactLogix L3
Compact I/O Affects Controller Power-up Sequence (Lgx00127867, Lgx00127768)
Anomaly Identified As Of Revision 20.011
Catalog Numbers:
- 5370 CompactLogix L2
- 5370 CompactLogix L3
|
Cat. No. |
Series |
Firmware Revision |
|
1769-ARM |
A |
3.1 |
|
1769-ASCII |
A |
2.001 |
|
1769-BOOLEAN |
A |
1.2 |
|
1769-HSC |
A |
1.1 |
|
1769-IA16 |
A |
3.1 |
|
1769-IA8I |
A |
3.1 |
|
1769-IF16C |
A |
1.2 |
|
1769-IF16V |
A |
1.2 |
|
1769-IF4 |
B |
2.1 |
|
1769-IF4XOF2F |
A |
1.2 |
|
1769-IF4I |
A |
1.2 |
|
1769-IF4XOF2 |
A |
1.1 |
|
1769-IF8 |
A |
1.1 |
|
1769-IG16 |
A |
3.1 |
|
1769-IM2 |
A |
3.1 |
|
1769-IQ16 |
A |
3.1 |
|
1769-IQ16F |
A |
3.1 |
|
1769-IQ32 |
A |
3.1 |
|
1769-IQ6XOW4 |
B |
3.1 |
|
1769-IR16 |
A |
3.1 |
|
1769-IT6 |
A |
2.2 |
|
1769-OA16 |
A |
3.1 |
|
1769-OA8 |
B |
3.1 |
|
1769-OB16 |
B |
3.1 |
|
1769-OB16P |
B |
3.1 |
|
1769-OB32 |
A |
3.1 |
|
1769-OB32T |
A |
3.1 |
|
1769-OB8 |
A |
3.1 |
|
1769-OF2 |
B |
2.1 |
|
1769-OF4 |
A |
1.1 |
|
1769-OF4CI |
A |
2.1 |
|
1769-OF4VI |
A |
2.1 |
|
1769-OF8C |
A |
2.1 |
|
1769-OF8V |
A |
2.1 |
|
1769-OG16 |
A |
3.1 |
|
1769-OV16 |
B |
3.1 |
|
1769-OV32T |
A |
3.1 |
|
1769-OW16 |
A |
3.1 |
|
1769-OW8 |
B |
3.1 |
|
1769-OW8I |
B |
3.1 |
|
1769-SDN |
B |
2.2 |
Disable Download Project Documentation and Extended Properties Features (Lgx00135928)
Known Anomaly First Identified As Of Firmware Revision 21.011
Studio 5000 Logix Designer First Identified As Of Version 21.00
PhaseManager™ and SequenceManager™ Show Different States of Phase in Program Mode (00183769)
Known Anomaly First Identified as of Firmware Revision 28.011
Catalog Numbers:
If the controller is switched to Program mode while a sequence and phase are running, the phase state changes to idle and displays idle, while the sequence continues to show running. On transition back to Run mode, the sequence displays inactive.
RPI for Local Expansion Modules (Lgx00136853)
Anomaly Identified As Of Revision 21.011
I/O Activity Affects Periodic Sampling for Data Logs (Lgx00129461)
Known Anomaly First Identified as of Firmware Revision 24.011
Catalog Numbers:
I/O activity can affect the repeatability of the periodic sampling for data logs. The result of this anomaly occurring is missed periods of data samples. That is, the time between two data samples is twice as long as expected.
The following are I/O activities:
Alarm Log Content Lost at Powerup (Lgx00138163)
Known Anomaly First Identified as of Firmware Revision 24.011
Catalog Numbers:
Alarm Log content can be lost if there is a Secure Digital (SD) card in the controller that contains a project that is configured to load the project on powerup.
Controller Appears to Be Stuck in the Transition to Run Mode (Lgx00154875)
Known Anomaly First Identified as of Firmware Revision 24.011 for:
Corrected Anomaly as of Firmware Revision 1.013 for 1732E-OB8M8SR
Known Anomaly First Identified as of Firmware Revision 1.012 for 1732E-OB8M8SR
If your project uses a 1732E-OB8M8SR module, upgrade the module firmware to firmware revision 1.013 or later.
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
20.011
|
38.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
38.011 and later
|
|
ControlLogix® 5570
|
18.012
|
38.011 and later
|
|
GuardLogix 5570
|
20.011
|
38.011 and later
|
|
CompactLogix 5380
|
28.011
|
38.011 and later
|
|
Compact GuardLogix 5380 SIL 2
|
31.011
|
38.011 and later
|
|
Compact GuardLogix 5380 SIL 3
|
32.013
|
38.011 and later
|
|
CompactLogix 5380 Process
|
33.011
|
38.011 and later
|
|
CompactLogix 5480
|
32.011
|
38.011 and later
|
|
ControlLogix 5580
|
28.011
|
38.011 and later
|
|
GuardLogix 5580
|
31.011
|
38.011 and later
|
|
ControlLogix 5580 Process
|
33.011
|
38.011 and later
|
Work arounds to consider:
Attribute Values Incorrect with Set System Value Instruction (00169713)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
When you use a Set System Variable (SSV) instruction to set the values for attributes available with the WallClockTime class, the values can be set incorrectly.
Wall Clock Value Different From Previous Value (00169756)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
After you set the wall clock for a controller, the actual time can be offset from the value that you set by approximately 2 seconds.
This anomaly occurs after Precision Time Protocol (PTP) is disabled in a controller that was previously synchronized with the grandmaster clock.
Expiration Times On a Logix Repository Record Can Differ (00171229)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
When the Logix Repository deletes a record, the cached value of the earliest expiration time and the actual expiration time value of the record can be different.
Unconnected Timeout Time Incorrect (00171872)
Known Anomaly First Identified as of Firmware Revision 27.011
Catalog Numbers:
The unconnected timeout time can be longer for a Forward Open service than expected.
Media Space Calculation Incorrect with 3rd-party Secure Digital Cards (00175295)
Known Anomaly First Identified as of Firmware Revision 28.011
Catalog Numbers:
The media space calculation that is done to determine the available memory on a Secure Digital (SD) card can be incorrect with 3rd-party SD cards that are 4 GB or greater.
This anomaly does not occur when you use SD cards available from Rockwell Automation. That is, the 1784-SD1 and 1784-SD2 cards.
We recommend that you use the SD cards available from Rockwell Automation with your controller.
While other SD cards can be used with the controller, Rockwell Automation has not tested the use of those cards with the controller. If you use an SD card other than those cards that are available from Rockwell Automation, you can experience data corruption or loss.
Controller Anomaly with Continuous Task, Indirect Addressing, and CONCAT or DTOS (1442602)
|
Controllers
|
First Known in
Firmware Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
29.011
|
—
|
|
Compact GuardLogix® 5370
|
29.011
|
—
|
|
ControlLogix® 5570
|
29.011
|
—
|
|
GuardLogix 5570
|
29.011
|
—
|
|
ControlLogix 5570 redundant
|
30.051
|
—
|
Controller applications with a continuous task with CONCAT or DTOS instructions where indirect addressing exists may result in a controller major nonrecoverable fault/assert when additional task(s) exist. See Knowledgebase Technote 5570/5370 Controller Anomaly with Continuous Task, Indirect Addressing and CONCAT or DTOS.
SequenceManager Event Client 2.0 Can Experience Slow Performance When Using the Start Up Recovery Option (1769621)
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in
Firmware Revision
|
|
CompactLogix™ 5370
|
28.011
|
36.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
36.011 and later
|
|
ControlLogix® 5570
|
28.011
|
36.011 and later
|
|
GuardLogix 5570
|
28.011
|
36.011 and later
|
After downloading a new project, the SequenceManager™ Event Client that started with the Start Up Recovery option should stop attempting to recover events immediately. However, the Event Client can continue to attempt recovery until the maximum number of events has been reached.
Workaround: Start the SequenceManager Event Client with the Start Up Recovery option disabled.
SequenceManager Event Client 2.0 Cannot Reliably Recover Events on Startup of The Service (1766682)
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in
Firmware Revision
|
|
CompactLogix™ 5370
|
28.011
|
36.011 and later
|
|
Compact GuardLogix® 5370
|
28.011
|
36.011 and later
|
|
ControlLogix® 5570
|
28.011
|
36.011 and later
|
|
GuardLogix 5570
|
28.011
|
36.011 and later
|
Starting the SequenceManager™ Event Client 2.0 service with the Start Up Recovery option enabled can result in missing data.
Module does not get IP Address Assigned from a DHCP Server (2188094, 2233611)
|
Modules
|
First Known in Firmware
Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix™ 5370
|
20.011
|
36.011
|
|
Compact GuardLogix®
5370
|
28.011
|
36.011
|
|
1756-EN2F
|
5.028 (Signed)
2.005 (Unsigned)
|
12.001 and later
|
|
1756-EN2T
|
5.028 (Signed)
|
12.001 and later
|
|
1756-EN2TP
|
10.020
|
12.001 and later
|
|
1756-EN2TR
|
5.028 (Signed)
1.003 (Unsigned)
|
12.001 and later
|
|
1756-EN3TR
|
5.028 (Signed)
3.004 (Unsigned)
|
12.001 and later
|
|
1756-ENBT
|
1.061
|
—
|
|
1768-ENBT
|
1.003
|
—
|
This anomaly was due to a change in the Dynamic Host Configuration Protocol (DHCP) standard, RFC 6842. This anomaly results in the module not being able to obtain an IP address through DHCP with some Stratix® switches that follow the updated standard.
For more information, see Knowledgebase Technote Some Ethernet devices do not obtain DHCP lease from Stratix 5800 as DHCP Server.
Controller Can Assert When Writing to the Message Backing Tag Timeout (TO) Bit Repetitively (3830685)
|
Controllers
|
First Known in Firmware
Revision
|
Corrected in Firmware
Revision
|
|
CompactLogix® 5370
|
34.011
|
—
|
|
Compact GuardLogix® 5370
|
34.011
|
—
|
The more message instructions that are enabled and have their timeout bits written to faster than one second, the more likely controller asserts are to occur.