Release Notes

ControlLogix Type: GuardLogix
Version 35.011 (released 11/2022)

Catalog Number 1756-L71S (series B)

These release notes describe version information for 1756-L71S, version 35.011 (released 11/2022).

Requirements

This release has the following requirements.

Compatible Software for Controller Firmware Revision 35.011

System Requirements as of Revision 35.011 for these catalog numbers:

This table identifies the minimum software versions that are compatible with firmware revision 35.011:

Software
Version
 
Studio 5000 Logix Designer®
35.00.00
 
RSLinx® Classic
4.30.00
 
FactoryTalk® Linx
6.31.00
 
ControlFLASH™
15.06.00
 
ControlFLASH Plus™
5.00.00
 




Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Mechanical Brake Delay (Lgx00113541, Lgx00107169)

Anomaly

Logix Firmware/RSLogix 5000™ Software 19.011

Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65, 1756-L72, 1756-L73, 1756-L74, 1756-L75

Logix Firmware/RSLogix 5000 Software 20.011

Catalog Numbers 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT

Catalog Numbers 1769-L18ERM-BB1B, 1769-L27ERM-QBFC1B, 1769-L30ERM, 1769-L33ERM, 1769-L36ERM

This anomaly occurs only in Integrated Motion on the EtherNet/IP network applications.

When you create a new CIP axis, the default value for Mechanical Brake Delay = 0. If you are using a motor with a brake on this axis and do not change the Mechanical Brake Delay value, the motor will not work properly when you attempt to execute motion.

To work around this anomaly, make sure that you set the Mechanical Brake Delay to the appropriate value before executing motion.

 

 

MSF Instruction (Lgx00113540, Lgx00108486)

Known Anomaly First Identified As Of

Catalog Numbers

- 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65, 1756-L72, 1756-L73, 1756-L74, 1756-L75 - Firmware Revision 19.011

- 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT - Firmware Revision 20.011

- 1769-L18ERM-BB1B, 1769-L27ERM-QBFC1B, 1769-L30ERM, 1769-L33ERM, 1769-L36ERM - Firmware Revision 20.011

This anomaly occurs only in Integrated Motion on the EtherNet/IP network applications.

Every time there is a Motion Servo Off (MSF) instruction/Motion Servo On (MSO) instruction cycle, the Position Trim value is added to the axis position. This change in axis position causes the axis to move unexpectedly by a distance equal to the Position Trim value.

 

Absolute Feedback Offset (Lgx00076298)

Known Anomaly First Identified as of:

Catalog Numbers:

 

If you issue an Absolute Feedback Offset, it results in a feedback fault. If you issue an Absolute Feedback Offset via an SSV instruction on the 1756-M02AS module, the result is a feedback fault. The feedback fault occurs regardless of whether feedback is on or off.

Alarm Log Content Lost at Powerup (Lgx00138163)

Known Anomaly First Identified as of Firmware Revision 24.011

Catalog Numbers:

 

Alarm Log content can be lost if there is a Secure Digital (SD) card in the controller that contains a project that is configured to load the project on powerup.

Controller Appears to Be Stuck in the Transition to Run Mode (Lgx00154875)

Known Anomaly First Identified as of Firmware Revision 24.011 for:

Corrected Anomaly as of Firmware Revision 1.013 for 1732E-OB8M8SR

Known Anomaly First Identified as of Firmware Revision 1.012 for 1732E-OB8M8SR 


If your project uses a 1732E-OB8M8SR module, upgrade the module firmware to firmware revision 1.013 or later.

PI Function Block (Lgx00070832)

Known Anomaly First Identified as of:

 

The PI Function block appears to stop executing as the output does not change and instruction faults are logged.

If the PI instruction is being used in Linear mode, this floating-point equation is used to calculate the ITerm.

graphic

Due to the use of the single-precision floating point values, it may be possible, depending on the values of WLD and KP, for the ITerm value to be small enough, less than 0.0000001, to be lost when adding to the ITermn-1.

For more information regarding the PI instruction, see the Logix5000™ Controllers Advanced Process Control and Drives Instructions User Manual, publication 1756-RM006.

 

Real Time Axis Attribute of VelocityFeedback (Lgx00107793)

Known Anomaly First Identified As Of:

Catalog Numbers 1756-L61, 1756-L61S, 1756-L62, 1756-L62S, 1756-L63, 1756-L63S, 1756-L63XT, 1756-L64, 1756-L65 Version 18.011

Catalog Numbers 1756-L72, 1756-L73, 1756-L74, 1756-L75 Version 19.011

Catalog Numbers 1756-L71, 1756-L72S, 1756-L73S, 1756-L73XT, 1756-L73SXT Version 20.011

 

This anomaly occurs only in SERCOS applications that use Kinetix SERCOS drives and linear motors.

Under certain conditions, it is possible that the Real Time Axis attribute VelocityFeedback contains an incorrect value. The inaccuracy is the result of incorrect scaling of that attribute.

Your program will have an incorrect value for the VelocityFeedback attribute if you follow these steps.

  1. While offline, you write your RSLogix 5000 program and, as part of that program, the VelocityFeedback attribute is selected.
  2. You save the program and download it to the controller.
  3. You go online.

The VelocityFeedback attribute value is incorrect because that attribute was enabled before the program was saved, downloaded, and put online.

To work around this anomaly, do not enable the VelocityFeedback attribute until the RSLogix 5000 program is online.

 

MAM Instruction With Merge Enabled (Lgx00078822)

Known Anomaly First Identified as of

Catalog numbers:


Under some rare occurrences, if a Motion Axis Move (MAM) instruction with Merge Enabled is activated during the deceleration segment of an active MAM instruction then the new MAM instruction may overshoot its programmed endpoint. The occurrence of the overshoot depends on the following factors:

•The original MAM instruction's remaining travel distance at the time of the merge and the new MAM instruction's remaining travel distance

•The relationship of the decel jerk of the new MAM instruction to the decel jerk of the original MAM instruction

•If the original MAM instruction is decelerating

 

Typically, the overshoot does not occur. If either of the following conditions exist, you will avoid the overshoot:

•The new MAM instruction is programmed with Merge Disabled. If there is no other motion active at the time of the merge, then the Merge Disable results in the same operation as the Merge Enable.

•The new MAM instruction has a slightly higher jerk (in units/seconds3) than the original MAM instruction. You should note, though, lower value of jerk in % of time results in higher value of jerk (in units/seconds3).

 

Safety Tag With Multicast Consuming Controllers (Lgx00104877)

Known Anomaly First Identified As Of:

Catalog Numbers

- 1756 GuardLogix® L6 Firmware Revision 18.011

- 1756 ControlLogix® L7 Firmware Revision 20.011


The use of a safety tag with several multicast consuming controllers at varying firmware revisions can result in a connection timeout.

If your application is configured with GuardLogix controllers consuming safety tags produced by a GuardLogix controller at revision 18.x, and the consuming controllers of one safety tag are at varying firmware revisions you may experience a connection timeout with error code 0x203. In the event of a connection timeout, all of the consuming controllers appear to connect to the tag and run for some time, but then the connection timeout occurs.

If you use a single consumer of a safety tag, that consumer will connect and remain connected.

To workaround this anomaly, set the revision of the producing controller to the same revision as the lowest revision of the consumers connecting to the safety tag. For example, if you have consuming GuardLogix controllers at revisions 17.x and 18.x, set the producing controller to revision 17.x to match the lowest revision of the consumers.

 

Accept Edits (Lgx00122528, Lgx00122622)

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

 

When you accept edits in LD, ST, and FBD, the controller will log an 'Online Edit' entry in the controller log. Accepting edits in a SFC routine is done by performing a partial import, resulting in a 'Transaction Commit' entry in the controller log. This is confusing because you can select to mask both entries separately. Selecting only Online edits would cause the Audit Value to change only when FBD, ST, and LD edits are made. SFC online edits would change the Audit Value only if the 'Partial Import Online Transaction Completed' bit was set.

Arithmetic State Flags (Lgx00122480)

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers:

 

  1. When dealing with Floating point numbers, the controller does not truncate denormalized values or -0.0… 0.0.
  2. For an integer divide, when the denominator is 0, the S:N and S:Z are not set.
  3. For the MOD instruction, the S:V is not set if an overflow occurred during the calculation.

Logix CPU Security Tool

Known Anomaly First Identified as of Firmware Revision 20.011

RSLogix 5000™ Version 20.00

Studio 5000 Logix Designer™ First Identified as of Version 21.00

 

Catalog numbers:


Corrected: Logix Firmware 20.014 for only

● 1756-L61, 1756-L62, 1756-L63, 1756-L63XT, 1756-L64, 1756-L65
● 1756-L71, 1756-L72, 1756-L73, 1756-L73XT, 1756-L74, 1756-L75


Absolute Immediate or Passive Home (Lgx00135080, Lgx00134716)

Anomaly

Logix Firmware/RSLogix 5000 Software 20.013, 21.011

Catalog Numbers:

● 1756-L61, 1756-L62, 1756-L63, 1756-L63XT, 1756-L64, 1756-L65

● 1756-L61S, 1756-L62S, 1756-L63S

● 1756-L71, 1756-L72, 1756-L73, 1756-L73XT, 1756-L74, 1756-L75

● 1756-L71S, 1756-L72S, 1756-L73S, 1756-L73SXT



Prior to RSLogix 5000 software, version 19.00.00, you could perform either an absolute immediate (SERCOS only) or a passive home with the drive in a safe off state. In RSLogix 5000 software, version 20.00.00, that feature was inadvertently changed to be blocked and generates the error 16#0028 'You are trying to run a motion command when the drive is locally disabled'.
 

SequenceManager Event Client 2.0 Can Experience Slow Performance When Using the Start Up Recovery Option (1769621)

Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix™ 5370
28.011
36.011 and later
Compact GuardLogix® 5370
28.011
36.011 and later
ControlLogix® 5570
28.011
36.011 and later
GuardLogix 5570
28.011
36.011 and later


After downloading a new project, the SequenceManager™ Event Client that started with the Start Up Recovery option should stop attempting to recover events immediately. However, the Event Client can continue to attempt recovery until the maximum number of events has been reached.

Workaround: Start the SequenceManager Event Client with the Start Up Recovery option disabled.



SequenceManager Event Client 2.0 Cannot Reliably Recover Events on Startup of The Service (1766682)

Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix™ 5370
28.011
36.011 and later
Compact GuardLogix® 5370
28.011
36.011 and later
ControlLogix® 5570
28.011
36.011 and later
GuardLogix 5570
28.011
36.011 and later


Starting the SequenceManager™ Event Client 2.0 service with the Start Up Recovery option enabled can result in missing data.


  

Safety Fault if GuardLogix Controller Not CST Master (Lgx00104194)

Known Anomaly First Identified as of Firmware Revision 20.011

Catalog Numbers


With earlier revisions of GuardLogix controller firmware, we recommended that you set the GuardLogix controller as the Coordinated System Time (CST) master to avoid nonrecoverable safety faults.

If you are using the CIP Sync enhancement with RSLogix™ 5000 software and a GuardLogix controller, we recommend that you configure the GuardLogix controller so that it becomes the CST master. To do so, select Enable Time Synchronization on the Date/Time tab of the Controller Properties dialog box. If you do not configure the GuardLogix controller to become the CST master and your project uses safety tags that are produced, I/O faults can occur when the project is downloaded.

For more information about enabling the GuardLogix controller to become the CST master, see the GuardLogix Controllers User Manual, publication 1756-UM020.

Incorrect Execution Schedule for Scheduled Output Module (Lgx00157174)

Known Anomaly First Identified as of Firmware Revision 24.011

Catalog Numbers:


This anomaly occurs with only 1756-OB16IEFS and 1732-OB8M8SR Scheduled Output modules.


The Scheduled Output module may schedule outputs incorrectly if the Motion Arm Output Cam (MAOC) instruction is enabled before the module’ s connection is in the RUNNING state. The following sequence must occur to observe the anomalous behavior.

  1. The MAOC issues a new schedule before the Scheduled Output module connection enters the RUNNING state.
  2. A change in system time occurs between the time the new schedule is created and the connection entering the RUNNING state.

To work around this anomaly, update your logic to verify that the scheduled output module is in the RUNNING state before executing the MAOC instruction.

Produce/Consume Communication Can Cause I/O Status Indicators to Blink (Lgx00135976)

Known Anomaly First Identified As Of Version 21.011

Catalog Numbers


If an application requires produce/consume communication between GuardLogix controllers, the I/O status indicator can blink, giving the indication that an I/O fault is present even though the system is functioning properly.

This status indicator behavior occurs when the following conditions exist:

IMPORTANT: In the conditions described previously, you must have two controller applications-one for the 1756-L6xS controller, that is, the consumer, and one for the 1756-L7xS controller, that is, the producer.

You cannot add a 1756-L7xS controller to a 1756-L6xS controller's RSLogix™ 5000 software project, if the project is version 19 or earlier.

To work around this anomaly, complete one of the following tasks:

This workaround causes the I/O status indicator to blink. Despite the blinking status indicator, there is no I/O fault.

Controller can Assert When Stopping an Axis That Is Executing an S-Curve Profile Jog (4913301, 4976159)
  
Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix™ 5370
20.011
38.011 and later
Compact GuardLogix® 5370
28.011
38.011 and later
ControlLogix® 5570
18.012
38.011 and later
GuardLogix 5570
20.011
38.011 and later
CompactLogix 5380
28.011
38.011 and later
Compact GuardLogix 5380 SIL 2
31.011
38.011 and later
Compact GuardLogix 5380 SIL 3
32.013
38.011 and later
CompactLogix 5380 Process
33.011
38.011 and later
CompactLogix 5480
32.011
38.011 and later
ControlLogix 5580
28.011
38.011 and later
GuardLogix 5580
31.011
38.011 and later
ControlLogix 5580 Process
33.011
38.011 and later

A controller assert can occur when a Motion Axis Stop (MAS) instruction is executed on the same axis that is concurrently executing an S-Curve Motion Axis Jog (MAJ) instruction.

Work arounds to consider:

• Change the MAJ profile from S-Curve to Trapezoidal.
or
• Add a condition to prevent MAS on an axis where MAJ with S-Curve profile is in progress; this would involve the axis .IP bit.

  

Axis Schedule Changes After Project Import and Download (00169297)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


An axis schedule can change when you import a Studio 5000 Logix Designer® application, versions 24 and 26, project into Logix Designer application, version 27.


Attribute Values Incorrect with Set System Value Instruction (00169713)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:

                                                    

When you use a Set System Variable (SSV) instruction to set the values for attributes available with the WallClockTime class, the values can be set incorrectly.



Wall Clock Value Different From Previous Value (00169756)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


After you set the wall clock for a controller, the actual time can be offset from the value that you set by approximately 2 seconds.

This anomaly occurs after Precision Time Protocol (PTP) is disabled in a controller that was previously synchronized with the grandmaster clock.



Cannot Save Firmware to Secure Digital Card (00170011)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers GuardLogix® 5570


The Load/Store button on the Nonvolatile Memory tab of the Controller Properties dialog can be disabled when the controller is online. As a result, you cannot save firmware to the Secure Digital (SD) card.



Expiration Times On a Logix Repository Record Can Differ (00171229)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


When the Logix Repository deletes a record, the cached value of the earliest expiration time and the actual expiration time value of the record can be different.



Unconnected Timeout Time Incorrect (00171872)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


The unconnected timeout time can be longer for a Forward Open service than expected.



Motion Run Axis Tuning Instruction Gets Stuck (00172234)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


A Motion Run Axis Tuning (MRAT) instruction can get stuck and the .IP (In Process) stays set to 1. This anomaly can occur when the MRAT instruction is used to command a motion module to run a tuning motion profile for an axis, the instruction



Media Space Calculation Incorrect with 3rd-party Secure Digital Cards (00175295)

Known Anomaly First Identified as of Firmware Revision 28.011

Catalog Numbers:


The media space calculation that is done to determine the available memory on a Secure Digital (SD) card can be incorrect with 3rd-party SD cards that are 4 GB or greater.

This anomaly does not occur when you use SD cards available from Rockwell Automation. That is, the 1784-SD1 and 1784-SD2 cards.

We recommend that you use the SD cards available from Rockwell Automation with your controller.

While other SD cards can be used with the controller, Rockwell Automation has not tested the use of those cards with the controller. If you use an SD card other than those cards that are available from Rockwell Automation, you can experience data corruption or loss.



Motion Instruction Interference Can Prevent Axis From Being Enabled (00175334)

Known Anomaly First Identified as of Firmware Revision 27.011

Catalog Numbers:


Intermittent execution of a Motion Group Shutdown Reset (MGSR) instruction and Motion Servo On (MSO) instructions can result in an error on the MSO instruction and failure to enable an axis.



Major Non-recoverable Fault on Safety Controller (00178080)

Known Anomaly First Identified as of Firmware Revision 28.011

Catalog Numbers GuardLogix® 5570


An oscillator diagnostic fault can cause a major non-recoverable fault on the controller. The diagnostic fault occurs as a result of the time that is elapsed between two oscillators is greater than 10%.


GuardLogix is a trademark of Rockwell Automation, Inc.

  

Safety Controller Can Fault and Incorrectly Enter Program Mode After Power Is Cycled (00172782)

Known Anomaly First Identified as of Firmware Revision 28.011

Catalog Numbers GuardLogix® 5570


After a powerup, the controller can experience a major non-recoverable fault (MNRF) and incorrectly enter Program mode instead of Run mode, as expected.

This anomaly occurs in the following conditions:

The revision is previous to revision 28, for example, firmware revision 26.


When the anomaly occurs, the controller experiences a fault of Type 14:Code 07 and the Safety Task is inoperable.

The anomaly resolution varies based on if the project uses a Safety Signature. For example, if a Safety Signature is used, there are two resolution options.

Safety Signature Is Applied to Project

Resolution # 1

  1. Clear the fault.
  2. Set the key to the desired mode, that is, Remote Run or Run mode.

Resolution # 2

  1. Cycle power to the controller again.
  2. Controller mode after the power cycle is determined by the mode before the power cycle and does not require user action:

Safety Signature Is Not Applied to Project

Resolution

  1. Cycle power to the controller.
  2. Controller mode before the power cycle determines the power mode after it:
  

PhaseManager™ and SequenceManager™ Show Different States of Phase in Program Mode (00183769)

Known Anomaly First Identified as of Firmware Revision 28.011

Catalog Numbers:

If the controller is switched to Program mode while a sequence and phase are running, the phase state changes to idle and displays idle, while the sequence continues to show running. On transition back to Run mode, the sequence displays inactive.


Controller Anomaly with Continuous Task, Indirect Addressing, and CONCAT or DTOS (1442602)

Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix™ 5370
29.011
Compact GuardLogix® 5370
29.011
ControlLogix® 5570
29.011
GuardLogix 5570
29.011
ControlLogix 5570 redundant
30.051


Controller applications with a continuous task with CONCAT or DTOS instructions where indirect addressing exists may result in a controller major nonrecoverable fault/assert when additional task(s) exist. See Knowledgebase Technote 5570/5370 Controller Anomaly with Continuous Task, Indirect Addressing and CONCAT or DTOS.


  

TSSM Instruction May Not Function as Documented (3343045, 3343050, 3343083, 3343105)

Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
Compact GuardLogix® 5370
28.011
37.011 and later
Compact GuardLogix® 5380 SIL 2
31.011
35.017, 36.014, 37.011 and later
Compact GuardLogix 5380 SIL 3
32.013
35.017, 36.014, 37.011 and later
GuardLogix 5560
17.008
GuardLogix 5570
20.011
37.011 and later
GuardLogix 5580
31.011
35.017, 36.014, 37.011 and later

The TSSM Muting Lamp (ML) output is enabled when Sensor 2 input transitions instead of waiting the configured TSSM S1S2-LC Min time.

For additional information, see Knowledgebase Article Unexpected TSSM Instruction Behaviour.





Controller Can Assert When Motion Instruction Accel And/Or Decel Operands Are Out of Range (3341103, 3453881, 3453882, 3453883, 3453889)
  
Controllers
First Known in Firmware Revision
Corrected in Firmware Revision
CompactLogix® 5370
20.011
37.011 and later
Compact GuardLogix® 5370
28.011
37.011 and later
ControlLogix® 5570
20.011
37.011 and later
GuardLogix 5570
20.011
37.011 and later
CompactLogix 5380
29.011
34.015, 35.014, 36.013, 37.011 and later
Compact GuardLogix 5380 SIL 2
31.011
34.015, 35.014, 36.013, 37.011 and later
Compact GuardLogix 5380 SIL 3
32.013
34.015, 35.014, 36.013, 37.011 and later
CompactLogix 5380 Process
33.011
34.015, 35.014, 36.013, 37.011 and later
CompactLogix 5480
32.011
34.015, 35.014, 36.013, 37.011 and later
ControlLogix 5580
28.011
34.015, 35.014, 36.013, 37.011 and later
GuardLogix 5580
31.011
34.015, 35.014, 36.013, 37.011 and later
ControlLogix 5580 Process
33.011
34.015, 35.014, 36.013, 37.011 and later

When MAM, MAJ, MCD, MAG, and MAS instruction Accel and/or Decel operands are near zero, a controller assert can occur.

For more information, see Knowledgebase Article Studio 5000® Motion Instruction Error Code 13 Accel and Decel out-of-range limits.


Application Notes

This release has the following application notes.

RunMode in GuardLogix Safety Produce Tag (Lgx00207807, Lgx00231800)
  
Controllers
Application Note First Identified in Firmware Revision
Compact GuardLogix® 5380 SIL 2
31.011
Compact GuardLogix 5380 SIL 3
32.013
GuardLogix 5580
31.011
Compact GuardLogix® 5370
28.011
GuardLogix 5570
20.011

When creating safety Produce and Consume tags, it is required to create a User-defined Data type (UDT), with the first element containing a tag of the CONNECTION_STATUS data type.
The CONNECTION_STATUS is used to monitor the RunMode state and the ConnectionFaulted state in the consuming controller.

The RunMode state will provide the mode of the Producing controller from within the Consuming tag’s data. The RunMode state does not provide unique values in the Producing tag’s data. To monitor the state of the Producing controller within the Producing controller’s logic, use a Get System Value (GSV), with the Object set to ControllerDevice and the Attribute set to Status.




Firmware Upgrade Guidelines for Safety Controllers

This application note applies to all firmware revisions of:

The IEC 61508 functional safety standard requires impact analysis before upgrading or modifying components in a certified, functional safety system. This release note provides high-level guidance on how you can perform the impact analysis for safety controller hardware/firmware upgrades. Reference the standard to make sure you fulfill all of the requirements as they relate to your application.
When you upgrade controller firmware to a newer version, consider the following:
For more controller-specific information, see one of the following:
Important: The 5580/5380 controllers have a different compiler than earlier controllers. You must revalidate that applications on earlier controllers compile correctly on 5580/5380 controllers.
For product change management guidelines and definitions of how Rockwell Automation manages product versions, see System Security Design Guidelines Reference Manual, SECURE-RM001.

For Example:
  1. From the Product Compatibility and Download Center:
    1. Review all firmware release notes, starting with the original firmware revision through the new firmware revision, to identify any changes that impact the safety-related implementation of the application.
    2. Review hardware and firmware compatibility to identify any restrictions between the original system components and the new system components.
  2. Perform a hazard and risk assessment for any changes identified during the impact analysis and determine what additional testing is necessary.
  3. Perform the online and offline edit process described in the safety reference manual for your controller. You can restrict the ‘Test the Application’ block to the testing identified by the hazard and risk assessment.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.