Release Notes

Free download of RSLinx Classic Lite
Version 4.31.00 (released 1/2023)

Catalog Number RSLinx Classic Lite (free) 

These release notes describe version information for RSLinx Classic Lite (free), version 4.31.00 (released 1/2023).

Requirements

This release has the following requirements.

RSLinx Classic version 4.31.00 (CPR 9 SR 13)

RSLinx Classic works within the system requirements of all Rockwell Automation® software products.

For the latest compatibility and driver support information, refer to the Rockwell Automation Product Compatibility and Download Center.

Hardware requirements

RSLinx Classic requires the following hardware:

Software requirements

RSLinx Classic has been tested on the following operating systems:

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Software compatibility

RSLinx Classic version 4.31.00 (CPR 9 SR 13) has been tested, and is compatible, with the following products:

RSLinx Classic version 4.31.00, Studio 5000 Logix Designer version 35.00.00, and device profiles that ship with Studio 5000 Logix Designer version 35.00.00 are not compatible with RSNetWorx version 9.00.00 or earlier. RSNetWorx and the DeviceNet Tag Generator must be upgraded to a version later than 9.00.00 prior to install these products.

Security requirements

To help meet secure system design requirements review these publications:

Features

This release includes the following system features.

There are no new features in RSLinx Classic version 4.31.00.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

There are no functional changes in RSLinx Classic version 4.31.00.

Application Notes

This release has the following application notes.

The following are the application notes for RSLinx Classic version 4.31.00.

Backup and restore

BOOTP/DHCP tool

Data Monitor

Data type

DDE/OPC

DF1 driver

DH+ and DH485

Driver certificate

EtherNet and EtherNet/IP

FactoryTalk Activation Manager

Hardware considerations

Impact of Microsoft deprecating VBScript

Installation

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Module statistics

No-interrupt configuration

Repair software

RSWho browse

Running mode

Security considerations

Server OPC Data (Local)

SLC

SmartGuard

SoftLogix

Unsolicited message

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ftsp-s
Specifies the FactoryTalk directory scope for restore. Only "Global" and "Local" scopes are supported.
This parameter is optional.
/ftsp-bak
Specifies the location where the restore file can be found.
This parameter is optional.
/ftsp-pp
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
/ftsp-value=enable/disable
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether or not a client computer account must exist in the directory to login.
This parameter is optional.
/DirectoryServer
Specifies the directory server name.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/InstallLocation="value"
Or
/InstallDrive="value"
Specifies the install location or install drive respectively.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/Uninstall
Use to uninstall RSLinx Classic. This parameter is optional.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_REBOOT_PENDING
3012
A restart is pending and is required before the installation can continue.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.

User account

User-defined type

User documentation

Certificates

The following certificates are installed while installing Rockwell Automation software.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.