Release Notes

FactoryTalk® Linx high performance communications software optimized for Logix5000 controllers. (included with FTSP)
Version 6.31.00 (released 11/2022)

Catalog Number FactoryTalk Linx (aka RSLinx Enterprise) 

These release notes describe version information for FactoryTalk Linx (aka RSLinx Enterprise), version 6.31.00 (released 11/2022).

Requirements

This release has the following requirements.

FactoryTalk Linx version 6.31.00 (CPR 9 SR 13)
FactoryTalk Linx works within the system requirements of all Rockwell Automation® software products.

For the latest compatibility and driver support information, refer to the Product Compatibility and Download Center.

Hardware requirements

FactoryTalk Linx recommends the following hardware for applications with typical data acquisition needs:

Lower level x86 based CPUs will also work in standalone configurations with reduced data acquisition needs.

For small applications, the following configuration was also evaluated:

It is recommended to run performance validation test on the planned computer hardware to ensure the desired capacity and performance can be achieved.

Software requirements

Operating systems

FactoryTalk Linx is tested on operating systems installed from original Microsoft® media only. FactoryTalk Linx runs on the 64-bit versions of the following Windows® operating systems:

For requirements specific to running FactoryTalk Linx within FactoryTalk View Studio, refer to the System requirements topic in the FactoryTalk View SE and FactoryTalk View ME Release Notes.

Software compatibility

FactoryTalk Linx version 6.31.00 has been tested with, and is compatible with, the following Rockwell Automation products:

Firmware requirements

To use the ControlNet communication feature with FactoryTalk Linx, the minimum requirements are:

To use the DeviceNet communication feature with FactoryTalk Linx, the minimum requirements are:

graphic
Note: FactoryTalk Linx also supports bridging from Ethernet (1756-ENxxx) to DeviceNet (1756-DNB) across a ControlLogix Chassis.
High Resolution Display Support

Windows 10 v1803 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display with scaling up to 125%.

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

Security Requirements

To help meet secure system design requirements, review these publications:

To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products Application Technique (publication SECURE-AT001).

Features

This release includes the following system features.

FactoryTalk Linx version 6.31.00 has the following new features:

New features
graphic
Tip: The remote server's IP address, remote server's display name, and driver name are not shown in FactoryTalk Administration Console.

Support for Concurrent Communication Protocol Enhancements

Feature

IMPORTANT:

If you update any part of the system before all versions and revisions are available to be upgraded at the same time, you will get error code 16#0008 Service Request Error: Unsupported service.

For more information, see section Error Codes below.

An attempt to install a Logix SIS Redundancy or GuardLogix 5580 controller application will result in error code 16#008 Service Request Error: Unsupported service. If you see this error with either of these applications, you cannot clear it until the required FLEXHA 5000 EtherNet/IP adapter and FLEXHA 5000 I/O module firmware revisions are available.


If you are using Concurrent Communication, your system must meet the following requirements:

Components
Software Version
Firmware Revision
Software
Studio 5000 Logix Designer®
37.00.00 or later
—
FactoryTalk® Linx
6.31.00 or later
—
ControlFLASH Plus™
5.00.00 or later
—
ControlLogix 5580 Redundancy System
ControlLogix 5580 controllers
—
37.011 or later
1756-EN4TR ControlLogix EtherNet/IP™ communication modules
—
7.001 or later
FLEXHA 5000 I/O System (5015)
FLEXHA 5000 EtherNet/IP adapter
—
3.011 or later
FLEXHA 5000 I/O modules
—
3.011 or later
  
Components
Software Version
Firmware Revision
Software
Studio 5000 Logix Designer
37.00.00 or later
—
FactoryTalk Linx
6.31.00 or later
—
ControlFLASH Plus
5.00.00 or later
—
ControlLogix 5580 System
ControlLogix 5580 controllers
—
37.011 or later
1756-EN4TR ControlLogix EtherNet/IP communication modules
—
7.001 or later
FLEXHA 5000 I/O System (5015)
FLEXHA 5000 EtherNet/IP adapter
—
3.011 or later
FLEXHA 5000 I/O modules
—
3.011 or later

  
  
Components
Software Version
Firmware Revision
Software
Studio 5000 Logix Designer
37.00.00 or later
—
FactoryTalk Linx
6.31.00 or later
—
ControlFLASH Plus
5.00.00 or later
—
Logix SIS Redundancy
GuardLogix® 5580 controllers
—
37.011 or later
1756-EN4TR ControlLogix EtherNet/IP communication modules
—
7.001 or later
FLEX 5000 Safety I/O System (5094)
FLEX 5000 EtherNet/IP adapter
—
6.011 or later
FLEX 5000 Safety I/O modules
—
Any
FLEXHA 5000 I/O System (5015)
FLEXHA 5000 EtherNet/IP adapter
—
3.011 or later
FLEXHA 5000 I/O modules
—
3.011 or later

IMPORTANT: You are not required to use both FLEX 5000 Safety I/O modules and FLEXHA 5000 I/O modules in Logix SIS Redundancy. The requirements are listed in case you use either or both.

  
Components
Software Version
Firmware Revision
Software
Studio 5000 Logix Designer
37.00.00 or later
—
FactoryTalk Linx
6.31.00 or later
—
ControlFLASH Plus
5.00.00 or later
—
GuardLogix 5580 System
GuardLogix 5580 controllers
—
37.011 or later
1756-EN4TR ControlLogix EtherNet/IP communication modules
—
7.001 or later
FLEX 5000 Safety I/O System (5094)
FLEX 5000 EtherNet/IP adapter
—
6.011 or later
FLEX 5000 Safety I/O modules
—
Any
FLEXHA 5000 I/O System (5015)
FLEXHA 5000 EtherNet/IP adapter
—
3.011 or later
FLEXHA 5000 I/O modules
—
3.011 or later

IMPORTANT: You are not required to use both FLEX 5000 Safety I/O modules and FLEXHA 5000 I/O modules in GuardLogix 5580 control systems. The requirements are listed in case you use either or both.


Error Code

If you attempt to upgrade or install a ControlLogix Redundancy System or ControlLogix 5580 controller application and see error code 16#0008 Service Request Error: Unsupported service, you must revert the system to the following software version and firmware revisions.

Component
Software Version
Firmware Revision
Studio 5000 Logix Designer® software
35 or 36 (all versions)
—
ControlLogix 5580 Redundancy System
or
ControlLogix 5580 controller
—
35 or 36 (all revisions)
1756-EN4TR ControlLogix EtherNet/IP communication modules
—
5 or 6 (all revisions)
FLEXHA 5000 EtherNet/IP adapter
—
 2 or earlier (all revisions)
FLEXHA 5000 I/O modules
—
2 or earlier (all revisions)


For more information, see the following:

  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk Linx version 6.31.00.

ASCII string convert modifier: SC##

The upper limit of the length of C style strings specifier (SC##) supported in FactoryTalk Linx is 400 bytes. The default upper limit value is SC30, and you can increase the upper limit manually.

Backup and restore
CIP connections
CIP Security
CIS Benchmarks test results

Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.

For more information about the guidelines and which products were tested against which CIS Benchmarks, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).

graphic
Note: If a product compliance with the benchmark is less than 100%, a link to a detailed spreadsheet is available. Download the spreadsheet to assist you in determining whether additional compensating controls are necessary.

FactoryTalk Linx version 6.31.00 has been tested on CIS Microsoft Windows 10 Enterprise (Release 21H2) Benchmark v1.12.0, CIS Microsoft Windows Server 2019 MS Benchmark v1.2.1, and CIS Microsoft Windows Server 2022 Benchmark v1.0.0.

Exceptions settings for FactoryTalk Linx version 6.31.00 are listed.

CIS Microsoft Windows 10 Enterprise (Release 21H2) Benchmark v1.12.0

Communication Setup editor
ControlNet I/O and DeviceNet I/O
Data access and tag browsing
DH+ limitations
EtherNet/IP compliance
ControlFLASH
FactoryTalk Alarms and Events
Fast User Switching
File Transfer Utility
Firmware Upgrade Wizard
Hardware and operating system

Impact of Microsoft deprecating VBScript

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Network Browser
Networks, drivers, and devices
Pass-through description
Predefined items
Remote I/O
Requestor’s subscription rate recommendation

In a FactoryTalk system, data moves from a source like a controller connected to FactoryTalk Linx to a software client when a data item’s value has changed. Once changes are detected, the data values are transferred between multiple components or services. The services use the subscription rate from the requestor to initiate a processing thread to transfer the data to its next destination in the system. Small processing delays by components, network delivery time, a high number of values changing at once, or a heavily loaded system can cause data to be processed and delivered slower than the requested rate. If the source data value changes faster than twice the subscription rate, a newer data value could likely overwrite a previous data value as it travels between the services.

In some cases, sampling at a rate faster than half of the speed of the value changes can help to ensure that data value changes are detected by the requester. Also, balancing the data subscriptions across multiple computers and services can reduce processing and delivery delays.

Shortcuts
Security considerations
System sizing recommendations
Component
Recommended guidelines
FactoryTalk Alarms and Events
 
FactoryTalk Alarms and Events servers per application
10 non-redundant servers or 10 redundant server pairs
FactoryTalk tag-based alarms per server
20,0001
Logix device-based alarms per server
10,0002
Total alarms per application
100,0003
FactoryTalk Linx
 
FactoryTalk Linx data servers per application
10 non-redundant servers or 10 redundant server pairs
Total device tags per application
1,000,0004
Tags per FactoryTalk Linx data server
100,0004
FactoryTalk View SE
 
HMI servers
10 non-redundant servers or 10 redundant server pairs
HMI tags per HMI Server
40,0005
Total data logged tags per HMI server (1-second scan rate)
5,000
FactoryTalk View SE client sessions simultaneously connected to the application
1204
FactoryTalk ViewPoint SE servers per application
4
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
50
  1. The number of alarm backing tags influences the maximum number of available alarms because they increase the resource requirements of the alarm server. When using backing tags for status and control, a good rule of thumb is to multiply the total number of backing tags by the total number of alarms, and ensure the result is less than 20,000. PlantPAx® users should refer to the PlantPAx Reference Manual PROCES-RM001 for alarm server sizing guidance for a PlantPAx application.
  2. This number is the sum of both instruction alarms and Logix tag-based alarms across all the controller shortcuts in each FactoryTalk Linx server.
  3. The total number of alarms per application includes all FactoryTalk Alarms and Events tag-based and device-based alarms in the application.
  4. Refer to Rockwell Automation Answer ID 1070902 to determine system scalability using this option.
  5. The maximum number of HMI tags that can be created on a single HMI server is 175,000. Extensive use of HMI tags has a significant performance impact on an HMI server, so Rockwell Automation recommends minimizing their use, and instead using direct-reference tags as much as possible.

Update Rate
Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows errors or restart messages.
When using this parameter, the installation will stop and display a prompt if there are errors or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/SetupLanguage="value"
Specifies which language will be displayed during the install process.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ftsp-s
Specifies the FactoryTalk directory scope for restore. Only "Global" and "Local" scopes are supported.
This parameter is optional.
/ftsp-bak
Specifies the location where the restore file can be found.
This parameter is optional.
/ftsp-pp
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
/ftsp-value=enable/disable
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether or not a client computer account must exist in the directory to log in.
This parameter is optional.
/FTSPWebAuth="value"
Specifies that the installation includes the FactoryTalk Web Authentication Server.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Web Authentication Server will be installed. The FactoryTalk Reverse Proxy will also be installed as it is required for operation of the FactoryTalk Web Authentication Server.
  • No
If the value is No, the FactoryTalk Web Authentication Server will not be installed.
/ReverseProxy="value"
Specifies that the installation includes the FactoryTalk Reverse Proxy.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Reverse Proxy will be installed.
  • No
If the value is No, the FactoryTalk Reverse Proxy will not be installed.
/FTSPWebEventServer="value"
Specifies that the installation includes the FactoryTalk Web Event Server.
This parameter is optional.
The value must be one of the following:
  • Yes
If the value is Yes, the FactoryTalk Web Event Server will be installed.
  • No
If the value is No, the FactoryTalk Web Event Server will not be installed.
/DirectoryServer
Specifies the directory server name.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/NoHTTPS
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/Repair
Runs a repair operation on the installed products.
This parameter is optional.
/InstallDrive="value"
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/Uninstall
Use to uninstall the product. This parameter is optional.

Examples

The following examples show how to use the installation commands.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was canceled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A restart is required to continue the installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restarting, the product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart is pending. Restart the computer to continue the installation.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.

Certificates

The following certificates are installed while installing Rockwell Automation software.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.