Release Notes

Logix Designer Compare and Merge Tool
Version 9.01.00 (released 10/2022)

Catalog Number Logix Designer Compare Tool 

These release notes describe version information for Logix Designer Compare Tool, version 9.01.00 (released 10/2022).

Requirements

This release has the following requirements.

Logix Designer Compare Tool version 9.01.00 (CPR 9 SR 13)

Logix Designer Compare Tool works within the system requirements of Studio 5000 Logix Designer. To see the system requirements of Studio 5000 Logix Designer, click Help > Release Notes, and then navigate to the System requirements topic.

For the latest compatibility information, refer to the Product Compatibility and Download Center.

Features

This release includes the following system features.

Logix Designer Compare Tool version 9.01.00 has the following enhanced features:

Corrected Anomalies in This Release

This release corrects the following anomalies.

The list identifies the anomalies corrected in Logix Designer Compare Tool version 9.01.00. Use the identification information provided in the anomaly heading to track the anomaly in future release or for reference when receiving assistance from Customer Support with a related issue.

Known Anomalies in This Release

This release has the following known anomalies.

Functional Changes

This release has the following functional changes from the previous release.

There are no functional changes for Logix Designer Compare Tool version 9.01.00.

Application Notes

This release has the following application notes.

The following are the application notes for Logix Designer Compare Tool version 9.01.00.

CIS Benchmarks test results

Rockwell Automation conducts tests using domain-joined computers configured according to CIS Benchmarks to help assure that software products perform as expected on computers that are hardened to industry best practices.

For more information about the guidelines and which products were tested against which CIS Benchmarks, see the Knowledgebase Document ID: QA63609 - Recommended guidelines for hardening software, computer, device, and network systems and infrastructure (CIS Benchmarks).

graphic
Note: If a product compliance with the benchmark is less than 100%, a link to a detailed spreadsheet is available. Download the spreadsheet to assist you in determining whether additional compensating controls are necessary.


4K resolution display support

If running Logix Designer Compare Tool with 4K resolution display, turn off fullscreen optimizations.

To turn off fullscreen optimizations, go to C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Rockwell Software\Logix Designer Tools, right-click Logix Designer Compare Tool, and then select Properties. In the Logix Designer Compare Tool Properties dialog box, select the Compatibility tab, and then select the Disable fullscreen optimizations checkbox.


Encrypted AOIs and routines comparison

The following table describes the different comparison results of license protected AIOs and routines with or without a license.

Projects
License protected components
Compare with a license
Compare without a license
Compact GuardLogix® 5370 Safety Controller, CompactLogix™ 5370 Controller, ControlLogix® 5570 Controller, and GuardLogix® 5570 Safety Controller projects
Routines or AOIs
The license protected routines or AOIs can be compared.
The comparison of license protected routines or AOIs will fail.
Compact GuardLogix 5380 Safety Controller, CompactLogix 5380 Controller, CompactLogix 5480 Controller, ControlLogix 5580 Controller, and GuardLogix 5580 Safety Controller projects
Routines
Locked
If the license protected routine only exists in one project, it will be marked as Content Protected in the compare result.
If the license protected routines of the same type exist in two projects, they will be treated as the same and will not show in the compare result.
The license protected routines will not be compared.
AOIs
Locked
If the license protected AOIs only exist in one project, it will be marked as Content Protected in the compare result.
If the license protected AOIs exist in two projects, the encrypted attributes will not be compared.
Routines or AOIs
Unlocked
The license protected routines or AOIs can be compared.
The comparison of license protected routines or AOIs will fail.


Unsupported Function Block Diagram instructions

The following FBD instructions are not supported:


VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.


Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation command-line parameters

This table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/InstallLocation="value"
Specifies the install location.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/AddLogixMenuItem="value"
Adds Compare Tool as a menu command in the Tools menu of Logix Designer. This is supported for Logix Designer version 13.00 or later.
This parameter is optional. The default value is 0, which specifies that Compare Tool will not be added as a menu command. Values except for 0 specify that Compare Tool will be added as a menu command.

Examples

These examples show how to use the installation commands.


Error codes

This table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A reboot is required to continue to installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_REBOOT_PENDING
3012
A restart is pending and is required before the installation can continue.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.



Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.