Release Notes

PanelView Plus 7 Performance (2711P-*9P) Firmware and compatibility that applies to all catalog items in this product line.
Version 12.104 (released 9/2022)

Catalog Number PanelView Plus 7 Performance (series B)

These release notes describe version information for PanelView Plus 7 Performance, version 12.104 (released 9/2022).

Requirements

This release has the following requirements.

2711P-PVP7 Performance 12.104 works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.

Hardware requirements

2711P-PVP7 Performance 12.104 requires the following hardware:

Component revisions

The following table identifies the new component revision information after 2711P-PVP7 Performance 12.104 is installed.

Components
Revisions
FactoryTalk View ME
12.00.77
FactoryTalk ViewPoint
12.00.05
FactoryTalk Services Platform
6.20.16
FactoryTalk Linx
6.20.35
Operating system
Windows 10 IoT Core Services 1809 v10.0.17763.1757
Platform revision
3.04.00
Fonts
2.00.00

Features

This release includes the following system features.

2711P-PVP7 Performance 12.104 has the following enhanced features.

Corrected Anomalies in This Release

This release corrects the following anomalies.

The list identifies the anomalies corrected in 2711P-PVP7 Performance 12.104.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

2711P-PVP7 Performance version 12.104 has no changes in functionality since the last release.

Application Notes

This release has the following application notes.

The following are the application notes for 2711P-PVP7 Performance 12.104.

How to get firmware updates?

Firmware Upgrade Packages are available from the Product Compatibility and Download Center. After signing in, a selection of updates will become available for download.

graphic

To get the firmware updates

  1. Select PanelView Plus 7 Performance and then select B.
  2. Select the version of the Firmware Upgrade Package and click Downloads.
  3. Click graphic and follow the web page instruction to complete the download.
    • If you update firmware via a USB storage device, download the CAB file.
    • If you update the firmware via ControlFLASH Plus or ControlFLASH, download the DMK file.
    graphic
    Tip: We don’t recommend using an SD card to update the firmware.

Rockwell Automation Knowledgebase Documents

Additional information regarding PanelView Plus 7 firmware updates can be found in Rockwell Automation Knowledgebase.

To locate pertinent documents, search using the keywords: "PanelView Plus 7", "PanelView Plus v7", "TOC", or "PVP7".

Unsupported features

The following features are not available in 2711P-PVP7 Performance 12.104:

For more information about the unsupported features, see PanelView Plus 7 Performance Series B* Terminals Important Information (publication 2711p-rn005).

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.