Release Notes

( 9324-RLDx ) RSLogix 5000 programming software. All you need for discrete, process, batch, motion, safety etc.
Version 20.06.00 (released 10/2022)

Catalog Number RSLogix 5000 

These release notes describe version information for RSLogix 5000, version 20.06.00 (released 10/2022).

Requirements

This release has the following requirements.

 System requirements for Logix Designer v20.06

For optimal performance of the RSLogix 5000 software, the personal computer should meet or exceed these hardware and software requirements.

graphic
Tip: The RSLogix 5000 software can be installed on a personal computer that meets the operating system minimum requirements, but may not meet performance expectations when used in a production system.
Hardware Requirements
Software Requirements
Important:
Keep these operating system considerations in mind:
  • Universal C Runtime (CRT) is a Windows operating system component that enables core functionality on the Windows operating system. It was introduced in Windows 10 and distributed to most computers running earlier supported operating systems. This component is present on computers that have been kept up to date.
When installing the RSLogix 5000 software on computers that have not been updated, a prompt displays to install Universal C Runtime or to update the computer to at least the Microsoft April 2014 update roll-up.
  • While the Windows 8.1 operating system runs on many touch-enabled devices, various features of the RSLogix 5000 software may not be touch-enabled. Most functions are expected to work with touch, but the software has only been tested with a keyboard and mouse.
  • RSLogix 5000 was tested with UAC set to the most restrictive level (Always notify). This version of the RSLogix 5000 software is also expected to operate correctly when UAC is configured for any less restrictive setting.
  
  
graphic
Note: The RSLogix 5000 software version 20.06 does not support SoftLogix.

Firmware requirements
To check and download the firmware compatible with this version of the RSLogix 5000 software, use the Product Compatibility and Download Center (http://compatibility.rockwellautomation.com/Pages/MultiProductDownload.aspx?crumb=112).
graphic
Tip: Most modules use Flash-ROM for the storage of firmware. If a module requires a firmware change, use the ControlFLASH™ tool to perform the update to the Flash-ROM. It is contained in the downloaded image or on a DVD-ROM shipped with the RSLogix 5000 software. Another option is to update the firmware automatically as part of the project download.
For additional information and assistance in performing a Flash-ROM update, review the ControlFLASH Firmware Upgrade Software User Manual, publication 1756-UM105.

Features

This release includes the following system features.

System features for Logix Designer v20.06

RSLogix 5000 software version v20.06 has no new features.

Corrected Anomalies in This Release

This release corrects the following anomalies.

Fatal error can occur when editing an RLL rung using ASCII Editor offline (1244059)

Attempting to delete a rung when online without accepting the edits and then going offline and attempting to accept the edits, puts the rung in an error state but does not delete the rung. Attempting to delete the rung code causes the RSLogix 5000 application to crash.

This anomaly first identified in version 32.04.

Tag does not reference valid reference or target (1241943)

When editing the Type and Data Type values in the Tag Properties dialog in a safety project, applying the changes causes an error Failed to modify the properties of the <project_name>. Tag doesn't reference valid object or target.

This anomaly first identified in version 32.00.

Unexplained motion (1090045, 1090058)

Unexplained motion possibly caused by the application not recognizing the motion database which could cause the motion configuration to change.

This anomaly first identified in version 12.00.

FactoryTalk Activation component causing incompatibility with Stratus (990492)

FactoryTalk Activation component delivered with RSLogix 5000 application v20.05 is incompatible with Stratus solutions. 

This anomaly first identified in version 20.00.

AssetCentre Backup and Compare tasks (942415, 981951, 981960, 1600636, 1170050, Lgx00225888)

AssetCentre Backup and Compare tasks run from one to several days without errors but will then start to receive the error *** RETRY *** - Event (0001) Done - State:256 Status: Logix 5000 Error: Failed to open file <file_name>. ExtErr" Could not CoCreate RSLogix5000Services. Please re-install Logix5000.

This anomaly first identified in version 20.01.

Known Anomalies in This Release

This release has the following known anomalies.

Brand name error on Installation Summary page (1811984)

The Installation Summary page for v20.06 inaccurately states the product name as Studio 5000. It should state the product name as RSLogix 5000.

This anomaly first identified in version 20.06.

Inaccurate size reported for install (1557642, 1822740)

Installing the <rslx5kt> software on a disk other than the C drive causes an inaccurate reporting of the estimated gigabytes required to install the application and the used gigabytes after the installation is complete. The installation fails if there is not enough free space on the C drive, but a warning message does not display to inform you that the installation failed.

This anomaly first identified in version 20.06.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

GDI Object Leaks, Child Windows (x66929)

Anomaly

First identified in RSLogix 5000 Software 16.x


Repeatedly opening and closing child windows may cause the number of graphics device interface (GDI) objects to increase when running RSLogix 5000 on Windows XP SP2 or on Windows Server 2003 with the Themes service started. Example child windows include, but are not limited to: the Controller Properties dialog, the Ladder Routine window, and the SFC Routine window. The leaks are minor in nature, but it is possible that unpredictable behavior can occur if the number GDI objects gets excessively high. This issue is documented in the Microsoft Knowledgebase article http://support.microsoft.com/?kbid=319740, which also provides instructions for obtaining a supported hotfix from Microsoft. A temporary work-around is to set the display properties to Windows Classic Theme.

Corrected

Blank Primary Window (Lgx0039239)

Anomaly

RSLogix 5000 Software 16.x


If you have a primary help window displayed and you open a help topic which displays a secondary window, the primary window may become blank. This is the result of a problem with the Windows Help compiler. To display the original topic, click Help Topics and re-select the original topic.

Unicode Characters, Does Not Display (Lgx00063773)

Anomaly

RSLogix 5000 Software 16.x


When the description of a task, program, routine, module, trend, etc. is edited, any audit records displayed using RSMACC Audit will not properly display Unicode characters.

Inserting Unicode Characters (Lgx00059649, Lgx00059650, Lgx00059825)

Anomaly

RSLogix 5000 Software 16.x


RSLogix 5000 employs a feature which allows the user to position the caret on an edit control and, without explicitly opening the edit control, to begin entering character data from the keyboard. This action will cause RSLogix 5000 to automatically open that edit control as character data entry continues. For many of the edit controls in RSLogix 5000, using this auto-open feature when inputting Unicode characters using an Input Method Editor (IME) will result in unexpected behavior or in a Fatal Error. 

To avoid this Fatal Error when entering Unicode characters, the edit control should be explicitly opened before beginning to enter character data from the keyboard. In most cases, pressing [Enter] on the keyboard will open the edit control which has the caret. In other cases, a single click or double click of the mouse is required. 

When using an IME to input Unicode characters, if the small IME character input dialog appears in the upper left corner of the display, then you have started to input a Unicode character string with no edit control opened. When this occurs, you can press [Esc] on the keyboard to cancel the input and then open the desired edit control before entering the Unicode character string.

User-Defined Data Type Size Limits (x03090, x06296)

Anomaly

RSLogix 5000 Software 16.x


You may not create a data type with more than 512 members either by editing in the Data Type Editor or by importing from an .L5K file. An individual UDT member may be an array with more than 512 elements.

Associated Tag, Non-Recoverable  (x77626)

Anomaly

RSLogix 5000 Software 16.x


In RSLogix 5000 V16.03, the ability to edit the Associated Tag configuration for analog and digital alarm tags has been enabled. If an alarm tag is referenced in executing logic, any attempt while online to remove an Associated Tag for that alarm tag may result in a Major Non-Recoverable Fault in the controller.

Module: Modify Properties (Lgx00072088)

Anomaly

RSLogix 5000 Software 16.x


With the security action “Motion: Modify Configuration” granted, you should be allowed to modify the motion configuration. You are allowed to change the axis association to a module from the Axis Properties dialog but are erroneously prevented from making this change from the Module Properties dialog. To allow the axis association to be configured on the Module Properties dialog, grant access for the security action “Module: Modify Properties”. This will enable all of the tabs of the Module Properties dialog, including the Axis Association tab.

Hardware Overtravel Fault (x66998)

Anomaly

RSLogix 5000 Software 16.x


For Kinetix 6000 axes configured in RSLogix 5000, if you have both Soft Overtravel and Hardware Overtravel Limits enabled, and you configure the Soft Overtravel Fault Action as "Status Only", be aware that a Hardware Overtravel Fault Action configured for "Stop Motion" may not "Stop Motion" due to the two faults existing together and the first fault action being set to "Status Only". For more information refer to Technical Note: ID=36709 "2094 Kinetix 6000; Soft Overtravel triggers first then sequential hard overtravel does not stop motion", and Technical Note: ID=21500 "How do I get off a Soft Overtravel?"

SERCOS Ring Phase Up (x43750, x43870, x44775)

Anomaly

RSLogix 5000 Software 16.x


If a motion Axis_Servo_Drive axis is configured with a Loop Configuration using auxiliary feedback, there are 3 choices for the units for Drive Counts per: Aux Rev, Aux Inch, Aux Millimeter. Only the default Aux Rev is valid for RA SERCOS Drives. Selecting Aux Inch or Aux Millimeter will cause a SERCOS Ring phase up fault at Phase 3. The SERCOS Fault reported will be “Position Data Scaling – Invalid attribute value”. To workaround the problem, select Aux Rev as the units when configuring a Loop Configuration using Dual/Auxiliary feedback.

Windows Vista Operating System (x81660)

Anomaly

RSLogix 5000 Software 17.x


There are a number of issues related to compatibility of RSLogix 5000 software with the Windows Vista operating system. The most significant of these includes the following:

  1. Although RSLogix 5000 software versions earlier than version 17 can be installed, they are not supported on Windows Vista operating systems.
  2. Although RSLogix 5000 software version 18 is supported with User Account Control (UAC) turned on, RSLogix 5000 software version 17 is supported only with UAC turned off.
  3. On some properties dialog boxes, there is no indicator shown when a control has focus. A workaround to display focus indicators is to select the Windows Vista setting to ‘Underline keyboard shortcuts and access keys’. Access this setting by using Personalize>Ease of Access>Make the keyboard easier to use>Underline keyboard shortcuts and access keys. (x113166)
  4. The 1784-PCIC(S) driver must be at version 4.06.01 or later. This driver is installed when RSLinx software is installed.


  

Operands Missing V17 (x80000)

Anomaly

First identified in RSLogix 5000 Software 17.x


Additional operands are required for the MCLM, MCCM, MCCD, and MCS Coordinated Motion instructions in Structured Text as part of the Multi-Axis Programmable Jerk feature introduced in version 17 of RSLogix 5000 software. When porting any of these instructions to version 17 from an earlier version of RSLogix 5000 software using copy and paste or drag and drop, the new operands are not automatically inserted This results in instructions that will not verify. When this occurs, it is necessary to make the appropriate corrections to the pasted instruction. Note that this anomaly does not exist for converted or imported projects. A suitable work-around for Structured Text instructions may be to use Routine Copy of Structured Text.

Emulated Controller, Select Slot 0(x79666)

Anomaly

RSLogix 5000 Software 17.x


RSLogix 5000 software does not support selection of slot 0 for an RSLogix Emulate 5000 Controller. If you need to emulate a controller in slot 0, you can perform the following steps:

1. With your emulator project open in RSLogix 5000 software, from the File menu choose Save As to export the project to an .L5K file.

2. Launch a text editor (for example, Notepad), and open the .L5K file.

3. Scroll through the content of the .L5K file until you find the MODULE Local section for the Emulator.

4. Locate the Slot entry, and change the value from its current slot value to slot 0 and save the file.

5. In RSLogix 5000 software, import the edited .L5K file.

You can now configure a controller in slot 0 in RSLogix Emulate 5000 software and then download your Emulator project.


Note that this workaround requires that RSLinx Classic software version 2.54.00 or later be used.

Tip: If you change the slot position of the emulator controller on the Controller Properties dialog box to a slot position other than slot 0, you cannot later return the slot position to 0 on the Controller Properties dialog box. To obtain these results, you must repeat the steps defined above. This also applies if you convert from a physical controller to an emulated controller.

Unable to Enable Security (x107466)

Anomaly

RSLogix 5000 18.x


The SetSecKeys tool included with RSLogix 5000 software version 17 and earlier do not work with User Account Control (UAC) turned on. When a SetSecKeys tool earlier than file version 18.0.0.0 is executed with UAC turned on, security appears to be enabled, yet security remains disabled in RSLogix 5000 software. If a version of SetSecKeys earlier than file version 18.0.0.0 is used inadvertently, SetSecKeys file versions 18.0.0.0 and later can still be used to enable security. (Note that depending on the operating system, the file version of SetSecKeys.exe can be viewed on either the Details tab or the Version tab of the File Properties dialog box.)

 

Slow Launch Times (x125369)

Anomaly

RSLogix 5000 Software 20.x


When RSLogix 5000 software is launched for the first time after restarting your personal computer, it may take 1 to 3 minutes for RSLogix 5000 software to be available for use. This behavior is also exhibited when launching FactoryTalk Administration Console or any other product that uses FactoryTalk Services Platform. Note that subsequent launches of these applications will not experience this behavior. This is only observed on the first launch of the application after a restart of the personal computer. If you experience launch times significantly longer than 3 minutes, refer to the firewall configuration settings in Tech Note #29402

Windows 7 Operating Systems (x111504, x113166, v124864)

Anomaly

RSLogix 5000 19.x


There are a number of issues related to compatibility of RSLogix 5000 software with the Windows 7 operating system. The most significant of these includes the following:

New EDS File Not Displayed (Lgx00124959)

Anomaly

RSLogix 5000 20.x


When a new EDS file is registered from outside RSLogix 5000 software, when RSLogix 5000 software is not running and RSLinx Classic software is running as an application (as opposed to as a service), then the newly registered device will not be available in the Select Module Type dialog box. Note that there is no problem with display of the device when registered outside of RSLogix 5000 software, provided that you first exit the RSLogix 5000 application and shut down the RSLinx Classic application. There is also no problem with display of the device when registered from within the RSLogix 5000 application (such as when using the “ Tools>EDS Hardware Installation Tool” menu). So, if the registered module is not displayed, you can use the “ Tools>EDS Hardware Installation Tool” menu to register the device again.

XML Full Project (x114197)

Anomaly

RSLogix 5000 20.x


Unable to Open Full Project XML Format File (.L5X) for Project File of Later Version of RSLogix 5000 Software than is Being Executed.

When attempting to open a full project xml format file (.L5X), an error may be reported indicating "Controller Revision not supported". This will occur when the major revision of the xml format file being opened is later than the revision of RSLogix 5000 software being executed.

 

For example, when executing RSLogix 5000 software version 19, an attempt to open an xml format file for version 20 will report the error. However, when executing RSLogix 5000 software version 20, an attempt to open an xml format file for version 19 will not exhibit the problem. When this error is observed, first switch to the RSLogix 5000 software version for the xml format file, and then open the file. This problem does not affect L5K or ACD files. (x114197)




 

"Log On to FactoryTalk" Displayed (Lgx00124955)

Corrected Anomaly with Studio 5000 Logix Designer 24.01

Known Anomaly First Identified as of  RSLogix 5000 20.x

When launching RSLogix 5000 software, the "Log On to FactoryTalk" dialog box may be displayed.

This dialog box may be seen when you do not have Administrator privileges on the personal computer and the current user does not exist in the FactoryTalk directory. If this dialog box is cancelled, the RSLogix 5000 software will not be launched. When the dialog box is displayed, entering the credentials for a user that exists in the FactoryTalk Directory will allow RSLogix 5000 software to be launched. Administrator accounts are included in the FactoryTalk Directory by default.

To avoid seeing this dialog box, you can add the current user or user group to the FactoryTalk directory. Follow these steps to add a user or user group to the FactoryTalk directory:

The "Log On to FactoryTalk" dialog bax may also be displayed when using Remote Desktop to connect to the personal computer that is running RSLogix 5000 software. This is due to FactoryTalk Security not recognizing the computer name. To enable access through Remote Desktop for a specific computer, you should add the name of the computer that is initiating the Remote Desktop connection to the "Network\System\Computers and Groups\Computers" folder in the FactoryTalk Administration Console. To allow remote computers to connect using the name of the host computer, open the FactoryTalk Administration Console and log in to the Network directory using your domain credentials. Then navigate to "Network\System\Policies\Security Policy". In the "Computer Policy Settings" section, set "Identify terminal server clients using the name of" to "Server Computer". To allow all computers to connect, set the value of "Require Computer accounts for all client machines" to disabled.

Note that if "Use single sign-on" is set to "disable" in FactoryTalk software, then the "Log on to FactoryTalk" dialog box will be displayed each time RSLogix 5000 software is launched and proper user credentials must be entered in order to continue. (By default, "Use single sign-on" is set to "enable".)

RSNetWorx Software Cannot Download to Controller (Lgx00124236)

Anomaly

RSLogix 5000 Software 20.x


When attempting to download a project using RSNetWorx software, if the controller firmware is at revision 20 and the controller is in Remote Run mode, then RSNetWorx software will not be able to change the controller mode in order to download. In this case, the controller mode must be changed either by using the keyswitch or by using RSLogix 5000 software version 20.

RSLogix 5000 Software Unresponsive (x129306)

Anomaly

RSLogix 5000 Software 20.x


When the server hosting the FactoryTalk Directory is restarted, RSLogix 5000 software may become unresponsive for about 3-5 minutes. When FactoryTalk Services then become available, RSLogix 5000 software will resume normal operation. 

CIP Path Displayed Using AutoFLASH (x124629, x124918)

Anomaly

RSLogix 5000 20.x


When using AutoFLASH to update firmware, a progress dialog box is presented to you during the update. This progress dialog box shows the communication path as ASCII values for the CIP path instead of displaying it in the typical display format such as "AB_ETH-1\10.20.30.40\Backplane\3". This path format is also shown in Audit log messages.






 

Long Timeout (x125029, x125045)

Anomaly

First identified in RSLogix 5000 20.x


When a PowerFlex 755 drive loses power during a firmware supervisor update, it can take over 10 minutes for RSLogix 5000 software to report the time out. Once the connection to the powered-up PowerFlex 755 drive has been restored, the firmware supervisor will then successfully update the drive's firmware.

References In Program Logic Will Not Update (x125220)

Anomaly

RSLogix 5000 20.x


If a project for a CompactLogix controller that is no longer supported is imported as a controller that has expansion I/O, any expansion I/O modules from the original controller are properly moved to the correct expansion slot; however, the references in program logic will not be correspondingly updated. This does not necessarily result in the program failing to verify. Instead, the logic may now be referencing the embedded modules for this controller. This is a problem only when opening a L5K or L5X project file. The references are properly adjusted when opening an ACD file.


Miscellaneous Known Anomalies V20

Anomaly
Logix Firmware/RSLogix 5000 Software 20.x
  
CIP-Axis effective resolution can get negative number (Lgx00136012)

Corrected Anomaly with Studio 5000 Logix Designer 24.01

On CIP-axis:

the associated Feedback attributes, (in Offline Configuration of Feedback Device) are:   

You can edit or enter these attributes in Offline Configuration of Feedback Device:

Revision |    values     |    Res      *    Interp     | =  effective
V18.00   | Defaults     |   1024     *    2048       |=  2097152          StartUp=[Incremental]
V18.00    | by hand     |   1024     *   2097152  | = 2147483648  
V18.00    | by hand     |   131072 *   10000000 | = 10240000000   (7 0's)

Revision  |    values     |    Res      *    Interp     | =  effective
V19.01    | Defaults     |   1024     *    2048       |=  2097152          StartUp=[Absolute]
V19.01    | by hand     |   1024     *   2097152   | = -2147483648    
V19.00    | by hand     |   131072 *   10000000 | = -2071986176   (7 0's)

Web-based Add-on Profiles launch as blank or empty windows with one or multiple instances of Logix Designer running on one PC (5582938, 5766864)

If a space exists in a Windows username and/or the user shell folder path, web-based user interface profiles will launch as an empty window under either of the following conditions:

This anomaly will be resolved in an upcoming release of Logix Designer Add-on Profiles.

This anomaly first identified in version 20.05.

Output data remains high for inhibited modules during testing (Lgx00177604)

Corrected Anomaly with Studio 5000 Logix Designer v29.00

Output data remains high for inhibited modules during testing.
This anomaly first identified in version 20.01.02.

Errors logged in the Logix Compare Tool and FTAC when running a compare (1170050, Lgx00225888)

When running the Logix Designer Compare Tool or FactoryTalk AssetCentre, the following errors can be logged:

This anomaly is caused by a component of Logix Designer, RSLogix5000Services.exe.

Note this anomaly will only occur with V20.05.00 of the Logix Designer application.

Refer to Knowledgebase document 1129863 for more information.

FactoryTalk AssetCentre error caused by the Logix Designer application (961951, Lgx00225888)

The following error will appear in FactoryTalk AssetCentre: "ExtErr: Could not CoCreate RSLogix5000Services. Please re-install Logix5000." 

This anomaly is caused by a component of the Logix Designer application, RSLogix5000Services.exe, experiencing a fatal error during the compare operation. (View this error in the Windows Event Logs).

While the error in FactoryTalk AssetCentre can affect all asset versions, the version of software causing the error will be apparent in the Windows Event Logs.

This anomaly first identified in version 20.04.

Please refer to Knowledgebase document 1129799 for more information.

Disable Download Project Documentation and Extended Properties features

To include or exclude project documentation and extended properties from a downloaded project, select or clear the


Fatal error can occur when an RLL rung is edited using ASCII Editor offline (1244044)

When the ASCII Editor is used to edit a rung where previously an online pending delete rung edit was accepted offline for the same rung, a fatal error occurs.

This anomaly first identified in version 20.00.




  

Unexplained motion (1090045)

Unexplained motion possibly caused by the application not recognizing the motion database which could cause the motion configuration to change.

This anomaly first identified in version 12.00.
  
Add-On Instruction tag members copied incorrectly (Lgx00217794)

Some PlantPAx P_PIDE Add-On Instruction instance values were set to denormalized low REAL values upon import of a P_PIDE 4.00.00 Add-On Instruction into a project that contained a P_PIDE 3.5.xx Add-On Instruction.

This anomaly first identified in version 18.00.

  
Invalid Add-On Instruction after upload - multi-dimensioned Add-On Instruction parameter tag (Lgx00224252)

After an Add-On Instruction was downloaded, uploading the project caused one of the Add-On Instruction's multi-dimensioned array parameter tag to become invalid. The Logix Designer application generated the error: USER_CONTROL, op errand 1: Invalid size of array. Argument must match number of dimensions.

This anomaly first identified in version 20.04.

  
BOOL tags did not retain value (Lgx00226143)

After changing a BOOL tag value to Decimal, and then saving, closing, and reopening the project file, the value had reset to Float. A BOOL tag reset to Float disabled manual changing of the value between 0 and 1.

This anomaly first identified in version 20.00.

  
Fatal error converting v20 project (Lgx00200539)

Trying to upgrade the project in the Controller Properties dialog box, from v20.00.00 to v30.00.00, maintaining the same controller, causes a fatal error.

This anomaly first identified in v20.01.




  
Export Add-On Instruction fails to parse on import (Lgx00200761)

Attempting to import some Add-On Instructions into an existing project generates the error message: Failed to import <file name>. Unable to parse the L5X content.

This anomaly first identified in version 17.00.

To work around this issue, export the Add-On Instruction, modify the file description to remove dashes. Or, open the L5X file in a plain text editor and modify the description to remove dashes. Import the Add-On Instruction.

Update Studio 5000 Logix Designer to support MSXML for DfS compliance (Lgx00193996)

The Logix Designer application has been upgraded to a version of MSXML that is supported by Microsoft.

This anomaly first identified in version 20.01.

Changing an Add-On Instruction alias parameter to a base tag can result in unexpected tag values (Lgx00214079, Lgx00217794)

This sequence of events can result in unexpected tag values:

1. An Add-On Instruction contains an alias parameter that points to a member of a local tag.

2. The alias parameter is changed to a base tag, either by editing the AOI definition directly or by importing a modified Add-On Instruction that overwrites the existing Add-On Instruction.

3. The instance values for the previously aliased parameters now contains unexpected values.

This anomaly first identified in version 18.00.

Follow one of these steps to work around the issue:

Installing v30.00 or the v30.00 AOP Bundle and adding ENBT, ENT2T, or EN2TR modules causes fatal error (Lgx00210565)

After installing version 30.00 or the version 30.00 AOP Bundle, adding an ENBT, ENT2T or EN2TR module causes a fatal error.

This anomaly first identified in version 20.00.

Cross Reference function causes fatal error (Lgx00209066)

Attempting to search a tag’s cross-reference multiple times may cause the software to crash.

This anomaly first identified in version 20.04.

The Logix Designer application stopped performing after multiple cross reference tasks (Lgx00208988)

After performing multiple cross reference tasks and closing the window after tasks, the Logix Designer application stopped performing with error 0xc0000005.

This anomaly first identified in version 20.01.

Adding a new case selection in a Structured Text routine (Lgx00166840)

Adding a new case selection in a Structured Text routine can cause the Logix Designer application to shut down.

This anomaly first identified in version 20.03.

Output Cam editor with UDT alias causes a crash when you click Apply (Lgx00161890)

When using the Output CAM Editor to make changes to an Output CAM that contains an Alias Tag, you will get a fatal error when you click Apply within the editor. The work around is to use the direct address for the Output CAM operand of the MAOC rather than the alias tag.

This anomaly first identified in version 20.01.

Unicode Characters, Does Not Display (Lgx00063773)

When the description of a task, program, routine, module, trend, or another component is edited, any audit records displayed using RSMACC Audit will not properly display Unicode characters.
This anomaly first identified in version 15.00.
  

Slow Launch Times (Lgx00125369)

When RSLogix 5000 software is launched for the first time after restarting your personal computer, it may take 1 to 3 minutes for RSLogix 5000 software to be available for use. This behavior is also exhibited when launching FactoryTalk Administration Console or any other product that uses FactoryTalk Services Platform.

Note that subsequent launches of these applications will not experience this behavior. This is only observed on the first launch of the application after a restart of the personal computer. If you experience launch times significantly longer than 3 minutes, refer to the firewall configuration settings in TechNote #29402.

This anomaly first identified in version 20.00.
  

Long Timeout (Lgx00125029, Lgx00125045)

When a PowerFlex 755 drive loses power during a firmware supervisor update, it can take over 10 minutes for RSLogix 5000 software to report the time out.

Once the connection to the powered-up PowerFlex 755 drive has been restored, the firmware supervisor will then successfully update the drive's firmware.

This anomaly first identified in version 20.00.

  

References In Program Logic Will Not Update (Lgx00125220)

If a project for a CompactLogix controller that is no longer supported is imported as a controller that has expansion I/O, any expansion I/O modules from the original controller are properly moved to the correct expansion slot; however, the references in program logic will not be correspondingly updated. This does not necessarily result in the program failing to verify. Instead, the logic may now be referencing the embedded modules for this controller. This is a problem only when opening a L5K or L5X project file. The references are properly adjusted when opening an ACD file.
This anomaly first identified in version 17.01.

Undefined Tag error (Lgx00190787)

Undefined Tag error displays when spaces are used between commas in the Ladder Editor. Spaces between commas are no longer needed.

This anomaly first identified in version 20.04.02.

Failed to create module library, not registered (Lgx00203463)

Failed to create module library in a project that uses the 1768-L45 controller. The 1768-L45 controller is no longer a supported controller.
This anomaly first identified in version 20.04.02.


  

Vendor specific error code (Lgx00137897)

When the controller attempts to open a connection with a 3rd-party device on EtherNet/IP, it causes the device to return a vendor specific error (0x01, 0x320). This error code is interpreted incorrectly in the Logix Designer application Module Properties dialog box, Connection tab.
This anomaly first identified in version 20.01.02.

Allow Unicast Consumer Connections check box (Lgx00159102)

When offline in the Logix Designer application, the Allow Unicast Consumer Connections check box clears or resets itself when changing the Max Consumers value of a safety product tag for the 1756-L73S/A controller, firmware version 20.01.00. This does not occur when modifying a standard product tag.
This anomaly first identified in version 20.01.02.

L1 Controller embedded I/O module firmware (Lgx00127607)

For the L1 controller, the controller’s embedded I/O module firmware may not be updated due to a corrupt embedded I/O module firmware image. For more information, see Rockwell Automation Knowledgebase document 498109.

This anomaly first identified in version 20.01.02.

Drive run at small coarse update period (Lgx00132326)

When the drive is running at small coarse update period such that late or lost Drive-to-Controller (D2C) updates are being seen, the Logix controller extrapolates the actual position during the lost D2C updates. The extrapolation algorithm computed the actual position incorrectly that resulted in incorrect velocity. If the actual velocity is plotted, you will see velocity spikes during lost D2C updates.

This anomaly first identified in version 20.01.02.

L1 Controller remove or insert local expansion POINT I/O modules (Lgx00131054)

For the L1 controller, if you remove or insert local expansion POINT I/O modules while under power, you can cause the controller to experience a Major Non-recoverable fault.

This anomaly first identified in version 20.05.00.

RUN LED on controller shows wrong state (Lgx00133064)

RUN LED on controller shows wrong state if you overload the system with very fast RPI limits on a CompactLogix controller that is communicating with SDN modules. It may cause the Run LED to incorrectly report Run mode when the controller has not finished its transition to the new mode. If this happens, cycle power to the controller and switch to Program mode when power is applied. 

This anomaly first identified in version 20.00.03.

RSLogix 5000 reports fatal error in Ladder instruction (Lgx00125908)

RSLogix 5000 reports a Fatal Error while typing in the tag operand field of a Ladder instruction.

This anomaly first identified in version 19.01.00. 

Fatal error on rung edited online (Lgx00127957)

A Fatal Error is reported when performing a copy and paste operation on a rung that is being edited while online.

This anomaly first identified in version 17.01.01.

Imported routine fatal error (Lgx00128439)

After configuring the import of a routine, if a tag is renamed and the Show differences only Data Comparison option is selected, a Fatal Error could be reported when the routine is imported.

This anomaly first identified in version 20.00.03.

Component tag deletion causes fatal error (Lgx00129693)

When attempting to delete a component of a tag, such as an array element or a structure member, a dialog box is displayed asking users if they wish to delete the entire tag. Clicking No results in a Fatal Error.

This anomaly first identified in version 20.00.03.

Fatal error searching for forces (Lgx00133070)

A Fatal Error can be reported when searching for forces in logic.

This anomaly first identified in version 19.01.00.

Safety modules fail to instantiate after installation of Ethernet module AOP profile 10.00.3664 (Lgx00170167)

Corrected Anomaly with Studio 5000 Logix Designer v29.00

After installing Ethernet module AOP profile 10.00.3664, safety modules fail to instantiate.
This anomaly first identified in version 17.01.01.

Tool tip for undefined tag in Ladder Editor needs improvement (Lgx00176367)

Corrected Anomaly with Studio 5000 Logix Designer v29.00

The tool tip for an undefined tag in the Ladder Editor needs improvement.
This anomaly first identified in version 20.01.02.

Tool tip for Dest FAL instruction indicates an undefined tag (Lgx00176367)

Corrected Anomaly with Studio 5000 Logix Designer v29.00

The tool tip for the Dest FAL instruction indicates an undefined tag.
This anomaly first identified in version 20.01.02.

Safety Lock LED sometimes fails to show correct status after you restore project from SD card (Lgx00178417)

Corrected Anomaly with Studio 5000 Logix Designer v29.00

The Safety Lock LED sometimes fails to show the correct status after you restore a project from the SD card.
This anomaly first identified in version 20.01.02.

Fatal error when converting a project to a newer major revision (1476922)]]]
A fatal error sometimes occurs when converting a project to a newer major revision where issues exist in the ChangeLog.
To work around this issue, export from the older project to a .L5K or .L5X file and import the project to a newer major revision to avoid the fatal error.
This anomaly first identified in version 16.00.
Error when attempting to run a trend (1435208)
The Logix Designer application is unable to run a trend in v29 or earlier after switching communication software from RSLinx Classic to FactoryTalk Linx in another instance of the Logix Designer application v31 and later on the same workstation.
Once a trend is run in the Logix Designer application v31 and later, using FactoryTalk Linx as the communication software, you will receive this error message if you then attempt to run a trend in the Logix Designer application v29 or earlier on the same workstation:
Error: <trend name> - : Can’t open the specified RSLinx driver. For more information, refer to the technical note BF23206.
This anomaly first identified in version 20.00.
This anomaly resolved in version 38.00.

Direct Add-on-Profile-to-Device Communication Could Result in Time Out Errors or Communication Routing to the Wrong Device (1927272)

Direct Add-on-Profile-to-device communication could result in time out errors or routing the communication to the wrong device in circumstances where all of the following conditions are met:

This applies to configuration data that goes through unconnected communication to the target I/O device (for instance, uploading/downloading device parameters).

This does not apply to I/O data.

This does not apply to commands from the controller (for instance, inhibiting/uninhibiting a device).

Please see technote BF28941 for additional details.

This anomaly first identified in version 20.00.

Mismatching display resolution and scaling may result in overlapping SFC elements (2122642)

Editing a Sequential Function Chart (SFC)) using a display with a given resolution (for example, 1920 x 1200) and Windows scale setting (for example, 100%), closing the ACD, and then opening the same ACD in another resolution (for example, 3840 x 2160) and Windows scale setting (for example, 150%) may result in overlapping SFC elements.

Fatal Error 0xe0434352 when creating, opening, or interacting with a module’s properties after installing a later version of the Studio 5000 Logix Designer application or after installing a new Add-on Profile (3219935)

Fatal Error 0xe0434352 occurs on creating, opening, or viewing of profiles updated with a web-based interface, including 1756 Ethernet modules, 5069 Ethernet Adapters, 5094 Ethernet adapters, 1734 Ethernet Adapters, and 1756 I/O.

This fatal error could occur after an installation of the Studio 5000 Logix Designer application or a stand-alone Add-On Profile (AOP), which causes an upgrade to all module profiles.

The fix for this anomaly is available in the Add-on Profiles update for the 1756 Analog Modules, v40.14.70. The Add-on Profiles can be downloaded from the Product Compatibility and Download Center. For more information on this anomaly and the solution, please see technote ID BF30201. 

This anomaly first identified in v20.05.

Functional Changes

This release has the following functional changes from the previous release.

Functional changes for Logix Designer v20.06

RSLogix 5000 version 20.06 has this change in functionality since the last release.

Security privileges

These security privileges are not supported in RSLogix 5000 version 20.06.

For additional information on FactoryTalk Security product policies, see Appendix A of the Logix 5000 Controllers Security Programming manual, publication 1756-PM016.

Import/Export

The Import/Export version number for this version of RSLogix 5000 software is 2.11. This table lists the Import/Export versions for previous releases.

Release Version
Import/Export Version
20.xx
2.11
19.xx
2.10
18.xx
2.09
17.xx
2.08
16.xx
2.07
15.xx
2.06
14.xx
2.05
13.xx
2.04
12.xx
2.03
11.xx
2.02
10.xx
2.01
9.00
2.00
5.02
1.02
2.xx, 6.xx, 7.xx, 8.xx
1.01
1.21, 1.23
1.00
1.10, 1.11
0.04


Application Notes

This release has the following application notes.

Error when launching RSLogix 5000 or Studio 5000 Logix Designer from CSPPEE
The CodeMeter Source Protection Provider Enterprise Edition (CSPPEE) client plugin sometimes generates an error when launching Logix Designer versions 24 and earlier in systems or workstations that also have Logix Designer versions 26 and later installed.
To work around this issue, install Logix Designer versions 24 and earlier on a separate workstation or on a virtual system.


  
Application notes for Logix Designer v20.06

These are the application notes for RSLogix 5000 version 20.06.

Supported Logix Controllers

While the programming software continues to extend its functionality with each new release, the physical controllers that it supports vary. New controllers are added, and in some cases, support for existing controllers may be removed. While a specific controller may not be supported by the current release, the side-by-side installation of multiple versions of the software provide, in most cases, a means to support the older hardware. If migrating from one controller to another, a project created for one controller can be easily converted to another controller using the Controller Properties configuration dialog box within the software.

If opening a project that is configured for a controller that is no longer supported and the older version of software is not installed, the software provides an appropriate warning and automatically provides the option to convert the project to one of the controllers supported by the release.

The table provides a breakdown of the various Logix 5000 controllers and the initial or minimum version of RSLogix 5000 application required to support the controller.

 Controller Catalog Number
Minimum Major Software Version
ControlLogix 1756-L61 Series A
12.00
ControlLogix 1756-L61 Series B
12.00
GuardLogix 1756-L61S Series B
14.001
ControlLogix 1756-L62 Series A
12.00
ControlLogix 1756-L62 Series B
12.00
GuardLogix 1756-L62S Series B
14.001
ControlLogix 1756-L63 Series A
10.00
ControlLogix 1756-L63 Series B
12.00
ControlLogix 1756-L63XT Series B
16.00
GuardLogix 1756-L63S Series B
17.00
ControlLogix 1756-L64 Series B
16.00
ControlLogix 1756-L65
17.00
ControlLogix 1756-L71 Series B
20.00
ControlLogix 1756-L71S Series B
20.01
ControlLogix 1756-L72 Series A
19.00
ControlLogix 1756-L72 Series B
20.00
GuardLogix 1756-L72S Series B
20.00
ControlLogix 1756-L73 Series A
18.00
ControlLogix 1756-L73 Series B
20.00
ControlLogix 1756-L73XT Series B
20.00
GuardLogix 1756-L73S Series B
20.00
GuardLogix 1756-L73SXT Series B
20.00
ControlLogix 1756-L74 Series A
19.00
ControlLogix 1756-L74 Series B
20.00
ControlLogix 1756-L75 Series A
18.00
ControlLogix 1756-L75 Series B
20.00
CompactLogix 1768-L43 Series A
15.00
CompactLogix 1768-L43 Series B
16.03
CompactLogix 1768-L43S Series A
18.00
CompactLogix 1768-L45 Series A
16.03
CompactLogix 1768-L45 Series B
16.03
CompactLogix 1768-L45S Series A
18.00
CompactLogix 1769-L16ER-BB1B Series A
20.00
CompactLogix 1769-L16ER-BB1B Series B
20.00
CompactLogix 1769-L18ER-BB1B Series A
20.00
CompactLogix 1769-L18ER-BB1B Series B
20.00
CompactLogix 1769-L18ERM-BB1B Series A
20.00
CompactLogix 1769-L18ERM-BB1B Series B
20.00
CompactLogix 1769-L23E-QB1
17.00
CompactLogix 1769-L23E-QBFC1
17.00
CompactLogix 1769-L23-QBFC1
17.00
CompactLogix 1769-L24ER-QB1B
20.00
CompactLogix 1769-L24ER-QBFC1B
20.00
CompactLogix 1769-L27ERM-QBFC1B
20.00
CompactLogix 1769-L30ER
20.00
CompactLogix 1769-L30ER-NSE
20.00
CompactLogix 1769-L30ERM
20.00
CompactLogix 1769-L31
13.002
CompactLogix 1769-L32C
13.002
CompactLogix 1769-L32E
13.002
CompactLogix 1769-L33ER
20.00
CompactLogix 1769-L33ERM
20.00
CompactLogix 1769-L35CR
20.002
CompactLogix 1769-L35E
12.002
CompactLogix 1769-L36ERM
20.00

1 Excludes RSLogix 5000 software version 15.

2 Excludes GuardLogix software version 14.

Microsoft® .NET Framework 4.6 may cause failure in earlier versions of the RSLogix 5000 application

When installing version 20.05 of RSLogix 5000, Microsoft .NET Framework 4.6 is installed automatically. However, .NET Framework 4.6 can cause these issues:

Follow one of these steps to work around the issue:
A higher upgrade is already installed on the computer

When installing RSLogix 5000 version 20.06, the installation fails with the message "A higher upgrade is already installed" when FactoryTalk® Linx™ 6.0 software is installed on the computer. The installation fails on RSLinx Enterprise 5.90.

To avoid this problem, do one of these options.

Clear the RSLinx® Enterprise check box on the Customize screen, and click Install.
  1. Uninstall FactoryTalk Linx 6.0 from Control Panel > Programs and Features. 
  2. Restart the Studio 5000 installation to install the software.
  3. When the installation is complete, reinstall FactoryTalk Linx 6.00 on the computer.

For more information, refer to Rockwell Automation Knowledgebase Answer ID 1072383.

Firmware update files may not be located in the search paths configured in ControlFLASH

When updating the firmware as part of the project download, the Update Module Firmware dialog box may display an error that it cannot find the location of the updated firmware files.

The installation of ControlFLASH version 15.01 moves the DMK files located in the ControlFLASH installation folder (C:\Program Files (x86)\ControlFLASH for 64-bit operating systems or C:\Program Files\ControlFLASH for 32-bit operating systems) to a new folder located in C:\Users\Public\Documents\Rockwell Automation\Firmware Kits.

Older versions of ControlFLASH and Logix Designer place DMK flash files in previous ControlFLASH file locations.

The work around if ControlFLASH cannot find the location of the DMK files:

  1. In the Choose Firmware Revision dialog box, click Browse.
ControlFLASH defaults to C:\Users\Public\Documents\Rockwell Automation\Firmware Kits.
  1. Depending on the operating system, browse to the location of the DMK files.

For more information, refer to Rockwell Automation Knowledgebase Answer ID 1071313.

Failed to go online with the controller error message appears twice when communications module is not located in a trusted slot

When attempting to go online with a controller that is set up to only allow communications through trusted slots, a failed to go online with the controller error message appears if the communication module is not located in a trusted slot.

Clicking OK to close the error message causes the error message to appear again. Click OK again to close error message.  

When a Flex I/O module is attached to Flex Ethernet adapter, select Compatible Module or Disable Keying as the Electronic Keying option in the classic Flex I/O profile

When a Flex I/O module is attached to a 1794-AENT adapter, on the General tab in the classic profile, select either Compatible Module or Disable Keying as the Electronic Keying option. Even though Exact Match is available as an Electronic Keying option, Flex modules do not use the Exact Match keying option. Electronic keying is based on an external Flex ID value which does not depend on the module's minor revision.

Versions 18.00 and later require updates to Custom Motion Database

When using a Custom RSLogix 5000 Motion Database in RSLogix 5000 software versions 12.00 through 17.00, update the motion database to work with versions 18.00 or later. The table lists the motion database revisions used with these application versions.

Version of Application
Motion Database Revision
20.06
14.39.00 [ Motion.mdb format ]
20.05
12.2.0 [ Motion.mdb format ]
20.01
8.12.00 [ Motion.mdb format ]
20.00
8.09.00 [ Motion.mdb format ]
19.01/ 19.00
7.05.00 [ Motion.mdb format ]
18.02 / 18.01 / 18.00
6.09.00 [ Motion.mdb format ]
17.01 / 17.00
5.03.00 [ *Motion.md format ]
16.04 / 16.03 / 16.00
4.02.00 [ *Motion.md format ]
15.03 / 15.02 / 15.01 / 15.00
3.24.00 [ *Motion.md format ]
14.01 / 14.00
3.12.00 [ *Motion.md format ]
13.04 / 13.03 / 13.02 / 13.01 / 13.00
3.12.00 [ *Motion.md format ]
12.06 / 12.05 / 12.04 / 12.03 / 12.02 / 12.01/ 12.00
3.03.00 [ *Motion.md format ]

* Before a Custom Motor can be used in version 18.00 or later, any Custom Motor currently in a motion database file at revision 5.00 or earlier (Motion.db format) must be converted to the newer Motion.mdb format.

To initiate the process of getting the database updated, please email the request to raeptechsupport@ra.rockwell.com. Please include any prior tech support case number if the current database includes non-Rockwell motors.

MSXML 4.0

This version of the software does not install or use MSXML 4.0. MSXML 4.0 has security risks associated with it and is no longer supported by Microsoft. For more information about MSXML and its availability, see the MSXML Roadmap. When installing products or components made by other vendors that use MSXML 4.0, contact the vendor for questions about the security risk associated with MSXML 4.0.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Installation Command-line parameters

This table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/ftsp-s
Specifies the FactoryTalk directory scope for restore. Only "Global" and "Local" scopes are supported.
This parameter is optional.
/ftsp-bak
Specifies the location where the restore file can be found.
This parameter is optional.
/ftsp-pp
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
/ftsp-value=enable/disable
Specifies to enable or disable the option Require computer accounts for all client machines in Security Policy. The option is used to determine whether or not a client computer account must exist in the directory to login.
This parameter is optional.
/DirectoryServer
Specifies the directory server name.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/NoHTTPS
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.
/Uninstall
Uninstalls the product.
The Logix Designer application does not support the /Uninstall option.
/SetupLanguage="value"
Specifies which language is displayed during install process.
The value must be the one of these:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be the one of these:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Or
/InstallDrive="value"
Specifies the install location or install drive respectively.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer uses the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.
Examples

These examples show how to use the installation commands.

Setup.exe /Q /IAcceptAllLicenseTerms
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /InstallDrive=D:
Error codes

This table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_REBOOT_CONTINUE
1641
A reboot is required to continue to installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_REBOOT_PENDING
3012
A restart is pending and is required before the installation can continue.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.

  
 
1

1756 Analog I/O Profile Not Retaining Engineering Units (1486580)

1756 Analog I/O Add-on Profiles allow users to set custom Engineering Units per channel, and these are stored as extended properties in the Studio 5000 Logix Designer application, versions 21 and later.

RSLogix 5000, versions 20 and earlier, does not support extended properties. When you use a 1756 Analog I/O Add-on Profile in RSLogix 5000, versions 20 and earlier, custom Engineering Units are not stored in the profile.

 
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.