Release Notes

20G - Firmware versions and revisions can be found in the Versions tab above
Version 16.002 Signed (released 7/2022)

Catalog Number PowerFlex 755 (series A)

These release notes describe version information for PowerFlex 755, version 16.002 Signed (released 7/2022).

Features

This release includes the following system features.


Configurable Communication Loss Fault for Option Modules

System Feature First Identified as of PowerFlex 755 Firmware Revision 16.002

System Feature First Identified as of PowerFlex 753 Firmware Revision 16.002

This feature allows you to configure the drive’s response to a communication loss fault (224…228 ‘Port n Comm Loss’) for an option module that is installed in slots 4…8 in the control pod of a PowerFlex® 753 or PowerFlex 755 drive.

New parameters 965 [Option Loss Actn] and 966 [Option Loss Dly] have been added to support the configuration of this new feature.

  


Configurable Programmable Logic Controller Outputs when in Program Mode

System Feature First Identified as of PowerFlex 755 Firmware Revision 16.002

This feature allows configuration of programmable logic controller outputs for integrated motion on the EtherNet/IP™ network (CIP) mode when the controller is set to program (IDLE mode).

See the “Integrated Motion on EtherNet/IP Application” appendix in the PowerFlex® 750-Series AC Drives Programming Manual, publication
750-PM001, for details on the attributes that have been added to support this feature.

  


Reduced Pulse Width Modulation to Help Improve Insulated Gate Bipolar Transistor Life

System Feature First Identified as of PowerFlex 755 Firmware Revision 16.002

System Feature First Identified as of PowerFlex 753 Firmware Revision 16.002

This feature allows you to configure a reduced Pulse Width Modulation (PM) carrier frequency when the carrier frequency reaches a specific threshold. Reduced PWM carrier frequency can help improve the life of the drive’s insulated gate bipolar transistors (IGBTs).

New parameters 39 [PWM Trans Freq] and 40 [Mtr Options Cfg] have been added to support this new feature.

  

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Feedback Selection

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 3.004

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 5.001

The HIM startup on the PowerFlex 755 drive includes a feedback device selection step. Depending on the option modules installed, that step may first ask the user to choose a port, then a parameter. In some situations, the list of ports incorrectly shows multiple copies of 'Port 0 - PowerFlex 755' followed by the feedback port/module.


The incorrect behavior happens only under the following conditions:

When the incorrect port list appears, it is still possible to successfully select the feedback module port by following one of these methods.

Persistent Stop Command with Profile Message Fault Action

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001

In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, a persistent stop command may appear in some cases. The action of disconnecting the Ethernet cable from the 20-750-ENETR module, which will result in the drive stopping, may follow with a nuisance fault action. This fault action previously noted is persistent communication of stop commands.

 
Saving Parameters Using DriveExplorer

Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001

Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001

In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, in which a user attempts to save all parameters using DriveExplorer® in some causes the save execution does not complete. When attempting to execute the save all parameters in DriveExplorer the software tool enters an infinite loop and does not progress through the save in some instances. To exit the loop, press the cancel button and check if the text file has been saved.

 
Support for Changing Permanent Magnet Direction Test Current

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 2.011

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 7.001

You cannot change the level of current used during the direction test on a permanent magnet motor while in Integrated Motion on EtherNet/IP (CIP Motion) mode. It is set at 10%. If the system requires more than 10% to turn the motor, it will fail to perform the test.

 
Delta Junction Temp at Zero Speed

Known Anomaly First as of PowerFlex 755 Drive Firmware Revision 2.011

The protection algorithms in frame 8 drives create false 168 “PWM Freq Reduced” exception events when running at zero speed. These can occur when the drive is first energizing the motor and establishing motor flux.

 
Diagnostic Item and Parameter Values Affected by Flash from Version 1 to Version 6

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 3.004

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 5.001

The following internal diagnostic items may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 2 [PBLT Pwrup Time], 3 [PBLT GatesOnTime], 4 [PBLT Mtr MW Hrs], 5 [PBLT Rgn MW Hrs] and 67 [PwrBd Pwr Cycles].

The following parameters may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 13[Elapsed MWH], 14 [Elapsed kWH], 15 [Elapsed Run Time], 16 [Elpsd Mtr MWHrs], 17 [Elpsd Rgn MWHrs], 18 [Elpsd Mtr kWHrs], 19 [Elpsd Rgn kWHrs], 490 [HSFan ElpsdLife], 497 [InFan ElpsdLife], 503 [MtrBrngElpsdLife], 508 [MtrLubeElpsdHrs], 512 [MchBrngElpsdLife] and 517 [MchLubeElpsdHrs].

These values will affect the associated calculated “ remaining life ” parameter values and predictive maintenance events.

 
Missing Error When Drive NV Selected in Integrated Motion Mode

Known Anomaly First Identified As of PowerFlex 755 Drive Firmware Revision 3.004

This anomaly affected customers using Integrated Motion on EtherNet/IP (CIP Motion). If you attempted to use Drive NV when configuring the motor on a motion axis with a PowerFlex 755, the drive would not return the appropriate error. This feature is not currently supported in the PowerFlex 755.

 
CIP Motion Axis Inhibit F927 Event

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 8.001

The drive may throw an F927 fault when an axis is inhibited. If this occurs, the drive will shut down allowing the motor to coast. The status LED will blink 27 times, pause, then repeat. If this occurs, cycle power to the drive to clear the fault.

 
F918 Exception Events

Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 6.004

Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 6.004

When running in Flux Vector open loop mode for induction motor or Interior Permanent Magnet (IPM) motor mode, the drive may experience an F918 exception event when the motor accelerates through a 7 Hz operating frequency due to the simultaneous transition from a 2 to 4 KHz carrier frequency. This exception can be avoided by setting parameter 40 [Mtr Options Cfg] bit 9 – PWM FreqLock], which will keep the carrier frequency at 4 KHz.

 

Universal Feedback Board Module Does Not Annunciate Fault

Known Anomaly First Identified as of:

When the UFB is configured to use the SSI Full Digital Feedback Device, the UFB does not annunciate a fault when the SSI Full Digital is the signal is lost. For full details on possible workarounds to this anomaly, see Technical Support Knowledgebase Article #463171. To determine if this notice affects you and for additional information, please refer to Knowledgebase Document Number #745654.


  

 

Application Notes

This release has the following application notes.

Determine PowerFlex 755 Drive Firmware Revision Level

Application Notes


Use the Drive LCD HIM

  1. Access the Status screen, which is displayed on HIM power up.

graphic

  1. Use the graphic or graphic key to scroll to Port 00 for the Host Drive.
  2. Press the graphic key to display its last-viewed folder.
  3. Use the graphic or graphic key to scroll to the DIAGNOSTIC folder.
  4. Use the graphic or graphic key to select Device Version.
  5. Press the graphic (Enter) key to display device version information.

FW Revision is listed under – Main Control Board.

graphic


Use DriveExplorer Lite/Full

Important: You need DriveExplorer version 6.01 or later to interface with the PowerFlex 755 drive. To obtain the latest version, visit the Allen-Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate

 

  1. Launch DriveExplorer and go online with the PowerFlex 755 drive. To connect to the drive, use a 1203-USB converter, a 1203-SSS converter, or an EtherNet/IP network connection.
  2. In the Devices hardware view, select the PowerFlex 755 drive.

Once selected, information regarding the PowerFlex 755 drive is shown in the right panel including the current firmware revision number.

graphic


Use DriveExecutive

Important: You need DriveExecutive version 5.01 or later to interface with the PowerFlex 755 drive. To obtain the latest version, visit the Allen- Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate

 

  1. Launch DriveExecutive and go online with the PowerFlex 755 drive. To connect to the drive, use a 1203-USB converter, a 1203-SSS converter, or an EtherNet/IP network connection.
  2. In the Drives hardware view, select the PowerFlex 755 drive (graphic).
  3. Click the information icon (graphic) to display the drive’ s Properties dialog box.

In the Properties dialog box the “ Revision:” field (graphic ) will show the drive ’s current firmware revision number.

graphic

 


Update PowerFlex 755 Drive Firmware

Product Updates and Replacements

PowerFlex® 755 firmware revision 14.004 or later is installed by using a *.dmk file. Firmware updates for PowerFlex 755 drives can be performed using the following software:

Software
Version
Additional Software
Communication Adapters
ControlFLASH Plus™
3.01.00
The following software must be installed before running ControlFLASH Plus:
  • FactoryTalk® Linx™ version 6.00.00 or later.
ControlFLASH Plus version 2.00.00 or later includes the installation package for FactoryTalk Linx.
One of the following communication devices must be used:
  • Embedded EtherNet/IP port on the main control board
  • 20-750-ENETR PowerFlex 750-Series Dual-port EtherNet/IP Option Module
ControlFLASH™
15.03.00
One of the following software packages must be installed before running ControlFLASH:
  • RSLinx® Classic Lite
  • RSLinx Classic
  • RSLinx Enterprise version 5.90 or FactoryTalk Linx 6.00
One of the following communication devices must be used:
  • Embedded EtherNet/IP port on the main control board
  • 20-750-ENETR - PowerFlex 750-series dual-port EtherNet/IP option module
  • 1203-USB – USB converter for DSI, DPI, and SCANPort-based devices.
  • 1203-SSS – RS232 serial converter for DPI and SCANPort-based devices


Before You Begin a Firmware Update

If necessary, download and install the preferred software from the Product Compatibility and Download Center.

For instructions on how to install ControlFLASH and ControlFLASH Plus software and upgrade your drive firmware by using these software tools, see these publications:

For information on connecting the 1203-USB or 1203-SSS converter to your drive, see these publications:

Use ControlFLASH Plus to Update the Firmware

See “Use ControlFLASH Plus to update firmware” in the ControlFLASH Plus Quick Start Guide, publication CFP-QS001

Use ControlFLASH to Update the Firmware

Follow these steps to update your PowerFlex 755 drive firmware.

  1. Download the applicable firmware revision from the Product Compatibility and Download Center.
  2. Place the *.dmk file in one of the following directories on your computer:

Note: In this example, the file name is PF755_App_v14_004_230_Secure.dmk.

graphic

  1. Verify that the drive is stopped and not communicating with a controller, by inhibiting the drive in the software.
  2. Open ControlFLASH on your computer.
  3. In the Welcome dialog box, choose RSLinx Classic or FactoryTalk Linx. RSLinx Classic is used in this example.

graphic

  1. Click Next.
  2. In the Catalog Number dialog box, select the appropriate drive family.

Important: Choose the appropriate “PowerFlex 755 xx” catalog number selection for your application. Do not choose an option that includes the “via…” option.

graphic

  1. Click Next.
  2. In the RSWho browser dialog box, select your drive.

graphic

  1. Click OK.
  2. In the Multiple Assemblies Found dialog box, select Port 0 – PowerFlex 755.

graphic

  1. Click OK.
  2. In the Firmware Revision dialog box, click Show all revisions.
  3. Below Revision, select the applicable firmware revision.

graphic

  1. Click Next.
  2. In the Summary dialog box, click Finish.

graphic

  1. In the ControlFLASH message box, click Yes.

graphic

  1. The firmware update begins and a Progress dialog box appears.

graphic

  1. When the firmware update is complete, the Update Status dialog box appears.

graphic

  1. Click OK.
  2. Exit ControlFLASH.

The drive firmware update has been completed.

  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.