This release has the following requirements.
The following are the system requirements for FactoryTalk Historian Vision version 3.06.01.
Software requirements
FactoryTalk Historian Vision version 3.06.01 has been tested on the following operating systems:
Software compatibility
FactoryTalk Historian Vision version 3.06.01 is compatible with these Rockwell Automation products:
|
|
Tip:
Due to the version of Asset Framework included with version 6.00.00,
search functionality and returned results only support name matches.
Versions 7.00.00 and later support name and description matches in
searches.
|
Supported browsers
FactoryTalk Historian Vision version 3.06.01 has been tested on the following browsers:
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Security requirements
To help meet secure system design requirements, review these publications:
This release includes the following system features.
FactoryTalk Historian Vision version 3.06.01 has the following enhanced features:
This release has the following functional changes from the previous release.
FactoryTalk Historian Vision version 3.06.01 has the following changes in functionality since the last release:
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).
This release has the following application notes.
The following are the application notes for FactoryTalk Historian Vision version 3.06.01.
Installation and Upgrade
We recommend that you read PI Vision 2021 Installation and Administration Guide before installing FactoryTalk Historian Vision.
The file <Installation package>\Setup.exe should be run locally as an administrator to install FactoryTalk Historian Vision. The installation includes:
|
|
Tip: Please note that this product uses cookies and that by installing this
product, you as Licensee acknowledge and confirm that your use of the
product will comply with all laws, rules, and regulations of the United States
and other countries that may be applicable to the product, including but not
limited to any relevant cookie directives.
|
Installation prerequisites
The following prerequisites must be met before installing the FactoryTalk Historian Vision application server. If these requirements are not met, the installation of FactoryTalk Historian Vision will not succeed.
Silent Installation
To invoke a silent installation of FactoryTalk Historian Vision, follow the instructions in the Perform silent installation section of the PI Vision 2021 Installation and Administration Guide.
Distribution Kit Files
FactoryTalk Historian Vision version 3.06.01 distributes the following major components as part of the installation.
Upgrading from an existing version of FactoryTalk Historian Vision
FactoryTalk Historian Vision version 3.06.01 supports upgrading from all previous installations of Vision, but only upgrades from the previous two releases have been tested.
Configuring FactoryTalk Historian Vision
The document PI Vision 2021 Installation and Administration Guide contains configuration information that must be completed before FactoryTalk Historian Vision will be functional. This includes creating and configuring a FactoryTalk Historian Vision database and connecting to appropriate FactoryTalk Historian SE system resources (Data Archives and Historian AF databases).
Uninstalling FactoryTalk Historian Vision version 3.06.01
To uninstall FactoryTalk Historian Vision, launch the Programs and Features Control Panel applet, select PI Vision 2021 Patch 1, and select Uninstall.
Overview of New Vulnerabilities Fixed or Mitigated
This section is intended to provide relevant security-related information to guide your installation or upgrade decision. Aggregate information about the number and severity of FactoryTalk Historian Vision security vulnerabilities that are fixed in this release are disclosed here.
|
Package Name
|
Version
|
CVE
|
CVSS
|
Mitigation
|
|
jQuery Mobile
|
1.3.2
|
CVE is not available. Reference:
https://gist.github.com/jupenur/e5d0c6f9b58aa81860bf74e010cf1685
|
6.5
|
This vulnerability is mitigated in
FactoryTalk Historian Vision by specifying
paths allowed by jQuery Mobile.
|
Documentation Overview
Kerberos Delegation
Some features within FactoryTalk Historian Vision (PI Vision) by default will attempt to impersonate the end user when trying to retrieve information. Impersonation is possible through Kerberos constrained delegation (or RBCD) when Windows authentication is being used but is also possible with Basic authentication. It is recommended to implement delegation as opposed to Basic authentication when possible as it's the more secure of the two options. The list of features below that have this default behavior is specific to this released version.
Impersonation to Asset Framework (AF)
FactoryTalk Historian Vision (PI Vision) will attempt to impersonate the end user for the following features which means, when Vision is using Windows Authentication, they will fail unless delegation has been configured.
Features that attempt delegation by default:
Impersonation can be disabled. However, we do not recommend disabling end user impersonation for these features as they were implemented as a security feature. Contact technical support for details on how to configure or change this setting.
Impersonation to Data Archive
FactoryTalk Historian Vision (PI Vision) will attempt to impersonate the end user for data calls in general and when searching for tags in Vision but will not fail without delegation configuration if a catch-all mapping or PI Trust is configured. When Vision is using Windows Authentication, the delegation would be needed in the specific scenarios listed below: