Release Notes

( 9301-OPCx , 9301M-KSETx) KEPServer Enterprise connects 3rd Party HW / SW, from plant control systems to enterprise information systems
Version 13.00.00 (released 3/2022)

Catalog Number KepServer Enterprise 

These release notes describe version information for KepServer Enterprise, version 13.00.00 (released 3/2022).

Requirements

This release has the following requirements.

The following are the system requirements for KEPServer Enterprise version 13.00.00.

KEPServer Enterprise works within the system requirements of all Rockwell Automation® software products.

For the latest compatibility information, refer to the Product Compatibility and Download Center.

Hardware requirements

KEPServer Enterprise was tested with the following hardware:

Software requirements

KEPServer Enterprise runs on these Windows® operating systems:

*For additional information about Windows 10 Support for the FactoryTalk Suite of Rockwell Software products, refer to Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products

graphic
Note: Windows Server Core deployments are not supported for Windows Server 2019 and Windows Server 2016.

Features

This release includes the following system features.

KEPServer Enterprise version 13.00.00 has the following new and enhanced features:

New features

Server

Fanuc Focas Ethernet Driver

Siemens TCP/IP Ethernet Driver

Torque Tool Ethernet Driver

Yokogawa GX Ethernet Driver

Enhanced features

Server

Automation DirectNET Driver

BACnet Driver

CODESYS Driver

Fanuc Focas Ethernet Driver

Mitsubishi Ethernet Driver

Modbus RTU Server Serial Driver

Modbus TCP/IP Ethernet Driver

MTConnect Driver

OPC DA Client Driver

Siemens TCP/IP Server Ethernet Driver

SIXNET UDR Driver

Telemecanique Uni-Telway Driver

Toyopuc Ethernet Driver

Corrected Anomalies in This Release

This release corrects the following anomalies.

The following list identifies the anomalies corrected in the KEPServer Enterprise version 13.00.00.

Server

Automation DirectNET Driver

Beckhoff TwinCAT Driver

Fanuc Focas Ethernet Driver

GE Ethernet Driver

Mitsubishi Ethernet Driver

Modbus TCP/IP Ethernet Driver

MTConnect Driver

OPC DA Client Driver

OPC UA Client Driver

OPC XML-DA Client Driver

Siemens TCP/IP Ethernet Driver

SIXNET UDR Driver

SNMP Driver

Known Anomalies in This Release

This release has the following known anomalies.

Functional Changes

This release has the following functional changes from the previous release.

KEPServer Enterprise version 13.00.00 has no changes in functionality since the last release.

Application Notes

This release has the following application notes.

The following are the application notes for KEPServer Enterprise version 13.00.00.

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Set DCOM authentication level of KEPServer Enterprise

When using KEPServer Enterprise, change the authentication level through the following:

  1. Open Component Services.
  2. Double-click Console Root > Component Services > Computers > My Computer > DCOM Config.
  3. Right-click KEPServerEnterprise x.xx and select Properties.
  4. On the General tab, select the authentication level in Authentication Level.
  5. Click OK and restart KEPServer Enterprise.

In addition to DCOM configuration, you must configure the following settings:

  1. From the notification area, right-click KEPServerEnterprise and select Settings.
  2. graphic
  1. In the Settings - KEPServerEnterprise dialog box, select Runtime Options > Use DCOM configuration settings.
  2. Click OK.

Supported Drivers

The PC edition of KEPServer Enterprise version 13.00.00 supports these drivers:

Driver list
Driver list
Driver list
Driver list
Advanced Simulator
GE SNP
Omron Host Link
Thermo Westronics Ethernet
Allen-Bradley® Bulletin 1609
GE SNPX
Omron NJ Ethernet
Thermo Westronics Serial
Allen-Bradley Bulletin 900
Hilscher Universal
Omron Process Suite
TIWAY Host Adapter
Analog Devices
Honeywell HC900 Ethernet
Omron Toolbus
Torque Tool Ethernet
Aromat Ethernet
Honeywell UDC Ethernet
OPC® DA Client
Toshiba Ethernet
Aromat Serial
Honeywell UDC Serial
OPC UA Client
Toshiba Serial
AutomationDirect DirectNET
IA Super SEL
OPC XML-DA Client
Toyopuc® PC2 Serial
AutomationDirect EBC
Idec Serial
Optimation OptiLogix
Toyopuc PC3/PC2 Ethernet
AutomationDirect ECOM
IOtech PointScan 100
Opto 22 Ethernet
U-CON (user-configurable)
AutomationDirect K Sequence
Keyence KV Ethernet
Partlow ASCII
Wago Ethernet
AutomationDirect Productivity Series Ethernet
KraussMaffei MC4 Ethernet
Philips P8/PC20
Wonderware InTouch Client
BACnet™/IP
Memory Based
SattBus Ethernet
Yaskawa Memobus Plus (SA85)
Beckhoff® TwinCAT®
Mettler Toledo Serial
SattBus Serial
Yaskawa MP Series Ethernet
Busware Ethernet
Micro-DCI™
Scanivalve Ethernet
Yaskawa MP Series Serial
CODESYS®
Mitsubishi® CNC Ethernet
Siemens® S5 (3964R)
Yokogawa Controller
Contrex® M-Series
Mitsubishi Ethernet
Siemens S5 (AS511)
Yokogawa CX Ethernet
Contrex Serial
Mitsubishi FX
Siemens S7 MPI
Yokogawa Darwin Ethernet
Cutler-Hammer D50/D300
Mitsubishi FX Net
Siemens S7-200
Yokogawa Darwin Serial
Cutler-Hammer ELC Ethernet
Mitsubishi Serial
Siemens TCP/IP Ethernet
Yokogawa DX Ethernet
Cutler-Hammer ELC Serial
Modbus® ASCII Serial
Siemens TCP/IP Slave Ethernet
Yokogawa DX Serial
Dataforth® isoLynx®
Modbus Plus
Simatic/TI 505 Ethernet
Yokogawa DXP Ethernet
DDE Client
Modbus RTU Serial
Simatic/TI 505 Serial
Yokogawa HR2400 Serial
Fanuc Focas Ethernet
Modbus Slave RTU Serial
Simulator
Yokogawa MW Ethernet
Fanuc Focas HSSB
Modbus TCP/IP Ethernet
SIXNET EtherTRAK®
Yokogawa MX Ethernet
Fuji Flex
MTConnect® Client
SIXNET UDR
Yokogawa YS100 Serial
GE® CCM
ODBC Client
SquareD Serial
 
GE Ethernet
Omron FINS Ethernet
System Monitor
 
GE Ethernet Global Data
Omron FINS Serial
Telemecanique Uni-Telway Slave
 

KEPServer Enterprise versions

This table displays the versions of KEPServer Enterprise and the related or equivalent versions for the following software:

KEPServer Enterprise version
5.00.00
8.00.00
9.00.00
10.00.00
11.00.00
12.00.00
12.01.00
13.00.00
KEPServerEX  equivalent version
4.5
5.13.235
5.19.476
5.21.158
6.6.504
6.9.572
6.9.636
6.11.725
FactoryTalk View SE and ME Station
5.00.00
8.00.00
9.00.00
10.00.00
11.00.00 (requires patch)
11.00.00
12.00.00
12.00.00
13.00.00
PanelViewPlus
5.00.00 to 5.10.00
8.00.00 to 8.20.00
9.00.00
10.00.00 to 12.00.00
Not supported
Not supported
Not supported
Not supported
MobileView
Not applicable
Not applicable
Optional installation
11.00.00 to 12.00.00
Not supported
Not supported
Not supported
Not supported

graphic
Tip: FactoryTalk View SE and ME Station versions 10.00.00 and 11.00.00 require this patch to use KEPServer Enterprise version 10.00.00: https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/1083527
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2025 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.