Release Notes
FactoryTalk® Linx high performance communications software optimized for Logix5000 controllers. (included with FTSP)
Version 6.30.00 (released 3/2022)
Catalog Number FactoryTalk Linx (aka RSLinx Enterprise)
These release notes describe version information for FactoryTalk Linx (aka RSLinx Enterprise), version 6.30.00 (released 3/2022).
Requirements
This release has the following requirements.
FactoryTalk Linx version 6.30.00 (CPR 9 SR 13)
FactoryTalk Linx works within the system requirements of all Rockwell Automation® software products.
For the latest compatibility and driver support information, refer to the Product Compatibility and
Download Center.
Hardware requirements
FactoryTalk Linx requires the following hardware:
- Intel® Core™ i5 Standard Power processor
- 4 GB of memory (RAM)
Software requirements
Operating systems
FactoryTalk Linx has been tested on the following operating systems:
- Windows® 10 (v2004, v20H2, v21H1, and v21H2)
FactoryTalk Linx adopts .NET 4.8 which is only supported in Windows 10 v1803 and later.
- Windows 10 IoT Enterprise 2016 Long-Term Servicing Branch (LTSB)
- Windows 10 IoT Enterprise 2019 Long-Term Servicing Channel (LTSC)
- Windows 11
- Windows Server® 2012
- Windows Server 2012 R2
- Windows Server 2016
- Windows Server 2019
For requirements specific to running FactoryTalk Linx within FactoryTalk View Studio, refer to the
System requirements topic in the FactoryTalk View SE and FactoryTalk View ME Release Notes.
Software compatibility
FactoryTalk Linx version 6.30.00 has been tested with, and is compatible with, the following Rockwell
Automation products:
- Studio 5000 Logix Designer version 34.00.00
- Studio 5000 View Designer version 8.02
- ControlFLASH version 15.07
- ControlFLASH Plus version 5.00
- FactoryTalk Services Platform version 6.30.00
- FactoryTalk Alarms and Events version 6.30.00
- FactoryTalk View version 13.00.00
- FactoryTalk Linx Gateway version 6.30.00
- FactoryTalk Linx OPC UA Connector version 6.30.00
- FactoryTalk Activation Manager version 4.06.13
- FactoryTalk Batch version 14.00
- Connected Components Workbench version 20.00.00
- FactoryTalk AssetCentre version 12.00.00
- FactoryTalk Policy Manager version 6.20.00
- FactoryTalk Logix Echo version 1.00.00
- FactoryTalk System Service version 6.30.00
- FactoryTalk Updater version 3.00.11
- EDS subsystem version 34.0.10
Firmware requirements
To use the ControlNet communication feature with FactoryTalk Linx, the minimum requirements are:
- 1784-PKTCS/B firmware version 4.10.
The PKTCS cards support I/O and messaging.
- 1784-PCICS/B and 1784-PCIC/B firmware version 4.10.
- 1784-PCICS/A and 1784-PCIC/A firmware version 3.10.
To use the DeviceNet communication feature with FactoryTalk Linx, the minimum requirements are:
|
|
Note: FactoryTalk Linx also supports bridging from Ethernet (1756-ENxxx)
to DeviceNet (1756-DNB) across a ControlLogix Chassis.
|
High Resolution Display Support
Windows 10 v1803 or later is the recommended operating system if running this software with a 2K or
4K High Resolution Display with scaling up to 125%.
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and
antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell
Software Products and Antivirus Software .
Supported browsers
The following web browsers have been tested and are supported for use with this release:
- Google® Chrome™ browser
- Microsoft® Edge™
- Mozilla® Firefox®
Security Requirements
To help meet secure system design requirements, review these publications:
To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products
(publication SECURE-AT001).
Features
This release includes the following system features.
FactoryTalk Linx version 6.30.00 has the following new features:
New features
- FactoryTalk Linx version 6.30.00 adds an option to enable or disable CIP Security (Port 2221) of a
server or a device.
- FactoryTalk Linx version 6.30.00 supports browsing 5015 adapters and optimizes the user
interface of 5015 adapters with their I/O modules.
- FactoryTalk Linx version 6.30.00 supports indicating the offline status of devices.
- FactoryTalk Linx version 6.30.00 adds one predefined tag (@TrackedStateValue) to show the
tracked state value from the controller.
- FactoryTalk Linx version 6.30.00 adds an LLDP tab in the Network Browser to view and edit the
Link Layer Discovery Protocol (LLDP) detection status of a device.
- FactoryTalk Linx version 6.30.00 adds @RedundancyEnabled and @RedundancyState
predefined tags associated with a processor shortcut, to indicate if the associated controller is
operating in a ControlLogix Redundancy configuration and its current operational state. These
tags are helpful for Human Machine Interface (HMI) displays that monitor the operation of a
redundant ControlLogix controller's operation.
- FactoryTalk Linx version 6.30.00 communication with the Studio 5000 v34 controllers but does not
support new time data types.
- FactoryTalk Linx Network Browser version 6.30.00 supports browsing of GuardLink connected
devices.
Corrected Anomalies in This Release
This release corrects the following anomalies.
The list identifies the anomalies corrected in the FactoryTalk Linx version 6.30.00. Use the identification
information provided in the anomaly heading to track the anomaly in future releases or for reference
when receiving assistance from Customer Support with a related issue.
- If communications to a device is inhibited in FactoryTalk Linx, it will take a long time for
FactoryTalk Live Data Test Client to browse tags. First identified in FactoryTalk Linx version
6.21.00. [Jira 978056]
- Online deleting or adding structure members in UDT (User Defined Data Type) is not reflected in
the FactoryTalk Linx namespace. As a result, reading from such a modified structure will not be
possible or may deliver incorrect results. This applies only to UDTs that exist in FactoryTalk Linx
namespace (tags of such UDTs were added for reading). [Jira 984705]
- When using the EDS Hardware Installation Tool to import specific EDS files, the tool might stop
responding. First identified in FactoryTalk Linx version 6.30.00. [Jira 825583, Jira 889508]
- When exporting to an XML file, the FactoryTalk Live Data Test Client might stop responding. First
identified in FactoryTalk Linx version 6.30.00. [Jira 1194497]
- In FactoryTalk View SE, after restarting your computer, the secondary HMI server in a redundant
pair cannot show the correct status. First identified in FactoryTalk Linx version 6.30.00. [Jira
1094689]
- In FactoryTalk Administration Console, if you select the Listen on EtherNet/IP encapsulation
ports option for the MAC address which has multiple IP addresses configured, the same option
status cannot be synchronized to the Network Browser. First identified in FactoryTalk Linx version
6.30.00. [Jira 1213523]
- If a driver name includes a space, the Device Configuration and Device Statistics dialog boxes
cannot be opened. First identified in FactoryTalk Linx version 6.30.00. [Jira 1057709]
- If you select the Listen on EtherNet/IP encapsulation ports option in FactoryTalk Administration
Console or the Network Browser, the configuration cannot be synchronized to the other
application. First identified in FactoryTalk Linx version 6.21.00. [Jira 1182725]
- In FactoryTalk Linx Configuration Import Export Tool, when selecting Delete all shortcuts &
drivers and then create new without a shortcut selected, the operation will fail. First identified in
FactoryTalk Linx version 6.30.00. [Jira 1060483]
- The EDS Upload option is not available when connecting the device via USB. First identified in
FactoryTalk Linx version 6.30.00. [Jira 1059138]
- After you add, edit, delete, backup, or restore shortcuts, the log message in FactoryTalk
Diagnostics shows that the Severity is Information but not Audit. First identified in FactoryTalk
Linx version 6.21.00. [Jira 977628]
- If the shortcut name is shorter than the server name in FactoryTalk Linx, the FactoryTalk
Namespace service might stop responding when accessing the tag namespace. First identified in
FactoryTalk Linx version 6.21.00. [Jira 1486570]
Known Anomalies in This Release
This release has the following known anomalies.
- When using the FactoryTalk Batch server to communicate Logix controllers and the
FactoryTalk Linx Network Browser on the same workstation is browsing the system at the
same time, the FactoryTalk Batch server might lose communication. First identified in
FactoryTalk Linx version 6.30.00. [Jira 1501398]
To avoid this problem, don't run FactoryTalk Linx Network Browser from the same
workstation that is used to provide FactoryTalk Batch communications.
To resolve the existing problem, close FactoryTalk Linx Network Browser and restart the
FactoryTalk Batch server.
Known Anomalies from Previous Releases
These anomalies are from previous releases but are still known in this release.
-
Extensive online modifications within Studio 5000 Logix Designer, including modifications to extended
tag properties, can lead to FactoryTalk Linx clearing cached extended tag properties but not properly
reloading them. This could result in FactoryTalk View SE displaying wireframes or default values for a
controller's extended tag properties. First identified in FactoryTalk Linx version 6.20.00. [Jira 2398000]
To address this issue, make online modifications to controllers only when FactoryTalk View SE displays
are not required. If the extended tag properties are missing, restart the appropriate FactoryTalk Linx
service (RSLinxNG01.exe or RSLinxNG02.exe). Occasionally, it may be necessary to restart the
FactoryTalk Linx service once more to restore the correct extended tag properties.
- If you rehost a FactoryTalk Linx data server (or an RSLinx Enterprise data server, in RSLinx
Enterprise version 5.90.00 and earlier) to a different computer, you may fail to browse the existing
device shortcuts in the Tag Browser. First identified in RSLinx Enterprise version 2.70.00.
[356075]
To solve the issue, reconfigure the shortcuts in the Communication Setup editor and reboot the
FactoryTalk Directory server.
- PanelView terminals cannot show in the Communications Setup editor.
If you use RSLinx Enterprise/FactoryTalk Linx to configure the Serial DF1 driver and specify the
baud rate to be 110, 300, or 600, the PanelView terminals cannot show on the communication
tree in the Communications Setup editor. First identified in RSLinx Enterprise version 5.60.00.
[275151]To avoid this problem, if your network includes a PanelView terminal that you want to browse,
select an alternate baud rate when configuring the Serial DF1 driver.
- FactoryTalk View fails to get the previously reading tag value from a ControlLogix device.
If you use RSLinx Enterprise/FactoryTalk Linx to browse and read tag value of a ControlLogix
device, when you manually change the Ethernet module IP address of this device and the IP
address of it in RSLinx Enterprise/FactoryTalk Linx device list, FactoryTalk View fails to get the
previously reading tag value. First identified in RSLinx Enterprise version 5.60.00. [341516]There is currently no workaround for this anomaly.
- Installation of a PCICS or PKTX card driver may result in device browse failure.
When installing a PCICS or PKTX card driver on a computer, after the new card driver is installed
into system device manager, the device may not show upon browsing. First identified in RSLinx
Enterprise version 5.70.00. [346194]
- FactoryTalk Linx cannot browse the 1794 FLEX™ I/O modules under the FLEX I/O adapters in
the Network Browser or in the Communication Setup editor. When you browse an online 1794
FLEX I/O adapter with 1794 FLEX I/O modules, the adapter shows in the communication tree,
while no downstream port shows. First identified in RSLinx Enterprise version 5.90.00.
To work around this problem, use RSLinx Classic to get a listing of the connected modules and
the related downstream port information.
- If you are running FactoryTalk Linx on Windows Server 2012, you cannot browse DH485 driver.
First identified in FactoryTalk Linx version 6.00.00. [367931]
Switch to a different operating system and try again.
- The value of the communication module predefine tag, @DevicePath, shows incorrectly on
Windows CE system. First identified in RSLinx Enterprise version 5.60.00. [274999]
There is currently no workaround for this anomaly.
- In FactoryTalk Diagnostics Counter Monitor, HMI tag items do not always show under
RnaDaSvr[TagSvr.exe]. First identified in RSLinx Enterprise version 2.51.00. [275196]
There is currently no workaround for this anomaly.
- A Datalogger error message may show up when using FactoryTalk Linx on FactoryTalk View ME.
First identified in FactoryTalk Linx version 6.00.00. [367974]
There is no impact on the terminal or the data log function, and the error message can be ignored.
- If the .mer file user created is version 11.00 or earlier, when checking the unsupported shortcut
path (using DHRIO connect to a ControlLogix Controller), the error message cannot be shown as
expected. [Jira 488722]
There is currently no workaround for this anomaly.
- On a computer that contains a loopback adapter, after creating an Ethernet driver with Local
Broadcast (Discovery Method > Broadcast > Local Broadcast) and Windows Default
(Advanced > Interface > Windows Default), the devices cannot be shown when you browse the
Ethernet driver. First identified in RSLinx Enterprise version 5.90.00. [Jira 489076]
To avoid this problem, disable the Microsoft Loopback Adapter from Control Panel > Network
and Internet > Network and Sharing Center > Change adapter settings or choose another
network interface card.
- When a user clicks the SLC/PLC, the icon is changed to the browsing state. [Jira 487435]
There is no workaround for this anomaly, but there is no impact on the shortcut creation.
- After changing the Ethernet driver name, the device path cannot be automatically updated to the
latest, so the Device Property page cannot establish connections. First identified in FactoryTalk
Linx version 6.21.00. [Jira 354185]
To solve this problem, browse the driver again and make sure the device path is updated to the
latest.
- After changing a driver's Interface under Configure Driver > Advanced, the Network Browser
may incorrectly show good status for some device that it is unable to communicate with. First
identified in FactoryTalk Linx version 6.21.00. [Jira 491731]
To solve this problem, delete the driver and re-create one with new Network Interface Card. Then,
the device will display correctly.
- Changing the configurations in FactoryTalk Policy Manager and then restarting the
FactoryTalk Linx service may cause FactoryTalk Linx to stop responding. First identified in
FactoryTalk Linx version 6.10.00. [191818]
To solve this problem, restart the computer that hosts FactoryTalk Linx.
- In an Ethernet driver with a Device List/Range, change the original network interface card
to another, the devices from the previous network are not removed. First identified in
RSLinx Enterprise version 5.90.00. [Jira 489110]
Manually delete the unwanted device.
- If the user adds a new shortcut or a new server containing a shortcut that has the same
name as an existing shortcut, all references to read or write tags from the original shortcut
will fail when new items are requested via the original shortcut or when the data server or
FactoryTalk software client (For example, FactoryTalk View SE or FactoryTalk Linx
Gateway) are restarted. [Jira 857439]
To avoid this problem, verify any new shortcuts do not utilize the same name as existing
shortcuts already in use; If a duplicate shortcut name is added, please edit or update all
tag references to the original shortcut in order to restore communications.
- Even though an EDS file is removed or unregistered by the EDS Hardware Installation
Tool, the associated device will still appear in the FactoryTalk Linx Network Browser with
the proper icon, but some communications to the device may fail. [Jira 749380]
Reinstall an EDS file for the device to recover normal operation.
- For a driver created in the Network Browser as part of ControlFlash or Studio 5000
software, the driver do appear in the FactoryTalk Linx (previously named RSLinx
Enterprise prior to version 6.00.00) configuration, but you can only view or change it from
within the Network Browser from ControlFlash or Studio 5000. First identified in RSLinx
Enterprise version 5.90.00. [363804]
There is currently no workaround for this anomaly.
- FactoryTalk Linx cannot browse the private network through a NAT device from the public
side or the second network interface on a CompactLogix controller. [Jira 967248]
To solve this problem, reconnect the workstation to the private network to browse its
devices.
- When multiple shortcuts in FactoryTalk Linx are configured to point at the same controller,
changes made to one shortcut's "Extended Tag Properties" and "Description
pass-through" settings will affect the operation of other shortcuts referencing the same
controller on the same FactoryTalk Linx data server. First identified in FactoryTalk Linx
version 6.10.00. [150898]
To solve this problem, configure all shortcuts to a device with matching settings.
- On a workstation that is configured with CIP security, disabling the network adapter,
restarting the computer, and re-enabling the network adapter will cause FactoryTalk Linx
Network Browser to be unable to browse new devices. First identified in FactoryTalk Linx
version 6.10.00. [193473]
To solve this problem, restart the computer and try browsing the devices again.
- The Access Rights of CIA message shortcut and symbolic shortcut should be read-only
but show as read-write in Tag Browser. First identified in FactoryTalk Linx version
6.21.00. [Jira 890371]
There is currently no workaround for this anomaly.
- If communications to a device is inhibit in FactoryTalk Linx, it will take a long time for FactoryTalk
Live Data Test Client to browse tags. First identified in FactoryTalk Linx version 6.21.00. [Jira
978056]
To avoid this problem, set the timeout value by registry key "SOFTWARE\ROCKWELL
SOFTWARE\RSLINXNG\LOGIXDP\VALIDATEITEMTIMEOUT". The unit for this value is
millisecond, the default timeout value is 5 minutes.
- Online deleting or adding structure member in UDT (User Defined Data Type) is not reflected in
the FactoryTalk Linx namespace. As a result, reading from such modified structure will not be
possible or may deliver incorrect results. This applies only for UDTs that exists in FactoryTalk
Linx namespace (tags of such UDTS were added for reading). [Jira 984705]
To solve the issue, restart the FactoryTalk Linx service.
Functional Changes
This release has the following functional changes from the previous release.
FactoryTalk Linx version 6.30.00 has the following changes in functionality since the last release:
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows
operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for
example, Windows 7 Professional, 64-bit).
Match the data type name
FactoryTalk Live Data common tag browser user interface included with FactoryTalk Services Platform
version 6.30.00 now uses data type names that match the types presented in Studio 5000 Logix
Designer.
Present array element index values in correct numerical order
FactoryTalk Live Data common tag browser user interface included with FactoryTalk Services Platform
version 6.30.00 presents array element index values with leading zeros to ensure they are listed in the
correct numerical order.
Extend supported subscription rate
FactoryTalk Live Data version 6.30.00 extends the supported subscription rates to include 600, 700,
800, and 900 ms.
Enhance the ethernet port configuration
FactoryTalk Linx version 6.30.00 enhances the ethernet port configuration to enable the selection of a
specific IP address on a workstation configured with multiple IP addresses on a computer’s Network
Interface Card (NIC), to enable FactoryTalk Linx and FactoryTalk Logix Echo to operate on the same
workstation.
Enhance to communication with more devices
FactoryTalk Linx version 6.30.00 is able to communicate to a controller or a device that was not
previously detected via the Network Browser.
Remove IO Linx communications driver
FactoryTalk Linx version 6.30.00 removed the "IO Linx" communications driver.
Stop support for an earlier version of FactoryTalk Policy Manager
FactoryTalk Linx version 6.30.00 will not support FactoryTalk Policy Manager v6.11.00.
Application Notes
This release has the following application notes.
The following are the application notes for FactoryTalk Linx version 6.30.00.
ASCII string convert modifier: SC##
The upper limit of the length of C style strings specifier (SC##) supported in FactoryTalk Linx is 400
bytes. The default upper limit value is SC30, and you can increase the upper limit manually.
Backup and restore
- When restore FactoryTalk Linx configuration in FactoryTalk Administration Console, the existing
drivers will be removed and new divers will be restored. The running shortcuts will be affected.
To avoid this issue, reconfigure the shortcuts after the restore process completed or use
FactoryTalk Linx Configuration Import Export Tool to make a backup in advance.
BOOTP/DHCP tool
- The host name information of a 1756-ENBT device cannot be configured through the
BOOTP/DHCP tool.
To avoid this problem, use FactoryTalk Linx to configure the device information.
CIP connections
CIP Security
- On a FactoryTalk Linx workstation where multiple IP addresses exist, only one of them can be
configured with CIP security in FactoryTalk Policy Manager.
Communication Setup editor
- Installing FactoryTalk Linx and RSLinx Classic on different drives result in icons displaying as
question marks in the Communications Setup editor.
To avoid this problem, FactoryTalk Linx must be installed on the same drive as RSLinx Classic.
- Attempt to create a run-time application (.mer file) when the Communication Setup editor is open
returns the message: Unable to save the project runtime file at default path.
To avoid this problem, close the Communication Setup editor before creating a run-time
application (.mer file).
ControlNet I/O and DeviceNet I/O
- Unexpected behavior occurs when browsing a BITSERIES alias with length exceed 32768 bits.
- Unexpected behavior occurs for different configurations in RSNetWorx™ and card's I/O map.
If the configuration specified in RSNetWorx for ControlNet™ or DeviceNet™ does not match what
is specified for the card's I/O map in FactoryTalk View ME, results can be unpredictable.To avoid this problem, verify the configuration in RSNetWorx matches what is specified for the
card's I/O map.
- FactoryTalk Linx may define more I/O than is actually on the interface card.
- When you are entering sequential ControlNet connections, the software incorrectly calculates the
maximum free status address.
To avoid this problem, create a connection at status word 252 prior to reaching the limit condition.
- If you sort by address selection for bit aliases, the results may be out of order.
- Large configurations may take up to several minutes to load.
This is most likely to happen if there is a large number (more than 500) of initial values of bit
arrays.
- Address String field changes may be lost.
If you make changes to the Address String box in an Alias Properties dialog box and then
select a different Alias Data Type, the changes to the Address String box are lost.
- The quality of an output array alias may remain unchanged.
If you have an output array alias whose data is delivered to two different controllers, the quality of
that data is only determined by the health of the connection(s) that cover the first byte of the array.If you have a connection that takes the sixth byte of an array, for example, and that connection
goes to a bad status, the quality of the array as a whole will remain unchanged.
Data access and tag browsing
- FactoryTalk Linx does not support some of the data types for Micro800® series controllers, which
include Date and Time, Structure and structure elements, Array of array. FactoryTalk Linx does
not support array data types with non-zero starting index. Moreover, FactoryTalk Linx cannot read
and write DINT bits directly, and it has no access to the User Defined Data Types. Bool Tags
Array are not accessible from the Micro800 series controllers.
- FactoryTalk Linx cannot read Safety-class string tags from the GuardLogix controller. If you need
to read these tags, copy the data to non-Safety-class tags.
- FactoryTalk Linx does not recognize or honor protected tags in the 1785-L46C15. Attempts to
write to any protected tags will succeed.
- Attempts to read or write input or outputs on the MicroLogix™ 1000 Series A controller will result
in data read as bad quality.
To avoid this problem, replace the Series A controller with a Series E controller.
- FactoryTalk Linx cannot browse for tags in PowerMonitor 3000 devices.
- FactoryTalk Linx cannot browse for tags secured by the FactoryTalk® AssetCentre security
feature.
- FactoryTalk Linx cannot browse for tags in SLC controllers that have been secured using the
FactoryTalk AssetCentre security feature introduced in RSLogix 500® v7.10 (CPR 7).
- FactoryTalk Linx cannot browse, read, or write the RI and PLS data table sections of a MicroLogix
1100 controller.
- FactoryTalk Linx cannot automatically browse PLC5-80E E/K Device.
- ASCII data cannot be read from SLC integer files.
- In RSLogix 5000 software or Studio 5000 Logix Designer application, if you delete a motion,
digital/analog alarm, or message tag on scan, there is no checking mechanism in the controller to
prevent the deletion. Further, there is no visual indication in RSLogix 5000 software or Studio
5000 Logix Designer application that these tag types have been deleted from scan; it will appear
as if these tags continue to receive data, but that data is invalid. If you have these types of tags on
scan, Rockwell Automation recommends that you do not delete them. For more information, see
the Knowledgebase Document ID: QA8279 - What tags in a Logix controller can be deleted whilst
on scan in an HMI application .
- In Studio 5000 Logix Designer, if you rename a program online, communications to tags using the
old name are not initially affected and the tag browser will not initially show the tags under the new
program name until the FactoryTalk Linx service is restarted, the controller is restarted or a new
application is downloaded into the controller, at which time communications to the tags using the
old program name will fail and the tag browser will show tags under the new program name.
To prevent this problem, avoid renaming a program online. If a program is renamed online, restart
the FactoryTalk Linx service or restart the controller, or redownload the controller's application
after renaming a program.
DH+ limitations
- FactoryTalk Linx added EtherNet/IP to DH+ Bridging, it can now read data from PLC5 and
SLC-500 controllers connected to DH+.
- When FactoryTalk Linx added EtherNet/IP to DH+ Bridging, the 1756-DHRIO supports up to 32
CIP connections per channel. If more connections are needed, utilize the second channel on the
1756-DHRIO module or install additional 1756-DHRIO modules in the ControlLogix Chassis.
- In FactoryTalk Linx, using DHRIO to connect a controller, the upper limit of connection through
this DHRIO module is 32 per channel. For ControlLogix Controllers, each shortcut can create 2-8
connections. For SLC/PLC controllers, each shortcut can create 1-4 connections. If a redundant
(secondary) FactoryTalk Linx server is configured, the number of connections through the DHRIO
Module will be doubled. FactoryTalk Linx added a user option to limit the number of connections
for a shortcut of SLC/PLC controllers, more information can be found in the Shortcut Properties
table in the FactoryTalk Linx Help.
- If a PanelView Plus 7 terminal needs to access data from PLC5 and SLC-500 controllers
connected to DH+, the upper limit of connection is 2 per shortcut, which is a fixed value and
cannot be adjusted.
- FactoryTalk Linx can only utilize solicited communication controllers on DH+ (the unsolicited
shortcut type cannot be used).
- FactoryTalk Linx does not support modifying the configuration of the DHRIO module or SLC/PLC
controllers under the DHRIO module.
- FactoryTalk Linx does not support Map PLC/SLC Message when user needs to read or write data
from ControlLogix controller connected to DH+ with PCCC protocol. User could use CIP instead to
read and write data from ControlLogix controller.
- FactoryTalk Linx is unable to support Logix controller based alarms or access to Extended Tag
properties of controllers connected using DH+. Disable the Enable alarm and event support,
Upload all extended tag properties, and Provide pass-through descriptions for tags options.
- For SLC or PLC controllers with the same node on different channels connected to a 1756-DHRIO
module, if the Enable Network Path (System > Policies > Product Policies > FactoryTalk Linx
> Server Setting > Shortcut Policy) is set to Disable, FactoryTalk Linx will browse the device
using the Device Path which does not contain node address information, so FactoryTalk Linx will
pick up the wrong device on other channel. If the Enable Network Path is set to Enable,
FactoryTalk Linx will browse the device using the Network Path which contains node address
information, so different SLC or PLC controllers with the same node address can be distinguished.
EtherNet/IP compliance
- This version of FactoryTalk Linx maintains compliance with the EtherNet/IP standard of Open
DeviceNet Vendor Association, Inc. (OVDA).
ControlFLASH
- FactoryTalk Linx version 6.00.00 cannot be used as the communication software if you are using
ControlFLASH version 14.00.00.
To avoid this problem, upgrade ControlFLASH to version 15.00.00 and try again, or use RSLinx
Classic as the communication software.
FactoryTalk Alarms and Events
- If FactoryTalk Linx is uninstalled and then reinstalled, controller-generated alarms will not be
shown.
To avoid this problem, reboot your computer before you reinstall FactoryTalk Linx.
- Duplicate alarms may exist when renaming or deleting a shortcut.
If a shortcut is renamed or deleted, the previous FactoryTalk Alarms and Events subscription to
that shortcut remains until the FactoryTalk Linx service is restarted.
To prevent generation of duplicate alarms, restart the FactoryTalk Linx service after you rename
or delete a shortcut.
- Special characters in shortcut names may results in unexpected behavior.
Device Shortcuts are defined in the Communications Setup editor for the FactoryTalk Linx
server. Using shortcut names containing special characters (for example, asterisks, pipes) results
in unexpected behavior in the FactoryTalk Alarms and Events system.To avoid this problem, do not use special characters in the device shortcut name for the
FactoryTalk Linx server when using FactoryTalk Alarms and Events to monitor device-based
alarms.
- If an analog alarm uses a DINT as the input value, the value may be reported incorrectly in
custom messages for very large DINTs (both positive and negative).
If the DINT value exceeds 24 significant bits, the controller will round it to the nearest REAL value
using 24 significant bits. This applies only to the input value and not associated tag values.
- If an alarm changes state ("out of alarm" to "in alarm") while FactoryTalk Linx is disconnected from
the network, the last transition message logged to the database is correct but duplicated.
- When rehosting a FactoryTalk Alarms and Events server to a different computer, the prior host
computer may fail to unload the running alarm server, and the new host computer may fail to load
the alarm server.
To avoid this problem, restart both the prior and new host computers.
Fast User Switching
- FactoryTalk Linx does not support the Fast User Switching feature in Windows operating systems.
File Transfer Utility
- In FactoryTalk View Studio, you cannot use the File Transfer Utility to upload/download
FactoryTalk View ME (*.mer) files from/to a network location. Although the upload/download
appears to complete (via the disappearance of the upload/download progress bar), a follow-up
dialog box notifies you that the operation did not complete.
Uploading/downloading FactoryTalk View ME (*.mer) files from/to your local computer works
properly. If you want to download a file, please copy it from the network location to your local hard
drive. If you want to upload a file, upload to a local hard drive and then copy it to the network
location.
Firmware Upgrade Wizard
- The operation of the Firmware Upgrade Wizard over the Serial-DF1 port is not supported.
To avoid this problem, it is strongly recommended that you create a Firmware Upgrade Package
on an external compact flash and use this as a means to upgrade your terminal.
Hardware and operating system
- Memory related counters and predefined tags are not displayed correctly for L8x controllers. This
information is normally obtained from the controller. However, the Logix L8 (ControlLogix 5580
and CompactLogix 5480) series of controllers do not provide this information because of
architectural changes within the controller firmware.
- Diagnostic counters:FreeMem, FreeMem Datatable, FreeMem General, FreeMem IO,
FreeMem Security, TotalMem, TotalMem Datatable, TotalMem General, TotalMem IO,
TotalMem Security
- Predefined tags: @FreeMem, @FreeMemIO, @FreeMemDT, @FreeMemGM,
@FreeMemSC, @TotalMem, @TotalMemIO, @TotalMemDT, @TotalMemGM,
@TotalMemSC
Impact of Microsoft deprecating VBScript
- Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
- FactoryTalk Linx versions 6.60.00 and earlier require VBScript for installation. Installation will
fail if VBScript is not enabled.
- To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS
KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was
raised to Packet Integrity.
|
IMPORTANT
|
Installing this product’s latest version with earlier unpatched
versions of other FactoryTalk products or products using Classic
OPC DA connections may cause a loss of connectivity due to the
difference in DCOM authentication level used. For additional
information, see the Knowledgebase Document ID: IN39461 -
Microsoft DCOM Hardening Information TOC .
|
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates
the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is
used by many Rockwell Automation products and may be affected by the change that is made by the
Microsoft patch. For additional information about the affected Rockwell Automation products, see the
Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation
products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch
(MS KB5004442) .
Network Browser
- The Who Browser is renamed to Network Browser in FactoryTalk Linx version 6.00.00.
- If multiple copies of the Network Browser are open and have the same driver selected, the
browser discovery for the selected driver may not work.
To avoid this problem, close other instances of the browser or have them select a different driver.
- The FactoryTalk Linx driver name are limited to a subset of ASCII characters. The FactoryTalk
Linx Network Browser fails to load if double-byte characters, a period (.), backslash (\), left bracket
([), or right bracket (]) are embedded in the name.
To avoid this problem, follow the naming rule of FactoryTalk Linx drivers.
- In FactoryTalk Linx Network Browser, the computer name should not exceed 15 characters.
Otherwise, the workstation name in Network Browser topology will be truncated to 15 characters.
This issue is first found in RSLinx Enterprise version 5.90.00.
Networks, drivers, and devices
- The 1756-DH485 module is not supported as bridge device in FactoryTalk Linx.
- On occasion, an attempt to download a large .mer file over a DF1 connection to a PanelView terminal fails.
To avoid this problem:
- Retry downloading the file.
- When communicating with PanelView Plus units, be sure to set the error-checking mode to CRC.
- The I/O card does not show up in the tag browser.
If you are unable to use the SLC I/O in the slot you have selected, the I/O card does not show up in the tag browser.
To avoid this problem, try to use a different slot.
- Addresses above word 99 in a MicroLogix 1500 input table does not show correctly.
To avoid this problem, use only addresses 0 to 99 for display purposes.
- When entering item names for a PLC, SLC, or MicroLogix device, FactoryTalk Linx recognizes a slash (/) as a bit qualifier, but does not recognize a period (.). For example:
- O:1/7 is acceptable
- O:1.7 is not acceptable and generates an error.
- FactoryTalk Linx may take a long time to show the Device Properties dialog box for PKTCS and PCICS cards.
- Devices accessed through a 1440-ACNR module may not be properly identified, and an error message may appear stating that FactoryTalk Linx fails to recognize the bus type.
- In FactoryTalk Linx version 6.20.00, after renaming a driver, any shortcuts pointing to devices referencing the driver may fail to communicate.
To prevent this problem, avoid renaming drivers. If a driver is renamed and communications through a shortcut fails, either restore the original driver name or use the shortcut configuration dialog to update any effected shortcuts to the correct device under the renamed driver.
Pass-through description
- If an alias tag is created with its base tag's data type as ALARM_ANALOG and ALARM_DIGITAL,
FactoryTalk Linx doesn't provide pass-through descriptions for this alias tag. Manually input
descriptions if needed.
Predefined items
- Starting with version 6.10.00, the FactoryTalk Linx "@RedundancyMode" pre-defined tag was
removed and is no longer supported. If an application attempts to access the data value for this
tag, it will only receive the default value "0" and the reference will show as a wireframe in
FactoryTalk View. To avoid this, remove references to this tag from the application.
Remote I/O
- Double-right-clicking a node in the I/O tree may show the menu for an unselected item.
- The 1771-SN sub-scanner does not support block transfers for remote I/O.
Shortcuts
- If you create a PLC5 or SLC500 shortcut with a name longer than 135 characters, you are not able to access that PLC or SLC.
To avoid this problem, limit the PLC or SLC shortcut names to less than 135 characters.
- If you change a FactoryTalk Linx shortcut from one driver type to another, for example, from Ethernet to ControlNet, you may not be able to access data on the newly configured shortcut.
To restore data access, reboot the FactoryTalk Linx computer.
- If you configure FactoryTalk View SE to run in a distributed environment, and disconnect (or power off) the computer functioning as the FactoryTalk Directory server, the Communication Setup editor cannot show any previously configured shortcuts.
To view your shortcuts, ensure that the computer functioning as the FactoryTalk Directory server is powered on and connected to the network.
- Clients may not re-establish communications to offline device shortcuts after rebooting FactoryTalk Linx data server.
For the shortcuts which are configured to offline devices, clients may fail to communicate to them after the FactoryTalk Linx data server is rebooted.
To recover communications to offline device shortcuts, click Show All Devices in the Communication Setup editor.
- In a FactoryTalk ME runtime application, if both Processor and CIP-CIA shortcuts point to the same device, after a connection break, the tag value on the terminal will take extended period of time to recover.
- When FactoryTalk Linx is utilized in a PlantPAX system, or a FactoryTalk View system that utilizes Logix Extended Tag properties or tag based alarms, tag data delivery times, controller and network loading are negatively impacted if the extended tag property checkboxes (Upload all extended tag properties and Display pass-through values for tag extended properties) for the primary and secondary FactoryTalk Linx data servers are not enabled.
To ensure the best operation, the extended tag properties checkboxes for the primary and secondary FactoryTalk Linx data servers should be enabled on both servers.
- If user deletes a shortcut or reconfigures a shortcut to a different device, the related connections are not released.
To avoid this problem, close and reopen the Live Data Test Client, or restart the FactoryTalk Linx service.
Security considerations
- For information on the security considerations when using Rockwell Automation products,
including:
System sizing recommendations
- When you design and set up a FactoryTalk system, we recommend using the following guidelines.
If you find that your system needs to expand beyond these guidelines, contact your Rockwell
Automation sales or distributor representative to discuss your application design.
|
Component
|
Recommended guidelines
|
|
FactoryTalk Alarms and Events
|
|
|
FactoryTalk Alarms and Events servers per application
|
10 non-redundant servers or 10 redundant server pairs
|
|
FactoryTalk tag-based alarms per server
|
20,0001
|
|
Logix device-based alarms per server
|
10,0002
|
|
Total alarms per application
|
100,0003
|
|
FactoryTalk Linx
|
|
|
FactoryTalk Linx data servers per application
|
10 non-redundant servers or 10 redundant server pairs
|
|
Total device tags per application
|
1,000,0004
|
|
Tags per FactoryTalk Linx data server
|
100,0004
|
|
FactoryTalk View SE
|
|
|
HMI servers
|
10 non-redundant servers or 10 redundant server pairs
|
|
HMI tags per HMI Server
|
40,0005
|
|
Total data logged tags per HMI server (1-second scan rate)
|
5,000
|
|
FactoryTalk View SE client sessions simultaneously connected to
the application
|
1204
|
|
FactoryTalk ViewPoint SE servers per application
|
4
|
|
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
|
50
|
- The number of alarm backing tags influences the maximum number of available alarms because they increase the
resource requirements of the alarm server. When using backing tags for status and control, a good rule of thumb is to
multiply the total number of backing tags by the total number of alarms, and ensure the result is less than 20,000.
PlantPAx® users should refer to the PlantPAx Reference Manual PROCES-RM001 for alarm server sizing guidance for
a PlantPAx application.
- This number is the sum of both instruction alarms and Logix tag-based alarms across all the controller shortcuts in each
FactoryTalk Linx server.
- The total number of alarms per application includes all FactoryTalk Alarms and Events tag-based and device-based
alarms in the application.
- Refer to Rockwell Automation Answer ID 1070902
http://rockwellautomation.custhelp.com/cgi-bin/rockwellautomation.cfg/php/enduser/std_adp.php?p_faqid=1070902 to
determine system scalability using this option.
- The maximum number of HMI tags that can be created on a single HMI server is 175,000. Extensive use of HMI tags
has a significant performance impact on an HMI server, so Rockwell Automation recommends minimizing their use, and
instead using direct-reference tags as much as possible.
|
Update Rate
- The FactoryTalk Live Data server has the following update rate settings:
- 10 ms
- 20 ms
- 50 ms
- 100 ms
- 250 ms
- 500 ms
- 600 ms
- 700 ms
- 800 ms
- 900 ms
- 1000 ms
- A number that is a multiple of 1000 ms
- When a client application sets an update rate different from the FactoryTalk Live Data server
settings, the FactoryTalk Live Data server will update the tag using the closest update rate. For
example, the client application sets a 70 msc update rate, the FactoryTalk Live Data server will
use 50 msc instead. If the client application update rate is configured as 1000 msc or larger, the
FactoryTalk Live Data server will use the integer seconds. For example, the client application sets
a 1600 msc update rate, the FactoryTalk Live Data server will use 2000 msc instead. Note that if
the client update rate is set as 0 msc, the FactoryTalk Live Data server will use 10,000 msc
instead.
- There are many factors that can impact the resulting speed that data can be accessed (controller
or network communications bandwidth, computer processing capacity, other operations being
performed on the computer running FactoryTalk Linx), because of this, requested data values
may/will be missed, particularly for the faster rates. Verify the system operation to ensure it
handles the resulting effective rate and handles cases where periodic values are not delivered.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Installation Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are
case-insensitive. However, if a specified value includes a space, be sure to enclose the value in
quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation
using an IT tool or script, and don’t expect any error or restart messages.
When using this parameter, check the error codes, and respond as needed.
For example, if the installation returns error code 1641, then the IT tool or
script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress
through the UI, it does not accept any input but still shows errors or restart
messages.
When using this parameter, the installation will stop and display a prompt if
there are errors or restart messages. For example, if an immediate restart is
required to complete the install, a restart message will be displayed to confirm
the restart. Installation resumes automatically from the point of interruption
after restart.
This parameter is required if /Q is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used
when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will
return either error code 1641 or 3010 if a restart is required, and unattended
install (/QS) will result in a confirmation prompt that must be agreed to before
the installation is completed.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during install process.
The value must be one of the following:
- ENU
- CHS
- DEU
- ESP
- FRA
- ITA
- JPN
- KOR
- PTB
This parameter is optional. If this parameter is not used, the default language
is the current user or operating system user interface language.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a
warning occurs.
|
|
/ftsp-s
|
Specifies the FactoryTalk directory scope for restore. Only "Global" and
"Local" scopes are supported.
This parameter is optional.
|
|
/ftsp-bak
|
Specifies the location where the restore file can be found.
This parameter is optional.
|
|
/ftsp-pp
|
Specifies the plain text used to decrypt the backup file.
This parameter is optional.
|
|
/ftsp-value=enable/disable
|
Specifies to enable or disable the option Require computer accounts for all
client machines in Security Policy. The option is used to determine whether
or not a client computer account must exist in the directory to login.
This parameter is optional.
|
|
/DirectoryServer
|
Specifies the directory server name.
This parameter is optional. If it is not specified, the setup turns on HTTPS for
communication, and a TLS certificate must be configured after installation.
|
|
/NoHTTPS
|
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for
communication, and a TLS certificate must be configured after installation.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/InstallDrive="value"
|
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install
location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is
installed on. Use /? to determine which parameter is supported.
|
|
/Uninstall
|
Use to uninstall the product. This parameter is optional.
|
Examples
The following examples show how to use the installation commands.
- To install the software with no user interface using the default settings during the installation
process. (Silent install)
Setup.exe /Q /IAcceptAllLicenseTerms
- To install the software with Chinese displayed during the install process and restart the computer
if necessary. (Unattended install)
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS
- To install the software with FactoryTalk security policy value specified.
Setup.exe /Q /IAcceptAllLicenseTerms /ftsp-value=enable
- To perform a restore during the install process.
Setup.exe /Q /IAcceptAllLicenseTerms /ftsp-bak="C:\aa.bak"
- To specify the FactoryTalk Directory machine.
Setup.exe /Q /IAcceptAllLicenseTerms /DirectorySever=severname
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support personnel.
|
|
ERROR_REBOOT_CONTINUE
|
1641
|
A restart is required to continue the installation.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restarting,
the product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart is pending. Restart the computer to continue the
installation.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the installation
log file for details. To complete the installation, restart the
computer.
|
Certificates
The following certificates are installed while installing Rockwell Automation software.
- Use Microsoft Management Console (MMC) to view the certificates in Console Root >
Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
- 2016-Rockwell-Driver-SHA1.cer
- 2016-Rockwell-SHA256.cer
- DriverCodeSigning2012-1.cer
- Drivers-10-10-2018.cer
- Drivers-11-03-2017.cer
- Drivers-12-06-2016.cer
- DriversSHA1-10-10-2018.cer
- Drivers-SHA1-11-27-2017.cer
- Logix-11-04-2016.cer
- Rockwell_2013.cer
- Rockwell_2014.cer
- Rockwell_2015.cer
- rockwellcert2010.cer
- rockwellcert2013.cer
- VeriSign Class 3 Public Primary Certification Authority -G5 2036.cer
- Use Microsoft Management Console (MMC) to view the certificates in Console Root >
Certificates (Local Computer) > Trusted Publishers > Certificates.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.