This release has the following requirements.
FactoryTalk ViewPoint version 13.00.00 (CPR 9 SR 13)
FactoryTalk ViewPoint works within the system requirements of all Rockwell Automation software products.
For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware Requirements
For the optimal performance of publishing applications, the personal computer is recommended to meet or exceed the following hardware requirements:
FactoryTalk ViewPoint has been tested with the following mobile devices:
FactoryTalk ViewPoint for Machine Edition requires the following PanelView™ Plus graphic terminal hardware:
Operating systems
FactoryTalk ViewPoint server has been tested on the following operating systems:
* For more information about the Windows 10 operating system support, see Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.
** For more information about the Windows Server 2016 operating system support, see Knowledgebase Document ID: IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.
Required software
FactoryTalk ViewPoint is an add-on to an existing FactoryTalk View system and requires FactoryTalk View version 13.00.00.
FactoryTalk ViewPoint for Site Edition automatically installs the following required software on the host computer, if necessary:
FactoryTalk ViewPoint for Machine Edition automatically installs the following required software on the host computer, if necessary:
Supported Browsers
The following web browsers have been tested and are supported for use with this release:
The following mobile web browsers have been tested and are supported for use with this release:
Windows Firewall Program and Services exception list
Firmware requirements
FactoryTalk View ME can create Machine Edition Runtime applications (.mer) that run on PanelView Plus graphic terminals. The PanelView Plus firmware must support the .mer file to host FactoryTalk ViewPoint content.
|
PanelView Plus Terminal
Firmware Version
|
Machine Edition Runtime
Version
|
FactoryTalk ViewPoint Content
(contained in .mer)
|
|
13.00-2022mmdd or later
|
13.00
|
13.00
|
|
12.00-2020mmdd or later
|
12.00
|
12.00
|
|
11.00-2019mmdd or later
|
11.00
|
11.00
|
|
10.00-2018mmdd or later
|
10.00
|
10.00
|
|
9.00-2016mmdd or later
|
9.00
|
9.00
|
|
8.20-2016mmdd or later
|
8.20
|
8.20
|
|
8.10-2015mmdd or later
|
8.10
|
8.10
|
|
8.00-2014mmdd or later
|
8.00
|
8.00
|
|
7.00-2012mmdd or later
|
7.00
|
2.60
|
|
6.1-2011mmdd or later
|
6.10
|
2.10
|
|
6.0-20110425 or later
|
6.00
|
1.20 or 2.00
|
|
5.10.01 or later
|
5.10
|
1.10
|
Security requirements
To help meet secure system design requirements, review these publications:
This release includes the following system features.
There are no new or enhanced features in FactoryTalk ViewPoint for Machine Edition version 13.00.00.
FactoryTalk ViewPoint for Site Edition version 13.00.00 has the following enhanced features:
Automatic Diagnostics messages are available in FactoryTalk ViewPoint, which now allows operators to easily access device diagnostic information remotely, from a mobile device.
You can visualize FactoryTalk View SE data log models on a web client in addition to information from an MS SQL Database.
FactoryTalk ViewPoint extends mobile trending capabilities by providing the ability to plot two sets of production data, one as a function of the other: y=f(x).
You can embed a FactoryTalk ViewPoint client on a webpage using the desktop URL.
This release corrects the following anomalies.
The list identifies the anomalies corrected in FactoryTalk ViewPoint version 13.00.00. Use the identification information provided in the anomaly heading to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
This release has the following known anomalies.
These anomalies are from previous releases but are still known in this release.
To unlock the user account in FactoryTalk ViewPoint, reload the application on the PanelView Plus family terminal.
For more information, see:
This release has the following functional changes from the previous release.
FactoryTalk ViewPoint version 13.00.00 has the following changes in functionality since the last release:
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).
FactoryTalk ViewPoint for Site Edition version 13.00.00 has the following changes in functionality since the last release:
An unlimited number of client connections
FactoryTalk ViewPoint will not check licenses.
HTTPS enabled by default
If you install FactoryTalk ViewPoint for Site Edition, the installation enables HTTPS by default.
If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk ViewPoint. For details on configuring a TLS certificate, see FactoryTalk ViewPoint Quick Start Guide.
This release has the following application notes.
The following are the application notes for FactoryTalk ViewPoint version 13.00.00.
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Shows the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface. This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart. This parameter is required if /QS is not specified. |
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages. When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart. This parameter is required if /Q is not specified. |
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms. This parameter is required for /Q or /QS parameters. |
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation. This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed. |
|
/Record
|
Records the installation options chosen to a recording file. This parameter is optional. |
|
/Playback
|
Plays back a recording file to specify the installation options. This parameter is optional. |
|
/Repair
|
Runs a repair operation on the installed products. This parameter is optional. |
|
/Uninstall
|
Uninstalls the product. |
|
/SetupLanguage="value"
|
Specifies which language will be shown during the install process. The value must be one of the following:
|
|
/InstallDrive="value"
|
Specifies the installation drive. This parameter is optional. If this parameter is not used, the default install drive is C:. |
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues. This parameter is optional. If it is not specified, the setup exits when a warning occurs. |
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to activate the software during installation. This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required, this parameter is not available. |
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation. This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required, this parameter is not available. |
|
/Version="value"
|
Specifies the version of the software to activate, which corresponds to the product version associated with the SerialNumber and ProductKey. This parameter is optional. If it is not specified, the installer will use the most recent product version available. Some software does not require activation. If activation is not required, this parameter is not available. |
|
/NoHTTPS
|
Specifies that the setup turns off HTTPS. This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation. |
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support personnel.
|
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a restart. After restart, the installation
will continue.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restart,
the product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart the computer for the installation to
continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the installation
log file for details. To complete the installation, restart the
computer.
|
Application notes for FactoryTalk ViewPoint for Site Edition version 13.00.00.
HTTPS enabled by default
If you install FactoryTalk ViewPoint for Site Edition, the installation enables HTTPS by default.
If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk ViewPoint. For details on configuring a TLS certificate, see FactoryTalk ViewPoint Quick Start Guide.
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
|
IMPORTANT
|
Installing this product’s latest version with earlier unpatched
versions of other FactoryTalk products or products using Classic
OPC DA connections may cause a loss of connectivity due to the
difference in DCOM authentication level used. For additional
information, see the Knowledgebase Document ID: IN39461 -
Microsoft DCOM Hardening Information TOC.
|
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk ViewPoint Site Edition versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
Unsupported FactoryTalk View features
Graphic displays that contain unsupported objects or features can still be published to a FactoryTalk ViewPoint server and viewed in a web browser. During the publishing process, unsupported objects are removed from displays, so that they do not interfere with the web application.
Each unsupported object or feature generates a warning during publishing, which is recorded in the publishing report. To check the report, after publishing is finished, click the link View publishing report.
FactoryTalk ViewPoint does not support the following FactoryTalk View objects or features:
Graphic display properties
Graphic objects and object properties
To avoid this problem, do not use Pattern Style properties to communicate any critical state or message in a FactoryTalk ViewPoint application.
|
Tabs
|
Properties
|
|
General
|
|
|
Display
|
|
|
Pens
|
|
|
X-Axis
|
|
|
Y-Axis
|
|
|
Overlays
|
All
|
|
Templates
|
All
|
|
Common
|
Other
|
|
Tabs
|
Properties
|
|
Common
|
|
|
Time Period
|
|
|
Chart
|
|
|
X-Axis
|
All
|
|
Application
|
All
|
|
Live Data
|
All
|
|
Retrieval
|
All
|
|
Y-Axis
|
|
|
Trace
|
|
Object animation
The number of places after the decimal point changes dynamically based on the linked tag value.
Logic and control functions
View the execution results in FactoryTalk Diagnostics Viewer.
Local message files
To convert the references successfully, open and save the local message file in FactoryTalk View Studio and then re-publish the web application.
Network Distributed application conversion
To avoid this problem, increase the size of the browser's temporary folder for the System user to 1024 MB.
Upgrading FactoryTalk ViewPoint from version 8.00.00 or earlier
Upgrading to FactoryTalk ViewPoint version 10.00.00 from version 8.00.00 or earlier changes existing FactoryTalk ViewPoint application and object behavior. Review the following list to determine if design or configuration changes are required in your application before performing an upgrade.
Re-publish all displays and download a new .mer file to each terminal after upgrading to FactoryTalk ViewPoint version 10.00.00.
Trend
Conversion to HTML 5
Text
String and Numeric input
Alarms
Regional settings
FactoryTalk Security
To address this issue, verify that the FactoryTalk user belongs to the FactoryTalk User Group that has Write or View access to the display that the user is trying to access. For updated information, subscribe to Knowledgebase Document ID: QA47921 - FactoryTalk ViewPoint 2.00 : Unauthorized: You are not authorized to view display [<display name>].
Note that the FactoryTalk Security user group, Administrators, cannot currently be used for FactoryTalk ViewPoint Security. If FactoryTalk user belongs to the Administrators group, the FactoryTalk User should be added to a different role or FactoryTalk Security user group that the desired permissions can be given to.
Installation
To avoid this problem, enable Static Content when configuring IIS for Windows 7 operating systems.
To avoid this problem, uninstall FactoryTalk ViewPoint first.
Currently there is no solution for this issue except to be aware that the full install of Supervisory Edition has not been performed on the engineering workstation however Machine Edition and ViewPoint will function properly. For updated information, subscribe to Knowledgebase Document ID: BF12388 - Installing ViewPoint Server on a computer with FactoryTalk View Studio for Machine Edition installed alters Studio behavior.
Publishing displays
To avoid this problem, manually republish the application.
To avoid this problem, ensure the primary FactoryTalk View SE server is online before publishing an application.
To avoid this problem, manually publish the application after the parameter file is changed.
To avoid this problem, after upgrading FactoryTalk ViewPoint, manually republish the application. This will allow the background publishing to operate properly and is only necessary the first time an application is accessed after an upgrade.
Navigation
To avoid this problem, refresh or reload the browser page.
To learn more, see Knowledgebase Document ID: BF11742 - Internet Explorer performance issues after running one FactoryTalk ViewPoint display for extended periods of time.
To avoid this problem, enable cookies.
Browser compatibility
To avoid this problem, disable the Display intranet sites in Compatibility View option in the browser's Compatibility View Settings.
KEPServer
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View Installation Guide.
Application notes for FactoryTalk ViewPoint for Machine Edition version 13.00.00.
Unsupported FactoryTalk View features
Graphic displays that contain unsupported objects or features can still be published to a FactoryTalk ViewPoint server and viewed in a web browser. During the publishing process, unsupported objects are removed from displays, so that they do not interfere with the web application.
Each unsupported object or feature generates a warning during publishing, which is recorded in the publishing report. To check the report, after publishing is finished, click the link View publishing report.
FactoryTalk ViewPoint does not support the following FactoryTalk View objects or features:
Multiple language support
Graphic display properties
Graphic objects and object properties
To avoid this problem, do not use Pattern Style properties to communicate any critical state or message in a FactoryTalk ViewPoint application.
|
Tabs
|
Properties
|
|
General
|
|
|
Display
|
All
|
|
Pens
|
|
|
X-Axis
|
|
|
Y-Axis
|
|
|
Overlays
|
All
|
|
Templates
|
All
|
|
Common
|
Other
|
|
Connections
|
|
Object animation
Logic and control functions
Number of lines of text
Internet Explorer performance issue
To learn more, see Knowledgebase Document ID: BF11742 - Internet Explorer performance issues after running one FactoryTalk ViewPoint display for extended periods of time.
Local message files created in RSView 4.00 (CPR 7) and earlier
To convert the references successfully, open and save the local message file in FactoryTalk View Studio and then re-publish the web application.
Upgrading FactoryTalk ViewPoint from version 8.00.00 or earlier
Upgrading to FactoryTalk ViewPoint version 10.00.00 from version 8.00.00 or earlier changes existing FactoryTalk ViewPoint application and object behavior. Review the following list to determine if design or configuration changes are required in your application before performing an upgrade.
Re-publish all displays and download a new .mer file to each terminal after upgrading to FactoryTalk ViewPoint version 10.00.00.
Trend
Conversion to HTML 5
Text
String and Numeric input
Regional settings
FactoryTalk Security
To address this issue, verify that the FactoryTalk user belongs to the FactoryTalk User Group that has Write or View access to the display that the user is trying to access. For updated information, subscribe to Knowledgebase Document ID: QA47921 - FactoryTalk ViewPoint 2.00 : Unauthorized: You are not authorized to view display [<display name>].
Note that the FactoryTalk Security user group, Administrators, cannot currently be used for FactoryTalk ViewPoint Security. If FactoryTalk user belongs to the Administrators group, the FactoryTalk User should be added to a different role or FactoryTalk Security user group that the desired permissions can be given to.
Navigation
To avoid this problem, enter the following URL, replacing ip_address with the IP address of the PanelView Plus terminal:
http:\\ip_address
To avoid this problem, refresh or reload the browser page.
To avoid this problem, enable cookies.
Installation
Currently there is no solution for this issue except to be aware that the full install of Supervisory Edition has not been performed on the engineering workstation however Machine Edition and ViewPoint will function properly. For updated information, subscribe to Knowledgebase Document ID: BF12388 - Installing ViewPoint Server on a computer with FactoryTalk View Studio for Machine Edition installed alters Studio behavior.
Publishing displays
To avoid this problem, manually republish the application.
KEPServer
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View Installation Guide.