This release has the following requirements.
FactoryTalk View ME version 13.00.00 works within the system requirements of all Rockwell Automation® software products. For the latest compatibility information, refer to the Product Compatibility and Download Center.
Hardware requirements
The following is a sample specification of computer hardware to run FactoryTalk View ME applications aligned with the hardware used in product development testing.
Software requirements
FactoryTalk View ME has been tested on the following operating systems:
* For more information about the Windows 10 and Windows Server 2016 operating system support, see Known anomalies inherited from previous releases.
** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.
Supported browsers
The following web browsers have been tested and are supported for use with this release:
Supported SQL Server
FactoryTalk View ME version 13.00.00 supports SQL Server 2019 Express LocalDB as HMI tag databases.
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Security requirements
To help meet secure system design requirements, review these publications:
To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products (publication SECURE-AT001).
This release includes the following system features.
FactoryTalk View ME version 13.00.00 has the following new and enhanced features:
New features
There are no new features in this release.
Enhanced features
The Cross Reference form adds the function to search object names.
The Image object supports the horizontal or vertical position animation.
RecipePlus is enhanced to write the runtime recipe name to a tag after downloading the recipe. It also provides the option to define decimal limits for ingredients.
This release corrects the following anomalies.
The list identifies the anomalies corrected in FactoryTalk View ME version 13.00.00. Use the identification information provided in the anomaly heading to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
This release has the following known anomalies.
There are no known anomalies reported in FactoryTalk View ME version 13.00.00.
These anomalies are from previous releases but are still known in this release.
To resolve this problem, reload the runtime application in FactoryTalk View ME Station.
To avoid this problem, you can use the PNG files provided in
Knowledgebase Document ID: BF17144 - Transparency is not working
correctly on the PanelView Plus 6/7 terminals for Symbol Factory objects.
There is currently no workaround for this anomaly.
To avoid this problem, go to Control Panel > Regional and Language Options, and select the appropriate language to match the desired language.
To avoid this problem, enter a valid value in the expression setting for the animation property of the base object first.
To avoid this problem, re-configure the project window size in the Project Settings window.
To successfully register or unregister an ActiveX Control object, do one of the following before the operation:
For more information about UAC, see Application notes.
To avoid this problem, put the Recipe ActiveX control object on a Replace display.
There is currently no workaround for this anomaly.
To avoid this problem, use a mouse and right-click the component to open the menu.
Parameters can be resolved in the test run or runtime mode.
Loading a web page every number of
seconds (s)
|
Approximate memory leak increase
by the number of kilobytes (KB)
|
Approximate cumulative memory
leak over a 600-second duration
|
30 s
|
56 KB
|
1,120 KB
|
60 s
|
58 KB
|
580 KB
|
300 s
|
133 KB
|
266 KB
|
There is currently no workaround for this anomaly.
To avoid this problem, follow the steps below:
C:\Program Files (x86)\Common Files\Rockwell\ on 64-bit operating systems
C:\Program Files\Common Files\Rockwell\ on 32-bit operating systems
where C: is the drive to which Rockwell Automation applications are installed.
regsvr32 RnaSecurityInterfaces.dll
There is currently no workaround for this anomaly.
To show the Chinese characters, link the Tahoma, Arial, and Courier New fonts with Arial Unicode MS.
To link a font with Arial Unicode MS
To ensure that the global connection for remote navigation works, close ME Custom String Popup Keyboard.
To avoid this problem, remove the parameter from the global object.
To avoid this problem, use a tag for the Data_Source connection instead of a tag placeholder.
There is currently no workaround for this anomaly.
To unlock the user account in FactoryTalk ViewPoint, reload the application on the PanelView Plus family terminal.
To avoid this problem, run the Microsoft Hotfix KB3201845 outlined in https://support.microsoft.com/en-us/kb/3201845.
Alternatively, you can run Windows 10 v1703 or other supported operating systems where this issue is not present.
For more information about Windows 10 operating system support, see Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.
For more information about Windows Server 2016 operating system support, see Knowledgebase Document ID: IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.
To avoid this problem, configure the data source name and target table. Then other changes can be saved on the ODBC Database tab.
This release has the following functional changes from the previous release.
FactoryTalk View ME version 13.00.00 has the following changes in functionality since the last release:
Web Browser ActiveX control on a PanelView Plus 7 Performance Series B terminal
On a PanelView Plus 7 Performance Series B terminal, the Web Browser ActiveX control becomes a button, which opens the specified URL in Microsoft Edge.
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).
Remove the support of upgrading firmware on a Windows CE 4.0 terminal
Firmware Upgrade Wizard no longer supports upgrading firmware on a PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal.
Remove the function of creating 5.0 and 5.10 runtime applications
FactoryTalk View ME version 13.00.00 removes the function of creating 5.0 and 5.10 runtime applications, but allows the upgrade of 5.0 and 5.10 applications to 13.0.
Remove the function of directly adding controller instruction faceplates in FactoryTalk View Studio
FactoryTalk View ME no longer supports directly adding controller instruction faceplates to an application in FactoryTalk View Studio. Alternatively, you can import controller instruction faceplates to an application in FactoryTalk View Studio. For the latest controller instruction faceplates, search "process library" on Product Compatibility and Download Center.
This release has the following application notes.
The following are the application notes for FactoryTalk View ME version 13.00.00.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
Parameter
|
Description
|
/?
|
Displays the usage options for installation parameters.
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface. This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart. This parameter is required if /QS is not specified. |
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages. When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart. This parameter is required if /Q is not specified. |
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms. This parameter is required for /Q or /QS parameters. |
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation. This parameter is optional. If this parameter is not used, silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed. |
/Record
|
Records the installation options chosen to a recording file. This parameter is optional.
|
/Playback
|
Plays back a recording file to specify the installation options. This parameter is optional. |
/Repair
|
Runs a repair operation on the installed products. This parameter is optional. |
/Uninstall
|
Uninstalls the product.
|
/SetupLanguage="value"
|
Specifies which language will be displayed during install process. The value must be the one of the following:
|
/Product="value"
|
Specifies which sub-products will be installed. This parameter is required. For FactoryTalk View ME, the value must be one of the following:
For FactoryTalk View SE, the value must be one of the following:
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed. The value must be one of the following:
|
/InstallDrive="value"
|
Specifies the installation drive. This parameter is optional. If this parameter is not used, the default install drive is C:. |
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues. This parameter is optional. If it is not specified, the setup exits when a warning occurs. |
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to activate the software during installation. This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required, this parameter is not available. |
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation. This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required, this parameter is not available. |
/Version="value"
|
Specifies the version of the software to activate, which corresponds to the product version associated with the SerialNumber and ProductKey. This parameter is optional. If it is not specified, the installer will use the most recent product version available. Some software does not require activation. If activation is not required, this parameter is not available. |
Error codes
The following table identifies the error codes that can be returned by an installation.
Error Code
|
Value
|
Description
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was canceled by the user.
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation.
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support personnel.
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a restart. After restart, the installation
will continue.
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restart,
the product is successfully installed.
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart the computer for the installation to
continue.
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
ERROR_SUCCESS_WARNING_REBOOT
|
3014
|
The installation succeeded with warnings. Check the installation
log file for details. To complete the installation, restart the
computer.
|
Examples
The following examples show how to use the installation commands.
Setup.exe /Q /IAcceptAllLicenseTerms /Product="Machine Edition Station for Windows"
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /Product="Studio for
Machine Edition" /InstallDrive=D: /SerialNumber=12345ABCDE /ProductKey=ABCD2-34KDC
/Version=13.00.00
Setup.exe /Q /Repair /Product="Studio for Machine Edition"
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Communications
To avoid this problem, ensure that your version of UltraVNC is earlier than 1.04.
To avoid this problem, follow the steps below:
"Do you want to replace the terminal's current communication configuration with the application's communication configuration?"
To avoid this problem, do not include a slash mark in a tag name.
Windows operating system
To avoid this problem, run the Microsoft Hotfix KB3201845 outlined in https://support.microsoft.com/en-us/kb/3201845.
Alternatively, you can run Windows 10 v1703 or other supported operating systems where this issue is not present.
For more information about Windows 10 operating system support, see Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products.
For more information about Windows Server 2016 operating system support, see Knowledgebase Document ID: IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.
To retain the files:
Disable silent cleanup by using either of the following methods:
schtasks.exe /Change /TN "\Microsoft\Windows\DiskCleanup\SilentCleanup" /Disable
KEPServer
"DF1: Failed to open COM2: as it may be already in use by another application."
To stop the error message, remove the default Serial DF1 driver. For more information, see Knowledgebase Document ID: BF15496 - Error opening COM1 [OS Error == 55] shows up in diagnostics list when running Kepserver on PanelView Plus.
To access the project file, go to \Users\Public\Public Documents\RSView Enterprise\ME\HMI Projects\<application name>\KEPServer.
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View Installation Guide.
RSNetWorx
If you are under a current technical support contract, you may download RSNetWorx v21 or later from the Product Compatibility and Download Center.
To download RSNetWorx:
RSNetWorx v21.00 or later is also available in Studio Professional v21.00 or later. If you are not under a current technical support contract, you may purchase an update for RSNetWorx by contacting Rockwell Automation sales.
For information about RSNetWorx version 11.00 and earlier incompatibility with Rockwell Automation software products, see Knowledgebase Document ID: PN785 - Product Notice 2013-10-001 - RSNetWorx V11 and Prior Incompatibility with Rockwell Automation Software Products (201310001).
PanelBuilder 1400e
Network security
For information about:
Internet security software
Before
installing or running FactoryTalk View Studio, configure your internet firewall
to allow the following .exe files to access the Internet:
Before installing or running FactoryTalk View ME Station, configure your Internet firewall to allow the following .exe files to access the Internet:
After configuring your firewall software to allow these files internet access, restart your computer to apply the changes.
Tip: If your computer is running a 64-bit operating system, the files are in \Program Files (x86), instead of \Program Files.
User Account Control settings
Turning off UAC is not recommended.
This action
|
Prompts for authentication or confirmation
before running this program
|
Setting or changing settings related to
DeskLock
|
DeskLock2000.exe
|
Creating an application by importing a
PanelBuilder application (*.pba) or a
PanelView terminal file (*.pva)
|
VStudio.exe
|
In the Networks and Communications dialog
box, double-clicking FactoryTalk Linx
Communications
|
MERuntime.exe
|
In the FactoryTalk Linx Configuration dialog
box, clicking Close
|
MERuntime.exe
|
In the Application Settings dialog box,
double-clicking Device Shortcuts
|
MERuntime.exe
|
In the ShortCuts dialog box, clicking Close
|
MERuntime.exe
|
Clicking OK in the FactoryTalk View ME
Station Startup dialog box
|
MERuntime.exe
|
Installing the FactoryTalk View software
|
Setup.exe
|
Installing the SQL Server Express 2008 R2
SP2 instance for FactoryTalk View
|
SQLServerInstall.exe
|
Uninstalling the FactoryTalk View software
|
UninstallAllFTView.exe
|
Constraints when using FactoryTalk View version 6.10.00 or later
Different versions of FactoryTalk View ME use different databases.
FactoryTalk View ME version
|
Tag database
|
6.0 and earlier
|
Watcom
|
6.10, 7.0, 8.0, 8.10, 8.20, and 9.0
|
Microsoft SQL Server 2008 R2 Express
|
10.0, 11.0, and 12.0
|
Microsoft SQL Server 2014 Express
LocalDB
|
13.0 and later
|
Microsoft SQL Server 2019 Express
LocalDB
|
When installing FactoryTalk View ME version 6.10.00 or later:
Due to this difference, some constraints with using FactoryTalk View ME version 6.10.00 or later are introduced on a 64-bit Windows OS.
To open or convert an application created with FactoryTalk View version 10.0 or later in FactoryTalk View version 9.0 or earlier, see Knowledgebase Document ID: QA48248 - Create Runtime Application: Pop-up Regarding Version 9.00 and Earlier.
For more information about constraints with creating and running MER on a 64-bit Windows operating system, review Appendix D, "Constraints when using FactoryTalk View version 6.10.00 or later" in FactoryTalk View ME Installation Guide for details.
Component names
Alarms
Application Documenter
To avoid the problem, open the restored application in FactoryTalk View Studio before opening it in the Application Documenter.
Application Manager
To avoid this problem:
To avoid this problem, open another application in FactoryTalk View Studio or close FactoryTalk View Studio before deleting or copying the application in Application Manager.
To avoid this problem, use Application Manager to convert the .mea application to an .med application. The .med application can then be imported using FactoryTalk View ME.
Data logging
To avoid this problem, access the log file after the data is logged.
To avoid this problem, rebuild the application and change the store path to other drives or a subfolder of drive C:, such as "C:\log" or "C\log\data".
To resume data logging, shut down and restart the application.
Domain controller
This will not happen if you authenticate domain users for personal computers.
Edit menu
To delete multiple rows, right-click in the editor and select Delete Row(s).
Embedded variable
For example, if a display containing an object with both visibility animation and embedded variables opens with the object invisible, and if the connection between the embedded variable and its tag is broken, FactoryTalk Diagnostics will not register communication errors for the object until the object becomes visible. If the object later becomes invisible, the communications errors will still be logged.
This also means that if one or more states of a multistate indicator include embedded variables, the variables will become active when those states are shown.
Firmware Upgrade Package
Global display
To avoid this problem, in the Language Configuration dialog box, clear the Display undefined strings using the default language check box before copying and pasting the object.
To avoid this problem, select a different font.
To avoid this problem, choose one of the following methods:
Import files
To avoid this problem, stop the runtime application before importing a tag CSV file.
To avoid this problem, import the application and then scale the graphics after import.
Language switching
To save Spanish (Traditional Sort), make the selection in the Property Panel instead of in the Properties dialog box.
Memory
To clear the accumulated print alarms, connect the configured printers. The memory will be released as each alarm prints.
Navigation
To avoid this problem, in FactoryTalk View ME Station, go to Terminal Settings > Input Device > Keyboard/Keypad and change the value for Repeat Rate to 2 or greater.
PanelView Plus 7 Standard application
PanelView Plus terminal
To show strings correctly on a PanelView Plus terminal, define all strings without spaces.
Parameter file
To avoid this problem, do not include an exclamation point in a parameter file name.
To avoid this problem, delete "@!=1" from the first line of the parameter file.
To avoid this problem, convert the parameter file from ANSI to Unicode format, for example, in WordPad.
Runtime
For more information about formatting an SD card using exFAT, see Appendix, "Format an SD card using exFAT" in the FactoryTalk View ME User's Guide.
This message can safely be ignored. It does not indicate that the Compact Flash card has failed. This option is intended for use at the time of manufacture only.
To ensure that the user can log in, change the group type of the Windows-linked user group to Security.
Shut down an application
To resolve this issue, reset the terminal.
Tag
To avoid this problem, remove spaces in tag names, device shortcuts, and direct references when the tags are in an embedded variable.
To apply the changes, close and reopen FactoryTalk View Studio.
To avoid this problem, keep the integer tag value less than 2,147,483,648.
Trend
To avoid this problem, set the buffer for extra data below the theoretical maximum.
To avoid this problem, add and use a Next Pen button to align the legend with the pen.