Release Notes

( 9701-VWSx ) FactoryTalk View® Site Edition is a supervisory HMI software package for enterprise solutions. [FTView, FTViewSE
Version 13.00.00 (released 3/2022)

Catalog Number FactoryTalk View Site Edition 

These release notes describe version information for FactoryTalk View Site Edition, version 13.00.00 (released 3/2022).

Requirements

This release has the following requirements.

The following are the system requirements for FactoryTalk View SE version 13.00.00.

Hardware requirements

The following is a sample specification of computer hardware to run FactoryTalk View SE applications aligned with the hardware used in product development testing.

Type
Description
CPU
RAM
Operator Workstation
FactoryTalk View SE Client
or
FactoryTalk View SE Station
Intel® Core™ i5 Standard Power processor
4 GB
Engineering Workstation
FactoryTalk View Studio Enterprise
FactoryTalk Linx
Studio 5000
Intel Core i5 Standard Power processor
8 GB
Application Server
FactoryTalk View SE server
FactoryTalk View Studio Enterprise
FactoryTalk Alarms and Events tag-based server
FactoryTalk Linx data server with FactoryTalk Alarms and Events enabled
Smaller systems:
Intel Core i5 Standard Power processor
4 GB
Medium to larger systems:
Quad core Intel Core Xeon family processor
8 GB

Software requirements

Operating systems

FactoryTalk View SE is tested on the following operating systems:

* For more information, see Rockwell Automation Knowledgebase Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell Software products and IN4718 - Windows Server 2016 Support for the FactoryTalk Suite of Rockwell Software products.

** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.

Domain controller requirements

The following operating systems are supported for use as domain controllers for FactoryTalk View SE client computers. Using a domain is recommended for applications that include more than 10 computers. If your application includes 10 or fewer computers, they can be organized in a workgroup.

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

Security requirements

To help meet secure system design requirements, review these publications:

To learn about implementing CIP Security, see CIP Security with Rockwell Automation Products (publication SECURE-AT001).

Features

This release includes the following system features.

FactoryTalk View SE version 13.00.00 has the following new and enhanced features.

New features

Enhanced features

Corrected Anomalies in This Release

This release corrects the following anomalies.

The following list identifies the anomalies corrected in FactoryTalk View SE version 13.00.00.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk View SE version 13.00.00 has the following changes in functionality since the last release.

HTTPS enabled by default

If you install Studio Enterprise, Site Edition Server, or FactoryTalk ViewPoint SE on a computer with no FactoryTalk View component installed, the installation enables HTTPS by default.

If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk View SE components. For details on configuring a TLS certificate, see FactoryTalk View Site Edition Installation Guide.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk View SE version 13.00.00.

HTTPS enabled by default

If you install Studio Enterprise, Site Edition Server, or FactoryTalk ViewPoint SE on a computer with no FactoryTalk View component installed, the installation enables HTTPS by default.

If HTTPS is enabled, you must configure a TLS certificate after installation. If you do not configure the certificate, there will be unexpected errors when operating FactoryTalk View SE components. For details on configuring a TLS certificate, see FactoryTalk View Site Edition Installation Guide.

Mitigation for Microsoft DCOM Hardening patch

In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.

IMPORTANT
Installing this product’s latest version with earlier unpatched versions of other FactoryTalk products or products using Classic OPC DA connections may cause a loss of connectivity due to the difference in DCOM authentication level used. For additional information, see the Knowledgebase Document ID: IN39461 - Microsoft DCOM Hardening Information TOC.

Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).

Change in operating system support

Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).

Considerations for application server host computers

In a network application, it is possible for a single server computer that meets the recommended requirements to host all of the following components:

If a network application requires multiple HMI servers, data servers, or alarm servers, to distribute the load, it is recommended that you install the necessary software and run the servers on multiple host computers.

For information about setting up redundant FactoryTalk View SE servers, see FactoryTalk View Site Edition User’s Guide.

FactoryTalk Diagnostics

FactoryTalk Diagnostics cannot log to a remote database using Microsoft Access. You can only log to a local database using Microsoft Access.

Find and Replace

If an HMI server at the root node of an SE Network distributed application has the same name as the application itself, the Find and Replace feature search results might include the application name even though you performed the search at the HMI server level.

Floating-point operations

Floating-point numbers may not precisely represent all real numbers. Floating points only has six digits of precision. As a result, expressions based on floating-point arithmetic operations may not evaluate as expected. This is a side effect of how the CPU represents the floating-point data. For this reason, in certain cases you may experience loss of precision and get unexpected results of floating-point operations.

KEPServer

If you are using KEPServer Enterprise as an OPC server with FactoryTalk View version 9.00.00 or later and using an HMI tag to connect to a third-party device, you will not be able to access the tag value. The cause is that the security enhancements in FactoryTalk View version 9.00.00 or later affect the communications with third-party devices. To access the tag value, additional Distributed Component Object Model (DCOM) configuration is required for KEPServer Enterprise on the computers.

For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View SE Installation Guide.

Pre-installation configuration

Before you install FactoryTalk View SE, there are a number of steps required to set up the installation environment. This will help ensure that the installation proceeds smoothly and that your new or upgraded FactoryTalk system operates as expected. For detailed information about pre-requisites before installation, see Chapter 3, Pre-installation configuration of FactoryTalk View Site Edition Installation Guide.

Security requirements

For information on the security considerations when using Rockwell Automation products, including

System sizing recommendations

When you design and set up a FactoryTalk system, we recommend using the following guidelines. If you find that your system needs to expand beyond these guidelines, contact your Rockwell Automation sales or distributor representative to discuss your application design.

Component
Recommended guidelines
FactoryTalk Alarms and Events
 
FactoryTalk Alarms and Events servers per FactoryTalk Directory
10 non-redundant servers or 10 redundant server pairs1
FactoryTalk tag-based alarms per server
20,0002
Logix device-based alarms per server
10,0003
Total alarms per FactoryTalk Directory
100,0004
FactoryTalk Linx
 
FactoryTalk Linx data servers per FactoryTalk Directory
10 non-redundant servers or 10 redundant server pairs1
Total device tags per FactoryTalk Directory
1,000,0005
Tags per FactoryTalk Linx data server
100,0005
FactoryTalk View SE
 
HMI servers per FactoryTalk Directory
10 non-redundant servers or 10 redundant server pairs1
HMI tags per HMI server
40,0006
Total data logged tags per HMI server (1 second scan rate)
5,000
FactoryTalk View SE client sessions simultaneously connected to the application
1205
FactoryTalk ViewPoint SE servers per application
4
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
50
  1. Because multiple applications can run simultaneously within the same FactoryTalk Directory, the recommended number refers to the sum of servers across applications in one FactoryTalk Directory.
  2. The number of alarm backing tags influences the maximum number of available alarms because they increase the resource requirements of the alarm server. When using backing tags for status and control, a good rule of thumb is to multiply the total number of backing tags by the total number of alarms, and ensure the result is less than 20,000. PlantPAx® users should refer to the PlantPAx Reference Manual PROCES-RM001 for alarm server sizing guidance for a PlantPAx application.
  3. This number is the sum of both instruction alarms and Logix tag-based alarms across all the controller shortcuts in each FactoryTalk Linx server.
  4. The total number of alarms per FactoryTalk Directory includes all FactoryTalk Alarms and Events tag-based and device-based alarms in the directory.
  5. Refer to Knowledgebase Document ID: IN7377 - Amounts of device tags that may have in FactoryTalk View SE application for detailed information to determine system scalability for the total device tags per FactoryTalk Directory.
  6. The maximum number of HMI tags that can be created on a single HMI server is 175,000. Extensive use of HMI tags has a significant performance impact on an HMI server, so Rockwell Automation recommends minimizing their use, and instead using direct-reference tags as much as possible.

Tag Browser

If you rename an HMI server while you are deploying an application, you may need to restart the computer in order to have the HMI tags show up in the Tag Browser.

Tools and utilities

Trend objects

The Trend objects cannot get the oldest data from FactoryTalk Historian server when you click the Oldest Data button.

TrendPro objects

UAC support

Turning off User Account Control (UAC) is not recommended.

This action
Prompts for authentication or confirmation before running this program
Configuring Internet Information Services (IIS)
RSViewWebManager.exe
CustomWebSite.exe
Updating Samples application directory information
RefreshSampleApplication.exe
End processes
VSClean.exe
DeskLock
DeskLock2000.exe
Legacy Tag Database Conversion
LegacyTagDBConvertTool.exe

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Unattended installation

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended when deploying the software installation using an IT tool or script, and don’t expect any error or restart messages. When using this parameter, check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used, silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/Repair
Runs a repair operation on the installed products.
This parameter is optional.
/Uninstall
Uninstalls the product.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Product="value"
Specifies which sub-products will be installed.
This parameter is required.
For FactoryTalk View ME, the value must be one of the following:
  • Studio for Machine Edition
  • Machine Edition Station for Windows
  • Stand-alone ME Transfer Utility
For FactoryTalk View SE, the value must be one of the following:
  • Studio Enterprise
  • Site Edition Server
  • Site Edition Client
  • Site Edition Station
  • FactoryTalk ViewPoint SE
  • Stand-alone FactoryTalk Linx Server
  • Stand-alone FactoryTalk Directory Server
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • FRA
  • JPN
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages, this parameter is not available.
/InstallDrive="value"
Specifies the installation drive.
This parameter is optional. If this parameter is not used, the default install drive is C:.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required, this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required, this parameter is not available.
/Version="value"
Specifies the version of the software to activate, which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified, the installer will use the most recent product version available.
Some software does not require activation. If activation is not required, this parameter is not available.
/DirectoryServer="value"
Specifies the FactoryTalk network directory if you are using a distributed system.
This parameter is optional. If it is not specified, the software will use its current computer as the FactoryTalk Directory server.
The value must be the host name of the FactoryTalk Directory server.
/NoHTTPS
Specifies that the setup turns off HTTPS.
This parameter is optional. If it is not specified, the setup turns on HTTPS for communication, and a TLS certificate must be configured after installation.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was canceled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart, the installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart, the product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart pending. Restart the computer for the installation to continue.
ERROR_SUCCESS_NOT_APPLICABLE
3013
The installation cannot proceed because the products are already installed.
ERROR_SUCCESS_WARNING_REBOOT
3014
The installation succeeded with warnings. Check the installation log file for details. To complete the installation, restart the computer.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2023 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.