Release Notes

It allows FactoryTalk enabled products to be activated via files generated by Rockwell Automation over the Internet.
Version 4.06.13 (released 2/2022)

Catalog Number FactoryTalk Activation 

These release notes describe version information for FactoryTalk Activation, version 4.06.13 (released 2/2022).

Requirements

This release has the following requirements.

Hardware requirements

FactoryTalk Activation Manager does not have any specific hardware requirements. It runs on any hardware platform that supports the required software, either locally or on a virtual machine.

Rockwell Automation recommends at least 80 MB of available drive space for FactoryTalk Activation Manager.

Software requirements

Features

This release includes the following system features.

New features

Enhanced features

Corrected Anomalies in This Release

This release corrects the following anomalies.

Language support only available in English

The online help and release notes are available in English only. Some user interface text may still display in the selected operating system language if the operating system is set to one of these languages:

FactoryTalk Activation Manager Client does not show expired activation but FactoryTalk Activation Manager Server shows expired activations [CLM 8671]

Activations that are not available, because they have either expired or not yet reached their start date, are displayed as disabled and show a red icon. Hovering over the icon displays a tooltip explaining why the row is disabled.

This is intended behavior.

Corrected in FactoryTalk Activation Manager version 4.06.11 by updating the Find available activations and Available Activations table help topics.

Unvailable activations display issues [291736, 289240]

Activations that are no longer available because of a disconnected Ethernet card or disconnected dongle may still appear in the Available activations list. However, for unavailable concurrent activations, "n/a" displays in the Total column under Available activations. There is no indicator for unavailable node-locked activations.

This behavior is intentional, as the activations are still assigned to the device and are not available for use. If a node-locked activation is assigned to a device and the device is no longer going to be used, rehost the activation before final removal of the device. If a concurrent activation is assigned to a device, make sure that the application is closed and the logged on user is logged out so that the activation is returned to the activation pool before the device is removed.

Corrected in FactoryTalk Activation Manager version 4.06.11 by updating the Types of activations, Find available activations, and Available Activations table help topics.

The concurrent license bound to a new dongle shows "na" in the Total column of Find Available Activations page [348174]

The concurrent license bound to a new dongle shows "na" in the Total column of the Find Available Activations page, even though the dongle is recognized by FactoryTalk Activation Manager.

This occasionally happens when there is a mismatch between the dongle hardware version and the dongle driver version. If you have recently updated your dongle hardware you may encounter this issue. First identified in FactoryTalk Activation Manager version 4.00.

If you encounter this issue, remove the existing dongle driver and then reinsert the dongle. When the dongle is detected the correct driver will be installed.

Corrected in FactoryTalk Activation Manager version 4.06.11 by updating the Available Activations table help topic.

Total number of concurrent activations displays incorrectly when there are corresponding node-locked activations [342881]

If you have both node-locked and concurrent activations for a product, the total number of concurrent activations will aggregate the node-locked activation into its count and display an incorrect value. First identified in FactoryTalk Activation Manager version 3.62.

There is no operational impact to this issue. Activations can still be checked out and used.

Corrected in FactoryTalk Activation Manager version 4.06.11 by updating the Available Activations table help topic.

  

High CPU utilization on multiple Remote Desktop Services sessions [955161]

High CPU utilization caused by FactoryTalk Activation Helper service when there are multiple Remote Desktop Services sessions. Corrected in FactoryTalk Activation Manager version 4.06.

Unable to generate CodeMeter file [894468]

Unable to generate the CodeMeter update file in the source computer when you borrow an activation by using a data file. Corrected in FactoryTalk Activation Manager version 4.06.

  

FactoryTalk Linx Gateway does not activate [1497995]

FactoryTalk® Linx™ Gateway version 6.11.00 does not activate when FactoryTalk Activation Manager version 4.06.00 or 4.06.11 is installed on the computer.

Corrected in FactoryTalk Activation Manager version 4.06.12.

  

Incorrect In Use value [1512886]

The Available Activations table displays an incorrect In Use value.
First identified in FactoryTalk Activation Manager version 4.06.00.
Corrected in FactoryTalk Activation Manager version 4.06.13.  

Known Anomalies in This Release

This release has the following known anomalies.

Error code LicenseRequestFileNeeded appears when activating a CodeMeter license type as a user with special characters (such as é) in their username. (2083170)
This anomaly first identified in FactoryTalk Activation Manager version 4.06.13. To work around this issue, either:

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Error code LicenseRequestFileNeeded appears when activating a CodeMeter license type as a user with special characters (such as é) in their username. (2083170)

This anomaly first identified in FactoryTalk Activation Manager version 4.06.13.

To work around this issue, either:

  

CodeMeter error messages display only in English for Korean and Portuguese installations [CLM 152723]

Some CodeMeter error messages are displayed only in English for Korean and Portuguese installations of the FactoryTalk Activation Manager.

Incorrect quantity of FlexNet Publisher (FNP) concurrent activations appears [1046664]

If you get multiple FlexNet Publisher (FNP) Concurrent and Node-Locked activations of the same feature name, the Total column in the Find Available Activations page might display incorrect values. First identified in FactoryTalk Activation Manager version 4.06.

To avoid this issue, get only either Concurrent activations or Node-Locked activations of a given feature name, not both.

Exceeding the NetBIOS name limit shortens the computer name of an FNP activation to the first 15 characters (1093582)
The shortened computer name appears in the Location column for that FNP activation in the Available Activations table. First identified in FactoryTalk Activation Manager version 4.06.
To avoid this issue, observe the NetBIOS name limit in the prompt that appears if you exceed the number of characters allowed when changing the computer name.


Functional Changes

This release has the following functional changes from the previous release.

Application Notes

This release has the following application notes.

Maximum borrow time for CodeMeter activations

For CodeMeter activations, you cannot exceed the maximum borrowing time specified in License Transfer Configuration on the CodeMeter server administration utility. See CodeMeter 7.30 User Help for more information.

Antivirus software might detect FactoryTalk Activation Manager executable file as a threat

Your antivirus software might detect the AutoGetFTA.exe file as a threat and cause an error when you activate a license.

To avoid this issue, exclude the AutoGetFTA.exe file from the virus scan.

For more information, see Knowledgebase Document ID: BF26715 - FactoryTalk Activation: Error creating process .

graphic
Tip: Sign in to your Rockwell Automation account to view Knowledgebase articles.

FactoryTalk Activation Manager version 4.04 supports renewing activations that have changed type from FlexNet to CodeMeter

In FactoryTalk Activation Manager versions 4.04 and later, renewals of activations can include an activation type change from FlexNet to CodeMeter in addition to the expiration date change.

This type change is supported only when the original FlexNet activation is bound to the computer and replaced with a CodeMeter activation bound to the computer.

For dongles, perform a rehost of the original activation and a get of the renewed activation for the activation type. For example, a rehost is necessary when:

In FactoryTalk Activation Manager versions 4.02 and later, renewals of activations bound to dongles or computers are supported in which the technology is not changing.

FactoryTalk Activation Manager versions 4.03 and earlier do not support renewing activations that have changed type from FlexNet to CodeMeter

FactoryTalk Activation Manager versions 4.03 and earlier do not renew activations that have changed type from FlexNet to CodeMeter. Rockwell Automation recommends installing version 4.06, which supports renewing activations that have changed type from FlexNet to CodeMeter. If upgrading to version 4.06 is not possible, perform a rehost of the original activation and a get of the renewed activation for the activation type.

FactoryTalk Activation Manager versions on client and server should match to support Subscription Portal License Manager

If upgrading either activation servers or clients from FactoryTalk Activation Manager 4.00 or earlier, upgrade both the servers and clients to FactoryTalk Activation Manager 4.06.  

Unavailable activations are listed only on FactoryTalk Activation Manager running on a server

Expired FlexNet activations do not appear on FactoryTalk Activation Manager running on client machines. This behavior is by design, because expired activations cannot be acted upon from a client machine. On FactoryTalk Activation Manager running on a server, activations that are not available, because they have either expired or not yet reached their start date, are displayed as disabled and show a red icon. Hovering over the icon displays a tooltip that explains why the row is disabled.

Rehost expired activations to remove them from the Find Available display.

Removing CodeMeter server address from search path causes errors

After a CM activation is borrowed, removing the CodeMeter server address from the search path on the Update Activation Search Path dialog box on the client PC causes these errors:

Date and time settings must match on client and server computers

To borrow CodeMeter activations correctly, the date and time settings of the client and server computers must match within one minute. If the date and time settings do not match, unexpected behavior occurs, such as the failure to activate valid licenses.

Borrowing or returning CodeMeter activations generates only client diagnostic message

Borrowing or returning CodeMeter activations generates only a client diagnostic message. However, borrowing or returning FlexNet Publisher (FNP) activations generates both server and client diagnostic messages.

This is intended behavior.

Updates to server search list

Rockwell Automation recommends using FactoryTalk Activation Manager exclusively to make updates to the server search list. If using CodeMeter Web Admin to update the server search list, the updates may not reflect accurately in the FactoryTalk Activation Manager search list.

Remote Desktop Connection to client computer running Windows Server limits return of activations and activation of products

When using a remote desktop connection to a client computer running a Windows Server operating system, borrowed CodeMeter activations are not displayed, borrowed activations cannot be returned manually (they are automatically returned when they expire), and products relying on the borrowed activation cannot be activated. To work around these limitations, log into the client computer directly. Rockwell Automation recommends not using a Windows Server operating system on a computer that uses borrowed activations or points to a FactoryTalk Activation server.

FactoryTalk Activation Manager is incompatible with Top Server 6 software

For FactoryTalk Activation Manager to operate correctly, Top Server 6 software must be uninstalled, and the FLEXID_LIBRARY_PATH environment variable must be removed.

For more information on this issue, see Knowledgebase Document ID: BF14522 FactoryTalk Activation Manager: FTAManager has stopped working .

graphic
Tip: Sign in to your Rockwell Automation account to view Knowledgebase articles.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

 

Parameter
Description
/Q
One of /Q and /QS is required if /Record is not specified.
Installs the product in the silent mode without any user interface.
/QS
One of /Q and /QS is required if /Record is not specified.
Installs the product in the unattended mode without user interaction during installation, and shows the progress, errors, or complete messages on the user interface.
/IAcceptAllLicenseTerms
Required for /Q or /QS.
Specifies that you read and acknowledge all license agreements, and agree to continue the installation.
/AutoRestart
Optional. If specified, the computer restarts automatically after the installation if a restart is required to complete the installation. If a restart is not required, the parameter is ignored.
/SetupLanguage
Optional. Specifies which language is displayed during the install process.
The value must be one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
If this parameter is omitted, the default language is the user or system user interface language.
/Record
Optional. Records inputs to a recording file.
/Playback
Optional. Plays back a recorded file.
/DisableAutoRenew
Optional. If specified, disables the FactoryTalk Activation Manager from automatically connecting to the Rockwell Automation Activation service to query for renewed activations to download. Activations are renewed automatically by default.

Examples

The following examples show how to use the installation commands.

Setup.exe /Q /IAcceptAllLicenseTerms

Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS

Setup.exe /Record

Setup.exe /Q /IAcceptAllLicenseTerms /Playback="C:\Filename.rec"

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
Installation completed successfully.
ERROR_INVALID_PARAMETER
87
One parameters is invalid.
ERROR_INSTALL_USEREXIT
1602
Installation cancelled by user.
ERROR_INSTALL_FAILURE
1603
Fatal error during installation.
ERROR_BAD_CONFIGURATION
1610
Configuration data for product corrupt. Contact support personnel.
ERROR_REBOOT_CONTINUE
1641
Restart required to continue installation.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
Restart required to complete installation. After restart, product is successfully installed.
ERROR_REBOOT_PENDING
3012
Restart pending. Restart computer for installation to continue.


  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.