Release Notes

( 9521-VPx ) Provides unified access to virtually all manufacturing/plant data sources, and produces web-based reports.
Version 8.31.00 (released 1/2022)

Catalog Number FactoryTalk VantagePoint EMI Server 

These release notes describe version information for FactoryTalk VantagePoint EMI Server, version 8.31.00 (released 1/2022).

Requirements

This release has the following requirements.

The following are the system requirements for FactoryTalk VantagePoint version 8.31.00.

FactoryTalk VantagePoint works within the system requirements of all Rockwell Automation® software products. For the latest information regarding software platform support, refer to Rockwell Automation Product Compatibility and Download Center.

The hardware required with FactoryTalk VantagePoint depends on the demands an application places on the system. The greater the demand, the more powerful system is required. In any application, faster processors and more memory will result in better performance. In addition, there should always be sufficient disk space to provide virtual memory that is at least twice the size of the physical memory.

Before installing, ensure your system meets the following requirements.

System Server

Items
Descriptions
Operating System
  • Microsoft Windows Server 2012 R2 Datacenter (64-bit)
  • Microsoft Windows Server 2012 R2 SP1 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Standard (64-bit)
  • Microsoft Windows Server 2019 Datacenter LTSC (64-bit)
  • Microsoft Windows Server 2019 Standard LTSC (64-bit)
Note: The VantagePoint IIS Application Pools are set to 32-bit mode only.
Software
  • Microsoft SQL Server 2012 Standard SP3 (64-bit)
  • Microsoft SQL Server 2012 Express SP3
  • Microsoft SQL Server 2016 Standard SP2
  • Microsoft SQL Server 2016 Express SP1
  • Microsoft SQL Server 2019 Express
  • Microsoft SQL Server 2019 Standard
  • Microsoft Office 2013 SP1 (32-bit only)
  • Microsoft Office 2016 (32-bit only)
  • Microsoft Office 2019 (32-bit only)
  • Microsoft Internet Explorer 11
  • Microsoft Edge 95 or later (Internet Explorer mode)
  • Microsoft .Net Framework 4.8 full version (included with install)
  • Microsoft .Net Framework 3.5 (added when installing and configuring IIS)
Hardware
  • 2.5 GHz
  • 2 GB Hard Drive Space
  • 4096 MB RAM

Full Client

Items
Descriptions
Operating Systems
  • Microsoft Windows 10 Enterprise (64-bit)
  • Microsoft Windows Server 2012 R2 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Standard (64-bit)
  • Microsoft Windows Server 2019 Datacenter LTSC (64-bit)
  • Microsoft Windows Server 2019 Standard LTSC (64-bit)
Note: Embedded versions are not supported.
Web Browser
  • Microsoft Internet Explorer 11
  • Microsoft Edge 95 or later (Internet Explorer mode)
Note:
  • The Metro App for Internet Explorer 11 is not supported.
  • You can use VantagePoint Mobile on Google Chrome 91 or later or Internet Explorer 11.
Software
  • Microsoft Office 2013 SP1 (32-bit)
  • Microsoft Office 2016 (32-bit)
  • Microsoft Office 2019 (32-bit)
  • Microsoft .Net Framework 4.8
  • Adobe Reader (for viewing Eventing/ReportSet reports)
Hardware
  • 1.5 GHz
  • 100 MB Hard Drive Space
  • 1024 MB Ram

Browser Client

Items
Descriptions
Operating System
  • Microsoft Windows 10 Enterprise (64-bit)
  • Microsoft Windows Server 2012 R2 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Datacenter (64-bit)
  • Microsoft Windows Server 2016 Standard (64-bit)
  • Microsoft Windows Server 2019 Datacenter LTSC (64-bit)
  • Microsoft Windows Server 2019 Standard LTSC (64-bit)
Note: Embedded versions are not supported.
Web Browser
  • Microsoft Internet Explorer 11
  • Microsoft Edge 95 or later (Internet Explorer mode)
Note:
  • The Metro App for Internet Explorer 11 is not supported.
  • You can use VantagePoint Mobile on Google Chrome 91 or later or Internet Explorer 11.
Software
  • Microsoft .Net Framework 4.8
  • Adobe Reader (for viewing Eventing/ReportSet reports)
Hardware
  • 1.5 GHz
  • 100 MB Hard Drive Space
  • 1024 MB Ram

Mobile Client

Items
Descriptions
Supported Devices
  • Android tablets and smart phones with OS 5.0 using Google Chrome
  • Apple iPad 4 or later or iPhone 5 or later with iOS 9.1 or 10.x using Safari
Note: A tablet is required to use the Import and Configure features.
Web Browsers
  • Google Chrome 91 or later
  • Microsoft Internet Explorer 11
  • Microsoft Edge 95 or later
Note:
  • The Metro App for Internet Explorer 11 is not supported.

Product compatibility

FactoryTalk VantagePoint is compatible with the following Rockwell Automation products:

Rockwell Automation Test Environment

Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.

Security requirements

To help meet secure system design requirements, review these publications:

Features

This release includes the following system features.

FactoryTalk VantagePoint version 8.31.00 has the following enhanced features.

Installation

Upgrade

New operating system support

New database support

New Transport Layer Security support

New software support

Corrected Anomalies in This Release

This release corrects the following anomalies.

FactoryTalk VantagePoint version 8.31.00 has no corrected anomalies.

Known Anomalies in This Release

This release has the following known anomalies.

FactoryTalk VantagePoint version 8.31.00 has no known anomalies.

Functional Changes

This release has the following functional changes from the previous release.

FactoryTalk VantagePoint version 8.31.00 has the following functional changes:

Use Mobile Dashboard to generate reports

Xcelsius is no longer supported since FactoryTalk VantagePoint version 8.10.00. We recommend that you use Mobile Dashboard to generate reports.

Application Notes

This release has the following application notes.

The following are the application notes for FactoryTalk VantagePoint version 8.31.00.

Synchronize FactoryTalk Historian connectors after the VantagePoint upgrade to version 7.00, 8.00, 8.10, 8.20, 8.30, or 8.31

After upgrading VantagePoint to version 7.00, 8.00, 8.10, 8.20, 8.30, or 8.31, we recommend that you synchronize your FactoryTalk Historian connectors to get the correct values of historian tags' properties.

Improved transparency in data presentation between VantagePoint and InSQL

VantagePoint has taken the following approach towards the InSQL data presentation:

If you want to do any of the following:

You need to overwrite the settings in VantagePoint Manager.

To overwrite the InSQL data presentation settings
  1. In VantagePoint Manager, go to System > Sources > InSQL.
  2. Right-click the InSQL connector for which you want to define the data presentation rules, and then click Edit.
  1. In the Description box, add the following options of the data presentation rules:
  • wwInterpolationType
  • General issues

    Review the following for additional information about issues you may encounter.

    Issues
    Description
    In a mixed Workgroup / Domain Environment user credentials must be cachedIn a mixed Workgroup / Domain Environment user credentials must be cached
    The first time a new client connects to a VantagePoint server across a security boundary where the connecting client’s logged-on user is not a valid user in the server’s security context; the client will be prompted to enter a valid user name and password. Upon entering valid credentials, you must select the Remember my password check box to ensure the proper function of the VantagePoint system. After this initial login, you will never again be prompted for a password, unless your password changes. Note that this procedure is not required and the user should not be prompted if the client is a valid user on the server’s Domain/Workgroup.
    Copy operation should not be used to copy a connector into another connector
    Avoid copying one connector, such as InSQL, into a similar connector type, such as ODBC. Doing so will result in an error when trying to use the connectors.
    Solution: Delete the connector that you copied under the original connector, and restart IIS on the VantagePoint server.
    Delete operation does not work on Folders or Items when permissions are granted to VantagePoint User
    A user with VantagePoint user rights is not able to delete a folder or its contents. This is seen when a VantagePoint user tries to delete folders or contents of folders that are directly below the My Enterprise node in the Model Browser.
    This issue reflects the way permissions are granted on items that contain other items. In order to delete an item, two conditions must be true:
    • The user must have Delete permission for the item.
    • The user must have Write permission on the parent item.
    These rules are required since the deletion of an item changes the parent item's collection or reference property that holds the item.
    Solution: Create folders for VantagePoint users that are two nodes down from the MyEnterprise root folder. (e.g. MyEnterprise > NoDeleteFolder > User Can Delete1, 2, 3 etc.)
    MFC71U.dll not found error after uninstalling VMware Tools version 7.2.9
    After uninstalling VMWare Tools version 7.2.9 and either performing an IISReset or rebooting the machine, you will receive the following error message indicating a problem with the Rockwell Activation tool.
    Error Message: 'flexsvr.exe-Unable to Locate Component"- "This application failed to start because MFC71U.DLL was not found. Reinstalling the application may fix the problem."
    Solution: Copy the MFC71U.dll to the C:\Windows\System32 directory. A copy of the MFC71U.dll is located on the VantagePoint DVD in the Resources folder.
    Clients must be installed in Local Intranet Zone
    VantagePoint only supports clients located in the Local Intranet Zone, so you must add the Portal URL to this zone. To add the URL to the Local Intranet Zone, in Internet Explorer, select Internet Options > Security tab > Local Intranet. Click Sites, and then click Advanced, and add the Portal URL.
    Clients from previous VantagePoint versions cannot be launched from the VantagePoint server
    The machine that hosts the VantagePoint server cannot launch clients from previous versions of VantagePoint because the policy files use assembly rebinding for core assemblies.
    Solution: Use a machine that is not hosting the VantagePoint server to launch clients from previous versions of VantagePoint.
    Error: Json Service: Unauthorized exception with FQDN or Host Header in IIS
    If the host header setting has been configured in IIS or if a fully qualified domain name is used for your site, Json returns an error message.
    Solution: To resolve this issue, see http://support.microsoft.com/kb/896861/en-us
    Sending emails over SSL using port 465 is not supported
    FactoryTalk VantagePoint supports only the SMTP Service Extension for Secure SMTP over Transport Layer Security. In this mode, the SMTP session begins on an unencrypted channel, then a STARTTLS command is issued by the client to the server to switch to secure communication using SSL. We recommend that you use the port number 587.
    An alternate connection method where an SSL session is established up front before any protocol commands are sent is not currently supported. This connection method is sometimes called SMTP/SSL, SMTP over SSL, or SMTPS and by default uses port 465.


    Installation and administration issues

    Review the following for additional information about issues you may encounter.

    Installation Issues
    Description
    Unable to configure the FactoryTalk Directory. Access Denied error during FactoryTalk Services Platform install
    (Windows 2012 R2) If FactoryTalk Services Platform is installed after FactoryTalk Activation Manager, this error occurs. You can ignore this error and click OK to continue the install; and FactoryTalk Services Platform will install correctly.
    VantagePoint server installs to the Root of the Default Web Directory
    The default web directory for IIS will typically be located on the C:\ drive. If you have limited space on this drive, you may want to install VantagePoint on a different drive. In order for VantagePoint to install on a different drive, you will need to first change the location of default web directory to the desired location. This is done through the Properties dialog box on the Default Web Site.
    Files in Use dialog appears during VantagePoint installation with a list of process ID
    During the VantagePoint installation, on some systems, a Files in Use dialog may appear, but the list of files consists of a list of process IDs.
    Solution: To continue installation, click Retry twice.
    Cannot change drive if drive is full when installing VantagePoint
    VantagePoint installs on the default system drive. Prior to installing VantagePoint, ensure that the default system drive contains at least 1 GB of free disk space.
    "Application cannot be started. Contact the Application vendor" error when installing a client
    This issue occurs if you have .NET 4.0 installed on the client machine.
    Solution: Upgrade to .NET 4.5 on the client machine.
    Upgrade Issues
    Description
    Upgrading a large VantagePoint system may take a long time to complete
    Upgrading a large VantagePoint system may take a long time to complete. During this time, attempts to access the VantagePoint system may result in timeout errors.
    After the indexes have been rebuilt and SQL Server is idle again, the VantagePoint system behaves normally.
    An HTTP status 503 error: "The type initializer for 'DataWorks.MI.Core.MiddleTier.Licensing.ClientLicense' threw an exception" appears after upgrade
    This error occurs if the following DLLs were moved into the incuity web application so that licensing does not occur in the Incuity service. This is no longer supported.
    • DataWorks.MI.Core.Branding.MiddleTier.dll
    • DataWorks.MI.Core.Branding.Service.dll
    Solution: Remove these two files from C:\Inetpub\wwwroot\Incuity\bin.
    Charts and Grids do not work after upgrading to VantagePoint
    After upgrading to the latest version of VantagePoint, Charts and Grids no longer work.
    Solution: Re-install Charts and Grids.
    Administration Issues
    Description
    VantagePoint log files are not deleted
    The VantagePoint server creates a log file detailing certain activity on the server. A new log file is created by default each day at midnight. The archived log files are not deleted. You should periodically check to ensure that the log files are not consuming too much of the available disk space. You can delete the log files using Windows Explorer. The old log files have a file extension ending in the date. Do not delete the logging configuration files (LoggingConfig.xml). Log files are created in the following directories:
    C:\Inetpub\wwwroot\Incuity\Logging
    C:\Inetpub\wwwroot\IncuityOffice\Logging
    C:\Inetpub\wwwroot\IncuityPortal\Logging
    C:\Program Files\Incuity\bin\Logging (on 32-bit operating systems)
    C:\Program Files (x86)\Incuity\bin\Logging (on 64- bit operating systems)
    For continuous server operation, IIS Default Application Pool Recycle Time needs to be disabled
    The VantagePoint server applications are installed in the default application pool of IIS which means that the applications are recycled every 29 hours. While this does not hurt VantagePoint, it can lead to gaps of a few minutes in the history of tags that are stored by VantagePoint storage. It also requires that a new instance of Excel be started the first time an Excel report is requested after a server restart. Every time this happens, report rendering will take significantly longer than normal.
    On the Windows Server operating system, the recycling of the Web applications can be disabled in the application pool that hosts the Web application. The VantagePoint web applications are installed into the default application pool. The recycling should only be disabled if there is no risk that other web applications in the same application pool will be affected. Preferably, the VantagePoint and VantagePoint Office web applications should be moved to a dedicated application pool as described in the Tech Note 'Creating Application Pools'. See Using the Default Application Pool for VantagePoint and IIS in the online help.
    Type packages designed for Sample Content must not be used for official modeling
    Sample content instances AND the type packages that are specific for the sample content are usually deleted as part of the upgrade to the next (future) version. You must not use types in the sample type packages for official modeling since the resulting instances or derived type packages will likely be deleted as part of a future upgrade.
    Cannot change Incuity System User when Current User is not an Admin for the IncuityStore
    This issue arises when VantagePoint is running on Server1 while the IncuityStore database is running on Server2.
    When you install VantagePoint, you get the chance to specify the database credentials used for setting up the IncuityStore database. These credentials are often different from the current Administrator that is running the install.
    When you later want to change the Incuity System user account, two groups of operations are required:
    1. Changes to the VantagePoint server's file system, registry, etc.
    2. Changing the owner of the IncuityStore db.
    For the latter, it must be possible to specify db credentials as offered during the install. However, the configuration UI of VantagePoint Manager does not offer an entry form for db credentials.
    Solution: Create an account on the VantagePoint server that is also an administrator on the machine running SQL Server. Log into the VantagePoint server with this account; and run VantagePoint Manager.
    After moving a database, the password no longer works
    If you move the database used by a database connector, the password no longer works after the move.
    Solutions:
    UAC error when adding or removing features using Add/Remove Programs
    When adding or removing a feature using Add/Remove Programs, if UAC is on, and you are logged on as a user that is part of the Administrators group but not the local Administrator, a blank error dialog box appears.
    Solutions: You can resolve this issue using any of the following methods:
    • Use the VantagePoint installer (setup.exe) to modify the current install.
    • Log in as the local Administrator before using Add/Remove Programs.
    • Disable UAC before using Add/Remove Programs.
    Error when launching Historian SDK
    When launching the Historian SDK, you receive the following error "The program can't start because rsdbgutils.DLL is missing from your computer."
    Solution: You will need to install the FactoryTalk Services Platform.
    If you do not want to install the FactoryTalk Services Platform, you can dismiss the error and the Historian SDK will launch successfully.


    Connector issues

    Review the following for additional information about issues you may encounter.

    FactoryTalk Connector Issues
    Description
    Support for a single FactoryTalk directory
    The FactoryTalk Connector in VantagePoint supports connectivity to a single Factorytalk Directory. This means that if your organization uses multiple FactoryTalk Directories, VantagePoint will only be able to access data from the sources that are part of the single FactoryTalk Directory that you specify when configuring a FactoryTalk connector (to Live, History, and Alarm & Event data). Data sources that are associated with other FactoryTalk Directories will not be accessible using the FactoryTalk connector. They may be accessible using a 3rd party connector that is available for VantagePoint. Please contact us for an update on this issue and possible workarounds.
    Error when browsing for LiveData tags
    When creating a FactoryTalk connector and browsing for LiveData tags, you receive the following error "String reference not set to an instance of a String. Parameter name: s."
    Solution: You will need to install the OPC Core Components from the VantagePoint DVD and perform an IISRESET.
    FactoryTalk EnergyMetrix Connector Issues
    Description
    Rate and Usage report fails if non-standard tagnames are used on the EnergyMetrix server
    To display the Rate and Usage report for a given meter type, the meter type must have tags with standardized names.
    Meter Type
    Standardized Tagnames
    Connector.FTEnergyMetrix.AirMeter
    - Air Flow Rate
    - Air Usage
    - Air Usage Totalizer
    Connector.FTEnergyMetrix.ElectricMeter
    - Real Energy Net
    - Real Energy Net Totalizer
    - Real Power Demand
    Connector.FTEnergyMetrix.GasMeter
    - Gas Flow Rate
    - Gas Usage
    - Gas Usage Totalizer
    Connector.FTEnergyMetrix.SteamMeter
    - Steam Flow Rate
    - Steam Usage
    - Steam Usage Totalizer
    Connector.FTEnergyMetrix.WaterMeter
    - Water Flow Rate
    - Water Usage
    - Water Usage Totalizer
     
    FactoryTalk Historian Connector Issues
    Description
    FactoryTalk Historian import fails with Unable to access SCM Manager
    When importing FactoryTalk Historian tags, an "Unable to access SCM Manager. 5" error message displays under the following scenarios:
    • In a workgroup environment
    • If the VantagePoint server is running as a user that does not have administrator privileges
    • After an IISReset has been done
    Solution: It is safe to ignore this error by closing the dialog box and importing again. Subsequent imports will not give this error.
    FactoryTalk Metrics Connector Issues
    Description
    Error when inserting a Database Query (IncuityLinkedQuery function) in the Excel Add-In using a FactoryTalk Metrics query that contains parameters as the source
    When inserting a Database Query (IncuityLinkedQuery function) in the Excel Add-In using a FactoryTalk Metrics query that contains parameters as the source, if you click the Edit Item button on the Insert Query page, a "Value cannot be null" error displays.
    IndustrialSQL Server Connector Issues
    Description
    Adding IndustrialSQL Server connector fails if Service Pack is not installed
    VantagePoint will not create an InSQL connector for IndustrialSQL Server 8.0 if the Service Pack is not installed. At the time of this release, an error message does not warn the user of the problem, however it is recorded in the VantagePoint log.
    Solution: Install the Service Pack for IndustrialSQL Server, and create the connector.
    Double type tag value becomes zero if it is invalid on the Industrial SQL (InSQL) server
    If a double type tag value is invalid on the Industrial SQL (InSQL) server, after importing the tag to FactoryTalk VantagePoint, the value becomes zero. First identified in FactoryTalk VantagePoint version 8.20.00.
    Solution: There is currently no workaround for this issue.
    ProficyHistorian Connector Issues
    Description
    Unsuported tags in VantagePoint
    The following types of tags from the ProficyHistorian server are not supported in the VantagePoint system and are not mapped to VantagePoint tag types when importing data:
    • UnsignedSingleInteger, for OLEDB Provider version 4.5 and earlier
    • Byte, for OLEDB Provider version 4.5 and earlier
    • Boolean, for OLEDB Provider version 4.5 and earlier
    • UnsignedDoubleInteger
    • UnsignedQuadInteger
    • BLOB
    • Time
    • QuadInteger
    • Undefined
    You can view information about ProficyHistorian tags which are not mapped to VantagePoint tag types in the log file located in C:\Inetpub\wwwroot\Incuity\Logging\.
    OPC DA Connector Issues
    Description
    Attempting to import items from an OPC DA server finishes, but no items are added
    Some OPC DA servers do not contain a tag dictionary (the optional IOPCBrowseServerAddressSpace interface) containing the necessary information about the items VantagePoint would typically import. In these cases, it is necessary to use the 'Import from file' operation of the OPC DA connector. This operation accepts a well formatted XML string as an import parameter and can be invoked by script. For more information on constructing this XML string or using a script to add items to your OPC DA connector, see Creating Aliases for OPC Items in the online help.
    OPC DA connector cannot browse Linx Classic tags
    Creating an OPC DA connector to a Linx Classic controller fails.
    Solution: Add the controller to a FactoryTalk Directory and create a FactoryTalk connector to the Linx Classic tags or use FactoryTalk Gateway.
    ProductionCentre Connector Issues
    Description
    Using the TimeOfDay operator to compare values requires the ProductionCentre time format
    When you use the TimeOfDay operator to compare time values, you must enter the time values in ProductionCentre format:
    YYYY-MM-DDThh:mm:ss.SSS
    where
    • YYYY is the year
    • MM is the month
    • DD is the day
    • T is the date and time separator
    • hh is the hour in a 24-hour format
    • mm is the minutes
    • ss is the seconds
    • SSS is the milliseconds
    Example of a correct query command:
    <XmlQuery Command="GetAreas">
    <Filter>
    <SearchConstraint FilterAttribute="CREATIONTIME"
    Operator="TimeOfDayEqual"
    Values="2000-01-01T23:29:45.000">
    </SearchConstraint>
    </Filter>
    </XmlQuery>
    Using the TimeOfDay operator to compare values will result in truncated values in ProductionCentre
    When you use the TimeOfDay operator to compare time values, ProductionCentre will truncate the values to seconds. For ProductionCentre, the milliseconds value equals 0.
    Solution: There is currently no workaround for this issue.
    Using the Equal operator to compare values in a comma separated list causes ProductionCentre to use only the first value for comparison
    When you use the Equal operator in the SearchConstraint section to compare values in a comma separated list, ProductionCentre will use only the first value from the list, and display the result in the query result set.
    If you want to include values in a comma separated list in a query, you must use the In operator.
    Example of a correct query command:
    <XmlQuery Command="GetAtRows">
    <Filter Name="CPG_SetList" MaxResultCount="*">
    <SearchConstraint Column="Key" Operator="In" Values="77,78,79">
    </SearchConstraint>
    </Filter>
    </XmlQuery>
    Creating a query for large amount of data may cause a timeout message to appear in ProductionCentre
    When you create a query for a large amount of data, a timeout message may appear.
    By default, the number of items displayed in the query result set is 10000, as defined in the MaxResultCount attribute. Changing the default value may cause timeout.
    Creating a query with the ExecuteSql command with data from more than one table will return an incorrect query result set in ProductionCentre
    When you create an SQL query with the ExecuteSql command and the Join function to get data from at least two tables, the result set will display incorrect data. This is due to the fact that both tables contain columns with the same names (e.g., both contain the Name, Description, and Key columns), which cannot be distinguished in the query result set.
    If you want to combine the results of more than one table, you must use the CombineXmlQuery special query.
    Creating queries from data tables with duplicate column names results in displaying values incorrectly in ProductionCentre
    When you query data from a table which contains duplicate column names distinguished only by the letter case (e.g., Name, NaMe, nAMe), the result set will not be displayed correctly in VantagePoint.
    You should disregard this because the query returns correct results when used in Microsoft Excel. The results are only displayed incorrectly in the data grid of a query result set in the VantagePoint model.
    The query result set displays incorrect information for the WithContainedObject attribute set to "false"
    When you query data from a table that contains certain columns with lists of keys, and you set the WithContainedObject attribute to false so that the lists of keys from these columns are not retrieved, they are displayed in the query result set anyway.
    The issue applies to the following columns in the following queries:
    Columns
    In queries
    WorkInstructionKeys
    Retrieving mulitiple objects, for example:
    - GetAreas
    - GetEquipment
    - GetProcessBoms
    RouteStepKeys
    GetParameters
     


    Excel add-in issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    Error: "The VantagePoint Office feature will not be installed because Microsoft Excel has not been installed on your machine"
    This problem can occur with "non-standard" installations of Office. The problem can be seen when installing the VantagePoint server or the VantagePoint client tools. If Microsoft Excel is installed and the error occurs, verify that the following Registry Key exists on your machine:
    Office 2010:
    HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Office\14.0\
    Excel\InstallRoot Path=<PathValue>
    If this registry key does not exist, you can create the key manually and provide a value for Path that points to your Excel.exe. Rerun the Client Install to complete installation of the VantagePoint Excel Add-In feature.
    Double-clicking an Excel file or selecting the Excel shortcut from the VantagePoint Start Menu does not work
    Xcelsius 2008 enables ’Live Office Compatibility’. As a result, the Excel advanced general option 'Ignore Applications that Use Dynamic Data Exchange (DDE)' gets selected. To resolve this issue:
    1. Select Excel Office > Excel Options > Advanced.
    1. In the General Section, clear the Ignore other applications that use Dynamic Data Exchange (DDE) check box.
    Excel workbook does not display at full size after running Xcelsius (Dashboard Builder)
    After running Xcelsius, if you open Excel, the workbook does not display at full size. 
    Solution: Click the maximize button for the Excel workbook to display full size.
    Hyperlinks are not removed if they exist in a cell with a conditional expression and the false condition occurs
    In Excel, if you create a conditional formula to execute a hyperlink condition, the hyperlink will not be removed if the false condition occurs.
    Solution: Prior to publishing the report, delete all hyperlinks in cells with these conditional formulas. To delete hyperlinks, right-click and select Delete hyperlinks.
    Limitations for UDFs when the function is array-entered into the maximum number of rows (1,048,576)
    UDFs now return values when the function is array-entered into the maximum number of rows (1,048,576); however, the following limitations exist:
    • In some cases, a 'system out of memory' or a message recommending you use 64-bit Office may occur when the UDF is close to the maxiumum number of rows.
    • When requesting >350K rows, if you use ‘interpolative’ sampling with one tag, narrow history, fewer tags than requested are returned. Note that this is not an issue if you use more than one tag.
    The TimeStamp information shows the incorrect start time
    When using multiple History functions to show tag values in an Excel worksheet, the TimeStamp information of the functions may show different start time. First identified in FactoryTalk VantagePoint v8.10.00.
    Solution: To show the correct start time in the TimeStamp information, select multiple tags to run a single History function.


    FactoryTalk services issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    Remote Desktop Console session prevents creation of a FactoryTalk connector
    FactoryTalk has an option to restrict which client computers can connect to the directory. This option can cause VantagePoint to fail to log into the directory if the following conditions occur:
    • VantagePoint System Account is configured to run as a user account that belongs to the server's Administrators group.
    • Any user account that belongs to the VantagePoint server's Administrators group logs onto the VantagePoint server via remote desktop from a client computer whose name is not in the directory.
    Solution: To avoid this issue, do the following:
    • Do not configure VantagePoint to run as an administrator.
    • Do not log into a remote desktop console if VantagePoint is configured to run as a user with administrative access.
    LiveData import does not validate that an ACD file for the selected controller is correct
    When performing a Live Data import, VantagePoint assumes that the selected ACD file is correct for the selected controller. VantagePoint performs no validation of the ACD file, and tags that are not found in the OPC server are not brought into VantagePoint.
    Solution: When performing a LiveData import, make sure that VantagePoint points to the correct ACD file for the selected controller.


    License issues
    Issue
    Description
    VantagePoint client application displays ’Failed to initialize the type repository’ error
    While using a VantagePoint client application, you may receive a 'Failed to initialize the type repository' error. This error occurs because the same user has logged into the VantagePoint system from multiple locations. This is a violation of the VantagePoint licensing system.
    Solution: After receiving this error, you must wait 20 minutes for the session from one of these locations to expire. After one of the location sessions has expired, you can continue to use the application.
    VantagePoint may display two error messages when you have a license violation
    If the VantagePoint system encounters a license violation, it may display two error messages. After closing the first license error message dialog box, you may receive the following error message "Object reference not set to an instance of an object".
    Solution: Close the second error message dialog box and resolve the licensing issue.


    Portal issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    VantagePoint Portal redirected home page does not display
    While using VantagePoint, a redirected Portal home page does not display.
    Solution: Add the redirected VantagePoint Portal home page site to the Local Intranet Zone prior to browsing to it. To add the home page to the Local Intranet Zone:
    1. In Internet Explorer, select Internet Options > Security > Local Intranet.
    1. Clear the Require server verification (https:) for all sites in this zone, if needed.
    1. Click Sites, and then click Advanced, and add the URL.
    Trend and XY Plotter reports will not display unless the Portal is in the Intranet Zone
    To view Trend and XY Plotter reports in the Portal, you must add the Portal URL to the Local Intranet Zone. To add the URL to the Local Intranet Zone, in Internet Explorer, select Internet Options > Security tab > Local Intranet. Click Sites, and then click Advanced, and add the Portal URL.
    Error occurs when generating Trend, XY Plot, or Dashboard reports on Windows 8.1
    This issue only occurs if you are prompted for credentials when logging into VantagePoint on Windows 8.1 systems.
    Solution: Ensure that you have applied Windows Updates to the system. Then, select the Enable Protected Mode check box under Security Level for this zone for the Local Intranet Zone under Internet Options > Security > Local Intranet.
    Trend must finish loading the interactive control before switching to another item in the Model Browser
    When selecting a trend in the Portal, an image of the trend displays while the interactive trend control loads. In most cases, this occurs quickly, and is not noticeable. However, you cannot select another report in the Model Browser tree until the interactive control finishes loading.
    Downtime Summary report may generate with an error
    Depending on the configuration of your VantagePoint server, the Downtime Summary report MyEnterprise.Samples.v4.Advanced.Production.Reports.Line Downtime Summary may fail to execute properly. The report uses a SQL Query object that is configured in the IncuitySample database connector.
    By default, the IncuitySample database connector is ”locked down” so that users without elevated privileges have limited access to the connector or child objects of the connector. In this case, the user in question is the VantagePoint Office user (used to generate Excel Reports in the Portal). If this user is not an administrator (or if the security settings of the IncuitySample database connector has not been altered), this report will generate with an error.
    For recommendations about configuring database security for the IncuitySample database, please see http://<ServerName>/VantagePointPortal/PortalInfoPages/IncuitySampleDB/DBConnectorSecurity.html
    Some composite reports in the Report Library cannot be generated for a new installation
    Under MyEnterprise.Samples v4.Support.Report Library.Composite, the ControlLoop, DowntimeEquipment, EquipmentTimePeriod, and Standard Equipment reports are used by a previous version of VantagePoint. If you are not upgrading VantagePoint from a previous version, these reports will be empty.
    Solution: Use the ControlLoop_v4, DowntimeEquipment_v4, EquipmentTimePeriod_v4, and Standard Equipment_v4 reports instead.
    Some reports have been reordered in the Model Browser
    If you have used Content Type Rules based on inherited types for items that display in the Portal, in previous releases, child types displayed first, followed by parent types. This was a defect that has been resolved, and the Portal now orders these items based on parent types first, followed by child types.
    For example, previously, the first report under Line 1 (MyEnterprise.Samples v4.Advanced.Production.Chicago Plant.Lines) was the Line Report, and the last report was the Equipment Trend. In this release, the first report under Line 1 is Equipment Trend, and the Line Report is the third report in the list.
    It is not possible to reorder these reports to the original display that sorted by child types first.
    StatusItems folders now display in the Model Browser
    A StatusItems folder now displays in the Model Browser, and in some cases, will include duplicate content from other nodes. For example, under MyEnterprise.Samples v4.Advanced.Production.Chicago Plant, a StatusItems folder now appears with Lines 1 and 2. This content is also available in its original location under the Lines folder.
    Solution: To hide the StatusItems folders:
    1. Select System > Applications > Portal > Settings > ContentViewer > ContentTypes.
    1. Right-click each folder below ContentTypes, and select Edit.
    1. Clear the PropagateToSubTypes check box, and click OK.
    1. In the Portal, select Reports > MyEnterprise to verify that the StatusItems folders have been removed.
    (Windows 2008, IE 10 only) When using the Lock Full Screen option to view reports, external websites open in new windows
    On Windows 2008 with IE 10 installed, when using the Lock Full Screen option, external websites open in new windows, and in some cases, the website will open in the main Portal window.
    Solution: Add the external website to the Trusted Sites. To do so:
    1. In Internet Explorer, select Internet Options > Security > Trusted Sites.
    1. Clear the Require server verification (https:) for all sites in this zone, if needed.
    1. Click Sites and add the URL.
    Memory leak while using the content rotator in Internet Explorer
    When the content rotator is used in Internet Explorer there is a memory leak.
    Solution: It is recommend to run the content rotator (except for any activeX control) in Chrome version 73. We also recommend using 60 seconds or more for the AutoRotationInterval time if running the content rotator in Chrome. Note that on some browser versions, a faster update rate may cause a small memory leak.


    Security issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    Changing a user's Windows local or domain group is not reflected by VantagePoint
    If you change a user's Windows local or domain group, this change is not reflected in VantagePoint. The VantagePoint server is not notified by Windows when the group membership of a local or domain group changes.
    Solution: For VantagePoint to recognize a change in a user’s Windows local or domain group, you must restart IIS after making the change.


    Storage issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    Size-based aging strategy is not supported in this release
    A size-based aging strategy for Storage Servers is planned for a future release of VantagePoint, and is not supported in this release.
    Floating point numbers for VantagePoint tags can result in rounding errors
    Floating point numbers in VantagePoint are typically stored with 8-bit precision resulting in rounding errors such as the following: a 55.22, value in the database is 55.2200012207031.
    After renaming an Incuity tag and performing an IISRESET, only the last value is retrieved
    If you rename an Incuity tag, any values created with the old name and values created with the renamed tag can be retrieved until an IISRESET is performed. Afterwards, only the last value entered can be retrieved.


    Trend and XY Plotter issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    How to improve performance in the Portal controls (Trend and XY Plotter)
    By default, each web service call into the VantagePoint server is individually authenticated. In Intranet environments, this level of security and the associated performance overhead is typically too much. For this reason, the VantagePoint client install configures the system to allow the authentication of a web service call into a given VantagePoint server to be reused for subsequent calls into the same server.
    Unable to view Trends in the Portal on Windows
    If the "System objects: Default owner for objects created by members of the Administrators group" Group Policy on your computer is set to Administrators, attempting to open a trend in the Portal may result in an error message.
    Solution: Apply the Microsoft Hotfix in http://support.microsoft.com/kb/954494, or reset the computer's Group Policy to the default setting of "Object Creator."


    Eventing and Report Set issues

    Review the following for additional information about issues you may encounter.

    Issue
    Description
    Automatic printing of reports
    An option in the Report Set allows you to automatically print a report when it is generated. You can configure this feature to print to any printer available on the network including virtual-printers such as PDFCreator, which prints to a PDF document on disk.
    Review the following for issues related to automatic printing:
    • Printing to PDFCreator is supported for PDFCreator version 1.2.3 but not for version 1.7.
    • Trend, XY Plotter, and SSRS reports cannot be printed automatically.
    QueryProvider
    The QueryProvider does not support NameSpaceFilter for folders with " and * in the name.
    Run all reports in a folder
    When the Report set source is selected as "Run all reports in a folder" and if there is an asterisk (*) character in the folder name, Reports will not be visible in public catalog.


    Mobile issues

    Review the following for additional information about issues you may encounter.

    Issues on All Devices
    Description
    "Communication error" may appear
    This issue may occur if:
    • The signal strength for your wireless network is low, you may see a "Communication error" while using a device. You can refresh the site or press Retry to continue, and should check your wireless network to see if the signal strength is an issue.
    • The VantagePoint server has run out of licenses and no more are available. You can verify that this has occurred by reviewing the Windows Event log.
    Hyperlink and Portal Report widget issues
    Review the following:
    • When browsing to a hyperlink in the model or adding a hyperlink to a Portal Report, an authentication window prompts you to log in. This only happens the fist time you access a hyperlink. Re-enter your credentials and the report appears and any new hyperlinks will work without prompting for credentials.
    • On iOS devices only, scrolling is disabled for hyperlinks and websites.
    Web site does not load in mobile site; page is blank
    Some web sites do not support being rendered in an iframe, which is what the Portal and Mobile site use to display content. If a site does not support iframes, the page will be blank in the mobile site.
    Displays created under folders do not support the Show in Portal option
    If you create a display under a folder or item that derives from a core.folder type, when saving the display, the Show in Portal option is not available.
    Tag collection that contains a period results in No Items Found error message and a broken breadcrumb
    If you navigate to a tag collection that contains a period, when selected, the breadcrumb changes to ?/ and the screen indicates that no items were found even though there are items in the collection.
    Performance limitations on devices with small amount of RAM
    When you are browsing, searching or selecting large data collections (for example, instances including multiple members) on devices with small amount of the random-access memory (RAM), any of the following may happen:
    • The page that you are currently viewing may get reloaded.
    • The web browser may crash.
    Importing members with restricted names fails
    If you create in Studio 5000 Logix Designer a member, use one of the restricted expressions listed below as its name, and then import it, the import will fail.
    The restricted expressions that cause the import failure are:
    • Name
    • CreatedOn
    • Description
    • FullyQualifiedName
    • IconIndex
    • ModifiedOn
    • TypeName
    Phone Issues
    Description
    Cannot create a display if the view name contains a forward slash
    If the View name on the Model page contains a forward slash(/), you cannot create a display.
    Workaround: On a tablet or desktop, rename the view and remove the forward slash. You can also use the rename feature in Manager to rename the view.
    On iPhones, buttons on the Action Bar may appear to be pressed or disabled when they are available
    Buttons on the Action Bar may look as if they have been pressed or are disabled even though they are available. You can tap the screen to make them change to white, or can tap them to perform an action.
    Occasionally, value boxes do not display on the iPhone in Portrait mode
    In Portrait mode on the iPhone, a cell containing a value box appears, but the actual value box does not appear.
    Workaround: Rotate the phone to landscape mode and back to portrait mode. The value box now appears.
    Some reports created with the Portal Report widget do not display correctly on the iPhone in Landscape mode
    Some reports created with the Portal Report widget do not display correctly on the iPhone in Landscape mode. You will need to rotate the phone to Portrait mode.
    Tablet or Desktop Issues
    Description
    When importing tags, details on the Summary page do not expand to the width of the browser in IE
    This issue occurs when using IE 11.0.9600.16663.
    Solution: Upgrade to IE 11.0.9600.18376CO.
    Adding tags to the Trend Report widget removes tags in the original report
    Attempting to add tags to an existing Trend Report widget removes the original tags in the report.
    When editing a display, you do not see the tags that are being used
    This occurs if the tags exist under a location that has been hidden from all views using a navigation rule.
    Using tag parameters in Portal Report widget
    If you want to add a tag parameter to an Excel Report, you must know the exact FQN of an existing tag parameter used in the report and enter that in the Name field. Otherwise, the report will continue to use the existing tag parameters.
    Solution: To locate the FQN
    1. Open Manager.
    1. Navigate to the report and select ParametersTypes.
    1. Copy or type the FQN name into the Name field.
    Linked content such as SSRS reports, etc., do not display on Android and iOS
    Netbios name resolution is not supported on iOS and Android operating systems so linked content such as SSRS reports will not display by default.
    Solution: Use the full computer name that includes the domain or the IP address to view the mobile site.


      



    Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

    Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
    Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
    To view a complete list of Rockwell Automation trademarks please click here.
    Trademarks not belonging to Rockwell Automation are property of their respective companies.