Release Notes

( 9324-RLDx ) Studio 5000 programming software. Design software for PanelView 5000 series HMI terminals
Version 8.01.00 (released 11/2021)

Catalog Number Studio 5000 View Designer 

These release notes describe version information for Studio 5000 View Designer, version 8.01.00 (released 11/2021).

Requirements

This release has the following requirements.

System requirements for Studio 5000 View Designer version 8.01.00

For optimal performance of the View Designer application, your personal computer should meet or exceed the following hardware and software requirements. View Designer can be installed on a personal computer that meets the operating system minimum requirements, but may not meet performance expectations when used in a production system.

Hardware Requirements

Software Requirements

View Designer requires the following software on the host computer:

IMPORTANT
While the Windows 8, Windows 8.1 and Windows 10 operating systems run on many touch-enabled devices, various features of the View Designer application may not be touch-enabled. Most functions are expected to work with touch, but the software has only been tested with a keyboard and mouse.


Firmware requirements

VMware Requirements

To install and run View Designer on a VMware® virtual machine, the following versions of VMware are required:

To use the View Designer emulator, enable 3D graphics acceleration in VMware.

Features

This release includes the following system features.

System features for Studio 5000 View Designer version 8.01.00

This release of the View Designer application includes new features and functionality listed in the following sections.

New features


Corrected Anomalies in This Release

This release corrects the following anomalies.

Screen error occurs when displaying a large number of alarms (253344)

An HMI device screen error occurs when the number of alarms exceeds the recommended value. To resolve this issue, do not exceed 4,000 alarms per controller.


Tags appear in error on the Emulator if items are modified in the Browse for Controller dialog (155926)

Tags appear in error on the Emulator with an error message of Read … failed because a CIP connection could not be made if items are modified in the Browse for Controller dialog used to browse for an Emulator to Controller Path. To resolve this issue, close the Emulator, browse for the Emulator to Controller Path, and launch the Emulator again.


Emulator instance appears smaller than expected after rebooting a Hyper-V Virtual Machine (153276)

Rebooting a Hyper-V Virtual Machine with View Designer installed or shutting down View Designer without first closing the VM window causes the first instance of the Emulator that opens after the reboot or restart to appear smaller than expected. Close and restart the Emulator.


Deleting and re-adding a PDF document from a project does not automatically refresh an instance of a PDF Viewer (153526)

Deleting and re-adding a PDF document from a project does not automatically refresh an instance of a PDF Viewer Add-On Graphic that references the PDF document. Close and reopen the project or screen containing the PDF Viewer Add-On Graphic, or select a different PDF document in the PDF Viewer Add-On Graphic and then reselect the re-added PDF document in the PDF Viewer Add-On Graphic.


Too many elements on the screen results that not all of them displays. (862116)

If multiple elements on a screen have state tables with many states and many of the properties of the elements are included in the state table, then some of the elements may not be visible on the screen. To work around this anomaly, use fewer properties in the state tables or have a smaller number of states.


Known Anomalies in This Release

This release has the following known anomalies.

Partial frame appears around PDF document displayed on the HMI device (1069225)

The PDF viewer from Toolbox > System may have a partial frame around the PDF document on the HMI device.


PanelView 5310 lose synchronization with CompactLogix 5370 controller when HMI devices are power-cycled while pushing HMIBC buttons (1273015)

PanelView 5310 HMI devices might not synchronize with CompactLogix 5370 controller after power disruption when an HMIBC button is pushed. The HMI devices after powering up show an indeterminate state. If this occurs, cycle power to the Logix controller.


.dmk file's digital signature verification fails when using ControlFLASH Plus (1339133)

When flashing the HMI device, ControlFLASH Plus returns an error failing to validate the digital signature of the .dmk file. This anomaly exists when using ControlFLASH Plus version 4.00. A future version of ControlFLASH Plus will resolve this anomaly.


Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Adding an initial user-defined data type property definition to a screen when a shortcut to the screen is open does not immediately show the new property on the Properties pane of the shortcut. Select the defining screen tab again and then reselect the shortcut tab. Alternatively, close and reopen the shortcut or click within the Project Explorer. [145474]

Copying Navigation menu commands causes invalid references. (814821)

Copying screens that contain elements with Navigation commands and pasting them to a different project may cause the copied navigation commands to reference different screens. After pasting the screens, make sure that any navigation commands reference the correct screens.


Data updates pause intermittently after network disruptions on CompactLogix 5370 controllers (460566)

When using CompactLogix 5370 controllers running V33 firmware, rapidly repeating network disruptions may cause PanelView 5000 HMI devices to intermittently pause updating data for two or three seconds at a time. If this occurs, cycle power to the switches in your network, or manually disconnect and reconnect ports.



Conflicting error messages appear after downloading a project containing a tag with a syntax error or invalid format (146146)

Downloading a project containing a tag with a syntax error or invalid format displays conflicting error messages. An incorrect message appears stating that the tag does not exist in the controller or has an External Access property set to None. The correct error message appears in the Errors pane.


Installing the Windows KB4055002 patch corrupts the Windows FontFamily element (1353640)

Installing the Windows KB4055002 patch corrupts the Windows FontFamily element. Binding to a text property for graphic element then displays an error and prevents the Properties pane from expanding. To prevent the error and expand the Properties pane when binding to a text property, install .NET framework update 4055532. This update includes patch Windows KB4074880 which resolves the corruption of the Windows FontFamily element.



The number of Navigation menu icons is different on View 5000Emulator and on the physical HMI device when using Windows 7 (DFCTS00365265)

In Windows 7, the number of screen icons that appear in the Navigation menu in the View 5000 Emulator window of an emulated project may be different than the number of screen icons that appear in the Navigation menu for the same project on the physical HMI device.


Some traces do not appear after pausing a trend chart (1353612)

Pausing a trend chart may cause some traces to no longer appear. This may occur when pausing and resuming a trend chart immediately after a download or screen navigation. The data does not appear if the trend chart has a higher sample rate than the data log. The trend chart plots only historical data for the sample period.


Inconsistent synchronization indications and tag communication errors when Logix controller is out of memory (1353614)

Inconsistent synchronization indications and tag communication errors may appear on the HMI device when the Logix controller is almost out of memory.


Windows 7 causes project download to fail (1353618)

A Windows 7 anomaly may cause a project download to fail with a message that View Designer cannot connect to the HMI device. See Rockwell Automation Knowledgebase Answer ID 2588507 and install the hotfix.


Reinserting the SD card immediately after ejection does not restart data logging (1353621)

Ejecting and immediately reinserting the SD card into the HMI device may not restart data logging. Data logging does not recognize that the SD card is present. Eject the SD card, wait several seconds, and reinsert the SD card to restart data logging.


View Designer creates .dmp files after opening a version 2.xx project on later View Designer versions (1353632)

Opening a View Designer version 2.xx project when View Designer version 3.01 or later is installed creates .dmp files in C:\ProgramData\Rockwell Automation\Studio 5000\CrashDumps. Delete the .dmp files to recover disk space. Rebooting the computer may stop the creation of .dmp files.


Project without a .vpd extension does not download to the HMI device (1353636)

A project that is open in View Designer version 3.01 that does not have a .vpd extension cannot download to the HMI device when both View Designer version 3.01 and version 4.01 or later are installed on the same computer. Rename the project file to end in the extension .vpd.


FAT 32 SD cards may corrupt the SD card file system on HMI device power loss (1353639)

SD cards formatted with FAT32 may corrupt the file system on the SD card if the HMI device loses power while data logging. Use an SD card formatted with EXT3.


Edit menu buttons are disabled after undocking Toolbox or Properties windows (DFCTS00342576)

Closing a project with the Toolbox or Properties window undocked disables the Cut, Copy, Paste, Delete, and Select All commands from the Edit menu when the project is re-opened. To enable the menu items, dock the Toolbox or Properties window.


State Enter event does not trigger when navigating from one shortcut to another shortcut representing the same screen (DFCTS00361627)

When two or more shortcuts navigate to the same screen and that screen has a State Table and a State Enter event, navigation from a shortcut triggers the State Enter event. When immediately navigating from the open shortcut to another shortcut that also represents the same screen, the State Enter event does not trigger.


Language files are lost when importing a project that uses a language not supported on the machine (DFCTS00363733)

If a project using a language in the language import/export file is created on a computer using a language that is not supported by the operating system on a second computer, when copying the project to the second computer and exporting the language file, the unsupported language data does not export and is lost. Ensure that the target computer supports the exported language.


Graphic elements added to the definition of an Add-On Graphic show outside of the selected Add-On Graphic after Cut and Paste (DFCTS00362720)

Graphic elements added to the definition of an Add-On Graphic after an instance of the Add-On Graphic is cut are shown outside of the selected Add-On Graphic instance when it is pasted. To resolve this issue, create a new instance of the Add-On Graphic instead of pasting the instance.


HMI device does not indicate a download in progress when a screen saver is running (DFCTS00342409)

When downloading to an HMI device on which the screen saver is running, there is no indication that the download is occurring, and the Home screen, rather than the last open screen, appears on the HMI device when the download is complete.


Events do not function when added to alarm tables (DFCTS00360544)

The Events tab is visible when selecting an Alarm table graphic element. Alarm table graphic elements have built-in events. Adding events to an alarm table graphic element may cause the built-in events to stop working. Do not add events to an alarm table graphic element.


View Designer terminates when running on a machine with InstantGo or Connected Standby (DFCTS00351966)

View Designer may crash when running on a device using the InstantGo or Connected Standby feature of Windows and the device enters Sleep mode. Restart View Designer. 


ShelveDuration and MaxShelveDuration values do not update when changed through a numeric input form the HMI device (DFCTS00339713)

The ShelveDuration and MaxShelveDuration values for an alarm are not updated if the values are changed through a numeric input from the HMI Device. The previous values are used instead. To change ShelveDuration and MaxShelveDuration for an alarm, use Logix Designer.


HMI device restarts when synchronizing with a controller with more than 50,000 tags (DFCTS00361416)

Projects referencing a controller with more than the recommended limit of 50,000 tags may experience a restart of the HMI device when performing an online synchronization with the controller. Reference a controller with no more than 50,000 tags.


Firmware update fails or HMI device faults when updating firmware using ControlFLASH and changing screens (DFCTS00356235)

Using ControlFLASH to update the firmware on the HMI device while the HMI device is changing screens may cause the following:

If the firmware update fails, use ControlFLASH again to complete the firmware update. If the HMI device faults, restart the HMI device and then use ControlFLASH again to complete the firmware update.

To avoid this issue, update the firmware on the HMI device when the HMI device is not changing screens.


Toolbox search using keyboards for Japanese and Chinese crashes View Designer (DFCTS00362734)

View Designer crashes when searching the Toolbox using keyboards for Chinese and Japanese.


Touch or key events triggered simultaneously on button release execute when the first button releases (DFCTS00354276)

The release action for Button Behavior events that are triggered simultaneously by a touch press or key press execute when the first touch or key releases. This occurs even when the other touch or key is still pressed.


Passed-through properties of aliased Logix Designer tags do not display on the HMI device (DFCTS00350204)

The HMI device does not display passed-through extended properties of aliased Logix Designer tags.


Text Input graphic element shifts down during inline editing on machines without DirectWrite support (DFCTS00342434)

On computers that do not support DirectWrite, the Text Input graphic element may shift down a line during inline editing. This does not affect how the text is displayed on the HMI device.


Functional Changes

This release has the following functional changes from the previous release.

Functional changes

View Designer version 8.01 has the following changes since the last release:

View Designer performance was improved in these functions:

Runtime performance was improved for:

Popup caching is now selectable using the Cacheable property on a popup.

Images are now limited in size to avoid performance issues.

To launch projects faster, View Designer now performs some background operations after the project is opened instead of waiting to open the project.


Application Notes

This release has the following application notes.

Application notes

The following are the application notes for View Designer version 8.01.

Installation

Installing View Designer requires local administrative privileges. If these privileges are unavailable or if your company uses third party privilege management software, work with your IT department to install View Designer. Virtual machines generally have local administrative privileges.

Multi-version support

SD card requirements

PanelView 5000 requires the following for SD cards:

IMPORTANT
  • FAT32 may corrupt an archive file in the event of a power outage.If the HMI device detects corruption on startup, this creates a new archive file, losing previous data.
  • EXT3 is less susceptible to corrupting an archive file.

I/O connection

When a PanelView 5000 is in the I/O tree of the Logix controller and the Logix controller becomes overloaded to the point where it no longer processes communication of tag data with the PanelView 5000, a loss of the I/O connection between the Logix controller and the PanelView 5000 HMI device may occur. The I/O connection re-establishes when the Logix controller has the bandwidth to handle tag data communications.

Project conversion

View Designer version 8.01 contains a new System Banner and predefined screens. When converting a project to View Designer version 8.01:

Firewall rules

View Designer does not require endpoint firewall rules because it is not a server product that allows remote clients.

Additional security considerations when using Rockwell Automation products include:

Limits

For best results, observe View Designer project limits:

Description
Limit
Notes
Number of controllers
1 (PanelView 5310)
4 (PanelView 5510)
 
Number of HMI devices per controller
4
 
Number of tag references on a single screen
2000
 
Total number of tag references in a View Designer project
20000
 
Number of screens and popups
100 for PanelView 5310 and 500 for PanelView 5510
Shortcuts and pre-defined screens do not count towards the limit.
Number of shortcuts in a project
400
 
Number of alarms in a controller
4000 tag-based or 1000 instruction-based
 
Number of alarms in a project
16000 tag-based or 4000 instruction-based
PanelView 5310 is still limited to 4000 tag-based or 1000 instruction-based alarms.
Number of elements on a single screen
1000
 
Number of graphic elements on a single screen
1000 or until reaching memory capacity
 
Number of Add-On Graphic definitions per project
500
 
Number of Add-On Graphic instances per project
500 or until reaching the 1000 tag reference limit for a screen
 
Number of Add-On Graphic instances on a screen
500 or until reaching the 1000 tag reference limit for a screen
 
Number of graphic elements in an Add-On Graphic
250
 
Number of properties defined for an Add-On Graphic
20
 
Number of tags in a controller
50000
View Designer counts every scalar, array element, structure member, and so forth, as  a separate tag.
Number of tags for all data logs in a project
250
 
Image size limit
10 MB
 
Number of project events per project
1000
 
Number of images on a screen
500 or memory full
 
Number of PDF viewer graphic elements on a screen
2
 
Number of PDF viewers appearing simultaneously on a screen and popup
2
 
Amount of metadata
Each analog tag referenced is capable of having eu/min/max. Each BOOLEAN tag referenced is capable of having state identifiers All referenced tags are capable of having  descriptions.
 
Number of View Designer instances open simultaneously
3
View Designer does not support opening the same project in more than one instance of View Designer.
Length of a text input
82 characters
 
Length of a text display reading from a STRING data type in the controller
476 characters
Using UTF-8 for STRING encoding may result in displaying 476 characters incorrectly. Each character may take multiple bytes of data.
Number of users defined in Security Administration
500
 
Number of simultaneous VNC connections to PV5000
1
 
Number of simultaneously running Emulators
1
 
Number of allowed data points to log
1.296 billion
This number of data points equals 250 data points at 500 milliseconds for 30 days.
Combined number of PanelView 5000 HMI devices and Logix controllers that can communicate with each other through a 1756-EN2T or 1756-EN3T Ethernet module is eight or fewer.
 
8 or fewer
Refer to technical support Answer ID QA30757 for more details.
Number of alarm transitions in the Alarm History
40000
 

Sample Applications

The Sample Applications for View Designer can be found at C:\Users\Public\Documents\Studio 5000\Samples\View Designer

  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2025 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.