Release Notes

Firmware for AADvance (T9110); a distributed, modular, complete SIS solution. IEC61508 ed2. Contains firmware for the I/O modules as well (T9401, T9402, T9431, T9432, T9451, T9481, T9482)
Version 1.041 (released 11/2021)

Catalog Number AADvance 

These release notes describe version information for AADvance, version 1.041 (released 11/2021).

Requirements

This release has the following requirements.

AADvance System Requirements for Version 1.041

AADvance Processor Firmware Revision 1.041

Catalog Numbers: T9100, T9110, T9300, T9401, T9402, T9431, T9432, T9451, T9481, T9482, T9033, T9030, T9040, T9082U, T9082D, T9083U, T9083D, T9084U, T9087

Each module has an Effective Date (ED), or a hardware revision letter and firmware revision number. These indicate the hardware and firmware build level on the module at manufacture time. This information can be found on the side label of each module.

Example of a hardware revision letter and firmware revision number:

graphic

If you have hardware that is not compatible, please contact Tech Connect.

Product
Version 1.041
Functionally Identical
Functionally Compatible
Not Compatible
Hardware Revision
Use Firmware
Hardware Revision
Use Firmware
T9033
AADvance DTM – HART
1.3
N/A
None
N/A
None
N/A
T9030
OPC Portal
1.20.508
N/A
None
N/A
None
N/A
T9040 OPC Server
2.1.510.1
N/A
None
N/A
None
N/A
T9082U
T9082D
T9083U
T9083D
T9084U
AADvance Workbench
1.40.000
N/A
None
N/A
None
1.20.520 and earlier
T9087
AADvance Workbench
2.1.2195
N/A
N/A
N/A
N/A
2.00.752
T9100
Processor Base
G
None
N/A
E
N/A
A to D and F
T9110
Processor Module
K
H to K
Normal Mode 1.041
and
Recovery Mode 1.001
None
N/A
A to G
T9300
I/O Base
D
B and C
N/A
None
N/A
A
T9401
8 Ch, Digital Input Module
I16
H and I
16 or 15
None
N/A
Hardware A to G
Firmware 14 or earlier
 
T9402
16 Ch, Digital Input Module
F16
F
16 or 15
D
16 or 15
Hardware A to C and E
Firmware 14 or earlier
T9431
8 Ch, Analog Input Module
I16
H and I
16 or 15
None
N/A
Hardware A to G
Firmware 14 or earlier
 
T9432
16 Ch, Analog Input Module
F16
F
16 or 15
D
16 or 15
Hardware A to C and E
Firmware 14 or earlier
T9451
8 Ch, Digital Output Module
K13
H, J, and K
13
None
N/A
Hardware A to G and I
Firmware 12 or earlier
T9481
3 Ch, Analog Output Module
K
J
14
None
N/A
Hardware A to I
Firmware 13 or earlier
T9482
8 Ch, Analog Output Module
P
O
14
None
N/A
Hardware A to N
Firmware 13 or earlier


T9110 Processor modules with a hardware revision H to K must be updated with the Normal Mode firmware 1.041 and Recovery Mode firmware 1.001.

Important: It is recommended that ControlFLASH version 15.04 or higher is used.


  


  

Features

This release includes the following system features.

Improved ISaGRAF eXchange Layer (IXL) protocol security (1364522)

Improvements to reduce security risk and add security capabilities for the ISaGRAF eXchange Layer (IXL) protocol for communications between ISaGRAF-based components.

For information, see Knowledgebase Document ID: PN1567 ISaGRAF Runtime Affected by Multiple Vulnerabilities.

Enhanced power supply (PSUP) data validation (486652)

Introduced an enhancement to help verify that the power supply (PSUP) monitor on the I/O module has the correct firmware revision.

  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Soft Error Detection (SED) faults (1052833)

CORRECTED Anomaly with Firmware Revision 1.41

AADvance modules report Soft Error Detection (SED) faults that can lead to memory corruption.

For information, see Knowledgebase Document ID: PN1520 Product Notice 2020-07-002 - Allen-Bradley 1715 and AADvance T9000 Nuisance Soft Error Detection Faults (202007002).

Firmware only permits a maximum of 31 Modbus masters for configuration (1364532)

CORRECTED Anomaly with Firmware Revision 1.41

The firmware only permits a maximum of 31 Modbus masters for configuration instead of 32.

Modbus master task may stop responding (1364545)

CORRECTED Anomaly with Firmware Revision 1.41

When there is a large number of Modbus messages configured for Mobus master and Modbus slave, certain command-line interface (CLI) commands may cause the Modbus master task to stop responding.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.