This release has the following requirements.
Review these minimum and recommended system requirements for installing, configuring, and running FactoryTalk Batch version 15.00. Unless noted, these requirements assume that no other applications are installed on the computer. Preferred operating systems and software applications are prioritized for support, testing, and post-release patch qualifications.
Hardware requirements
Supported operating systems
Supported database applications
(for storing recipes, materials, reports, and journal archives)
Web browsers
(for FactoryTalk Batch View only)
Logix firmware requirements
(for FactoryTalk Batch only)
Logix Designer Application requirements
(for FactoryTalk Batch only)
FactoryTalk View SE requirements
(for integration of FactoryTalk Batch View HMI Controls)
FactoryTalk Services requirements
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information, see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
Warranty
The warranty does not cover systems that do not meet the minimum requirements for the version of software.
IMPORTANT: FactoryTalk Batch version 15.00 supports only the U.S. English versions of operating systems. For more information about supported operating systems and other Rockwell Software product version support, refer to the Product Compatibility and Download Center (PCDC).This release includes the following system features.
FactoryTalk Batch version 15.00 has the following new and enhanced features:
New features
FactoryTalk Batch
FactoryTalk Batch version 15.00 adds a property that specifies the controller program name of the Equipment Phase or Equipment Sequence for phases and operation sequences when connected to a a Logix5000 CIP data server. This enables modular design concepts, promotes the reuse of code and simplifies the integration of skids into a common system.
The FactoryTalk Batch Server in version 15.00 supports area models that contain up to 210,000 total tags. This provides better support for OPC/Live Data tags.
Enhanced features
FactoryTalk Batch version 15.00 supports deleting objects from an area model while the batch is running. This feature makes the FactoryTalk Batch system more flexible and easier to adapt to changing requirements while still improving the amount of system uptime and overall productivity. Changes made to the area model are saved, but only applied to the runtime system when explicitly deployed to the runtime server. Deployment is conditional based on verification of both the changes to the area model and the impact to runtime system.
FactoryTalk Batch View and FactoryTalk Batch View HMI Controls can be installed using the same installation program as the other FactoryTalk Batch software.
Deprecated features
The FactoryTalk eProcedure Client, legacy FactoryTalk Batch View Client, and the FactoryTalk Batch ActiveX Controls are not included nor supported by FactoryTalk Batch 15.00. If your production system has dependencies on these products, transition to the modern FactoryTalk Batch View and FactoryTalk Batch View HMI Controls before upgrading to FactoryTalk Batch 15.00.
This release corrects the following anomalies.
The following list identifies the anomalies corrected in FactoryTalk Batch version 15.00. Use the identification information provided in the brackets [] to track the anomaly in future releases or if you need assistance from Customer Support with a related issue.
BatchIDCreation project update needed for Batch Server [914495]
Custom BatchIDCreation project in .Net format is needed. Current version is out of date
with modern development tools.
In FactoryTalk Batch 15.00 a new BatchIDCreate project is provided.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Recipe Editor allows the use of reserved words in expressions [914545]
In FactoryTalk Batch 15.00 the Recipe Editor will provide Recipe Verification Warnings for step collisions where the name of a Parameter or Report collides with a step attribute (such as ERROR, MODE, FAILURE, OWNER, and so on). The Transition Expression Editor Dialog will display an error message if name collision warnings are detected.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Master Recipe List slow to populate [914551]
In FactoryTalk Batch 15.00 the Recipe Object Model processing was improved to provide a faster load time.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 13.02
Recipe Editor terminates when saving formulation to SQL database [982003, 1369929]
When using the SQL storage format attempting to save or validate a recipe that contains one or more formulations, the Recipe Editor crashes and the changes to the recipe are lost. In FactoryTalk Batch 15.00 the recipes are saved and validated without issue.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Batch View Server Product Policies missing on remote FactoryTalk Directory [1063952]
In FactoryTalk Batch 15.00 the Batch View Server Product Policies are installed as part of FactoryTalk Services Platform 6.30.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
FactoryTalk Batch View Server fails to provide eProcedure instructions for multiple recipes [1064202]
When FactoryTalk Batch View does a getInstruction or getState call to the eProcedure Server it provides the set of createIDs for the Batches that correspond the the eProcedure instructions. If the client requests multiple createIDs and one of them is wrong the eProcedure server returns an error saying: "Unable to retrieve recipe step information for the specified procedure" and none of the instructions are provided. In FactoryTalk Batch 15.00 each createID is evaluated individually and the relevant instructions are provided.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch View 1.02
FactoryTalk Event Archiver Installation failure when using SQL Server on a named instance [1105890]
In FactoryTalk Batch 15.00 the installation program has been updated to use a different method of determining if SQL Server is installed.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Recipe Editor is slow to open when first started [1144064]
When using RDB recipe format, with approval workflows enabled, the Recipe Editor may take a long time to open and may appear to be stuck. It may also take longer than expected to launch and display the Open Recipe dialog. These performance issues are especially noticeable when using a large number of recipes. FactoryTalk Batch 15.00 improves the performance of the Recipe Editor when using RDB recipe format with approval workflow enabled.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Recipe Editor open file dialog delayed response [1146906]
When using SQL recipe storage format, the Open File dialog would take a long time to to open. FactoryTalk Batch 15.00 improves the performance of the Open Dialog when using SQL storage format.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Batch Server service unexpectedly terminates when logging error information [1172391]
The Batch Server service terminates when handling a small number of uncommon errors. In FactoryTalk Batch 15.00 the error handling was updated so that the Batch Server responds appropriately.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Batch Server service terminates when a batch created from a UPC recipe is remove from the Batch List [1176902]
In FactoryTalk Batch 14.00 the removal of a unit procedure from the batchlist could randomly cause the Batch Server service to unexpectedly terminate. In FactoryTalk Batch 15.00 the removal logic was revised to allow removing of the batch.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Batch Server Memory growth when using formulations [1194413]
When reading formulation data, the BatchSvr.exe memory usage grows. This memory growth may lead to performance issues with the FactoryTalk Batch system and may lead to termination of the Batch Server service. This can occur when using any the FactoryTalk Batch Client applications, or by using the INFO_TRIMMED, FOMULATION_DATA, and FORMULATIONS_INFO API calls directly. The memory growth is especially fast when using large recipes with a large number of formulation sets. In FactoryTalk Batch 15.00 the system correctly handles allocation and deallocation of memory for the API calls.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
eProcedure Step Verification Signature does not include the full user name [1302092]
In FactoryTalk Batch 15.00 a new way to configure the step verification signature was implemented. This method made changes to the following:
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 13.00.02
No indication when the Batch server has issues writing entries to the Batch event journal [1325957]
In FactoryTalk Batch 13.00.02 there is no indication if the Batch server has issues writing entries to the Batch event journal. In FactoryTalk Batch 15.00, if the Batch server has issues writing entries to an event journal, it will attempt to log a message to the FactoryTalk Diagnostics log, and when possible, will include the details of the errant journal event in that message.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 13.00.02
FactoryTalk Batch installation does not set the correct service account for eProcedure Server [914598]
When adding FactoryTalk eProcedure and Material Manager Editor to an existing FactoryTalk Batch install, the installer will incorrectly set the service account used to run the eProcedure Server. It also does not configure the computer name of the Material Manager Server. The installer for FactoryTalk Batch 15.00 now prompts the user for the required information.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Unsupported integer datatypes result in error [914582]
Tags with USINT, SINT, UINT, INT, and UDINT datatypes in the controller are not supported by FactoryTalk Batch. Attempting to read or write to these tag types may result in a phase failure.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Upgrade failure when installing FactoryTalk Batch with FactoryTalk Event Archiver [914577]
Upgrade may fail unexpectedly when installing FactoryTalk Batch with FactoryTalk Event Archiver. In this situation, the install does not complete and system becomes unresponsive. This situation occurs because previous versions of the FactoryTalk Batch uninstall program do not always successfully remove the existing ODBC DSN entry for the Batch Event Archiver data source. The FactoryTalk Batch 15.00 installer checks for an existing "FactoryTalk Batch Events" DSN during the install process. If there is, it will remove the existing DSN and create a new one.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
Area model updates: When deploying runtime area model updates the system does not check for activations [00369234]
The system only checks for licenses when the Batch Server is started. If the area model modifications require more activations than are available, a restart of the Batch Server will fail during the license check.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
FactoryTalk Batch View
FactoryTalk Batch 14.00 included FactoryTalk Batch View 2.00. FactoryTalk Batch 15.00 includes FactoryTalk Batch View 2.01. Anomalies corrected in patches released subsequent to the release of FactoryTalk Batch 14.00 are included in the list of anomalies corrected in this release.
Using "textarea" tag in eProcedure html file causes a command error in Batch View [990743]
If an eProcedure html instruction file uses a "textarea" tag for a phase report parameter it will prevent the instruction from completing, when you select the OK button after filling in the text box you get the error "Control Step was already responded to by another client". In <FTBV 2.01 the FactoryTalk Batch View client and server were updated to properly handle textarea tags
Corrected Anomaly with FactoryTalk Batch View 2.01
Known Anomaly First Identified in FactoryTalk Batch View 2.00
Batch Reports not working in FactoryTalk Batch View HMI Control [1277219]
Selecting the Reports control in the FactoryTalk Batch View HMI User Controls results in a white display. In FactoryTalk Batch View 2.01 the HMI User Controls open the Reports view as expected.
Corrected Anomaly with FactoryTalk Batch View 2.01
Known Anomaly First Identified in FactoryTalk Batch View 2.00
Signature cancellation causes issues with future steps [1430586]
Completing a sign-off of a manual instruction signature request generated after a cancellation of a manual instruction signature causes FactoryTalk Batch View to become unresponsive.
Corrected Anomaly with FactoryTalk Batch View 2.00.11
Known Anomaly First Identified in FactoryTalk Batch View 2.00
Modern FactoryTalk Batch View client only allows scaling up to 1000% [1327777]
The legacy FactoryTalk Batch View client had a limit of 3.4028238 on the Batch Scale setting. The modern FactoryTalk Batch View client was designed to place an upper limit of 1000% on the Batch Scale setting. Patch 2.00.10 replaces this limit with the previous limit of 3.4028238 returning the Batch View functionality to parity with the legacy client.
Corrected Anomaly with FactoryTalk Batch View 2.00.10
Known Anomaly First Identified in FactoryTalk Batch View 2.09
User ID is blank in FactoryTalk Batch journal when eProcedure instructions are completed using FactoryTalk Batch View [1302090]
Event Signatures from the eProcedure server did not include the User ID (also referred to as user login name and user name), making it difficult to validate the signatures. This release updates the FactoryTalk Batch View Server to provide the option to store the User ID of the user that completes the eProcedure instruction in the event journal.
Corrected Anomaly with FactoryTalk Batch View 2.00.09 and FactoryTalk Batch
14.00.00.309
Known Anomaly First Identified in FactoryTalk Batch 2.00.08 and FactoryTalk Batch
14.00
FactoryTalk eProcedure instructions result in unresponsive client [1072655]
When requesting FactoryTalk eProcedure instruction information for multiple recipes, the request will fail for all recipes if there is an issue with any of the recipes in the request. This can lead to performance issues with FactoryTalk eProcedure instructions, and a potentially unresponsive client.
With FactoryTalk Batch View 2.00.08, FactoryTalk eProcedure Instruction information requests for recipes that do not have errors will be processed, regardless of whether other recipes have errors or not.
Corrected Anomaly with FactoryTalk Batch View 2.00.08
Known Anomaly First Identified in FactoryTalk Batch 2.00.07
FactoryTalk Batch View resubmitting completed instructions [1064081]
FactoryTalk Batch View submits the completion of an instruction multiple times, which can result in the next instance of an eProcedure phase being skipped.
Corrected Anomaly with FactoryTalk Batch View 2.00.07
Known Anomaly First Identified in FactoryTalk Batch 1.02.66
Batch View Server stops responding after FactoryTalk Batch View error [1064112]
FactoryTalk Batch View encounters an error while processing an expression, which may cause the Batch View Server to stop responding.
Corrected Anomaly with FactoryTalk Batch View 2.00.07
Known Anomaly First Identified in FactoryTalk Batch View1.02.60
UserID is blank in FactoryTalk Batch journal when eProcedure instructions are completed using FactoryTalk Batch View [1064092]
In FactoryTalk Batch View 2.00.07 the UserID of the user that completes the eProcedure instruction is passed to the Batch Server and included in the event journal.
Corrected Anomaly with FactoryTalk Batch View 2.00.07
Known Anomaly First Identified in FactoryTalk Batch View 1.02.66
FactoryTalk users have read-only access when using FactoryTalk Batch View [CLM 5101]
Product policies for FactoryTalk Batch View were not installed. Product policies now install correctly.
Corrected Anomaly with FactoryTalk Batch View 2.00.05
Known Anomaly First Identified in FactoryTalk Batch View 1.01
Batch View Security: The Batch View 1.02 policies and 2.00 policies do not coexist in a FactoryTalk directory [899076]
Security granularity has changed from FactoryTalk Batch View 1.02 to 2.0. New security policies were added for FactoryTalk Batch View and FactoryTalk Batch View HMI controls. In the initial release of FactoryTalk Batch View version 2.00 the policies that were used by FactoryTalk Batch View 1.02 and FactoryTalk Batch View HMI Controls 1.02 were no longer available.
In FactoryTalk Batch View version 2.00.05 the FactoryTalk Batch View 1.02 security policies were restored and disambiguated from the FactoryTalk Batch View version 2.00 security policies so that they could coexist in the FactoryTalk Directory and both clients can be supported.
Corrected Anomaly with FactoryTalk Batch View 2.00.05
Known Anomaly First Identified in FactoryTalk Batch View 1.01
FactoryTalk Batch Material Manager
Material Server not able to access the material database remotely [925005]
The installation program for the Material Server was not setting the RemoteAccessEnabled key for remote access to the material database.
Corrected Anomaly with FactoryTalk Batch 15.00
Known Anomaly First Identified in FactoryTalk Batch 14.00
This release has the following known anomalies.
The following list identifies the anomalies that were identified during testing of FactoryTalk Batch version 15.00. Use the identification information provided in the brackets [] to track the anomaly in future releases or if you need assistance from Customer Support with a related issue.
FactoryTalk Batch View
Port conflict when using HTTPS [1536376]
FactoryTalk View SE, FactoryTalk Services Platform and FactoryTalk Batch View support secure communication using HTTPS and use the default HTTPS port 443. There are two situations in which this port conflict could impact FactoryTalk Batch View.
To work around this issue, install FactoryTalk Batch View after FactoryTalk View SE.
Use one of these workarounds to resolve this issue:
These anomalies are from previous releases but are still known in this release.
Installing FactoryTalk Batch version 14.00 and later updates FactoryTalk Services Platform to version 6.20 [00369202]
There is a known anomaly in FactoryTalk Services Platform 6.11 and 6.20 that impacts FactoryTalk Event Archiver components. When FactoryTalk Diagnostics version 6.11 or 6.20 and Microsoft SQL Server Reporting Services 2017 or 2019 are installed on the same computer, Microsoft SQL Server Reporting Services fails to work. This anomaly was first identified in FactoryTalk Services Platform version 6.11.00.
To avoid this problem, change the default port used by Microsoft SQL Server Reporting
Services from 8082 to another port.
For steps to address the issue after installation is complete, see Knowledgebase
Document ID: BF25929 - SQL Server Reporting Services stops working after installing
FactoryTalk Diagnostics.
FactoryTalk Batch Material Manager
Material Editor cannot access the material database after upgrading FactoryTalk Batch [929120]
The MTUser account is not in the correct database. Anomaly first identified in FactoryTalk Batch 14.00.
To work around this issue use these steps:
FactoryTalk eProcedure
Cannot create HMI Server on a computer with FactoryTalk eProcedure and FactoryTalk View SE [00369237]
After adding eProcedure to a FactoryTalk Batch and FactoryTalk View SE install, an HMI Server cannot be created.
To work around this issue, restart the computer after installing eProcedure, then create the HMI Server.
FactoryTalk Batch View 2.00
Pop-up notifications are persistent [519919, 519912]
For example: When an invalid login is used, a pop-up notification is displayed, indicating that the login is invalid. The notification is not cleared even after a successful login is completed.
Anomaly first identified in FactoryTalk Batch View 2.00.
To work around this issue, the user must close the notification.
Unintended actions from Arbitration Summary page [98187]
On the Arbitration Summary page, when the More menu is open and a user selects
Enter, the first item in the More menu is executed, resulting in possible unintended
actions.
Anomaly first identified in FactoryTalk Batch View 2.00.
To avoid this issue, in FactoryTalk Security, enable confirmation messages, which prompt to confirm before actions are performed in FactoryTalk Batch View.
Spurious "No master recipes are released to production" message [263925]
When adding a batch to the batch list, the client may display a "No master recipes are released to production" message while the system is gathering the control recipe data.
Anomaly first identified in FactoryTalk Batch View 2.00.
To work around this issue, wait for the recipes to load. The message disappears after the recipes are loaded.
Spurious client reports of control recipe removal [471548]
During the runtime area model update, the control recipe may be inaccessible to the client, causing the client to report that the control recipe has been removed.
Anomaly first identified in FactoryTalk Batch View 2.00.
The control recipe is not actually removed, so you can ignore this message
Filters not functioning on Arbitration Summary page [760902]
On the Arbitration Summary page, when performing a warm restart or applying a run-time area model update, applied filters may not function as expected.
Anomaly first identified in FactoryTalk Batch View 2.00.
To work around this issue, reapply filters.
Filter values are not cleared automatically [98193]
When a user sets filter values on a phase while on the Equipment page and then restarts the FactoryTalk Batch View Server, the filter values are not cleared automatically.
Anomaly first identified in FactoryTalk Batch View 2.00.
To work around this issue, after restarting the FactoryTalk Batch View Server, manually clear the filter values.
FactoryTalk Batch View HMI Controls 1.00
FactoryTalk View SE Client process lock [360350]
When a Display Client is closed while running a FactoryTalk View SE display that contains the FactoryTalk Batch HMI Controls, the Display Client process keeps running as a background process. This may prevent the ability to launch subsequent instances of the Display Client.
Anomaly first identified in FactoryTalk Batch View HMI Controls 1.00
To work around this issue, reboot the machine on which the FactoryTalk View SE Display Client is executing.
FactoryTalk View Batch server authorization changes only reflected in FactoryTalk View SE user interface only after login [362225]
If a change is made to the FactoryTalk Batch View authorization policies when a FactoryTalk View SE display containing an HMI Control is in runtime, the change is not reflected in the user interface.
The user is required to log out and then login with valid credentials for the new authorization policy changes to be reflected in the user interface.
Removed BaseFilter batch remains on batch list [CLM 4578]
If a BaseFilter batch state is applied (such as State:Running) and the state changes for a currently visible batch on the Batch List, the batch is visibly removed from the list and the message: Control Recipe <name> has been removed appears.
Even though the applied BaseFilter removes visibility to the batch, the batch is actually still on the batch list and can be viewed from other clients or HMI Controls that do not filter based on the batch state.
This release has the following functional changes from the previous release.
FactoryTalk Batch version 15.00 has the following functional changes:
Change in operating system support
Beginning in this release, the product installer prevents installation on all 32-bit versions of Windows operating systems (for example, Windows 10, 32-bit) and any Windows 7 operating system (for example, Windows 7 Professional, 64-bit).
Installation
eProcedure
This release has the following application notes.
The FactoryTalk Batch version 15.00 release has the following application notes.
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk Batch versions 18.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
Mitigation for Microsoft DCOM Hardening patch
In response to Microsoft Distributed Component Object Model (DCOM) Hardening patch (MS KB5004442), the minimum DCOM authentication level used by Rockwell Automation products was raised to Packet Integrity.
Microsoft releases the DCOM Hardening patch in response to CVE-2021-26414. This patch elevates the minimum DCOM authentication level that is required to establish a DCOM connection. DCOM is used by many Rockwell Automation products and may be affected by the change that is made by the Microsoft patch. For additional information about the affected Rockwell Automation products, see the Knowledgebase Document ID: PN1581 - Product Notification 2022-01-001 - Rockwell Automation products unable to establish proper DCOM connection after installing Microsoft DCOM Hardening patch (MS KB5004442).
Upgrade
FactoryTalk Batch
Immediately start the installation of FactoryTalk Batch 15.00 after the Remote Registry service is started.
FactoryTalk Linx version 6.20 installs two instances of the FactoryTalk Linx data server. Only the first instance named FactoryTalk Linx Instance01 Server supports the necessary communication interfaces to connect to PhaseManager and SequenceManager on a Logix controller.
When configuring a Logix5000 CIP data server for communications with PhaseManager or SequenceManager, be sure to select the data server that is using the first instance of the FactoryTalk Linx service.
Use these steps to identify which instance of FactoryTalk Linx is assigned to a data server:
You must log in to FactoryTalk before using the FactoryTalk Batch Service Manager.
This is because performing a deployment to a runtime server is treated as an elevated privileges operation when launched from the FactoryTalk Batch Service Manager. To run with elevated privilege the FactoryTalk Batch Service Manager must:
Command-line parameters
Use command-line parameters to perform an unattended or silent installation of the software.
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
Common Rockwell Automation parameters
These parameters are applicable for all Rockwell Automation software that are available in the installation package.
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user
interface.
This parameter is recommended if you are deploying the
software installation using an IT tool or script, and don’t
expect to see any error or restart messages. When using this
parameter, your IT tool or script should check the error codes,
and respond as needed. For example, if the installation
returns error code 1641, then the IT tool or script should
restart the computer and relaunch the installation after restart.
This parameter is required if /QS is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and
shows progress through the UI, it does not accept any input
but still shows error or restart messages.
When using this parameter, you will not have to check the
error codes, and the installation will stop and display a prompt
if there are error or restart messages. For example, if an
immediate restart is required to complete the install, a restart
message will be displayed for you to confirm the restart.
Installation resumes automatically from the point of
interruption after restart.
This parameter is required if /Q is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is
complete. Used when a restart is required to complete the
installation.
This parameter is optional. If this parameter is not used silent
install (/Q) will return either error code 1641 or 3010 if a
restart is required, and unattended install (/QS) will result in a
confirmation prompt that must be agreed to before the
installation is completed.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during install
process.
The value must be the one of the following:
This parameter is optional. If this parameter is not
used, the default language is the current user or
operating system user interface language.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/Product="value"
|
Specifies which sub-products will be installed.
Only required if sub-products are included with the install
package.
If the software does not include sub-products this parameter is
not available.
|
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed.
The value must be the one of the following:
This parameter is optional. If this parameter is not
used, the default language is the same as the setup
language.
If the software does not support multiple languages
this parameter is not available.
|
| /InstallLocation="value"
Or
/InstallDrive="value"
|
Specifies the install location or install drive respectively.
This parameter is optional. If this parameter is not used, the
default install location is "C:\Program Files (x86)\Rockwell
Software".
Some software restricts the installer to only change the drive
the software is installed on. Use /? to determine which
parameter is supported.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed.
This is used to activate the software during installation.
This parameter is optional. If it is not specified the software
must be activated manually after installation if activation is
required.
Some software does not require activation. If activation is not
required this parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during
installation.
This parameter is optional. If it is not specified the software
must be activated manually after installation if activation is
required.
Some software does not require activation. If activation is not
required this parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate which
corresponds to the product version associated with the
SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will
use the most recent product version available.
Some software does not require activation. If activation is not
required this parameter is not available.
|
FactoryTalk Batch-specific command line parameters
The command-line install of FactoryTalk Batch performs a full install of FactoryTalk Batch. To install FactoryTalk Batch, FactoryTalk <EA>, FactoryTalk Batch Material Manager, or FactoryTalk Batch View HMI Controls separately use the installation wizard instead of the command-line.
These options are specific to installing FactoryTalk Batch software:
|
Parameter
|
Description
|
|
BatchServerName
|
Required for Batch. Machine name where the Batch
server is installed.
|
|
eProcedureServerName
|
Required for eProcedure. Machine name where the
eProcedure Server is installed.
|
|
MaterialManagerServerName
|
Required for Material Manager. Machine name where
Material Manager Server is installed.
|
|
FirstInSystem
|
Optional. Set to "No" to add a Batch or Material
Manager install to an existing system.
If omitted, the default is "Yes"
|
|
DomainWorkgroup
|
Optional. Set to "WORKGROUP" to indicate for a
Batch, eProcedure, or Material Manager install that the
machine is not connected to a domain.
If omitted, the default is "DOMAIN"
|
|
BatchDomain
|
Required for Batch, eProcedure, and Material
Manager.
Specifies the domain name of the machine where the
product is being installed. Value should be set to the
local machine name when installing in a workgroup.
|
|
BatchUserName
|
Required for Batch, eProcedure, and Material
Manager.
|
|
BatchPassword
|
Required for Batch, eProcedure, and Material
Manager.
|
|
RecipesInSQL
|
Optional. Set to "Yes" to indicate for a Batch or
Material Manager install that recipes should be stored
in SQL.
If omitted, the default is "No"
|
|
FTDirectory
|
Optional. Set to "Local" to indicate for a Batch or
eProcedure install that FTSP should use the Local
directory.
If omitted, the default is "Network"
|
|
MaterialJournaling
|
Optional. Set to "Yes" for a Material Manager install to
record activity to the MaterialBasedRecipe_MAJ
database.
If omitted, the default is "No"
|
|
ArchiverSqlAuth
|
Optional. Set to "Yes" to indicate for an Event Archiver
Database install to use SQL authentication with the
user and password values passed in /ArchiverSqlUser
and/ArchiverSqlPass.
If omitted, the default is "No"
|
|
ArchiverSqlUser
|
Optional for Event Archiver Database Feature.
|
|
ArchiverSqlPass
|
Optional for Event Archiver Database Feature.
|
|
ArchiverDbAction
|
Required for Event Archiver Database Feature.
"Migrate" updates pre-Batch 12 DB schema to current
format
"Upgrade" updates only stored procedures and reports
"Create" generates a new DB, overwriting an existing
one
|
|
ArchiverServerName
|
Required for Event Archiver Database Feature.
|
|
ArchiverInstanceName
|
Optional for Event Archiver Database Feature.
|
|
ArchiverDataSourceName
|
Required for Event Archiver Database Feature.
|
|
ArchiverWithReports
|
Optional. For an Event Archiver Database install, set
to:
"Yes" to use a BatchHistoryEx database with reporting
"No" to use a BatchHistory database without reporting
If omitted, the default is "Yes"
|
|
HTTPS_PORT_USER
|
Optional for BatchView Server.
If omitted, the default value is 443.
To define a custom port, specify the value of the
desired port (port value must follow the validation rules
for port number assignment).
|
|
CopyCustomerContentSelected
|
Optional for BatchView Server.
If omitted, the default is "No".
|
Example
The following example shows how to use the installation commands.
Setup.exe /Q /IAcceptAllLicenseTerms /DomainWorkgroup=Domain /BatchDomain=MyDomain /BatchUserName=User1 /BatchPassword=s3cretp@ssw0rd! /Product=FTBatch /BatchServerName=BatchServer1 /HTTPS_PORT_USER=8443 /CopyCustomerContentSelected=Yes
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed
successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was
invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was cancelled
by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during
installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this
product is corrupt. Contact your
support personnel.
|
|
ERROR_SUCCESS_REBOOT_INITIATED
|
1641
|
The installer has initiated a
restart. After restart installation
will continue.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to
complete the installation. After
restart the product is
successfully installed.
|
|
ERROR_SUCCESS_RELAUNCH_REQUIRED
|
3011
|
Restart of setup needed before
installation can continue.
|
FactoryTalk Batch Material Manager
FactoryTalk Batch Enterprise Integration Server
The FactoryTalk Batch EI Server.msi file is in the EIServer folder of your FactoryTalk Batch 15.00 installation media.