This release has the following requirements.
|
Type
|
Description
|
CPU
|
RAM
|
|
Operator Workstation
|
FactoryTalk AssetCentre
Client
|
Intel® Core™ i5 Standard Power
processor
|
4 GB
|
|
Engineering Workstation
|
FactoryTalk AssetCentre
Client
FactoryTalk AssetCentre Agent
|
Intel Core i5 Standard Power processor
|
8 GB
|
|
System Agent
|
FactoryTalk AssetCentre
Agent
|
Intel Core i5 Standard Power processor
|
8 GB
|
| Application Server | FactoryTalk AssetCentre
Server
|
Small systems:
Intel Core i5 Standard Power processor
|
8 GB
|
| Medium to large systems:
Intel® Xeon® quad-core family processor
|
8 GB
|
FactoryTalk AssetCentre version 11.00.00 is compatible with the following Rockwell Automation products. For the latest compatibility information, refer to the Rockwell Automation Product Compatibility and Download Center.
FactoryTalk AssetCentre Server
FactoryTalk AssetCentre Client
FactoryTalk AssetCentre Agent
|
Asset
|
Compatible Software
|
Version
|
|
PLC-5
|
RSLogix 5
|
8.00 or later
|
|
SLC 500, MicroLogix
|
RSLogix 500
|
8.40 or later
|
|
ControlLogix, CompactLogix
|
Studio 5000 Logix Designer
|
21.00 or later
|
|
RSLogix 5000
|
16.00 or later
| |
|
RSLogix 5000 Compare Utility or Logix Designer Compare
Tool
|
8.12
| |
| PanelView Plus, MobileView
|
FactoryTalk View ME Transfer Utility
|
12.00
|
|
FactoryTalk Linx (formerly known as RSLinx Enterprise)
|
6.21
| |
|
FactoryTalk View Site Edition
|
FactoryTalk View Studio Enterprise
|
12.00
|
|
Rockwell Automation drives
|
DriveExecutive Lite
|
5.02 or later
|
|
PowerFlex Drive
|
UDC
|
4.07
|
FactoryTalk AssetCentre has been tested on the following operating systems:
|
Important:
|
Turn off the Windows updates on production computers.
Installing Microsoft Service Pack release or Windows
operating system updates may affect the operation of
Rockwell Automation software installed on the
computer. To avoid this problem, see Knowledgebase
Document ID: QA2151 - Microsoft Patch Qualifications
.
|
FactoryTalk AssetCentre Server
This version of FactoryTalk AssetCentre Server was tested on these 64-bit operating systems:
FactoryTalk AssetCentre Client and Agent
This version of FactoryTalk AssetCentre Client and Agent were tested on these 64-bit operating systems:
FactoryTalk AssetCentre Web Client
FactoryTalk AssetCentre Server
The following are minimum software requirements for FactoryTalk AssetCentre Server.
SQL Server databases
FactoryTalk AssetCentre has been tested on the following SQL Servers:
FactoryTalk AssetCentre Client
The following are minimum software requirements for FactoryTalk AssetCentre Client.
FactoryTalk AssetCentre Agent
The following are minimum software requirements for FactoryTalk AssetCentre Agent.
FactoryTalk AssetCentre Web Client
The following are minimum software requirements for FactoryTalk AssetCentre Web Client.
Windows 10 v1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software.
To help meet secure system design requirements review these publications:
This release includes the following system features.
FactoryTalk AssetCentre version 11.00.00 has the following new and enhanced features:
This release corrects the following anomalies.
In this release, only SYSTEM, Administrators, and IIS_USERS have the permissions to access it.
In this release, the asterisk passwords are displayed with 15 characters by default and password interception is prevented.
In this release, an Asset Extended Property search can be run successfully through FactoryTalk AssetCentre Web Client.
In this release, the messages from AutoIt script can be logged to FactoryTalk AssetCentre database successfully.
In this release, the reported number of differences match.
In this release, performing file check-in succeeds.
There is currently no workaround for this problem.
To avoid this problem, move the newly added Logix5000 Controller device out of the container and add it back again.
There is currently no work around for this anomaly.
To avoid this problem, use a different browser such as Chrome or Internet Explorer.
To resolve this problem, manually select the Tools check box or its sub items'.
This release has the following known anomalies.
When running a Disaster Recovery schedule for Allen-Bradley Logix5000 Controller, the compare PDF report cannot be generated to FactoryTalk AssetCentre Desktop Client if no differences are detected. First identified in FactoryTalk AssetCentre version 11.00.00. [Jira 3173223]
Corrected in FactoryTalk AssetCentre version 13.00.00.
To avoid this problem, do the following:
When performing Archive version to version compare of a DNO file associated with a PowerFlex 755, an error message appears. First identified in FactoryTalk AssetCentre version 9.00.00. [Jira 1285794]
To resolve this problem, do the following:
Using the FactoryTalk AssetCentre Client, check out and open the DNO file.
Go online with the target PowerFlex 755 device.
Close the DNO file, and check in the DNO file.
When updating an earlier version FactoryTalk AssetCentre Server with SSL enabled to version 11.00.00, failure to restart the computer using either the Restart Now or Restart Later in the installation user interface, prevents the FactoryTalk AssetCentre Client from launching. First identified in FactoryTalk AssetCentre version 11.00.00. [Jira 1046534]
To resolve this problem, you can do the following steps:
Open the Server Settings utility.
In the Configure Server Settings Utility window, clear the Use the secure communication channel check box, and then select the Apply button.
Select OK.
If your Microsoft SQL server uses Windows Authentication as the server’s authentication mode and subsequently install FactoryTalk AssetCentre server using a Managed Service Account to access the SQL Server, then the Archive Management of Change capability cannot function properly. First identified in FactoryTalk AssetCentre version 11.00.00. [Jira 1224432]
Corrected in FactoryTalk AssetCentre version 13.00.00.
When using the silent or unattended setup to upgrade FactoryTalk AssetCentre version 8.00.00 or later, if any of the additional software components’ version (for example, Logix Designer Compare Tool) on the computer is equal to or higher than the version you will upgrade to, the upgrade will fail. First identified in FactoryTalk AssetCentre version 11.00.00. [Jira 1444198]
To avoid this problem, you can do one of the following:
Upgrade FactoryTalk AssetCentre version 8.00.00 or later using the Setup wizard.
Enter /IgnoreWarning when upgrading FactoryTalk AssetCentre version 8.00.00 or
later using the silent or unattended setup.
Example:
C:\Users\Administrator\Desktop\11.00.00-FTAssetCentre-DVDD\Setup.exe
/Q /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=ENU
/Product="AssetCentre Server" /SerialNumber=2740J00396
/ProductKey=RYN62-LWBQ6 /Version=11.00.00 /InstallDrive=D:
/SqlServer="(local)" /DirectoryServer=FTDIRECTORY/ IgnoreWarningWhen a large binder, more than 1GB in total size, is being promoted in the Archive, running an Archive Check In and Check Out Status search schedule will fail. Once the promotion is completed the schedule can be executed successfully. First identified in FactoryTalk AssetCentre version 9.00.00. [Jira 1309942]
There is currently no workaround for this anomaly.
If running the FactoryTalk AssetCentre Client on Windows 10 version 1903, when opening a PowerFlex drive Backup & Compare comparison report (CSV file) in the Event Log, an error message appears. Please note Windows 10 version 1903 reached Microsoft End of Service on 8.Dec.2020. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 1285815]
To avoid this problem, configure the default application to open the CSV file via the operating system Settings > Apps > Default apps. Notepad.exe is recommended
These anomalies are from previous releases but are still known in this release.
When performing an Asset Inventory WMI to scan the software, with the Changes only option selected, the scan can not detect installation changes for applications that do not maintain installation information (for example, you uninstall the software today and then install it on another day). First identified in FactoryTalk AssetCentre version 7.00.00.[358777]
There is currently no work around for this anomaly.
Cannot modify or uninstall the software FactoryTalk AssetCentre Client or FactoryTalk AssetCentre Agent application by double-clicking Setup.exe in the installation package and selecting AssetCentre Custom Installation. First identified in FactoryTalk AssetCentre version 8.00.00. [46429]
To modify or uninstall the software components, go to the Programs and Features list of the Control Panel.
When configuring a PanelView asset's Addressing Info, if a device other than a PanelView is selected, several extraneous error messages may display. First identified in FactoryTalk AssetCentre version 9.00.00. [Jira 242271]
To avoid this problem, choose the proper device type when configuring the Addressing Info of a PanelView asset.
A PanelView Plus or MobileView Disaster Recovery schedule will fail with a communication error message, if the Address Info is not set for the device using FactoryTalk Linx Browser located on the FactoryTalk AssetCentre agent computer. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 395652]
To avoid this problem, after configuring the Addressing Info property of a PanelView Plus asset or a MobileView asset, the user must browse for the device in FactoryTalk Linx Browser from the FactoryTalk AssetCentre agent computer when the agent computer is not collocated with the FactoryTalk AssetCentre client.
When the Report Incremental Differences option is enabled for a Logix 5000 controller asset within a Disaster Recovery schedule, the task will fail if the controller firmware version does not match the firmware version of the ACD file associated with the Incremental Checkpoint label. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 806906]
To avoid this problem, you can do the following steps:
After upgrading or downgrading a Logix 5000 controller’s firmware, open the FactoryTalk AssetCentre archive to check in the ACD file that matches Logix 5000 controller firmware version.
Select Add Label to move the Incremental Checkpoint, and then select the Allow reuse of existing labels check box.
In the Label box, enter the label name exactly as Incremental Checkpoint.
The Disaster and Recovery schedule will now run successfully.
FactoryTalk AssetCentre has limited support for 4K displays, when display scaling is greater than 100%. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 355367]
To avoid this problem, set the display scaling to 100% and restart the computer.
When uninstalling FactoryTalk AssetCentre Agent, FactoryTalk AssetCentre Agent will remain in the Control Panel, Add/Remove until all supporting applications (for example, RSLogix 500) are also removed. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 488955]
To resolve this problem, uninstall all software installed together with FactoryTalk AssetCentre Agent 10.00.00 installation and then it will be removed.
When repairing a FactoryTalk AssetCentre Agent installation on a computer upon which Logix Designer Compare Tool is not installed, FactoryTalk AssetCentre will generate a nuisance warning message indicating that Logix Designer Compare Tool requires that Microsoft .NET Framework 3.5 to be installed. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 566002]
This issue currently has no workaround. The behavior does not adversely impact the FactoryTalk AssetCentre Agent installation repair process.
This release has the following functional changes from the previous release.
FactoryTalk AssetCentre version 11.00.00 has the following changes in functionality since the last release:
This release has the following application notes.
The following are the application notes for FactoryTalk AssetCentre version 11.00.00.
Impact of Microsoft deprecating VBScript
Microsoft announced the phased deprecation of VBScript in 2024. VBScript is now an optional feature beginning in Windows 11 24H2 and Windows Server 2025. Many FactoryTalk software products released before September 1, 2026, use VBScript during installation.
FactoryTalk AssetCentre versions 16.00.00 and earlier require VBScript for installation. Installation will fail if VBScript is not enabled.
To mitigate the problem, enable VBScript manually. For more information, see the Knowledgebase Document ID: IN41397 - Impact of Microsoft deprecating VBScript. FactoryTalk software products released after September 1, 2026, no longer rely on VBScript.
Disaster Recovery schedule tasks fail with Device Not Found recorded in the FactoryTalk AssetCentre Event log
When a Logix controller asset’s Addressing property was configured using RSLinx Classic, Disaster Recovery schedule tasks may start failing with Device Not Found recorded in the FactoryTalk AssetCentre Event log. Rebooting the FactoryTalk AssetCentre Agent(s) will temporarily address the error; however, the task failures will eventually return.
This behavior is addressed in a RSLinx Classic patch. See technote BF27867 for additional details.
Secure communication with TLS and SSL protocols
Windows implements SSL and TLS through Schannel Security Support Provider (SSP). The Schannel SSP implementation of the TLS and SSL protocols use algorithms from a cipher suite to create keys and encryption information. Starting from FactoryTalk AssetCentre version 9.00, the operating system's capability is used to automatically filter out the unsecure ciphers.
For all cipher suites listed for different operating systems, refer to Cipher Suites in TLS/SSL (Schannel SSP).
If you have a preference on the cipher suites and need to customize the priorities in group policy, refer to Prioritizing Schannel Cipher Suites.
To enable or disable specific ciphers in the registry, refer to How to restrict the use of certain cryptographic algorithms and protocols in Schannel.dll.
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
|
IMPORTANT |
When installing or upgrading FactoryTalk AssetCentre to version 11.00.00 or later with SQL Server Authentication, you must use silent or unattended setup to install it. |
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are
case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter |
Description |
|
/? |
Displays the usage options for installation parameters. |
|
/Q |
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart. This parameter is required if /QS or /Record is not specified. |
|
/QS |
Unattended Install, install runs in a quiet simple mode and shows progress
through the UI, it does not accept any input but still shows error or restart
messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart. This parameter is required if /Q or /Record is not specified. |
|
/IAcceptAllLicenseTerms |
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters. |
|
/AutoRestart |
Automatically restarts the computer after the installation is complete. Used
when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed. |
|
/SetupLanguage="value" |
Specifies which language will be displayed during install process.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language. |
|
/Record |
Records the installation options chosen to a recording file.
This parameter is optional. |
|
/Playback |
Plays back a recording file to specify the installation options.
This parameter is optional. |
|
/IgnoreWarning |
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs. |
|
/Product="value" |
Specifies which sub-products will be installed.
The product name must be one of followings:
|
|
/Uninstall |
Uninstalls the product.
This parameter is optional. |
|
/ProductLanguage="value" |
Specifies the language version of the software being installed.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default language is the same as the setup language. If the software does not support multiple languages this parameter is not available. |
|
/SerialNumber="value" |
Specifies the serial number of the software being installed. This is used to
activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required this parameter is not available. |
|
/ProductKey="value" |
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required. Some software does not require activation. If activation is not required this parameter is not available. |
|
/Version="value" |
Specifies the version of the software to activate which corresponds to the
product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available. Some software does not require activation. If activation is not required this parameter is not available. |
|
/InstallDrive="value" |
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software". Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported. |
|
/ftsp-value="value" |
Specifies the FactoryTalk security policy value.
This parameter is optional. Use the enable or disable value to change the state of RequireComputerAccounts during installation. |
|
/noHTTPS |
Specifies that the setup turns off HTTPS and continues.
This parameter is optional. |
|
/SqlServer="value" |
Specifies FactoryTalk AssetCentre database server (Microsoft SQL Server)
location.
This parameter is required when installing the FactoryTalk AssetCentre server software. |
|
/MSA="value" |
Specifies the Group Managed Service Account (gMSA) or Managed Service
Account (MSA) that will be used by FactoryTalk AssetCentre Server to access
the Microsoft SQL Server database when using Windows Authentication.
|
|
/sql |
Uses SQL Authentication between the FactoryTalk AssetCentre and Microsoft
SQL Servers. The use of SQL Authentication is discouraged due to security
concerns.
This parameter is optional. |
|
/sa="value" |
Uses SQL Authentication for SQL Server Logins. If you use SQL Server Authentication to perform silent or unattended installation, the parameters /SqlAdmin, and /SqlAdminPwd are required. |
|
/SqlAdmin="value" |
Specifies the Microsoft SQL Server administrator account name. |
|
/SqlAdminPwd="value" |
Specifies the Microsoft SQL Server administrator account password. |
|
/DirectoryServer="value" |
Specifies the FactoryTalk network directory if you are using a distributed
system.
This parameter is optional. If it is not specified, the software will use its current computer as the FactoryTalk Directory server. The value must be the host name of the FactoryTalk Directory server. |
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code |
Value |
Description |
|
ERROR_SUCCESS |
0 |
The installation completed successfully. |
|
ERROR_INVALID_PARAMETER |
87 |
One of the parameters was invalid. |
|
ERROR_INSTALL_USEREXIT |
1602 |
The installation was cancelled by the user. |
|
ERROR_INSTALL_FAILURE |
1603 |
A fatal error occurred during installation or the software component to be installed already exists on the computer. |
|
ERROR_BAD_CONFIGURATION |
1610 |
The configuration data for this product is corrupt. Contact your support personnel. |
|
ERROR_REBOOT_CONTINUE |
1641 |
A reboot is required to continue to installation. |
|
ERROR_SUCCESS_REBOOT_REQUIRED |
3010 |
A restart is required to complete the installation. After restart the product is successfully installed. |
|
ERROR_REBOOT_PENDING |
3012 |
A restart is pending and is required before the installation can continue. |
|
ERROR_SUCCESS_NOT_APPLICABLE |
3013 |
The installation cannot proceed because the products are already installed. |
FactoryTalk AssetCentre Client
All FactoryTalk AssetCentre clients must have identical RSLinx Classic communication driver configurations.
When performing backups or backup and compares on Generic FTP devices containing subdirectories, the FTP device must support both the "DIR" and "ls" commands.
FactoryTalk AssetCentre Agent
The agent installation now provides the ability to create and set security credentials needed for secured Logix editors.
Note: This configuration step can be skipped during installation. If skipped, you may configure it manually later.
For details, see the Installation Guide, chapter "Install FactoryTalk AssetCentre agents", section "Configure for security-enabled RSLogix family software".
If you enable the security option for RSLogix 5, which is used by the FactoryTalk AssetCentre Recovery agent, you must install a service patch.
For details, see Knowledgebase Document ID: BF20056 - RSLogix 5 7.x Patch for comms path getting erased, which breaks FactoryTalk AssetCentre.
If you enable the security option for RSLogix 500 using a version prior to 8.10, which is used by the FactoryTalk AssetCentre Disaster Recovery agent, you must install a service patch.
For details, see Knowledgebase Document ID: BF20057 - RSLogix 500 7.20/8.00 Patch for comms path getting erased, which breaks FactoryTalk AssetCentre.
FactoryTalk AssetCentre agents belonging to the same agent group must meet the following requirements:
Have identical RSLinx Classic and FactoryTalk Linx (formerly known as RSLinx Enterprise) communication driver configurations.
Be able to communicate with all assets configured for use with that agent group.
For example, if an agent group supports both SLC 500 and Logix 5000 controllers, then each agent belonging to that agent group must have both RSLogix 500 and the appropriate version of RSLogix 5000 or Logix Designer installed.
The amount of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system
The following is the amount of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system at the same time. More clients, agents, or agent groups running will impact the system performance.
Client: 150
Agent: 50
Agent groups: 50
Agent computers in each agent group: 5
Considerations for generating large PDF reports
Generating very large PDF reports may result in generation failures, incomplete report content, or reports that cannot be opened. Common factors that can affect large PDF report generation include:
System resources and environment
Available memory and system conditions can affect the successful generation of large reports.
Content complexity
Reports that contain significant differences between versions or a large number of tags require additional processing resources.
To help avoid problems when generating large PDF reports:
Upgrade to FactoryTalk AssetCentre version 16.00.00 or later.
For large Logix 5000 compare reports, consider clearing the All Tag Values option in the Compare Options dialog.
If an asset inventory scan fails because of a large number of changes, run a backup task to establish a new baseline.
Use FactoryTalk Linx to browse Logix 5000 controllers of firmware revision 38.00 or later
Beginning with the version 38.00 firmware release, Logix 5000 controllers running firmware revision 38.00 or later can only be browsed using FactoryTalk Linx. RSLinx Classic cannot be used to browse controllers with these newer revisions in Studio 5000 Logix Designer nor FactoryTalk AssetCentre. The following table illustrates communication software support:
| Design Software | Version | RSLinx Classic | FactoryTalk Linx |
| RSLogix 5000 | 18-20 | Supported | Not supported |
| Studio 5000 Logix Designer | 21-30 | Supported | Not supported |
| Studio 5000 Logix Designer | 31-37 | Supported | Supported |
| Studio 5000 Logix Designer | 38 or later | Not supported | Supported |
After upgrading an existing FactoryTalk AssetCentre system from an earlier version to version 16.00 and later, scheduled backup, backup and compare, and source code validation tasks will fail when:
A Logix 5000 controller originally added to the asset tree using RSLinx Classic is later updated to firmware revision 38.00 or later.
A Logix 5000 controller of firmware revision 38.00 or later is added to the asset tree via the import tool, and that controller was browsed using RSLinx Classic.
To resolve this problem, follow the steps to configure FactoryTalk Linx to browse Logix 5000 controllers:
In FactoryTalk AssetCentre Client, select Design.
In the asset tree, right-click the Allen-Bradley Logix 5000 Controller asset, and then select Properties.
In the Addressing Info box, select the browse button.
In the Network Browser list, select FactoryTalk Linx.
Find and select your device from the device list.
Select OK.
Synchronizing life-cycle information with the Rockwell Automation life cycle website
To synchronize life-cycle information, the FactoryTalk AssetCentre server and client communicate directly with the Rockwell Automation life cycle website. To enable this function, ensure that the external address https://api.rockwellautomation.com is accessible by the FactoryTalk AssetCentre server and client.
Synchronize life-cycle information in the FactoryTalk AssetCentre server and client with the data on the Rockwell Automation life cycle website. For more information about securely accessing the Rockwell Automation lifecycle website from your OT zone-based FactoryTalk AssetCentre Server, please refer to this document Cloud Connectivity to a Converged Plantwide Ethernet Architecture https://literature.rockwellautomation.com/idc/groups/literature/documents/td/enet-td017_-en-p.pdf in Rockwell Automation Literature Library.
FactoryTalk Directory asset compare
Differences are always found between two FactoryTalk Directory backup files after a Backup and Compare schedule, even though no changes are made to the FactoryTalk Directory. This is because the BAK files include timestamp information, which is detected as a difference during the binary compare of the backup files.
Event Log Attachment Extractor
The Event Log Attachment Extractor utility cannot properly extract event log attachments in the following two cases:
For Backup and Compare schedules that compare both backup data and configuration data, the event log attachment of the configuration data cannot be extracted by the Event Log Attachment Extractor utility.
When running a Backup and Compare schedule on the Generic FTP device with a custom compare engine, only the last compare report attachment can be extracted.
About Microsoft SQL Server 2012 Express Edition with Advanced Services (x64)
FactoryTalk AssetCentre v6.10 or higher supports Microsoft SQL Server Express. Some FactoryTalk AssetCentre catalog numbers contain Microsoft SQL Server 2012 Express Edition with Advanced Services (x64), which is a free and unlicensed edition of Microsoft SQL Server. This is intended for storing the FactoryTalk AssetCentre database. SQL Server 2012 Express Edition with Advanced Services (x64) has the following limitations:
10GB database size limit
Tip: FactoryTalk AssetCentre 6.1 or higher has capabilities for managing database size.
1GB memory limit for SQL Server database engine
4GB memory limit for reporting services
Maximum compute capacity limited to the lesser of 1 socket or 4 cores
No SQL agent services
No integration services
No business intelligence tools
No SQL profiler
Limited reporting services capabilities
FactoryTalk AssetCentre also supports other versions of SQL Server as described in this Release Notes.
You may upgrade to Microsoft SQL Server 2012 Standard Edition, which is a licensed edition, by purchasing from the following list of Rockwell Automation catalog numbers:
9319-DBSVRCALENE - FactoryTalk Database License Server Client Access License (CAL)
9319-DBADCALENE - FactoryTalk Database License 1 CAL
9319-DBCOR4ENE - FactoryTalk Database License 4 Core
9319-DBADCOR2ENE - FactoryTalk Database License 2 Core
The licenses in the previous catalog numbers can be used only with Rockwell Automation products, including FactoryTalk AssetCentre. More information on SQL Server licensing with Rockwell Automation products can be found in Knowledgebase Document ID: IN31446 - FAQ: Using Microsoft SQL Server with Rockwell Automation FactoryTalk Products.
Alternatively, you may purchase licenses for a supported version and edition of SQL Server from Microsoft. A complete comparison of SQL Server 2012 Editions can be found here: https://technet.microsoft.com/en-us/library/cc645993(v=sql.110).
Install product updates
For the latest Product Updates and Patch information, refer to Knowledgebase Document ID: QA15600 - FactoryTalk AssetCentre Patch Roll-up for 3.0 and later.
You can subscribe to be notified when new product updates, or patches are released via the
Knowledgebase by clicking below the Knowledgebase answer title.
To directly download software or firmware updates, and patch roll-ups, go to Product Compatibility and Download Center http://www.rockwellautomation.com/compatibility/#/scenarios.
Security requirements
For information on the security considerations when using Rockwell Automation products, including
File extensions created by Rockwell Automation software, firewall rules, and service dependencies, see Knowledgebase Document ID: PN826 - Security considerations when using Rockwell Automation Software Products.
TCP/UDP ports used by Rockwell Automation products, see Knowledgebase Document ID: BF7490 - TCP/UDP Ports Used by Rockwell Automation Products.