Release Notes

Kinetix 5500 Servo Drives: (2198-Hxxx)
Version 7.013 (released 1/2021)

Catalog Number Kinetix 5500 (2198-Hxxx) (series A)

These release notes describe version information for Kinetix 5500 (2198-Hxxx), version 7.013 (released 1/2021).

Features

This release includes the following system features.

Kinetix 5500 Servo Drives Firmware Revision 7.013 Enhancements

Catalog Numbers 2198-H003-ERS, 2198-H008-ERS, 2198-H015-ERS, 2198-H025-ERS, 2198-H040-ERS, 2198-H070-ERS, 2198-H003-ERS2, 2198-H008-ERS2, 2198-H015-ERS2, 2198-H025-ERS2, 2198-H040-ERS2, 2198-H070-ERS2

 


  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Kinetix 5500 Servo Drives Firmware Revision 7.013 Corrected Anomalies

Catalog Numbers 2198-H003-ERS, 2198-H008-ERS, 2198-H015-ERS, 2198-H025-ERS, 2198-H040-ERS, 2198-H070-ERS, 2198-H003-ERS2, 2198-H008-ERS2, 2198-H015-ERS2, 2198-H025-ERS2, 2198-H040-ERS2, 2198-H070-ERS2

 


  

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

Kinetix 5500 Servo Drives Known Anomalies

Catalog Numbers 2198-H003-ERS, 2198-H008-ERS, 2198-H015-ERS, 2198-H025-ERS,
2198-H040-ERS, 2198-H070-ERS, 2198-H003-ERS2, 2198-H008-ERS2, 2198-H015-ERS2,
2198-H025-ERS2, 2198-H040-ERS2, 2198-H070-ERS2


Drive Instability With Wall Clock Time Update Requests and Grandmaster Clock Changes


Requests to update the controller wall clock time in applications that use Integrated Motion over an EtherNet/IP network can cause drive instability. 

The following are examples of wall clock time update requests:


In addition, drive instability can occur when the Grandmaster clock changes from one module to another. The following are examples of drive behavior when the anomaly occurs:


Configure the controller Grandmaster clock priority to prevent the Grandmaster clock from switching to a different module and do not update the wall clock time while there is an active motion connection. Inhibit all axes before changing the wall clock time and the Grandmaster clock priorities. Alternatively, reset the motion connection by inhibiting and uninhibiting the Ethernet module that is handling the motion connection between the controller and axes.


  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.