This release includes the following system features.
Alarm History Export
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Export the alarm history to an SD card or USB drive for external analysis or storage of historical alarm transitions. The alarm history export is in the form of a zipped csv file.
Alarm History Viewer
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
The PanelView 5000 now stores up to 40,000 alarm transitions and maintains them through downloads and power cycles. View this alarm history on the pre-defined alarm history screen or on your own screen using the Alarm History Viewer graphic element. The Alarm History Viewer supports sortable columns, filtering by alarm transition type and by time, and a details pane for more information about a selected alarm transition.
Configurable Screen Update Rates
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
A new UpdateRate property on screens and popups lets you configure the update rate to 100, 250, or 500 msec for better visualization of higher speed data or for smoother movement animations.
2500 States in a State Table
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
State tables now support up to 2500 states for applications such as displaying error code strings.
Logix Extended Tag Properties in Alarm Messages
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Alarm messages now support the inclusion of Logix extended tag properties such as descriptions or min/max values when used with a Logix firmware version 33 or later controller.
Larger Keypad and Keyboard Option
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Select between the normal size or a larger size keypad and keyboard as part of Project Properties. The larger size is useful for easier touch operation, particularly for gloved operators.
Binding to the Image Element’s ImageName Property
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
You can now bind the ImageName property of an image element to tags or expressions. It is also possible to use the ImageName property in a state table. This is useful for changing the appearance of images based on machine or process conditions and is more efficient than using stacked images with visibility.
Arc Drawing Tool
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Draw curved lines by placing a starting point, end point, and curve adjustment point.
Clear Data Log Command
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Clear the contents of the data logs with this new command. This is useful for batching operations or machine runs where you want to clear the data logs of older values before starting a new batch or machine run.
Color Adjustment HMI Device Tags
System Feature First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
Three new tags allow you to adjust the red, green, and blue color levels on the HMI Device by referencing these tags in numeric inputs you add to a screen. The BlueAdjustment, GreenAdjustment, and RedAdjustment tags are located in the "Display" HMI Device Tags grouping.
Firmware Requirements
System Requirement First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5310, PanelView 5510
This release has the following known anomalies.
Controller Tag Reference
Corrected Anomaly with Firmware Revision 9.001
Known Anomaly First Identified as of Firmware Revision 3.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
Projects referencing a controller with more than the recommended limit of 50,000 tags may experience a restart of the HMI device when performing an online synchronization with the controller. [DFCTS00361416]
Reference a controller with no more than 50,000 tags.
Issues When Using ControlFLASH During Screen Change
Known Anomaly First Identified as of Firmware Revision 3.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
The use of ControlFLASH™ to update the firmware on the HMI device while the HMI device is changing screens can cause the following anomalies:
[DFCTS00356235]
If the firmware update fails, use the ControlFLASH again to complete the firmware update. If the HMI device faults, restart the HMI device and use the ControlFLASH again to complete the firmware update.
To avoid this anomaly, update the firmware on the HMI device when the HMI device is not changing screens.
Error When Number of Alarms is Exceeded
Known Anomaly First Identified as of Firmware Revision 3.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
An HMI device screen error occurs when the number of alarms exceeds the recommended value. [DFCTS00361167]
To resolve this issue, do not exceed 1,000 alarms.
Data Logging
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
If you eject and immediately reinsert the SD card into the HMI device, data logging might not restart. Data logging does not recognize that the SD card is present. Eject the SD card, wait several seconds, and reinsert the SD card to restart data logging. [46846]
Aliased Logix Designer Tags
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
The HMI device does not display passed-through extended properties of aliased Logix Designer tags. [DFCTS00350204]
Error When Binding to Module-defined Tags
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
A binding to a module-defined tag shows an invalid syntax error on the HMI device when adding the module online. [DFCTS00360870]
Enumerated Properties
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
Enumerated properties that are bound to a string tag do not work if the content of the string tag, including case, does not match the enumeration on the user interface. For example, the rounding property value Nearest does not equal nearest. [DFCTS00351889]
To resolve this issue, make sure that the letter casing for bound properties matches the casing for properties on the user interface.
State Enter Event Does Not Trigger
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
When two or more shortcuts navigate to the same screen and that screen has a State Table and a State Enter event, navigation from a shortcut triggers the State Enter event. When immediately navigating from the open shortcut to another shortcut that also represents the same screen, the State Enter event does not trigger. [DFCTS00361627]
Events on Alarm Table
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
The Events tab is visible when selecting an Alarm table graphic element. Alarm table graphic elements have built-in events. By adding events to an alarm table graphic element, the built-in events can stop working. [DFCTS00360544]
Do not add events to an alarm table graphic element.
Repeated Disconnect and Reconnect
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
If the network between the PanelView 5500 terminal and the Logix controller disconnects for less than 3 seconds or repeatedly disconnects and reconnects, the PanelView 5500 project can occasionally resynchronize with the Logix controller project. Depending on the size of your project, this resynchronization can cause tag values and alarms to take up to a few minutes to start showing values again after the network is reconnected. Any data values show one of these error messages:
[DFCTS00363667]
During this time, no alarms appear on the PanelView 5500 terminal.
Button Behavior
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
The release action for Button Behavior events, which a touch press or key press triggers simultaneously, execute when the first touch or key releases. This action occurs even when the other touch or key is still pressed. [DFCTS00354276]
ShelveDuration and MaxShelveDuration Values
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
The ShelveDuration and MaxShelveDuration values for an alarm are not updated if the values are changed through a numeric input from the HMI device. The previous values are used instead. [DFCTS00339713]
To change ShelveDuration and MaxShelveDuration for an alarm, use Logix Designer.
Trend Chart
Corrected Anomaly with Firmware Revision 9.001
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510 and PanelView 5310
Pausing a trend chart can cause some traces to no longer appear. This can occur when pausing and resuming a trend chart immediately after a download or screen navigation. The data does not appear if the trend chart has a higher sample rate than the data log. The trend chart plots only historical data for the sample period. [1353612]
Inconsistent Synchronization Indications and Tag Communication Errors
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
Inconsistent synchronization indications and tag communication errors can appear on the HMI device when the Logix controller is almost out of memory. [47168]
Tertiary DNS Configuration
Corrected Anomaly with Firmware Revision 9.001
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
When the HMI device automatically obtains IP settings by using DHCP, the system tag ::Local:HMIDevice.Enet[0].TertiaryDNSConfig does not update to reflect the tertiary DNS configuration that is obtained through DHCP. To display the tertiary DNS configuration that is obtained through DHCP, use the system tag ::Local:HMIDevice.Enet[0].TertiaryDNS. [1353622]
Download While Screen Saver Is Running
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
When downloading to an HMI device on which the screen saver is running, there is no indication that the download is occurring, and the Home screen, rather than the last open screen, appears on the HMI device when the download is complete. [DFCTS00342409]
SD Card Corrupt File System
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
SD cards formatted with FAT32 can corrupt the file system on the SD card if the HMI device loses power while data logging.
To work around this issue, use an SD card formatted with EXT3. [57822]
Conflicting Error Messages
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Downloading a project containing a tag with a syntax error or invalid format displays conflicting error messages. An incorrect message appears stating that the tag does not exist in the controller or has an External Access property set to None. The correct error message appears in the Errors pane. [59562]
@AlarmSet Values
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Reading .@AlarmSet values at a controller or program level from a version 31 Logix controller displays an error message. The HMI device cannot immediately read .@AlarmSet values at a controller or program level from a version 31 Logix controller.
To work around this issue, wait several seconds after opening the page with the graphic element that displays the .@AlarmSet values. The correct values appear. [150257]
No Tag Values In Alarm Annunciation
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
When displaying a version 31 Logix controller tag-based alarm in the In Alarm state on a PanelView 5000 HMI device, and the Use and evaluate alarm configuration is disabled and then enabled, no associated tag values appear in the alarm annunciation.
To work around the issue, update the Logix controller to version 32. [159028]
Screen Errors When Exceeding Recommended Alarm Limits
Known Anomaly First Identified as of Firmware Revision 6.001
Bulletin Numbers: PanelView™ 5500, PanelView 5510, and PanelView 5310
An HMI device screen error occurs when the number of alarms exceeds the recommended value. [4092]
To resolve this issue, do not exceed 4,000 alarms per controller.
Traces Not Appearing
Corrected Anomaly with Firmware Revision 9.001
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Pausing a trend chart can cause some traces to no longer appear. This can occur when pausing and resuming a trend chart immediately after a download or screen navigation. The data does not appear if the trend chart has a higher sample rate than the data log. The trend chart plots only historical data for the sample period. [1353612]
Synch and Communication Errors
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Inconsistent synchronization indications and tag communication errors can appear on the HMI device when the Logix controller is almost out of memory. [2582]
Elements Not Visible On The Screen
Known Anomaly First Identified as of Firmware Revision 7.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
If multiple elements on a screen have state tables with many states and many of the properties of the elements are included in the state table, then some of the elements may not be visible on the screen.
To work around this anomaly, use fewer properties in the state tables or have a smaller number of states. [6572]
HMI Devices Pause Data Updates
Known Anomaly First Identified as of Firmware Revision 7.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
When using CompactLogix 5370 controllers running version 33 firmware, rapidly repeating network disruptions may cause PanelView 5000 HMI devices to intermittently pause updating data for two or three seconds at a time.
If this issue occurs, cycle power to the switches in your network, or manually disconnect and reconnect ports. [5395]
Parameterized Popups
Corrected Anomaly with Firmware Revision 7.002
Known Anomaly First Identified as of Firmware Revision 7.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Corrected: Anomaly where parameterized popups did not update tag data correctly when repeatedly displayed with the same tag instances.
These anomalies are from previous releases but are still known in this release.
Read Fails Tag Does Not Exist or External Access Property Set to None
Known Anomaly First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
A graphic element bound to an array element or structured tag member that does not exist can display an incorrect error message on the HMI device when the read fails. The incorrect error states that the read fails because the tag does not exist in the controller or has an External Access property set to None. The read actually fails because even though the parent tag exists, the binding specifies an array element or structure member which does not exist.
To work around this issue, bind to an existing array element or structured tag member. [59562]
Events on Alarm Tables
Known Anomaly First Identified as of Firmware Revision 4.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
The Events tab is visible when selecting an Alarm table graphic element. Alarm table graphic elements have built-in events. Adding events to an alarm table graphic element can cause the built-in events to stop working. [DFCTS00360544]
Do not add events to an alarm table graphic element.
Download Failure
Known Anomaly First Identified as of Firmware Revision 6.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
A Windows 7 anomaly may cause a project download to fail with a message that View Designer cannot connect to the HMI device.
See Rockwell Automation Knowledgebase Answer ID 2588507 and install the hotfix. [2605]
Project Cannot Download
Known Anomaly First Identified as of Firmware Revision 3.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
A project that is open in View Designer version 3.01 that does not have a .vpd extension cannot download to the HMI device when both View Designer version 3.01 and version 4.01 or later are installed on the same computer.
Rename the project file to end in the extension .vpd. [2397]
This release has the following functional changes from the previous release.
FactoryTalk Linx Adoption
Functional Change First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5510 and PanelView 5310
View Designer now uses FactoryTalk Linx for browsing for controller or HMI device paths and for communication when using the Emulator. FactoryTalk Linx must be at version 6.20 or later, which is the version shipped with Logix Designer version 33. View Designer version 7.01 and later no longer uses RSLinx Classic.
Screen Switch Performance
Functional Change First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5510 and PanelView 5310
Better screen switch performance with parameterized screens and popups. Improved initial display times when the following apply:
• Screens or popups with custom properties tied to Logix data types
• The Logix controller project has many tag instances of that data type
Downloads Over a Slow Network
Functional Change First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5510 and PanelView 5310
Improved support for View Designer downloads over a slow network. View Designer version 7.01 starts downloads using the normal large block size for more efficient downloads. If the download causes connection timeouts because of a slow network, View Designer automatically retries with a smaller block size. This smaller block size allows downloads to complete with a much slower network connection – as slow as 200 Kbps.
This release has the following application notes.
Project Limits
Application Notes First Identified as of Firmware Revision 5.001
Bulletin Numbers: PanelView™ 5510 and PanelView 5310
Limits
For best results, observe View Designer project limits:
|
Description
|
Limit
|
Notes
|
|
Number of controllers
|
1 (PanelView 5310)
4 (PanelView 5510)
|
|
|
Number of HMI devices
|
4
|
|
|
Number of tag references
on a single screen
|
1000
|
|
|
Total number of tag
references in a View
Designer project
|
5000
|
|
|
Number of screens and
popups
|
100 (PanelView 5510)
100 (PanelView 5310)
|
Shortcuts and pre-defined screens do not count towards the
limit.
|
|
Number of shortcuts in a
project
|
200
|
|
|
Number of alarms in a
controller
|
1000
|
|
|
Number of alarms in a
project
|
4000
|
|
|
Number of graphic elements
on a single screen
|
500
|
|
|
Number of Add-On Graphic
definitions
|
200
|
|
|
Number of Add-On Graphic
instances per project
|
500 or until reaching the 1000
tag reference limit for a
screen
|
|
|
Number of graphic elements
in an Add-On Graphic
|
250
|
|
|
Number of properties
defined for an Add-On
Graphic
|
20
|
|
|
Number of tags in a
controller
|
200,000 across four
controllers
|
View Designer counts every scalar, array element, structure
member, and so forth, as a separate tag.
|
|
Number of tags for all data
logs in a project
|
250
|
|
|
Image size limit
|
10 MB
|
|
|
Number of images on a
screen
|
500 or memory full
|
|
|
Number of PDF viewer
graphic elements on a
screen
|
2
|
|
|
Number of PDF viewers
appearing simultaneously
on a screen and popup
|
2
|
|
|
Amount of metadata
|
Each analog tag referenced is
capable of having
eu/min/max. Each BOOLEAN
tag referenced is capable of
having state identifiers All
referenced tags are capable
of having descriptions.
|
|
|
Number of View Designer
instances open
simultaneously
|
3
|
View Designer does not support opening the same project in
more than one instance of View Designer.
|
|
Length of a text input
|
82 characters
|
|
|
Length of a text display
reading from a STRING
data type in the controller
|
476 characters
|
Using UTF-8 for STRING encoding may result in displaying 476
characters incorrectly. Each character may take multiple bytes
of data.
|
|
Number of users defined in
Security Administration
|
500
|
|
|
Number of simultaneous
VNC connections to PV5000
|
1
|
|
|
Number of simultaneously
running Emulators
|
1
|
|
|
Number of allowed data
points to log
|
1.296 billion
|
This number of data points equals 250 data points at 500
milliseconds for 30 days.
|
|
Combined number of
PanelView 5000 HMI
devices and Logix
controllers that can
communicate with each
other through a 1756-EN2T
or 1756-EN3T Ethernet
module
|
8 or fewer
|
|
Firewall Rules
Application Notes First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5510 and PanelView 5310
View Designer does not require endpoint firewall rules because it is not a server product that allows remote clients.
Additional security considerations when using Rockwell Automation products include:
Project Limits 7.001
Application Notes First Identified as of Firmware Revision 7.001
Catalog Numbers: PanelView™ 5510 and PanelView 5310
For best results, observe View Designer project limits:
|
Description
|
Limit
|
Notes
|
|
Number of controllers
|
1 (PanelView 5310)
4 (PanelView 5510)
|
|
|
Number of HMI devices per controller
|
4
|
|
|
Number of tag references on a single
screen
|
1000
|
|
|
Total number of tag references in a View
Designer project
|
5000
|
|
|
Number of screens and popups
|
100 (PanelView 5310
and PanelView 5510)
|
Shortcuts and pre-defined
screens do not count
towards the limit.
|
|
Number of shortcuts in a project
|
200
|
|
|
Number of alarms in a controller
|
4000 tag-based or
1000 instruction-based
|
|
|
Number of alarms in a project
|
16000 tag-based or
4000 instruction-based
|
PanelView 5310 is still
limited to 4000 tag-based or
1000 instruction-based
alarms.
|
|
Number of graphic elements on a single
screen
|
500
|
|
|
Number of Add-On Graphic definitions
|
200
|
|
|
Number of Add-On Graphic instances per
project
|
500 or until reaching
the 1000 tag reference
limit for a screen
|
|
|
Number of graphic elements in an Add-On
Graphic
|
250
|
|
|
Number of properties defined for an
Add-On Graphic
|
20
|
|
|
Number of tags in a controller
|
50000
|
View Designer counts every
scalar, array element,
structure member, and so
forth, as a separate tag.
|
|
Number of tags for all data logs in a project
|
250
|
|
|
Image size limit
|
10 MB
|
|
|
Number of project events per project
|
1000
|
|
|
Number of images on a screen
|
500 or memory full
|
|
|
Number of PDF viewer graphic elements
on a screen
|
2
|
|
|
Number of PDF viewers appearing
simultaneously on a screen and popup
|
2
|
|
|
Amount of metadata
|
Each analog tag
referenced is capable
of having eu/min/max.
Each BOOLEAN tag
referenced is capable
of having state
identifiers All
referenced tags are
capable of having
descriptions.
|
|
|
Number of View Designer instances open
simultaneously
|
3
|
View Designer does not
support opening the same
project in more than one
instance of View Designer.
|
|
Length of a text input
|
82 characters
|
|
|
Length of a text display reading from a
STRING data type in the controller
|
476 characters
|
Using UTF-8 for STRING
encoding may result in
displaying 476 characters
incorrectly. Each character
may take multiple bytes of
data.
|
|
Number of users defined in Security
Administration
|
500
|
|
|
Number of simultaneous VNC connections
to PV5000
|
1
|
|
|
Number of simultaneously running
Emulators
|
1
|
|
|
Number of allowed data points to log
|
1.296 billion
|
This number of data points
equals 250 data points at
500 milliseconds for 30
days.
|
| Combined number of PanelView 5000 HMI
devices and Logix controllers that can
communicate with each other through a
1756-EN2T or 1756-EN3T Ethernet module
is eight or fewer.
|
8 or fewer
|
|
|
Number of alarm transitions in the Alarm
History
|
40000
|
|