Release Notes

1734 POINT I/O EtherNet/ IP Adapters
Version 6.013 (released 9/2020)

Catalog Number 1734-AENTR (series C)

These release notes describe version information for 1734-AENTR, version 6.013 (released 9/2020).

Features

This release includes the following system features.

Enable and disable web server in AOP

Feature First Identified as of Series B Firmware Revision 5.018

Feature First Identified as of Series C Firmware Revision 6.013

Catalog Numbers:                                   


The web server feature for POINT I/O™ and ArmorPOINT® I/O EtherNet/IP™ adapters can be enabled or disabled in AOP version 7.01.01 or later.




  

Corrected Anomalies in This Release

This release corrects the following anomalies.

Web server anomalies

Corrected Anomaly with Series B Firmware Revision 5.018

Corrected Anomaly with Series C Firmware Revision 6.013

Known Anomaly First Identified as of Series B Firmware Revision 5.015

Known Anomaly First Identified as of Series C Firmware Revision 6.011

Catalog Numbers:                                   


The following web server anomalies can occur due to improper validation and authentication:

  1. Malicious code can be executed in the web browser due to cross-site scripting.
  2. Local files can be exposed on the web server due to local file inclusion.
  3. Login password and web form fields can be changed without logging in to the web server due to unauthenticated configuration.


POINTBus indicator blinks red after cable break

Corrected Anomaly with Series B Firmware Revision 5.018

Corrected Anomaly with Series C Firmware Revision 6.013

Known Anomaly First Identified as of Series B Firmware Revision 5.016

Known Anomaly First Identified as of Series C Firmware Revision 6.011

Catalog Numbers:                                   


The POINTBus™ indicator blinks red continuously after a safety application is downloaded to the Logix controller. The rack consists of an adapter and a combination of standard and safety modules. No errors are communicated to the controller from the adapter when this scenario occurs. The setup works as expected.


IP address conflict is not detected during ARP Probe

Corrected Anomaly with Series B Firmware Revision 5.018

Corrected Anomaly with Series C Firmware Revision 6.013

Known Anomaly First Identified as of Series B Firmware Revision 5.017

Known Anomaly First Identified as of Series B Firmware Revision 6.012

Catalog Numbers:                                   


An IP address conflict is not detected when an ARP Probe is performed to validate an IP address on the network.


Functional Changes

This release has the following functional changes from the previous release.

Web page validation and constraints

Functional Changes First Identified as of Series B Firmware Revision 5.018

Functional Changes First Identified as of Series B Firmware Revision 6.013

Catalog Numbers:                                   


The following table lists the constraints when validating the form fields in each web page.

Web Page
Form Field
Constraints
Identity.html
Module Description
  1. Alphanumeric characters accepted
  2. Only ‘-‘ and ‘ ’ (space) special characters are accepted
  3. First character cannot be a special character
  4. Length of string cannot exceed 64 bytes
Module Location
Chassis Size
  1. Only numeric characters accepted
  2. Character length cannot exceed two
  3. Chassis size cannot be less than or equal to zero
  4. Chassis size cannot be greater than 64
NetConfig.html
Domain Name
  1. Alphanumeric characters accepted
  2. Only ‘-‘ and ‘ ’ (space) special characters are accepted
  3. First and last character cannot be a special character
  4. Length of string cannot exceed 48 bytes
IP Address, Subnet, Gateway, Primary, Secondary
  1. Only numeric and ‘.’ characters are accepted
  2. Follow standard IP address format
  3. Cannot set IP address to 192.168.1.0




  

Application Notes

This release has the following application notes.

Update adapter firmware with ControlFLASH

Application Notes First Identified as of Series B Firmware Revision 5.018

Application Notes First Identified as of Series C Firmware Revision 6.013

Catalog Number:


When ControlFLASH™ is used to update the adapter firmware, select the adapter from Node 1 as shown in the following example. If you select the adapter from Node 2, the firmware update fails and results in improper functioning of the web server feature.

ControlFLASH example

graphic

ControlFLASH software required:

  
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.