This release has the following requirements.
System Requirements Identified as of PowerFlex 755 Drive Firmware Revision 3.004
System Requirements Identified as of PowerFlex 753 Drive Firmware Revision 5.001
The Customer Configurable Response to HIM Communications Loss feature requires a new enhanced style HIM (20-HIM-A6, 20-HIM-C6S). This feature will not work with older contemporary 7-Class HIM’ s (20-HIM-A3, 20-HIM-A5, 20-HIM-C3S, 20-HIM-C5S).
System Requirement Identified as of PowerFlex 755 Drives Firmware Revision 8.001
System Requirement Identified as of PowerFlex 753 Drives Firmware Revision 9.001
System Requirements Identified as of PowerFlex 753 Drive Firmware Revision 5.001
The new Auto/Manual HIM Preload feature requires firmware in the HIM that is newer than 2.
EtherNet/IP Port and 20-750-ENETR Require Quality of Service (QoS)
System Requirements Identified as of PowerFlex 755 Drive Firmware Revision 9.001
System Requirements Identified as of PowerFlex 753 Drive Firmware Revision 9.001
With this firmware revision, the EtherNet/IP port and 20-750-ENETR require the EtherNet/IP scanner to use a compatible method of specifying Quality of Service (QoS). The following table details the compatible products and firmware revisions.
Product
|
Compatible Rev. No.
|
DriveLogix 5730 Embedded
Ethernet Port
|
Rev. 3.1.4
|
CompactLogix (1769-L2x/L3x)
|
Rev. 17.03
|
ControlLogix (1756-ENBT)
|
Rev. 4.005
|
CompactLogix (1768-ENBT)
|
Rev. 2.001
|
FlexLogix (1788-ENBT)
|
Rev. 2.004
|
ControlLogix 1756-EN2T (F)(XT)
|
No Update needed
|
SoftLogix I/O Messaging
|
No Update needed
|
These anomalies are from previous releases but are still known in this release.
Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 3.004
Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 5.001
The HIM startup on the PowerFlex 755 drive includes a feedback device selection step. Depending on the option modules installed, that step may first ask the user to choose a port, then a parameter. In some situations, the list of ports incorrectly shows multiple copies of 'Port 0 - PowerFlex 755' followed by the feedback port/module.
The incorrect behavior happens only under the following conditions:
When the incorrect port list appears, it is still possible to successfully select the feedback module port by following one of these methods.
Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001
Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001
In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, a persistent stop command may appear in some cases. The action of disconnecting the Ethernet cable from the 20-750-ENETR module, which will result in the drive stopping, may follow with a nuisance fault action. This fault action previously noted is persistent communication of stop commands.
Known Anomaly First Identified as of PowerFlex 755 Drives Firmware Revision 8.001
Known Anomaly First Identified as of PowerFlex 753 Drives Firmware Revision 8.001
In an application with the use of a PowerFlex 755 or PowerFlex 753 along with the 20-750-ENETR dual port Ethernet/IP module, in which a user attempts to save all parameters using DriveExplorer® in some causes the save execution does not complete. When attempting to execute the save all parameters in DriveExplorer the software tool enters an infinite loop and does not progress through the save in some instances. To exit the loop, press the cancel button and check if the text file has been saved.
Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 2.011
Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 7.001
You cannot change the level of current used during the direction test on a permanent magnet motor while in Integrated Motion on EtherNet/IP (CIP Motion) mode. It is set at 10%. If the system requires more than 10% to turn the motor, it will fail to perform the test.
Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 3.004
Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 5.001
The following internal diagnostic items may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 2 [PBLT Pwrup Time], 3 [PBLT GatesOnTime], 4 [PBLT Mtr MW Hrs], 5 [PBLT Rgn MW Hrs] and 67 [PwrBd Pwr Cycles].
The following parameters may contain incorrect data after upgrading a PowerFlex 755 from revision 1 to revision 6 firmware: 13[Elapsed MWH], 14 [Elapsed kWH], 15 [Elapsed Run Time], 16 [Elpsd Mtr MWHrs], 17 [Elpsd Rgn MWHrs], 18 [Elpsd Mtr kWHrs], 19 [Elpsd Rgn kWHrs], 490 [HSFan ElpsdLife], 497 [InFan ElpsdLife], 503 [MtrBrngElpsdLife], 508 [MtrLubeElpsdHrs], 512 [MchBrngElpsdLife] and 517 [MchLubeElpsdHrs].
These values will affect the associated calculated “ remaining life ” parameter values and predictive maintenance events.
Known Anomaly First Identified as of PowerFlex 755 Drive Firmware Revision 6.004
Known Anomaly First Identified as of PowerFlex 753 Drive Firmware Revision 6.004
When running in Flux Vector open loop mode for induction motor or Interior Permanent Magnet (IPM) motor mode, the drive may experience an F918 exception event when the motor accelerates through a 7 Hz operating frequency due to the simultaneous transition from a 2 to 4 KHz carrier frequency. This exception can be avoided by setting parameter 40 [Mtr Options Cfg] bit 9 – PWM FreqLock], which will keep the carrier frequency at 4 KHz.
Universal Feedback Board Module Does Not Annunciate Fault
Known Anomaly First Identified as of:
When the UFB is configured to use the SSI Full Digital Feedback Device, the UFB does not annunciate a fault when the SSI Full Digital is the signal is lost. For full details on possible workarounds to this anomaly, see Technical Support Knowledgebase Article #463171. To determine if this notice affects you and for additional information, please refer to Knowledgebase Document Number #745654.
This release has the following application notes.
Application Notes
Use the Drive LCD HIM
FW Revision is listed under – Main Control Board
Use DriveExplorer Lite/Full
Important: You need DriveExplorer version 6.02 or later to interface with the PowerFlex 753 drive. To obtain the latest version, visit the Allen-Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate
Once selected, information regarding the PowerFlex 753 drive is shown in the right panel including the current firmware revision number.
Use DriveExectuive
Important: You need DriveExecutive version 5.02 or later to interface with the PowerFlex 753 drive. To obtain the latest version, visit the Allen- Bradley Web Updates site located at http://www.ab.com/support/abdrives/webupdate
Product Updates and Replacements
PowerFlex® 753 firmware revision 14.004 or later is installed by using a *.dmk file. Firmware updates for PowerFlex 753 drives can be performed using the following software:
Software
|
Version
|
Additional Software
|
Communication Adapters
|
ControlFLASH
Plus™
|
3.01.00
|
The following software
must be installed before
running ControlFLASH
Plus:
ControlFLASH Plus
version 2.00.00 or later
includes the installation
package for FactoryTalk
Linx.
|
The following communication
device must be used:
|
ControlFLASH™
|
15.03.00
|
One of the following
software packages must
be installed before
running ControlFLASH:
|
One of the following
communication devices must
be used:
|
Before You Begin a Firmware Update
If necessary, download and install the preferred software from the Product Compatibility and Download Center.
For information on connecting the 1203-USB or 1203-SSS converter to your drive, see these publications:
Use ControlFLASH Plus to Update the Firmware
See “Use ControlFLASH Plus to update firmware” in the ControlFLASH Plus Quick Start Guide, publication CFP-QS001
Use ControlFLASH to Update the Firmware
Follow these steps to update your PowerFlex 753 drive firmware.
Note: PowerFlex 755 and firmware revision 14.004 are shown in the images as an example only. Where required, make your selections for a PowerFlex 753 and the applicable firmware revision.
Important: Choose the appropriate “PowerFlex 753 xx” catalog number selection for your application. Do not choose an option that includes the “via…” option.
The drive firmware update has been completed.