Release Notes

( 9357-x ) RSNetWorx™ provides design and configuration management services for ControlNet™, DeviceNet™, and EtherNet/IP™.
Version 28.01.00 (released 6/2019)

Catalog Number RSNetWorx 

These release notes describe version information for RSNetWorx, version 28.01.00 (released 6/2019).

Requirements

This release has the following requirements.

 

RSNetWorx for DeviceNet works within the system requirements of all Rockwell Automation® software products. For the latest information regarding software platform support, refer to Rockwell Automation Product Compatibility and Download Center .

Hardware requirements

Software requirements

Operating systems

RSNetWorx for DeviceNet is tested on operating systems installed from original Microsoft® media only. It runs on either the 32-bit or 64-bit versions of the following Windows® operating systems:

Compatible software

The following software is compatible with this version of RSNetWorx:

Firmware requirements

If you are using any of the Allen-Bradley modules listed in the following table, they must have the association minimum firmware revision installed:

Module
Firmware Revision
1747-SDN
Version 2.004 or later; version 3.001 for slave mode support; version 4.008 for ADR support; version 4.015 for pass-through (bridging) support.
1756-DNB
Version 1.003 or later; version 1.5 or later for pass-through (bridging) support; version 3.001 or later for ADR support.
1769-SDN/B
Version 2.001 or later for ADR support.
1770-KFD
Version 1.004 or later.
1794-ADN
Version 1.4 or later; or version 2.1 or later.


High Resolution Display Support

Windows 10 build 1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

 

RSNetWorx for ControlNet works within the system requirements of all Rockwell Automation® software products. For the latest information regarding software platform support, refer to Rockwell Automation Product Compatibility and Download Center .

Hardware requirements

Software requirements

Operating systems

RSNetWorx for ControlNet is tested on operating systems installed from original Microsoft® media only. It runs on either the 32-bit or 64-bit versions of the following Windows® operating systems:

Compatible software

The following software is compatible with this version of RSNetWorx:

Firmware requirements

RSNetWorx for ControlNet can configure single-keeper networks or multi-keeper networks. You can mix both single-keeper and multi-keeper devices on the same ControlNet™ network as long as the lowest node address is a multi-keeper device.

Rockwell Automation ControlNet 1.5 or ControlNet International 2.0 specifications

For Hot Backup support, the PLC-5®C processors must be at the following series/revision levels or later:

For multi-keeper and Merged Edits support, the PLC-5C processors must be at the following series/revision levels or later:

For multi-keeper support, the 1756-CNB devices must be at the following series/revision levels or later:

High Resolution Display Support

Windows 10 build 1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.

Supported browsers

The following web browsers have been tested and are supported for use with this release:

RSNetWorx for EtherNet/IP works within the system requirements of all Rockwell Automation® software products. For the latest information regarding software platform support, refer to Rockwell Automation Product Compatibility and Download Center .

Hardware requirements

Software requirements

Operating systems

RSNetWorx for EtherNet/IP is tested on operating systems installed from original Microsoft® media only. It runs on either the 32-bit or 64-bit versions of the following Windows® operating systems:

Compatible software

The following software is compatible with this version of RSNetWorx:

Supported browsers

The following web browsers have been tested and are supported for use with this release:

High Resolution Display Support

Windows 10 build 1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.

Features

This release includes the following system features.

RSNetWorx for DeviceNet version 28.01.00 has no new features or enhanced features.

RSNetWorx for ControlNet version 28.01.00 has no new features or enhanced features.

RSNetWorx for EtherNet/IP version 28.01.00 has no new features or enhanced features.

Corrected Anomalies in This Release

This release corrects the following anomalies.

There are no corrected anomalies in this release.

Known Anomalies in This Release

This release has the following known anomalies.

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

      When navigating between the Graph and Spreadsheet views for the network configuration, you may encounter a situation where the items selected in one view are not selected among the other available views. For example, if you select your entire network configuration in the Graph view, navigate to the Spreadsheet view and click the adapters to display the modules contained within the chassis, and then return to the Graph view, the chassis originally selected in the Graph view is no longer selected. First reported in version 5.00. [363935]
      To avoid this issue, select the desired devices again in the final destination view.
      When initiating concurrent browses in multiple instances of RSNetWorx through the same communication device, the software will encounter General Protection Faults (GPFs). First reported in version 5.00. [363936]
      To avoid this issue, do not initiate multiple browses of RSNetWorx through the same communications device.
      If you have a connection from an EtherNet/ IP scanner to a target peer device (for example, another EtherNet/IP scanner), the Diagnostic view will not indicate an error when the target is in Program Mode. First reported in version 5.00. [363937]
      To avoid this issue, manually change the peer target device to Program mode prior to running diagnostics.
      If you are running RSNetWorx MD in one instance of RSNetWorx and perform connection edits in a second instance of RSNetWorx, the diagnostics in the first instance of RSNetWorx MD will be stopped. First reported in version 5.00. [363938]
      To avoid this issue, you must manually restart diagnostics in the first instance of RSNetWorx to resume diagnosing your network.
      After you have defined connections to any 1747 or 1794 adapter modules in a chassis, any subsequent edits to the chassis (for example, adding devices) does not alter the associated slot mask for the adapter module. First reported in version 3.00. [363939]
      To avoid this issue, delete any affected adapter connections and redefine them.
      If you have a connection from a non-PLC-5, non-ControlLogix scanner (for example, a 1747-SCNR) to a 1771 module, the Diagnostic view will not indicate a connection error when there is a connection error. First reported in version 5.00. [363940]
      To work around this issue and view the actual connection error, launch the Scanlist Configuration Tool for the non-PLC-5, non-ControlLogix scanner and view the Connection Status view.
      To avoid this issue, ensure that your 1771 target exists in the network configuration and the device is communicating properly on the network before opening the Diagnostic View.
      If you have a connection from a non-PLC-5, non-ControlLogix scanner (for example, a 1747-SCNR) to a peer target device (for example, a PLC-5 processor), the Diagnostic view does not indicate a connection warning when the target is not in Program Mode. First reported in version 5.00. [363941]
      To avoid this issue, manually change the peer target device to Program mode prior to running diagnostics.
      If you are running NetWorx Health Diagnostics in one instance of RSNetWorx and perform connection edits in a second instance of RSNetWorx, the diagnostics in the first instance of Networx Health Diagnostics will be stopped. First reported in version 4.00. [363942]
      To avoid this issue and resume diagnosing your network, manually restart diagnostics in the first instance of RSNetWorx.
      When saving a configuration file (*.xc) online that specifies a Redundant owner connection from a PLC-5C (Series F, Revision A or later) processor that does not have the Hot Backup cartridge (1785-CHBM) installed, the Scanlist Configuration Tool displays an error message. In this cases, the PLC-5 returns information about the redundant connection that conflicts with the stored configuration. First reported in version 3.00. [363943]
      To avoid this issue, ensure that the PLC-5C processors used in the Hot Backup configuration have the Hot Backup cartridge installed when the Redundant owner connection type is specified in the Scanlist Configuration Tool.
      If you are connected to a ControlNet network through a ControlLogix gateway and the 1756-CNB is the active keeper device on your network, updates to a PLC-5C keeper on that same network are not recognized. First reported in version 4.00. [363944]
      To avoid this issue, perform one of the following:
      • Use a 1756-CNB other than the one that is currently configured as the active keeper device on your ControlNet network.
      • Update the PLC-5C firmware to series F, revision C.1 (or later).
      • Open the Keeper Status dialog box and update the individual keeper that failed to update (particularly if the failure occurred during a save or download operation).


      If you are running multiple instances of RSNetWorx for DeviceNet (instance A and instance B), and attempting to bridge from the offline configuration file in the first instance to the second offline configuration file in the second instance, the software stops responding. First reported in version 3.00. [363931]
      To avoid this issue, we recommend using only a single instance of RSNetWorx for DeviceNet when configuring device bridging or using associated networks.
      To avoid this issue, open the original configuration, and then go online to download SmartGuard EIP to restore its configuration.
      If you are using the SmartGuard USB driver in RSLinx Classic or EtherNet/IP port of SmartGuard EIP and attempt to download to a 1753-DNSI DeviceNet Safety Scanner (in RSNetWorx for DeviceNet, right-click the 1753-DNSI DeviceNet Safety Scanner, and then select Download to Device), the download operation fails. First reported in version 9.00. [363933]
      To avoid this issue, use a direct connection from your computer to the DeviceNet network (for example, a 1784-PCD driver) or bridge to your DeviceNet network through another device.
      RSNetWorx for DeviceNet reports a communication error if you are communicating to a safety device (for example, 1753-DNSI, 1791DS-IB12, 1791DS-IB4XOW4, 1791DS-IB8XOB8) using a revision of 1756-DNB prior to v6.002, and you try to lock/Unlock that safety device. First reported in version 6.00. [363934]
      To avoid this issue, update the flash firmware for the 1756-DNB module to v6.002 or higher. For more information, contact Technical Support.

Functional Changes

This release has the following functional changes from the previous release.

There are no functional changes in RSNetWorx for ControlNet version 28.01.00.

There are no functional changes in RSNetWorx for DeviceNet version 28.01.00.

There are no functional changes in RSNetWorx for EtherNet/IP version 28.01.00.

Application Notes

This release has the following application notes.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates .

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Specifies the install location.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_SUCCESS_RELAUNCH_REQUIRED
3011
Restart of setup needed before installation can continue.

Scanlist Configuration Tool

While downloading a PLC-5C processor via RSLogix 5, close the corresponding Scanlist Configuration Tool. This prevents a potential General Protection Fault (GPF) in the Scanlist Configuration Tool, while also improving the performance of the download.

Security considerations

For information on the security considerations when using Rockwell Automation products, see the following Answer ID's:

Software updates

The Rockwell Automation Knowledgebase maintains the current list of Rockwell Automation product updates.

For the latest product updates and patch information see the following Answer ID's:

Click the Subscribe to Updates link at the top of each article to receive an email notification when the article is updated.

Alternatively, follow the instructions provided in "Subscribing to Product Safety Advisory (PSA) or Product Notice (PN) Notifications" Answer ID 35704  to choose specific products about which to receive notifications.

To directly download software or firmware updates, and patch roll-ups , go to Product Compatibility and Download Center .


  

Note for SmartGuard 600 Safety Controllers users only

To write logic for the SmartGuard PLC, bulletin 1752-L24BBBxx, the RSNetWorx for DeviceNet installation includes the SmartGuard editor, which requires MSXML 4.0 to function properly. However, MSXML 4.0 is not installed with RSNetWorx for DeviceNet. To use a SmartGuard PLC, you need to download and install  it manually. MSXML 4.0 is no longer supported by Microsoft and has security risks associated with it. When installing MSXML 4.0, read the MSXML Roadmap  for security considerations.

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates .

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Specifies the install location.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_SUCCESS_RELAUNCH_REQUIRED
3011
Restart of setup needed before installation can continue.

RSNetWorx MD

If you are diagnosing a DeviceNet network in RSNetWorx MD, we do not recommend that you attempt to commission any device on that same network with the Node Commissioning Tool. Attempting to perform both of these operations at the same time may cause a conflict on the network and result in abnormal behavior (for example, no reads in the Diagnostics view or the inability to connect to a device with the Node Commissioning Tool) in RSNetWorx.

Security considerations

For information on the security considerations when using Rockwell Automation products, see the following Answer ID's:

Software updates

The Rockwell Automation Knowledgebase maintains the current list of Rockwell Automation product updates.

For the latest product updates and patch information see the following Answer ID's:

Click the Subscribe to Updates link at the top of each article to receive an email notification when the article is updated.

Alternatively, follow the instructions provided in "Subscribing to Product Safety Advisory (PSA) or Product Notice (PN) Notifications" Answer ID 35704  to choose specific products about which to receive notifications.

To directly download software or firmware updates, and patch roll-ups , go to Product Compatibility and Download Center .

VeriSign Universal Root Certification Authority certificate

If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.

Unattended or silent install

Use command-line parameters to perform an unattended or silent installation of the software.

Command-line parameters

The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").

Parameter
Description
/?
Displays the usage options for installation parameters.
/Q
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
/QS
Unattended Install, install runs in a quiet simple mode and shows progress through the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the installation will stop and display a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be displayed for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
/IAcceptAllLicenseTerms
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
/AutoRestart
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return either error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
/SetupLanguage="value"
Specifies which language will be displayed during install process.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
/Record
Records the installation options chosen to a recording file.
This parameter is optional.
/Playback
Plays back a recording file to specify the installation options.
This parameter is optional.
/IgnoreWarning
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning occurs.
/ProductLanguage="value"
Specifies the language version of the software being installed.
The value must be the one of the following:
  • ENU
  • CHS
  • DEU
  • ESP
  • FRA
  • ITA
  • JPN
  • KOR
  • PTB
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages this parameter is not available.
/InstallLocation="value"
Specifies the install location.
This parameter is optional. If this parameter is not used, the default install location is "C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed on. Use /? to determine which parameter is supported.
/SerialNumber="value"
Specifies the serial number of the software being installed. This is used to activate the software during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/ProductKey="value"
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter is not available.
/Version="value"
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent product version available.
Some software does not require activation. If activation is not required this parameter is not available.

Error codes

The following table identifies the error codes that can be returned by an installation.

Error Code
Value
Description
ERROR_SUCCESS
0
The installation completed successfully.
ERROR_INVALID_PARAMETER
87
One of the parameters was invalid.
ERROR_INSTALL_USEREXIT
1602
The installation was cancelled by the user.
ERROR_INSTALL_FAILURE
1603
A fatal error occurred during installation.
ERROR_BAD_CONFIGURATION
1610
The configuration data for this product is corrupt. Contact your support personnel.
ERROR_SUCCESS_REBOOT_INITIATED
1641
The installer has initiated a restart. After restart installation will continue.
ERROR_SUCCESS_REBOOT_REQUIRED
3010
A restart is required to complete the installation. After restart the product is successfully installed.
ERROR_SUCCESS_RELAUNCH_REQUIRED
3011
Restart of setup needed before installation can continue.

EtherNet/IP file service

An error message is logged when uploading to network with devices configured for L1y, L2y, or L3y controllers with connections. A message like the following is displayed:

A connect exists from address 10.224.107.244, slot 00. The error 'Unexpected Failure (Error code: 0xD0:0x0000)' occurred while attempting to communicate with Originator Connection List Object.

In this case, ignore the message. The uploading was actually successful.

Performance

If your network contains a large number of devices (for example, more than 75), you may notice some performance degradation when using the Graph view.

To achieve better performance, use the Spreadsheet view by selecting View > Spreadsheet.

Security considerations

For information on the security considerations when using Rockwell Automation products, see the following Answer ID's:

Software updates

The Rockwell Automation Knowledgebase maintains the current list of Rockwell Automation product updates.

For the latest product updates and patch information see the following Answer ID's:

Click the Subscribe to Updates link at the top of each article to receive an email notification when the article is updated.

Alternatively, follow the instructions provided in "Subscribing to Product Safety Advisory (PSA) or Product Notice (PN) Notifications" Answer ID 35704  to choose specific products about which to receive notifications.

To directly download software or firmware updates, and patch roll-ups , go to Product Compatibility and Download Center .

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.