Release Notes

ControlLogix Redundancy Enhanced Module (where applicable with Configuration Tool)
Version 20.010 (released 4/2019)

Catalog Number 1756-RM2 (series A)

These release notes describe version information for 1756-RM2, version 20.010 (released 4/2019).

Features

This release includes the following system features.

Redundancy Module Configuration Tool for Revision 31.052_kit1

Catalog Numbers

IMPORTANT: You must uninstall any existing versions of the Redundancy Module Configuration Tool (RMCT) before you install version 8.5.1.0 of the RMCT. If you do not uninstall the previous versions, you can have difficulty if you try to uninstall version 8.5.1.0 later.

You can use 1756-RM2 or 1756-RM2XT redundancy modules to commission a redundant system. You can commission a system without any additional programming. However, there is additional functionality available if you use the modules with the RMCT.

This redundancy system revision requires the RMCT, version 8.5.1.0, that is packaged with this redundancy system revision bundle.

graphic

You can use the RMCT with the redundancy modules to complete these tasks:
For a complete list of RMCT functionality, see the ControlLogix Redundancy User Manual, publication 1756-UM535.

*ControlLogix 5570 controllers include all ControlLogix-XT® and K versions.
**Includes the 1756-RM2K module.
  

Known Anomalies in This Release

This release has the following known anomalies.

Flashing Firmware From 20.030 To 20.010 Results in The Module Loading BOOT Firmware (00233910)

Devices
First Known in Firmware Revision
Corrected in Firmware Revision
1756-RM2/1756-RM2XT
20.010
5570 Redundancy
30.051_kit2

When a redundancy module is at firmware version 20.030 and an attempt is made to flash to 20.010, the module reverts to 20.022.0.

A workaround to recover from this is to flash the module in the following order: 20.030 -> 20.009 -> 20.010.

For more information, see Knowledgebase Technote Flashing 1756-RM2 from v20.030 to v20.010.

Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.