This release has the following requirements.
Hardware requirements
|
Type
|
Description
|
CPU
|
RAM
|
|
Operator Workstation
|
FactoryTalk AssetCentre Client
|
Intel® Core™ i5 Standard Power processor
|
4 GB
|
|
Engineering Workstation
|
FactoryTalk AssetCentre Client
FactoryTalk AssetCentre Agent
|
Intel Core i5 Standard Power processor
|
8 GB
|
|
System Agent
|
FactoryTalk AssetCentre Agent
|
Intel Core i5 Standard Power processor
|
8 GB
|
| Application Server | FactoryTalk AssetCentre Server
|
Small systems:
Intel Core i5 Standard Power processor
|
8 GB
|
| Medium to large systems:
Intel® Xeon® quad-core family processor
|
8 GB
|
Product compatibility
FactoryTalk AssetCentre version 10.00.00 is compatible with the following Rockwell Automation products. For the latest compatibility information, refer to the Rockwell Automation Product Compatibility and Download Center .
FactoryTalk AssetCentre Server
FactoryTalk AssetCentre Client
FactoryTalk AssetCentre Agent
|
Asset
|
Compatible Software
|
Version
|
|
PLC-5
|
RSLogix 5
|
8.00 or later
|
|
SLC 500, MicroLogix
|
RSLogix 500
|
8.40 or later
|
|
ControlLogix, CompactLogix
|
Studio 5000 Logix Designer
|
21.00 or later
|
|
RSLogix 5000
|
16.00 or later
| |
|
RSLogix 5000 Compare Utility or Logix Designer Compare
Tool
|
8.12
| |
| PanelView Plus, MobileView
|
FactoryTalk View ME Transfer Utility
|
12.00
|
|
FactoryTalk Linx (formerly known as RSLinx Enterprise)
|
6.20
| |
|
FactoryTalk View Site Edition
|
FactoryTalk View Studio Enterprise
|
12.00
|
|
Rockwell Automation drives
|
DriveExecutive Lite
|
5.02 or later
|
|
PowerFlex Drive
|
UDC
|
4.06
|
Operating systems
FactoryTalk AssetCentre has been tested on the following operating systems:
|
Important:
|
Turn off the Windows updates on production computers.
Installing Microsoft Service Pack release or Windows
operating system updates may affect the operation of
Rockwell Automation software installed on the
computer. To avoid this problem, see Knowledgebase
Document ID: QA2151 - Microsoft Patch Qualifications
.
|
FactoryTalk AssetCentre Server
FactoryTalk AssetCentre Client and Agent
FactoryTalk AssetCentre Web Client
Software requirements
FactoryTalk AssetCentre Server
The following are minimum software requirements for FactoryTalk AssetCentre Server.
SQL Server databases
FactoryTalk AssetCentre has been tested on the following SQL Servers:
FactoryTalk AssetCentre Client
The following are minimum software requirements for FactoryTalk AssetCentre Client.
FactoryTalk AssetCentre Agent
The following are minimum software requirements for FactoryTalk AssetCentre Agent.
FactoryTalk AssetCentre Web Client
The following are minimum software requirements for FactoryTalk AssetCentre Web Client.
High Resolution Display Support
Windows 10 v1703 or later is the recommended operating system if running this software with a 2K or 4K High Resolution Display.
Preferred operating systems
Preferred operating systems are prioritized for support, testing, and post-release patch qualifications. These operating systems are preferred for this release:
Rockwell Automation Test Environment
Rockwell Automation tests software products under a standard configuration of operating systems and antivirus software. For additional information see the Knowledgebase Document ID: PN24 - Rockwell Software Products and Antivirus Software .
Security requirements
To help meet secure system design requirements review these publications:
This release includes the following system features.
FactoryTalk AssetCentre version 10.00.00 has the following new and enhanced features:
New features
|
Note:
|
When FIPS (Federal Information Processing Standard) compliance is
turned on, backup and backup & compare tasks for E300 Overload
Relay, contained in a FactoryTalk AssetCentre schedule, will fail.
The E300 Overload Relay does not comply with FIPS. There is no
workaround for this behavior.
|
Enhanced features
This release corrects the following anomalies.
There is currently no workaround for this anomaly.
In this release, two options, Portrait and Landscape, can be selected as the print format.
This release has the following known anomalies.
When configuring a PanelView asset's Addressing Info, if a device other than a PanelView is selected, several extraneous error messages may display. First identified in FactoryTalk AssetCentre version 9.00.00. [Jira 242271]
To avoid this problem, choose the proper device type when configuring the Addressing Info of a PanelView asset.
A PanelView Plus or MobileView Disaster Recovery schedule will fail with a communication error message, if the Address Info is not set for the device using FactoryTalk Linx Browser located on the FactoryTalk AssetCentre agent computer. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 395652]
To avoid this problem, after configuring the Addressing Info property of a PanelView Plus asset or a MobileView asset, the user must browse for the device in FactoryTalk Linx Browser from the FactoryTalk AssetCentre agent computer when the agent computer is not collocated with the FactoryTalk AssetCentre client.
When the Report Incremental Differences option is enabled for a Logix 5000 controller asset within a Disaster Recovery schedule, the task will fail if the controller firmware version does not match the firmware version of the ACD file associated with the Incremental Checkpoint label. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 806906]
To avoid this problem, you can do the following steps:
After upgrading or downgrading a Logix 5000 controller’s firmware, open the FactoryTalk AssetCentre archive to check in the ACD file that matches Logix 5000 controller firmware version.
Select Add Label to move the Incremental Checkpoint, and then select the Allow reuse of existing labels check box.
In the Label box, enter the label name exactly as Incremental Checkpoint.
The Disaster and Recovery schedule will now run successfully.
FactoryTalk AssetCentre has limited support for 4K displays, when display scaling is greater than 100%. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 355367]
To avoid this problem, set the display scaling to 100% and restart the computer.
When uninstalling FactoryTalk AssetCentre Agent, FactoryTalk AssetCentre Agent will remain in the Control Panel, Add/Remove until all supporting applications (for example, RSLogix 500) are also removed. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 488955]
To resolve this problem, uninstall all software installed together with FactoryTalk AssetCentre Agent 10.00.00 installation and then it will be removed.
When repairing a FactoryTalk AssetCentre Agent installation on a computer upon which Logix Designer Compare Tool is not installed, FactoryTalk AssetCentre will generate a nuisance warning message indicating that Logix Designer Compare Tool requires that Microsoft .NET Framework 3.5 to be installed. First identified in FactoryTalk AssetCentre version 10.00.00. [Jira 566002]
This issue currently has no workaround. The behavior does not adversely impact the FactoryTalk AssetCentre Agent installation repair process.
There is currently no workaround for this problem.
There is currently no work around for this anomaly.
To avoid this problem, use a different browser such as Chrome or Internet Explorer.
To resolve this problem, manually select the Tools check box or its sub items'.
These anomalies are from previous releases but are still known in this release.
When performing an Asset Inventory WMI to scan the software, with the Changes only option selected, the scan can not detect installation changes for applications that do not maintain installation information (for example, you uninstall the software today and then install it on another day). First identified in FactoryTalk AssetCentre version 7.00.00.[358777]
There is currently no work around for this anomaly.
Cannot modify or uninstall the software FactoryTalk AssetCentre Client or FactoryTalk AssetCentre Agent application by double-clicking Setup.exe in the installation package and selecting AssetCentre Custom Installation. First identified in FactoryTalk AssetCentre version 8.00.00. [46429]
To modify or uninstall the software components, go to the Programs and Features list of the Control Panel.
To avoid this problem, move the newly added Logix5000 Controller device out of the container and add it back again.
This release has the following functional changes from the previous release.
FactoryTalk AssetCentre version 10.00.00 has the following changes in functionality since the last release:
Process device capabilities removal
Starting from FactoryTalk AssetCentre version 10.00.00, process device capabilities are not supported.
|
Important:
|
After upgrading to FactoryTalk AssetCentre version
10.00 from earlier versions, you will no longer be able
to use Process Device Configuration and Calibration
Management functionality.
|
After upgrading from FactoryTalk AssetCentre version 9.00 or earlier to version 10.00, General DTM Device, Equipment, Instrument, Loop, System, and Test Instrument process devices are not available in the asset catalog. The Process Device Configuration Field Edition, ProcalV5 Data Source Configuration, and Procal DB Connector Installer will be removed.
If Process Device Configuration is required for your system, we recommend you considering Endress+Hauser FieldCare which offers a comprehensive tool for managing process instruments called FieldCare SFE500. Endress+Hauser FieldCare is scalable, which allows to fulfill tasks from Device Setup to Plant Asset Management. FieldCare can be used with instruments communicating via Profibus-PA, Foundation Fieldbus, and HART.
All calibration records and information are retained in ProCalV5, thus the previously existing process device assets will be displayed in the asset tree. You can still cut, copy, and paste the existing process devices in the asset tree. However, their hardware and asset properties will be disabled. The ProCalV5 Company and ProCalV5 Linked Item properties of Instrument, Equipment, Loop, System, and Test Instrument are removed from the asset properties dialog box. Process devices will still consume the capacity activation. If you are still owning FactoryTalk AssetCentre Calibration Management, we recommend you contacting the following vendors for more solutions:
This release has the following application notes.
The following are the application notes for FactoryTalk AssetCentre version 10.00.00.
Disaster Recovery schedule tasks fail with Device Not Found recorded in the FactoryTalk AssetCentre Event log
When a Logix controller asset’s Addressing property was configured using RSLinx Classic, Disaster Recovery schedule tasks may start failing with Device Not Found recorded in the FactoryTalk AssetCentre Event log. Rebooting the FactoryTalk AssetCentre Agent(s) will temporarily address the error; however, the task failures will eventually return.
This behavior is addressed in a RSLinx Classic patch. See technote BF27867 for additional details.
Secure communication with TLS and SSL protocols
Windows implements SSL and TLS through Schannel Security Support Provider (SSP). The Schannel SSP implementation of the TLS and SSL protocols use algorithms from a cipher suite to create keys and encryption information. Starting from FactoryTalk AssetCentre version 9.00, the operating system's capability is used to automatically filter out the unsecure ciphers.
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Displays the usage options for installation parameters.
|
|
/Q
|
Silent Install, install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation using
an IT tool or script, and don’t expect to see any error or restart messages. When using
this parameter, your IT tool or script should check the error codes, and respond as
needed. For example, if the installation returns error code 1641, then the IT tool or
script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
|
|
/QS
|
Unattended Install, install runs in a quiet simple mode and shows progress through
the UI, it does not accept any input but still shows error or restart messages.
When using this parameter, you will not have to check the error codes, and the
installation will stop and display a prompt if there are error or restart messages. For
example, if an immediate restart is required to complete the install, a restart message
will be displayed for you to confirm the restart. Installation resumes automatically
from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms.
This parameter is required for /Q or /QS parameters.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used when a
restart is required to complete the installation.
This parameter is optional. If this parameter is not used silent install (/Q) will return
either error code 1641 or 3010 if a restart is required, and unattended install (/QS)
will result in a confirmation prompt that must be agreed to before the installation is
completed.
|
|
/SetupLanguage="value"
|
Specifies which language will be displayed during install process.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default language is the
current user or operating system user interface language.
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/IgnoreWarning
|
Specifies that the setup ignores warnings and continues.
This parameter is optional. If it is not specified, the setup exits when a warning
occurs.
|
|
/Product="value"
|
Specifies which sub-products will be installed.
The product name must be one of followings:
|
|
/Uninstall
|
Uninstalls the product.
This parameter is optional.
|
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed.
The value must be the one of the following:
This parameter is optional. If this parameter is not used, the default language is the
same as the setup language.
If the software does not support multiple languages this parameter is not available.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to activate the
software during installation.
This parameter is optional. If it is not specified the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter
is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required this parameter
is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate which corresponds to the product
version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified the installer will use the most recent
product version available.
Some software does not require activation. If activation is not required this parameter
is not available.
|
|
/InstallDrive="value"
|
Specifies the install drive.
This parameter is optional. If this parameter is not used, the default install location is
"C:\Program Files (x86)\Rockwell Software".
Some software restricts the installer to only change the drive the software is installed
on. Use /? to determine which parameter is supported.
|
|
/SqlServer="value"
|
Specifies FactoryTalk AssetCentre database server (Microsoft SQL Server) location.
This parameter is required when installing the FactoryTalk AssetCentre server
software.
|
|
/sa="value"
|
Uses SQL Authentication for SQL Server Logins. If you use SQL Server
Authentication to perform silent or unattended installation, the parameters /SqlAdmin,
/SqlAdminPwd, /SqlUser, and /SqlPwd are required.
|
|
/SqlAdmin="value"
|
Specifies the Microsoft SQL Server administrator account name.
This parameter is required when installing the FactoryTalk AssetCentre server
software.
|
|
/SqlAdminPwd="value"
|
Specifies the Microsoft SQL Server administrator account password.
This parameter is required when installing the FactoryTalk AssetCentre server
software.
|
|
/SqlUser="value"
|
Specifies the user name for the account that will be used to access the Microsoft SQL
Server database.
This parameter is required when installing the FactoryTalk AssetCentre server
software.
|
|
/SqlPwd="value"
|
Specifies the Microsoft SQL Server database user account password.
This parameter is required when installing the FactoryTalk AssetCentre server
software.
The database user account password cannot be the following terms associated with
the installation computer:
The database user account password must be more than 8 characters and no more than
128 characters in length and satisfy at least three of the following four criteria:
|
|
/DirectoryServer="value"
|
Specifies the FactoryTalk network directory if you are using a distributed system.
This parameter is optional. If it is not specified, the software will use its current
computer as the FactoryTalk Directory server.
The value must be the host name of the FactoryTalk Directory server.
|
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
The installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One of the parameters was invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
The installation was cancelled by the user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
A fatal error occurred during installation or the software component to
be installed already exists on the computer.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
The configuration data for this product is corrupt. Contact your
support personnel.
|
|
ERROR_REBOOT_CONTINUE
|
1641
|
A reboot is required to continue to installation.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
A restart is required to complete the installation. After restart the
product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
A restart is pending and is required before the installation can
continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are already
installed.
|
FactoryTalk AssetCentre Client
FactoryTalk AssetCentre Agent
|
Note:
|
This configuration step can be skipped during installation. If
skipped, you may configure it manually later.
For details, see the Installation Guide, chapter "Install FactoryTalk
AssetCentre agents", section "Configure for security-enabled
RSLogix family software".
|
The amount of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system
The following is the amount of clients, agents, and agent groups qualified within one FactoryTalk AssetCentre system at the same time. More clients, agents, or agent groups running will impact the system performance.
Synchronizing life-cycle information with the Rockwell Automation life cycle website
To synchronize life-cycle information, the FactoryTalk AssetCentre server and client communicate directly with the Rockwell Automation life cycle website. To enable this function, ensure that the external address https://api.rockwellautomation.com is accessible by the FactoryTalk AssetCentre server and client.
Synchronize life-cycle information in the FactoryTalk AssetCentre server and client with the data on the Rockwell Automation life cycle website. For more information about securely accessing the Rockwell Automation lifecycle website from your OT zone-based FactoryTalk AssetCentre Server, please refer to this document Cloud Connectivity to a Converged Plantwide Ethernet Architecture https://literature.rockwellautomation.com/idc/groups/literature/documents/td/enet-td017_-en-p.pdf in Rockwell Automation Literature Library.
FactoryTalk Directory asset compare
Differences are always found between two FactoryTalk Directory backup files after a Backup and Compare schedule, even though no changes are made to the FactoryTalk Directory. This is because the BAK files include timestamp information, which is detected as a difference during the binary compare of the backup files.
Event Log Attachment Extractor
The Event Log Attachment Extractor utility cannot properly extract event log attachments in the following two cases:
About Microsoft SQL Server 2012 Express Edition with Advanced Services (x64)
FactoryTalk AssetCentre v6.10 or higher supports Microsoft SQL Server Express. Some FactoryTalk AssetCentre catalog numbers contain Microsoft SQL Server 2012 Express Edition with Advanced Services (x64), which is a free and unlicensed edition of Microsoft SQL Server. This is intended for storing the FactoryTalk AssetCentre database. SQL Server 2012 Express Edition with Advanced Services (x64) has the following limitations:
|
Tip:
|
FactoryTalk AssetCentre 6.1 or higher has capabilities for
managing database size.
|
FactoryTalk AssetCentre also supports other versions of SQL Server as described in this Release Notes.
You may upgrade to Microsoft SQL Server 2012 Standard Edition, which is a licensed edition, by purchasing from the following list of Rockwell Automation catalog numbers:
The licenses in the previous catalog numbers can be used only with Rockwell Automation products, including FactoryTalk AssetCentre. More information on SQL Server licensing with Rockwell Automation products can be found in Knowledgebase Document ID: IN31446 - FAQ: Using Microsoft SQL Server with Rockwell Automation FactoryTalk Products .
Alternatively, you may purchase licenses for a supported version and edition of SQL Server from Microsoft. A complete comparison of SQL Server 2012 Editions can be found here: https://technet.microsoft.com/en-us/library/cc645993(v=sql.110) .
Install product updates
For the latest Product Updates and Patch information, refer to Knowledgebase Document ID: QA15600 - FactoryTalk AssetCentre Patch Roll-up for 3.0 and later .
You can subscribe to be notified when new product updates, or patches are released via the
Knowledgebase by clicking below the Knowledgebase answer title.
To directly download software or firmware updates, and patch roll-ups , go to Product Compatibility and Download Center.
Security requirements
For information on the security considerations when using Rockwell Automation products, including