Release Notes
More information: PowerFlex® 525 Site
Version 5.002 (released 2/2019)
Catalog Number PowerFlex 525 (series A)
These release notes describe version information for PowerFlex 525, version 5.002 (released 2/2019).
Corrected Anomalies in This Release
This release corrects the following anomalies.
Security Vulnerability in PowerFlex 525 AC Drives with Embedded EtherNet/IP
(152230)
Corrected Anomaly with PowerFlex® 525 Drives Firmware Revision 5.002
Known Anomaly First Identified as of PowerFlex 525 Drives Firmware Revision 1.003
Catalog Number: 25B
This product release remediates a security vulnerability in the firmware. This
vulnerability may affect the availability of network communications to this product due to
resource exhaustion and/or memory corruption. An affected product would require
manual intervention to recover. For complete details on the vulnerability and
recommended mitigations, refer to KnowledgeBase article 1082684.
Application Notes
This release has the following application notes.
Update PowerFlex 525 Firmware
Product Updates and Replacements
Using the USB Utility Application
- Separate the Control Module from the Power Module.
TIP
|
For more information on how to separate the Control Module from the
Power Module, see the PowerFlex® 520-Series Adjustable Frequency AC
Drive User Manual, publication 520-UM001.
|
- Connect one end of a USB cable to the USB port on the back of the Control
Module.
- Connect the other end to the PC. A Windows® Explorer window appears.

- Launch the PF52XUSB utility application. The PowerFlex 520-Series USB
Application window appears.

- Click Flash and select the firmware with which you want to update the module.
- Click Yes. The Confirm Flash Update dialog box appears. It displays the current
firmware revision and the new revision to be flashed.

- Click Flash.
- When the process is complete, click OK.
- Close the application and disconnect the Control Module from the PC.
- Connect the Control Module to the Power Module and power cycle the drive.
- During the boot-up sequence, the following commands are displayed on the drive’ s
LCD display: BOOT > COPY1 > COPY2 > ERASE > BOOT
- When fault F105 “C Connect Err” occurs, clear the fault to complete the flash
update.
- The LCD display shows the drive data and current firmware revision.
Alternatively, you can verify the firmware revision by checking parameter b029
[Control SW Ver].
TIP
|
If the firmware revision did not update properly, you may need to reset the
drive to default and cycle drive power.
|
Using the ControlFLASH™ Software
- Install the flash kit utility for the PowerFlex 525 drive. You can download the flash
kit utility from the Allen-Bradley Web Updates site at:
http://www.ab.com/support/abdrives/webupdate/
- Launch the ControlFLASH software.
- On the ControlFLASH Welcome screen, click Next. The Catalog Number dialog box
appears.

- Select the communication device you will use to update the firmware revision and
click Next. For this example, select “PowerFlex 525 via PowerFlex 520-Series
Comms” .
- In the Select Device to Update dialog box, expand the hardware view by clicking
the “+” symbol next to the communication path you are using. For this example,
click the “+” next to “AB_ETHIP-1, Ethernet ”.

- Select the entry of the PowerFlex 525 drive you are updating and click OK. The
Firmware Revision dialog box appears.

- Select the firmware revision you want to flash and click Next.
- Follow the remaining prompts to complete the flash update. When the process is
complete, the new firmware revision is displayed in the dialog box.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2025 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.