Release Notes

( 9324-RLMx ) This software allows you to create, modify and monitor application programs for A-B MicroLogix controllers.
Version 12.00.01 (released 12/2018)

Catalog Number RSLogix Micro 

These release notes describe version information for RSLogix Micro, version 12.00.01 (released 12/2018).

Known Anomalies from Previous Releases

These anomalies are from previous releases but are still known in this release.

·         Poor response time of ladder editor when connecting a project with many complex instructions

Selecting Cross Reference for an address in the ladder editor is slow when online with a SLC 5/05 processor with a project containing many complex instructions such as EEM, DEM, CEM, and MSG. First identified in RSLogix Micro version 8.10.00. [262714]

There is currently no work around for this anomaly.

·         Unable to edit a rung with an LBL instruction online in remote run mode

Online editing of a rung with an LBL instruction fails on an SLC 500 processor in remote run mode if the matching JMP instruction exists in the project and UNTEST is selected. First identified in RSLogix Micro version 5.50.00. [80585]

To resolve this problem, put the LBL instruction on its own rung.

·         Unable to verify the MicroLogix 1200 or MicroLogix 1500 project

In a MicroLogix 1200 or MicroLogix 1500 project, if a CLR instruction with an HSC:0.ACC or HSC:1.ACC operand exists in the rung with a nested branch (for example:BST XIC B3:0/0 CLR HSC:1.ACC NXB ADD 0 N12:1 N7:0 BND), the project verification will fail and a compiler error will be displayed. First identified in RSLogix Micro version 7.00.00. [82259]

There is currently no work around for this anomaly.

·         The broadcast message destination node 1 is not accepted

With a MicroLogix 1500 LRP Series C Channel 1 Radio modem, the broadcast message destination node 1 is not accepted when verifying the project. The error message invalid local DH-485 Station Number (0-254) displays even though 1 is a valid local DH-485 station number when Channel 1 is set for DF1 Radio modem and a broadcast message is requested. First identified in RSLogix Micro version 7.20.00. [77766]

There is currently no work around for this anomaly.

·         RSLogix 500 may stop responding when changing DNP3 Data Set configuration

When changing DNP3 Data Set configuration from Data Element (DAEL) to Prototype (PTYP) several times, RSLogix Micro may stop responding. First identified in RSLogix Micro version 10.00.00. [355325]

To resolve this problem, restart RSLogix Micro.

·         Unable to go online with MicroLogix 1400 Series B security project with password

If an MicroLogix 1400 Series B security project's password is set using RSLogix Micro version 11, an error messages shows and cannot be closed as you try to upload and go online with the project using RSLogix Micro version 10 or earlier. First identified in RSLogix Micro version 11.00.00 [363763, 362682, 364135]

There is currently no work around for this anomaly.

·         Cannot restore the SMTP settings from EEPROM

If the MicroLogix 1400 program is saved to EEPROM memory module with status bits set to Load Memory Module Always or Load Memory Module on Memory Error, the MicroLogix 1400 Chan 1 - SMTP settings cannot be restored from the EEPROM memory module at power up after changing the SMTP settings. First identified in RSLogix Micro version 8.40.00. [272814]

There is currently no work around for this anomaly.

·         Unable to save online edits of MicroLogix 1400 Series B controllers

In rare cases, during the online editing of a MicroLogix 1400 Series B controller that is online and in Run mode, an error messages may show when saving the edits. First identified in RSLogix Micro version 8.00.00. [360390]

There is currently no work around for this anomaly.

·         Unable to go online with MicroLogix controllers

If the project file for MicroLogix is password protected, after going offline with the project, going online with it will fail even if the correct password is entered. First identified in RSLogix Micro version 9.05.00. [356265]

To resolve this problem, clear the CPU before accessing it again.

Known anomalies
The following is a list of known anomalies at the time this version of RSLogix Micro was released.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.

Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please click here.
Trademarks not belonging to Rockwell Automation are property of their respective companies.