This release has the following requirements.
For the latest information regarding software platform support, refer to http://www.rockwellautomation.com/compatibility/#/scenarios
Hardware requirements
Your personal computer must meet the following hardware requirements:
Software requirements
Operating systems
RSLogix 500 runs on either the 32-bit or the 64-bit versions of the following Windows or Windows Server® operating systems:
Required software and versions
The following software is required to use RSLogix 500:
This release includes the following system features.
New features
This release has the following known anomalies.
When RSLogix 500 instructions are exported to Logix Designer with indirect bit level parameters, they are unavailable in Logix Designer. First identified in RSLogix 500 version 12.00.00. [91676, 97576, 98286]
To resolve this problem, remove the indirect bit level parameters in RSLogix 500 or correct the parameters used by the migrated instructions in Logix Designer.
When the exporting dialog box opens, the RSLogix 500 window can be focused, which allows you to edit the project being exported. First identified in RSLogix 500 version 12.00.00. [80602]
There is currently no work around for this anomaly.
Data files RI, RIX, and MG, and function files HSC (LOP and UNF) and DAT (CN[4]'s [1] - [3]) cannot be converted to Logix Designer correctly. First identified in RSLogix 500 version 12.00.00. [97139]
To resolve this problem, correct the values of these data files and function files in RSLogix 500 before exporting.
When exporting to Logix Designer, some RSLogix 500 I/O points (for example: 1746-NR8 to 1734-IR2) cannot be exported correctly. First identified in RSLogix 500 version 12.00.00. [97536]
To resolve this problem, correct the I/O modules' parameters in Logix Designer.
When parsing the instructions with the argument PWMX: 0.ADD, the Syntax Error dialog box opens. After closing the dialog box, an error messages "Export ACD file failed" shows. First identified in RSLogix 500 version 12.00.00. [98296]
To resolve this problem, remove the argument PWMX: 0.ADD before exporting to Logix Designer.
When there are unrecognizable characters in the exporting process, the Syntax Error dialog box opens. After closing the dialog box, an error message "Export ACD file failed" shows. First identified in RSLogix 500 version 12.00.00. [102633]
To resolve this problem, remove the unrecognizable characters that are shown in the Syntax Error dialog box before exporting to Logix Designer.
RSLogix 500 projects with 1747-MNET will fail to export to Logix Designer projects. First identified in RSLogix 500 version 12.00.00. [64848]
To resolve this problem, remove 1747-MNET from the project before exporting to Logix Designer.
The instructions DCD, DDV, DLG, ENG, HSC, HSD, HSE, HSL, LCD, IID, IIE, IIM, IOM, PTO, PWM, RAC, RCP, REF, RHC, RMP, RPI, RTA, SQC, STS, SUS, SVC, SWP, TDF, UID, UIE, and UIF are not supported to convert to Logix Designer. These instructions will migrate to a PCE (Program Conversion Error) instruction in Logix Designer and then must be manually migrated to a valid Logix instruction. First identified in RSLogix 500 version 12.00.00. [64832, 95574]
There is currently no work around for this anomaly.
Selecting Cross Reference for an address in the ladder editor is slow when online with a SLC 5/05 processor with a project containing many complex instructions such as EEM, DEM, CEM, and MSG. First identified in RSLogix 500 version 8.10.00. [262714]
There is currently no work around for this anomaly.
Online editing of a rung with an LBL instruction fails on an SLC 500 processor in remote run mode if the matching JMP instruction exists in the project and UNTEST is selected. First identified in RSLogix 500 version 5.50.00. [80585]
To resolve this problem, put the LBL instruction on its own rung.
In a MicroLogix™ 1200 or MicroLogix 1500 project, if a CLR instruction with an HSC:0.ACC or HSC:1.ACC operand exists in the rung with a nested branch (for example:BST XIC B3:0/0 CLR HSC:1.ACC NXB ADD 0 N12:1 N7:0 BND), the project verification will fail and a compiler error will be displayed. First identified in RSLogix 500 version 7.00.00. [82259]
There is currently no work around for this anomaly.
With a MicroLogix 1500 LRP Series C Channel 1 Radio modem, the broadcast message destination node 1 is not accepted when verifying the project. The error message invalid local DH-485 Station Number (0-254) displays even though 1 is a valid local DH-485 station number when Channel 1 is set for DF1 Radio modem and a broadcast message is requested. First identified in RSLogix 500 version 7.20.00. [77766]
There is currently no work around for this anomaly.
When changing DNP3 Data Set configuration from Data Element (DAEL) to Prototype (PTYP) several times, RSLogix 500 may stop responding. First identified in RSLogix 500 version 10.00.00. [355325]
To resolve this problem, restart RSLogix 500.
If an MicroLogix 1400 Series B security project's password is set using RSLogix 500 version 11.00.00 and 12.00.00, an error messages shows and cannot be closed as you try to upload and go online with the project using RSLogix 500 version 10.00.00 or earlier. First identified in RSLogix 500 version 11.00.00. [363763, 362682, 364135]
There is currently no work around for this anomaly.
If the MicroLogix 1400 program is saved to EEPROM memory module with status bits set to Load Memory Module Always or Load Memory Module on Memory Error, the MicroLogix 1400 Chan 1 - SMTP settings cannot be restored from the EEPROM memory module at power up after changing the SMTP settings. First identified in RSLogix 500 version 8.40.00. [272814]
There is currently no work around for this anomaly.
In rare cases, during the online editing of a MicroLogix 1400 Series B controller that is online and in Run mode, an error messages may show when saving the edits. First identified in RSLogix 500 version 8.00.00. [360390]
There is currently no work around for this anomaly.
If the project file for SLC 5/01, SLC 5/02, or MicroLogix is password protected, after going offline with the project, going online with it will fail even if the correct password is entered. First identified in RSLogix 500 version 9.05.00. [356265]
To resolve this problem, clear the CPU before accessing it again.
These anomalies are from previous releases but are still known in this release.
When RSLogix 500 instructions are exported to Logix Designer with indirect bit level parameters, they are unavailable in Logix Designer. First identified in RSLogix 500 version 12.00.00. [91676, 97576, 98286]
To resolve this problem, remove the indirect bit level parameters in RSLogix 500 or correct the parameters used by the migrated instructions in Logix Designer.
When the exporting dialog box opens, the RSLogix 500 window can be focused, which allows you to edit the project being exported. First identified in RSLogix 500 version 12.00.00. [80602]
There is currently no work around for this anomaly.
Data files RI, RIX, and MG, and function files HSC (LOP and UNF) and DAT (CN[4]'s [1] - [3]) cannot be converted to Logix Designer correctly. First identified in RSLogix 500 version 12.00.00. [97139]
To resolve this problem, correct the values of these data files and function files in RSLogix 500 before exporting.
When exporting to Logix Designer, some RSLogix 500 I/O points (for example: 1746-NR8 to 1734-IR2) cannot be exported correctly. First identified in RSLogix 500 version 12.00.00. [97536]
To resolve this problem, correct the I/O modules' parameters in Logix Designer.
When parsing the instructions with the argument PWMX: 0.ADD, the Syntax Error dialog box opens. After closing the dialog box, an error messages "Export ACD file failed" shows. First identified in RSLogix 500 version 12.00.00. [98296]
To resolve this problem, remove the argument PWMX: 0.ADD before exporting to Logix Designer.
When there are unrecognizable characters in the exporting process, the Syntax Error dialog box opens. After closing the dialog box, an error message "Export ACD file failed" shows. First identified in RSLogix 500 version 12.00.00. [102633]
To resolve this problem, remove the unrecognizable characters that are shown in the Syntax Error dialog box before exporting to Logix Designer.
RSLogix 500 projects with 1747-MNET will fail to export to Logix Designer projects. First identified in RSLogix 500 version 12.00.00. [64848]
To resolve this problem, remove 1747-MNET from the project before exporting to Logix Designer.
The instructions DCD, DDV, DLG, ENG, HSC, HSD, HSE, HSL, LCD, IID, IIE, IIM, IOM, PTO, PWM, RAC, RCP, REF, RHC, RMP, RPI, RTA, SQC, STS, SUS, SVC, SWP, TDF, UID, UIE, and UIF are not supported to convert to Logix Designer. These instructions will migrate to a PCE (Program Conversion Error) instruction in Logix Designer and then must be manually migrated to a valid Logix instruction. First identified in RSLogix 500 version 12.00.00. [64832, 95574]
There is currently no work around for this anomaly.
Selecting Cross Reference for an address in the ladder editor is slow when online with a SLC 5/05 processor with a project containing many complex instructions such as EEM, DEM, CEM, and MSG. First identified in RSLogix 500 version 8.10.00. [262714]
There is currently no work around for this anomaly.
Online editing of a rung with an LBL instruction fails on an SLC 500 processor in remote run mode if the matching JMP instruction exists in the project and UNTEST is selected. First identified in RSLogix 500 version 5.50.00. [80585]
To resolve this problem, put the LBL instruction on its own rung.
In a MicroLogix™ 1200 or MicroLogix 1500 project, if a CLR instruction with an HSC:0.ACC or HSC:1.ACC operand exists in the rung with a nested branch (for example:BST XIC B3:0/0 CLR HSC:1.ACC NXB ADD 0 N12:1 N7:0 BND), the project verification will fail and a compiler error will be displayed. First identified in RSLogix 500 version 7.00.00. [82259]
There is currently no work around for this anomaly.
With a MicroLogix 1500 LRP Series C Channel 1 Radio modem, the broadcast message destination node 1 is not accepted when verifying the project. The error message invalid local DH-485 Station Number (0-254) displays even though 1 is a valid local DH-485 station number when Channel 1 is set for DF1 Radio modem and a broadcast message is requested. First identified in RSLogix 500 version 7.20.00. [77766]
There is currently no work around for this anomaly.
When changing DNP3 Data Set configuration from Data Element (DAEL) to Prototype (PTYP) several times, RSLogix 500 may stop responding. First identified in RSLogix 500 version 10.00.00. [355325]
To resolve this problem, restart RSLogix 500.
If an MicroLogix 1400 Series B security project's password is set using RSLogix 500 version 11.00.00 and 12.00.00, an error messages shows and cannot be closed as you try to upload and go online with the project using RSLogix 500 version 10.00.00 or earlier. First identified in RSLogix 500 version 11.00.00. [363763, 362682, 364135]
There is currently no work around for this anomaly.
If the MicroLogix 1400 program is saved to EEPROM memory module with status bits set to Load Memory Module Always or Load Memory Module on Memory Error, the MicroLogix 1400 Chan 1 - SMTP settings cannot be restored from the EEPROM memory module at power up after changing the SMTP settings. First identified in RSLogix 500 version 8.40.00. [272814]
There is currently no work around for this anomaly.
In rare cases, during the online editing of a MicroLogix 1400 Series B controller that is online and in Run mode, an error messages may show when saving the edits. First identified in RSLogix 500 version 8.00.00. [360390]
There is currently no work around for this anomaly.
If the project file for SLC 5/01, SLC 5/02, or MicroLogix is password protected, after going offline with the project, going online with it will fail even if the correct password is entered. First identified in RSLogix 500 version 9.05.00. [356265]
To resolve this problem, clear the CPU before accessing it again.
·
Poor
response time of ladder editor when connecting a project with many complex
instructions
Selecting Cross Reference for an
address in the ladder editor is slow when online with a SLC 5/05 processor with
a project containing many complex instructions such as EEM, DEM, CEM, and MSG.
First identified in RSLogix 500 version 8.10.00. [262714]
There is currently no work around for this anomaly.
·
Unable to
edit a rung with an LBL instruction online in remote run mode
Online editing of a rung with an LBL instruction
fails on an SLC 500 processor in remote run mode if the matching JMP
instruction exists in the project and UNTEST is selected.First identified in
RSLogix 500 version 5.50.00. [80585]
To resolve this problem, put the LBL instruction on
its own rung.
·
Unable to
verify the MicroLogix 1200 or MicroLogix 1500 project
In a MicroLogix 1200 or MicroLogix 1500 project,
if a CLR instruction with an HSC:0.ACC or HSC:1.ACC operand exists in the rung
with a nested branch (for example:BST XIC B3:0/0 CLR HSC:1.ACC NXB ADD 0 N12:1
N7:0 BND), the project verification will fail and a compiler error will be
displayed. First identified in RSLogix 500 version 7.00.00. [82259]
There is currently no work around for this anomaly.
·
The
broadcast message destination node 1 is not accepted
With a MicroLogix 1500 LRP Series C Channel 1 Radio
modem, the broadcast message destination node 1 is not accepted when verifying
the project. The error message invalid local DH-485 Station Number
(0-254) displays even though 1 is a valid local DH-485 station number
when Channel 1 is set for DF1 Radio modem and a broadcast message is requested.
First identified in RSLogix 500 version 7.20.00. [77766]
There is currently no work around for this anomaly.
·
RSLogix
500 may stop responding when changing DNP3 Data Set configuration
When changing DNP3 Data Set configuration from Data
Element (DAEL) to Prototype (PTYP) several times, RSLogix 500 may stop
responding. First identified in RSLogix 500 version 10.00.00. [355325]
To resolve this problem, restart RSLogix 500.
·
Unable to
go online with MicroLogix 1400 Series B security project with password
If an MicroLogix 1400 Series B security project's
password is set using RSLogix 500 version 11, an error messages shows and
cannot be closed as you try to upload and go online with the project using
RSLogix 500 version 10 or earlier. First identified in RSLogix 500 version
11.00.00. [363763, 362682, 364135]
There is currently no work around for this anomaly.
·
Cannot
restore the SMTP settings from EEPROM
If the MicroLogix 1400 program is saved to EEPROM
memory module with status bits set to Load Memory Module Always or Load Memory
Module on Memory Error, the MicroLogix 1400 Chan 1 - SMTP settings cannot be
restored from the EEPROM memory module at power up after changing the SMTP
settings. First identified in RSLogix 500 version 8.40.00. [272814]
There is currently no work around for this anomaly.
·
Unable to
save online edits of MicroLogix 1400 Series B controllers
In rare cases, during the online editing of a
MicroLogix 1400 Series B controller that is online and in Run mode, an error
messages may show when saving the edits. First identified in RSLogix 500
version 8.00.00. [360390]
There is currently no work around for this anomaly.
·
Unable to
go online with SLC 5/01, SLC 5/02, and MicroLogix controllers
If the project file for SLC 5/01, SLC 5/02, or MicroLogix
is password protected, after going offline with the project, going online with
it will fail even if the correct password is entered. First identified in
RSLogix 500 version 9.05.00. [356265]
To resolve this problem, clear the CPU before
accessing it again.
This release has the following application notes.
Installing RSLogix 500
You can only install one version or edition of RSLogix 500 within a Windows operating system.
Upgrading or downgrading RSLogix 500
You can install a newer version (version 6.3x or later) of RSLogix 500 without uninstalling the old version first. To install an older version of RSLogix 500 over a newer version, you must first uninstall the newer version by using Add/Remove Programs in the Windows Control Panel .
Need Administrator privilege to execute certain tasks
If User Account Control (UAC) is enabled, you may be prompted to confirm your Administrator privileges when executing certain tasks (like import/export). To execute these tasks, make sure you have Administrative privileges. If not, contact your System Administrator.
Unable to import the database or process the native Import A.I. Database file when opening an .ACH file
When opening an .ACH file with Database or native Import A.I. Database file functions, you must open the file as an Administrator. Otherwise, the database in the .ACH file cannot be imported or the native Import A.I. Database file process will fail.
Errors occur when performing online saves with the Excel database editor opened
If the Excel database editor (Pro only) opens, performing online saves causes errors in the .RSS file. Make sure the Excel database editor is closed before performing online saves.
Download to processors with DDE communications may fail
If you are using RSLinx® to perform DDE communications with a processor and you download a project to the same processor, the download may fail. If this occurs, the processor loads its default program. To avoid this situation, cease DDE communications to your target processor when you plan to download a project to the same processor.
Online and offline images of the project file (projectname.RSS) are not synchronized
The project file (projectname.RSS) contains both an online and offline image of your project. This speeds the process of connecting to a processor. These images can become unsynchronized; this occurs if you do not save your changes when going from online to offline. To synchronize the images, you must download, upload, or save the project while online.
Make the database file available when sharing the database information of the project file (projectname.RSS)
The project file (projectname.RSS) contains all database- and project-related files. If you need to share a project with someone, provide them with the projectname.RSS file and they will receive all project-related information. When sharing RSLogix™ database information with other Rockwell Automation Software programs, like RSView®32, you must use the Save database as external file check box on the File>Save As dialog box to make the database file available to that program.
Unable to print ladder report as a text file
RSLogix 500 prints ladder logic reports as graphic files. The ladder report cannot be printed as a text file. Other RSLogix 500 reports can be printed as a text file using the Windows text-only printer driver.
The Floating Point constant is not supported in an SCP instruction
RSLogix 500 does not allow the use of a Floating Point constant in an SCP instruction.
Compatibility issues occur when using an older version of RSLogix 500 with the MicroLogix 1100 Series B controller
To support the MicroLogix 1100 Series B controller, RSLogix 500 handles PTO and PWM frequencies (PTO.OF, PTO.OFS, PTO.JF, PWM.OF, and PWM.OFS) as unsigned 16-bit integers (0 - 65535) for MicroLogix 1100 Series B. If you are using an older version of RSLogix 500 (version 7.0 and version 7.10) with the MicroLogix 1100 Series B controller, there will be compatibility issues. These include:
To avoid this problem, copy PTO/PWM frequencies to long integer before manipulation. For greater detail refer to Appendix F: How to use 40kHz PTO/PWM of MicroLogix 1100 Series B Controller, publication 1763-RM001.
Unable to update the Trend applet description once the address description in a data file is changed
If the address description in a data file is changed, the description in the Trend applet cannot be updated.
Certain symbol characters cannot be used
The following characters cannot be used in RSLogix 500 symbols, `~!@#$%^&*()-+={}[]|\\:;""'<>?,./ . If you have used these characters in a previous release of RSLogix 500, the symbols will appear in your ladder views and reports; however, you cannot modify the symbol.
We recommend that you export the database to the ASCII CSV format to help locate illegal symbol
characters.