This release has the following requirements.
The following are the system requirements for FactoryTalk View SE version 11.00.00 (CPR 9 SR 11).
Hardware requirements
For the optimal performance of FactoryTalk View SE applications, the personal computer is recommended to meet or exceed the following hardware requirements.
| Type | Description | CPU | RAM |
| Operator Workstation | FactoryTalk View SE Client or FactoryTalk View SE Station |
Intel® Core™ i5 Standard Power processor | 4 GB |
| Engineering Workstation | FactoryTalk View Studio Enterprise RSLinx Classic FactoryTalk Linx Studio 5000 |
Intel Core i5 Standard Power processor | 8 GB |
| Application Server | FactoryTalk View SE Server FactoryTalk View Studio Enterprise FactoryTalk Alarms & Events Tag Based Server FactoryTalk Linx Data Server with FactoryTalk Alarms and Events enabled |
Smaller systems: Intel Core i5 Standard Power processor |
4 GB
|
|
Medium to larger systems: Quad core Intel Core Xeon family processor |
8 GB |
Software requirements
Operating systems
FactoryTalk View SE is tested on the following operating systems:
* For more information, see Answer ID 964391 for Windows 10 support and Answer ID 991031 for Windows Server 2016 support in the Rockwell Automation Knowledgebase.
** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.
Domain controller requirements
The following operating systems are supported for use as domain controllers for FactoryTalk View SE client computers. Using a domain is recommended for applications that include more than 10 computers. If your application includes 10 or fewer computers, they can be organized in a workgroup.
This release includes the following system features.
FactoryTalk View SE version 11.00.00 has the following new and enhanced features.
New features
Enhanced features
This release corrects the following anomalies.
The following list identifies the anomalies corrected in FactoryTalk View SE version 11.00.00.
This release has the following known anomalies.
The following list identifies the known anomalies or limitations of FactoryTalk View SE version 11.00.00 at the time of the release.
These anomalies are from previous releases but are still known in this release.
Datalogoff <name of datalog> and then the command
Datalogon <name of datalog>.Pause 5 command between the launch of each SE client file. This will allow the start of each SE client to be offset from each other.HKEY_USERS\.DEFAULT\Software\Rockwell Software\RSView Enterprise\Data Log
HKEY_USERS\S-1-5-18\Software\Rockwell Software\RSView Enterprise\Data Log
This release has the following functional changes from the previous release.
FactoryTalk View SE version 11.00.00 has the following changes in functionality since the last release.
DeskLock utility
FactoryTalk View has enhanced the security of the utility. We strongly recommend that you reconfigure the utility to secure your system.
FactoryTalk View ME Application Manager
Application Manager is renamed to FactoryTalk View ME Application Manager and supports ME applications only.
FactoryTalk View SE Application Manager
Distributed Application Manager is renamed to FactoryTalk View SE Application Manager. The tool supports all types of SE applications.
Legacy HMI tag alarms
Starting from FactoryTalk View version 11.00, legacy HMI tag alarms are no longer supported.
After upgrading to version 11.00, legacy HMI alarm definitions in your existing application are stored in the HMI tag database. Use the FactoryTalk View Alarm Migration tool to migrate them to FactoryTalk Alarms and Events. For an example of instructions, see the YouTube page of Rockwell Automation.
Redundancy
The Save edits to both active and standby HMI servers option is selected by default.
This release has the following application notes.
The following are the application notes for FactoryTalk View SE version 11.00.00.
Considerations for application server host computers
In a network application, it is possible for a single server computer that meets the recommended requirements to host all of the following components:
If a network application requires multiple HMI servers, data servers, or alarm servers, to distribute the load, it is recommended that you install the necessary software and run the servers on multiple host computers.
Running more than one HMI server on a single computer is not recommended. If you plan to deploy a network distributed application that uses more than two servers (or two pairs of redundant servers) and more than 20 clients, or if you would like architectural assistance, contact your local Rockwell Automation Sales office for architectural assistance.
For information about setting up redundant FactoryTalk View SE servers, see FactoryTalk View Site Edition User’s Guide .
FactoryTalk Diagnostics
FactoryTalk Diagnostics cannot log to a remote database using Microsoft Access. You can only log to a local database using Microsoft Access.
Find and Replace
If an HMI server at the root node of an SE Network distributed application has the same name as the application itself, the Find and Replace feature search results might include the application name even though you performed the search at the HMI server level.
Floating-point operations
Floating-point numbers may not precisely represent all real numbers. As a result, expressions based on floating-point arithmetic operations may not evaluate as expected. This is a side effect of how the CPU represents the floating-point data. For this reason, in certain cases you may experience loss of precision and get unexpected results of floating-point operations.
KEPServer
If you are using KEPServer Enterprise as an OPC server with FactoryTalk View version 9.00.00 or later and using an HMI tag to connect to a third-party device, you will not be able to access the tag value. The cause is that the security enhancements in FactoryTalk View version 9.00.00 or later affect the communications with third-party devices. To access the tag value, additional Distributed Component Object Model (DCOM) configuration is required for KEPServer Enterprise on the computers.
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View SE Installation Guide.
Pre-installation configuration
Before you install FactoryTalk View SE, there are a number of steps required to set up the installation environment. This will help ensure that the installation proceeds smoothly and that your new or upgraded FactoryTalk system operates as expected. For detailed information about pre-requisites before installation, see Chapter 3, Pre-installation configuration of FactoryTalk View Site Edition Installation Guide.
Security requirements
For information on the security considerations when using Rockwell Automation products, including
System sizing recommendations
When you design and set up a FactoryTalk system, we recommend using the following guidelines. If you find that your system needs to expand beyond these guidelines, contact your Rockwell Automation sales or distributor representative to discuss your application design.
|
Component
|
Recommended guidelines
|
|
FactoryTalk Alarms and Events
|
|
|
FactoryTalk Alarms and Events servers per application
|
10 non-redundant servers or 10 redundant server pairs
|
|
FactoryTalk tag-based alarms per server
|
20,0001
|
|
Logix device-based alarms per server
|
10,0002
|
|
Total alarms per application
|
100,0003
|
|
FactoryTalk Linx
|
|
|
FactoryTalk Linx data servers per application
|
10 non-redundant servers or 10 redundant server pairs
|
|
Total device tags per application
|
1,000,0004
|
|
Tags per FactoryTalk Linx data server
|
100,0004
|
|
FactoryTalk View SE
|
|
|
HMI servers
|
10 non-redundant servers or 10 redundant server pairs
|
|
HMI tags per HMI Server
|
40,0005
|
|
Total data logged tags per HMI server (1 second scan rate)
|
5,000
|
|
FactoryTalk View SE client sessions simultaneously connected to
the application
|
1204
|
|
FactoryTalk ViewPoint SE servers per application
|
4
|
|
FactoryTalk ViewPoint SE concurrent clients per ViewPoint server
|
50
|
|
|
Tag Browser
If you rename an HMI server while you are deploying an application, you may need to restart the computer in order to have the HMI tags show up in the Tag Browser.
Tools and utilities
Trend objects
The Trend objects cannot get the oldest data from FactoryTalk Historian server when you click the Oldest Data button.
TrendPro objects
Clicking on the X-axis or Y-axis takes it into the free layout mode. In this case, anything done to the canvas is how you want it and it does not resize. The free mode does not persist scale and removes tags from the trend. Avoid using the free mode in the trend.
UAC support
Turning off User Account Control (UAC) is not recommended.
|
This action
|
Prompts for authentication or confirmation before running this
program
|
|
Configuring Internet Information Services (IIS)
|
RSViewWebManager.exe
CustomWebSite.exe
|
|
Updating Samples application directory
information
|
RefreshSampleApplication.exe
|
|
Terminate processes
|
VSClean.exe
|
|
DeskLock
|
DeskLock2000.exe
|
|
Legacy Tag Database Conversion
|
LegacyTagDBConvertTool.exe
|
Unattended installation
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Shows the usage options for installation parameters.
|
|
/Q
|
Silent Install. Install runs in a quiet mode without any user interface.
This parameter is recommended if you are deploying the software installation
using an IT tool or script, and don’t expect to see any error or restart
messages. When using this parameter, your IT tool or script should check the
error codes, and respond as needed. For example, if the installation returns
error code 1641, then the IT tool or script should restart the computer and
relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
|
|
/QS
|
Unattended Install. Install runs in a quiet simple mode and shows progress
through the UI. It does not accept any input, but still shows error or restart
messages.
When using this parameter, you will not have to check the error codes, and
the installation will stop and show a prompt if there are error or restart
messages. For example, if an immediate restart is required to complete the
install, a restart message will be shown for you to confirm the restart.
Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms and agreement to continue
the installation.
This parameter is required.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used
when a restart is required to complete the installation.
This parameter is optional. If this parameter is not used, silent install (/Q) will
return error code 1641 or 3010 if a restart is required, and unattended install
(/QS) will result in a confirmation prompt that must be agreed to before the
installation is completed.
|
|
/SetupLanguage="value"
|
Specifies which language will be shown during install process.
This parameter is optional. If this parameter is not used, the default language
is the current user or operating system user interface language.
The value must be one of the following:
|
|
/Record
|
Records the installation options chosen to a recording file.
This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options.
This parameter is optional.
|
|
/Repair
|
Runs a repair operation on the installed products.
This parameter is optional.
|
|
/Product="value"
|
Specifies which product will be installed.
This parameter is required.
The value must be the one of following:
|
|
/Uninstall
|
Uninstalls components that are already installed with the product specified.
This parameter is optional.
|
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed.
This parameter is optional. If this parameter is not used, the default language
is the same as the setup language.
If the software does not support multiple languages, this parameter is not
available.
The value must be one of the following:
|
|
/InstallDrive="value"
|
Specifies the installation drive.
This parameter is optional. If this parameter is not used, the default install
drive is C:.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to
activate the software during installation.
This parameter is optional. If it is not specified the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation.
This parameter is optional. If it is not specified, the software must be activated
manually after installation if activation is required.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate which corresponds to the
product version associated with the SerialNumber and ProductKey.
This parameter is optional. If it is not specified, the installer will use the most
recent product version available.
Some software does not require activation. If activation is not required, this
parameter is not available.
|
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
Installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One parameters is invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
Installation cancelled by user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
Fatal error during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
Configuration data for product corrupt. Contact support
personnel.
|
|
ERROR_REBOOT_CONTINUE
|
1641
|
Restart required to continue installation.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
Restart required to complete installation. After restart, product is
successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart computer for installation to continue.
|
|
ERROR_SUCCESS_NOT_APPLICABLE
|
3013
|
The installation cannot proceed because the products are
already installed.
|
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates .