Release Notes
( 9701-VWMx ) FactoryTalk® View Machine Edition is machine-level HMI software. [FTView, FTViewME, FTView ME, RSView, RSViewME, FactoryTalk View ME]
Version 10.00.01 (released 2/2018)
Catalog Number FactoryTalk View Machine Edition
These release notes describe version information for FactoryTalk View Machine Edition, version 10.00.01 (released 2/2018).
Requirements
This release has the following requirements.
FactoryTalk View ME version 10.00.00 (CPR 9 SR 10)
Hardware requirements
FactoryTalk View requires the following hardware:
- Intel® Core™ 2 Duo processor running at 2.66 Ghz
- 4 GB memory (RAM)
Software requirements
FactoryTalk View Machine Edition is tested and supported on the operating systems installed from original Microsoft media only. FactoryTalk View Machine Edition runs on either the 32-bit or 64-bit versions of the following operating systems:
- Windows® 7 Enterprise with Service Pack 1
- Windows 7 Professional with Service Pack 1
- Windows 7 Ultimate with Service Pack 1
- Windows 7 Embedded Standard with Service Pack 1^
- Windows 8 Enterprise
- Windows 8 Professional
- Windows 8.1 Enterprise
- Windows 8.1 Professional
- Windows Embedded 8.1 Industry Pro
- Windows 10 Enterprise*
- Windows 10 Professional*
- Windows 10 IoT Enterprise 2016 Long Term Servicing Branch (LTSB) Embedded**
- Windows Server® 2008 R2 Enterprise with Service Pack 1
- Windows Server 2008 R2 Standard with Service Pack 1
- Windows Server 2012 Datacenter
- Windows Server 2012 Standard
- Windows Server 2012 R2 Datacenter
- Windows Server 2012 R2 Standard
- Windows Server 2016 Datacenter*
- Windows Server 2016 Standard*
For operating systems installed by the computer vendor, see Answer ID 26842 in the Rockwell Automation Knowledgebase.
* For more information about the Windows 10 and Windows Server 2016 operating system support, see the Known anomalies section of "Anomalies".
** This operating system is supported with the Allen-Bradley® 61xx family of industrial computers and CompactLogix™ 5480 family of controllers.
^ For more information about the Windows 7 Embedded Standard with Service Pack 1 operating system support, see Answer ID 619825 in the Rockwell Automation Knowledgebase.
Supported browsers
The following web browsers have been tested and are supported for use with this release:
- Google® Chrome™ browser
- Internet Explorer® 11
- Mozilla® Firefox®
Supported SQL Server
FactoryTalk View Machine Edition 10.00.00 supports SQL Server 2014 Express LocalDB as HMI tag databases.
Features
This release includes the following system features.
FactoryTalk View ME version 10.00.00 has the following new and enhanced features:
New features
- On-board audit trail
FactoryTalk View Machine Edition version 10.00.00 provides the function to report operator actions using audit graphic objects and record the actions in audit log files.
- CSV export of audit, diagnostics, alarm history
FactoryTalk View Machine Edition version 10.00.00 provides the function to configure CSV export settings at design time and export audit, alarm, and diagnostics information to CSV files at run time.
- Dynamic local message and echo message
FactoryTalk View version 10.00.00 provides the function to dynamically specify local message file and write triggered message to a string tag.
- Installation Record and Playback from the Install user interface
Use Record and playback from the Install user interface to record inputs to a record file and to playback the record on other computers. Record and Playback provides an easier option to using parameters. Also use Record and Playback to customize the installation of components and features.
- HTML Help
To modernize the customer experience, in this release the online help is delivered as HTML5 compliant content that runs in a browser with full Unicode character support. It includes native platform support for Windows, Macintosh, Linux, Smartphone (Android, iOS), and Tablet (Android, iOS).
Javascript is a core component of HTML Help and Javascript must be enabled in the browser. In high security environments, a system administrator may choose to disable Javascript in Internet Explorer using security policy. If Javascript is disabled, the HTML Help displays the text, “Javascript must be enabled to view Help. Contact your administrator to enable Javascript in your browser.”
Enhanced features
- Opening and converting earlier versions of runtime applications
FactoryTalk View Machine Edition version 10.00.00 removes the constraints of opening and converting version 5.00, 5.10, and 6.00 runtime applications on a 64-bit operating system.
- Version information
FactoryTalk View Machine Edition Station shows the software version information in the title bar of the startup dialog box.
- Rockwell Automation CSV Data Log Tamper Detection Utility installation
FactoryTalk View version 10.00.00 installation media provides the installation file of Rockwell Automation CSV Data Log Tamper Detection Utility in ...\Tools\CSV Data Log Tamper Detection Utility.
- Auto dock of Property Panel and Object Explorer
FactoryTalk View Studio version 10.00.00 automatically docks the Property Panel and Object Explorer on the right of the main window.
- Multiple components deleting and removal
FactoryTalk View version 10.00.00 provides the component selection dialog box to delete and remove multiple components at one time.
- Support for KEPServer version 5.21
FactoryTalk View Machine Edition version 10.00.00 works with KEPServer version 5.21.
Corrected Anomalies in This Release
This release corrects the following anomalies.
The following list identifies the anomalies corrected in FactoryTalk View Machine Edition version 10.00.00.
- DataStorePlus ActiveX control deletes all old CSV data log files when system date changes from December 31, 2016 to January 1, 2017. First identified in FactoryTalk View Machine Edition version 8.20.00. [364507]
In this release, CSV data log files are retained when system date changes from December 31, 2016 to January 1, 2017.
- Runtime application cannot be loaded after the recipe load operation by a Recipe 2 Enhanced ActiveX control. First identified in FactoryTalk View Machine Edition version 9.00.00. [365360]
In this release, runtime application can be loaded successfully.
- Acknowledging or remote acknowledging alarms changes alarm messages. First identified in FactoryTalk View Machine Edition version 8.20.00. [365888]
In this release, acknowledging or remote acknowledging alarms does not change alarm messages.
- Font attributes of an alarm list change when creating an earlier version of runtime application (.mer). First identified in FactoryTalk View Machine Edition version 9.00.00. [367041]
In this release, font attributes of an alarm list do not change when creating a runtime application.
Known Anomalies in This Release
This release has the following known anomalies.
The following list identifies the known anomalies or limitations of FactoryTalk View Machine Edition version 10.00.00 at the time of the release.
- When a screen saver is active on a PanelView Plus family terminal, the terminal exits the screen saver mode on receiving an alarm, but remotely acknowledging the alarm does not restart the screen saver mode. First identified in FactoryTalk View Machine Edition v5.10.00. [348432]
To restart the screen saver mode, perform an action on the terminal through the touchscreen or an input device, for example, clicking the mouse, or hitting a key on the keyboard or touchscreen.
- If a gauge or bar graph object is not assigned a Value connection, the object will appear as an outline, showing a wireframe of the object at run time and test run. First identified in FactoryTalk View Machine Edition version 5.10.00. [365184]
To avoid this problem, assign a Value connection to the object.
- At runtime, if a display that contains a Chart ActiveX control is open, downloading a Logix Designer project file may alter the X-Axis or Y-Axis range of the chart. First identified in FactoryTalk View Machine Edition version 8.20.00. [360482]
To show the correct range, close and reopen the display.
- If you try to copy or rename a Machine Edition application of version 8.0 or earlier, an error message shows. First identified in FactoryTalk View Machine Edition version 8.00.00. [346788]
To avoid this problem, convert the application to the current version in FactoryTalk View Studio before copying or renaming the application.
- If Application Manager is denied access in FactoryTalk Service Application Authorization, operating Application Manager will cause unexpected errors. First identified in FactoryTalk View Machine Edition version 8.00.00. [343836]
To avoid this problem, allow Application Manager access in FactoryTalk Service Application Authorization.
- If the decimal symbol on a PanelView Plus 7 or PanelView Plus 6 terminal is set to a character other than the decimal point (.), for example, a comma (,), when the operator inputs a floating point number using the decimal point (.), the system will not be able to interpret the input correctly. For example, if the decimal symbol is set to a comma (,) on a terminal, and “13.14” is entered in a numeric input box, the system cannot decipher the value. First identified in FactoryTalk View Machine Edition version 5.10.00. [264301]
To successfully input the floating point value, set the decimal symbol to a period (.), or input the floating point value using the configured decimal symbol, the comma (,), “13,14”, in this example.
- When importing a JPG or PNG graphic image in FactoryTalk View ME, the image file extension is changed to .bmp, but the file type remains what the original image is. First identified in FactoryTalk View Machine Edition version 7.00.00. [342956]
There is currently no work around for this anomaly.
- When using Tag Import and Export Wizard to import a CSV file to an opened ME application, if the application's private directory file (.prd) in the PrivateDirectory folder is missing, no database index (DBI) log files are generated. First identified in FactoryTalk View Machine Edition version 8.00.00. [343919]
There is currently no work around for this anomaly.
- When upgrading FactoryTalk View version 6.00 or 6.10 to 9.00, the following message may be shown: "The following installed products are dependent on this installed package and may not function properly if this package is uninstalled:" First identified in FactoryTalk View version 9.00.00. [363810]
To resolve this problem, click Yes in the dialog box and continue with the upgrade.
- When running applications on PanelView Plus 7 or PanelView Plus 6 terminals, if you switch the language to Chinese, the following characters may show as square boxes:
- The captions and shorter messages in the pop-up windows of User Management buttons
- The captions in keypads
First identified in FactoryTalk View Machine Edition version 7.00.00. [347723]
To show the Chinese characters, do one of the following on terminals:
- Copy the simsun.ttc file to \Windows\
- (Recommended) Link the Tahoma, Arial, and Courier New fonts with Arial Unicode MS.
To link a font with Arial Unicode MS
- Go to Terminal Settings/Font Linking, select the font you want to edit, and press Show Links.
- Press Edit Link.
- In the Add Linked Font window, select Arial Unicode MS, and press Add Font.
- After edit all the fonts, go to the FactoryTalk View ME Station window, and press Reset.
- Some object properties that are configured in character sets for East Asian languages, such as
Chinese or Japanese, will show a question mark in the result list when you use the Find and
Replace, Cross Reference, or Undo feature. First identified in FactoryTalk View ME version
7.00.00. [338894]
To avoid this problem, go to Control Panel > Regional and Language Options, and
select the appropriate language to match the desired language.
- If the expression setting for the animation property of the base object is empty when you change the
LinkAnimation property of a reference object to Link without expressions and change the expression
setting for the animation property, the expression setting change cannot be saved. First identified in
FactoryTalk View ME version 6.00.00. [272937]
To avoid this problem, enter a valid value in the expression setting for the animation property of the base
object first.
- Applying color animations to an object group as well as to the individual objects in the group
causes unexpected behaviors. First reported in version 8.00.00. [346758]
To set up color animations for an object group, either apply the color animations to the group, or to
the individual objects in the group.
- When loading web pages in Web Browser, the ActiveX control causes a memory leak. First identified in
FactoryTalk View ME version 7.00.00. [275838, 276309]
See the following table for more information.
|
Loading a web page every number of
seconds (s)
|
Approximate memory leak increase
by the number of kilobytes (KB)
|
Approximate cumulative memory
leak over a 600-second duration
|
|
30 s
|
56 KB
|
1,120 KB
|
|
60 s
|
58 KB
|
580 KB
|
|
300 s
|
133 KB
|
266 KB
|
There is currently no workaround for this anomaly.
- When registering or unregistering an ActiveX Control object in FactoryTalk View Studio with User
Account Control (UAC) enabled in the operating system, an error message shows. First identified in
FactoryTalk View ME version 8.00.00. [346124]
To successfully register or unregister an ActiveX Control object, do one of the following
before the operation:
- Turn off UAC and restart the computer
- Run FactoryTalk View Studio as administrator
For more information about UAC, see Application notes.
- If you installed the Stand-alone ME Transfer Utility on your computer and then uninstalled the ME Transfer
Utility from Windows Control Panel, when you launch FactoryTalk Administration Console, the System
node is missing from the directory tree. First identified in FactoryTalk View ME version 7.00.00. [348016]
To avoid this problem, follow the steps below:
- In the Command Prompt window, navigate to
C:\Program Files (x86)\Common Files\Rockwell\ on 64-bit operating systems
C:\Program Files\Common Files\Rockwell\ on 32-bit operating systems
where C: is the drive to which Rockwell Automation applications are installed.
Type the following command to register the RnaSecurityinterfaces.dll file:
regsvr32 RnaSecurityInterfaces.dll
Restart your computer after registration.
- When running applications on a PanelView Plus 7 or PanelView Plus 6 terminal, if you switch the
language to Chinese, the captions and shorter messages in the pop-up windows of User
Management buttons may show as square boxes. First identified in FactoryTalk View ME version
8.20.00. [Jira 1191837]
To show the Chinese characters, link the Tahoma, Arial, and Courier New fonts with Arial
Unicode MS.
To link a font with Arial Unicode MS
- Go to Terminal Settings/Font Linking, select the font you want to edit, and press Show Links.
- Press Edit Link.
- In the Add Linked Font window, select Arial Unicode MS, and press Add Font.
After editing all the fonts, go to the FactoryTalk View ME Station window, and press Reset.
- When ME Custom String Popup Keyboard is open, the global connection for remote navigation
does not work. First identified in FactoryTalk View ME version 6.00.00. [270634]
To ensure that the global connection for remote navigation works, close ME Custom String
Popup Keyboard.
- When using a tag placeholder for the Data_Source connection, the Chart ActiveX control does not
show any data in the test display mode, and an error message shows in FactoryTalk Diagnostics:
“Failed to resolve item’s ID ”#” because it does not exist on any server.” First identified in
FactoryTalk View ME version 8.20.00. [363775]
To avoid this problem, use a tag for the Data_Source connection instead of a tag
placeholder.
- On Microsoft Surface® tablets, the press and hold gesture may not open a component's menu if the
component is a text box. First identified in FactoryTalk View 9.00.00. [362400]
To avoid this problem, use a mouse and right-click the component to open the menu.
- If a user account is locked in FactoryTalk ViewPoint, the account is still active in FactoryTalk
View ME. First identified in FactoryTalk View ME version 8.00.00 [367826]
To unlock the user account in FactoryTalk ViewPoint, reload the application on the
PanelView Plus family terminal.
- When running FactoryTalk View ME applications on Windows Server 2016 or Windows 10 v1607
operating systems, initiating a network connectivity break by disabling NIC adaptors in Device
Manager can cause application failures requiring a restart of the application. This issue was
introduced in the Windows Server 2016 operating system and the Windows 10 v1607 feature build.
[363223]
To avoid this problem, run the Microsoft Hotfix KB3201845 outlined in
https://support.microsoft.com/en-us/kb/3201845.
Alternatively, you can run Windows 10 v1703 or other supported operating systems where
this issue is not present.
For more information about Windows 10 operating system support, see Knowledgebase
Document ID: IN4493 - Windows 10 Support for the FactoryTalk Suite of Rockwell
Software products.
For more information about Windows Server 2016 operating system support, see
Knowledgebase Document ID: IN4718 - Windows Server 2016 Support for the FactoryTalk
Suite of Rockwell Software products.
Functional Changes
This release has the following functional changes from the previous release.
FactoryTalk View Machine Edition version 10.00.00 has the following changes in functionality
since the last release:
Demo mode limits
Starting from FactoryTalk View Machine Edition version 10.00.00, more than five graphic
displays and a full use of Symbol Factory library are allowed in demo mode.
Software name change
RSLinx® Enterprise is renamed to FactoryTalk® Linx™.
Application Notes
This release has the following application notes.
The following are the application notes for FactoryTalk View Machine Edition version 10.00.00.
Unattended or silent install
Use command-line parameters to perform an unattended or silent installation of the software.
Command-line parameters
The following table identifies the installation command-line parameters. Command-line parameters are case-insensitive. However, if a specified value includes a space, be sure to enclose the value in quotation marks (for example, "value with spaces").
|
Parameter
|
Description
|
|
/?
|
Shows the usage options for installation parameters.
|
|
/Q
|
Silent Install. Install runs in a quiet mode without any user interface. This parameter is recommended if you are deploying the software installation using an IT tool or script, and don’t expect to see any error or restart messages. When using this parameter, your IT tool or script should check the error codes, and respond as needed. For example, if the installation returns error code 1641, then the IT tool or script should restart the computer and relaunch the installation after restart.
This parameter is required if /QS or /Record is not specified.
|
|
/QS
|
Unattended Install. Install runs in a quiet simple mode and shows progress through the UI. It does not accept any input, but still shows error or restart messages. When using this parameter, you will not have to check the error codes, and the installation will stop and show a prompt if there are error or restart messages. For example, if an immediate restart is required to complete the install, a restart message will be shown for you to confirm the restart. Installation resumes automatically from the point of interruption after restart.
This parameter is required if /Q or /Record is not specified.
|
|
/IAcceptAllLicenseTerms
|
Acknowledges acceptance of the license terms and agreement to continue the installation. This parameter is required.
|
|
/AutoRestart
|
Automatically restarts the computer after the installation is complete. Used when a restart is required to complete the installation. This parameter is optional. If this parameter is not used, silent install (/Q) will return error code 1641 or 3010 if a restart is required, and unattended install (/QS) will result in a confirmation prompt that must be agreed to before the installation is completed.
|
|
/SetupLanguage="value"
|
Specifies which language will be shown during install process. The value must be one of the following:
- ENU
- CHS
- DEU
- ESP
- FRA
- ITA
- JPN
- KOR
- PTB
This parameter is optional. If this parameter is not used, the default language is the current user or operating system user interface language.
|
|
/Record
|
Records the installation options chosen to a recording file. This parameter is optional.
|
|
/Playback
|
Plays back a recording file to specify the installation options. This parameter is optional.
|
|
/Product="value"
|
Specifies which product will be installed. This parameter is required.
|
|
/ProductLanguage="value"
|
Specifies the language version of the software being installed. The value must be one of the following:
This parameter is optional. If this parameter is not used, the default language is the same as the setup language.
If the software does not support multiple languages, this parameter is not available.
|
|
/InstallDrive="value"
|
Specifies the installation drive. This parameter is optional. If this parameter is not used, the default install drive is C:.
|
|
/SerialNumber="value"
|
Specifies the serial number of the software being installed. This is used to activate the software during installation. This parameter is optional. If it is not specified the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required, this parameter is not available.
|
|
/ProductKey="value"
|
Specifies the product key used to get activation keys during installation. This parameter is optional. If it is not specified, the software must be activated manually after installation if activation is required.
Some software does not require activation. If activation is not required, this parameter is not available.
|
|
/Version="value"
|
Specifies the version of the software to activate which corresponds to the product version associated with the SerialNumber and ProductKey. This parameter is optional. If it is not specified, the installer will use the most recent product version available.
Some software does not require activation. If activation is not required, this parameter is not available.
|
Error codes
The following table identifies the error codes that can be returned by an installation.
|
Error Code
|
Value
|
Description
|
|
ERROR_SUCCESS
|
0
|
Installation completed successfully.
|
|
ERROR_INVALID_PARAMETER
|
87
|
One parameters is invalid.
|
|
ERROR_INSTALL_USEREXIT
|
1602
|
Installation cancelled by user.
|
|
ERROR_INSTALL_FAILURE
|
1603
|
Fatal error during installation.
|
|
ERROR_BAD_CONFIGURATION
|
1610
|
Configuration data for product corrupt. Contact support personnel.
|
|
ERROR_REBOOT_CONTINUE
|
1641
|
Restart required to continue installation.
|
|
ERROR_SUCCESS_REBOOT_REQUIRED
|
3010
|
Restart required to complete installation. After restart, product is successfully installed.
|
|
ERROR_REBOOT_PENDING
|
3012
|
Restart pending. Restart computer for installation to continue.
|
Examples
The following examples show how to use the installation commands.
- To install FactoryTalk View Machine Edition Station using the default settings during the installation process. (Silent install)
Setup.exe /Q /IAcceptAllLicenseTerms /Product="Machine Edition Station for Windows"
- To install the Chinese language version of the FactoryTalk View Studio for Machine Edition version 10.00.00 software on the D: drive and show the progress, error, or complete messages during installation, and restart the computer if necessary. The language shown during installation is Chinese. (Unattended install)
Setup.exe /QS /IAcceptAllLicenseTerms /AutoRestart /SetupLanguage=CHS /Product="Studio for Machine Edition" /InstallDrive=D: /SerialNumber=12345ABCDE /ProductKey=ABCD2-34KDC /Version=10.00.00
VeriSign Universal Root Certification Authority certificate
If the VeriSign Universal Root Certification Authority certificate does not exist on the local computer, the certificate is installed while installing Rockwell Automation software. Use Microsoft Management Console (MMC) to view the certificate in Console Root > Certificates (Local Computer) > Trusted Root Certification Authorities > Certificates.
Communications
- When using UltraVNC version 1.04 or later with FactoryTalk View, a crash may occur when navigating in FactoryTalk View Studio or loading an application in FactoryTalk View Machine Edition Station.
To avoid this problem, ensure that your version of UltraVNC is earlier than 1.04.
- If you are using remote OPC servers at run time and if the remote OPC server fails:
- Data on the clients appears to be valid, but does not update
- Animations do not show in wireframes
- Date displays do not show asterisks
- Strings do not show questions marks
- Tags that use a FactoryTalk Linx remote OPC server will show a value in the Numeric Display object even when there is no communication, for example, when the Ethernet cable has been disconnected from the CE terminal, instead of showing asterisks or logging an error message to Diagnostics.
- If you connect to ControlLogix controllers via Ethernet network, there is no additional support for other Allen-Bradley devices or network hops through bridging modules to DH+ or RIO network.
- When you run an application by double-clicking the .mer file, the application may not be able to communicate. It is because the communications file will not be automatically overwritten, and the terminal has no communication configuration or another .mer file with a different communication configuration ran on the terminal.
To avoid this problem, follow the steps below:
- If it is the first time you run the application, load the application in ME Station.
- When the following message shows, click Yes.
"Do you want to replace the terminal's current communication configuration with the application's communication configuration?"
- If a slash mark (/) exists in a tag name, the application will not run correctly on a PanelView Plus terminal although it runs correctly during Test Run.
To avoid this problem, do not include a slash mark in a tag name.
KEPServer
- FactoryTalk View Machine Edition version 10.00.00 can work with the following versions of KEPServer Enterprise:
- Version 5.13 or later on Windows 8, Windows 8.1, Windows 10, Windows Server 2012, and Windows Server 2016 operating systems
- Version 5.0 or later on Windows 7 and Windows Server 2008 operating systems
- To run KEPServer Enterprise 5.0 or later on Windows 7 or Windows Server 2008 operating systems, disable UAC and log in as an administrator.
- When using a remote Kepware data server, to run FactoryTalk View Machine Edition version 6.00.00 or later applications on a Windows 7 or Windows Server 2008 operating system, you need set DCOM manually.
- If an application running on a PanelView Plus terminal uses KEPServer as the OPC Data Server, a conflict is created with the Serial DF1 driver installed by default with FactoryTalk Linx. This produces the following recurring error message:
"DF1: Failed to open COM2: as it may be already in use by another application."
To stop the error message, remove the default Serial DF1 driver. For more information, see Answer ID 32449 in the Rockwell Automation Knowledgebase.
- If a runtime application (.mer) that contains a KEPServer Enterprise project file is converted to a design time application, the location of the project file is not shown to the user.
To access the project file, go to \Users\Public\Public Documents\RSView Enterprise\ME\HMI Projects\<application name>\KEPServer.
- If you are using KEPServer Enterprise as an OPC server with FactoryTalk View version 9.00.00 or later and using an HMI tag to connect to a third-party device, you will not be able to access the tag value. The cause is that the security enhancements in FactoryTalk View version 9.00.00 or later affect the communications with third-party devices. To access the tag value, additional Distributed Component Object Model (DCOM) configuration is required for KEPServer Enterprise on the computers.
For more information about the configuration, see Appendix, "Troubleshoot KEPServer Enterprise" in the FactoryTalk View Installation Guide.
RSNetWorx
- If you use RSNetWorx, RSNetWorx version 10.00 or later is required. Rockwell Automation recommends RSNetWorx version 21.00 or later.
If you are under a current technical support contract, you may download RSNetWorx v21 or later from the Product Compatibility and Download Center .To download RSNetWorx
- Click the Download Software Updates link and enter your Rockwell Automation Member identification.
- Enter your Company Name and the Software Serial Number for your current RSNetWorx.
- Follow the instructions to download and install the updated software product.
RSNetWorx v21.00 or later is also available in Studio Professional v21.00 or later. If you are not under a current technical support contract, you may purchase an update for RSNetWorx by contacting Rockwell Automation sales.
For the information about RSNetWorx version 11.00 and earlier incompatibility with Rockwell Automation software products, see Answer ID 566967 in the Rockwell Automation Knowledgebase.
PanelBuilder 1400e
- If you are installing PanelBuilder 1400e and FactoryTalk View Studio on the same computer, install PanelBuilder 1400e first. If you install FactoryTalk View Studio first, the PanelBuilder software will open, but you cannot create applications or open existing applications.
Network security
- For the latest network security considerations when using Rockwell Automation products, visit the Rockwell Automation Knowledgebase.
- For information about:
- File extensions created by Rockwell Automation software, firewall rules, and service dependences, see Answer ID 609492 in the Rockwell Automation Knowledgebase.
- TCP/UDP ports used by Rockwell Automation products, see Answer ID 898270 in the Rockwell Automation Knowledgebase.
Internet security software
- If third party Internet firewall software is enabled on a computer, FactoryTalk View Machine Edition cannot be installed or run.
Before installing or running FactoryTalk View Studio, configure your internet firewall to allow the following .exe files to access the Internet:
- C:\Program Files\Common Files\Rockwell\Rsvchost.exe
- C:\Program Files\Common Files\Rockwell\RnaDirServer.exe
- C:\Program Files\Common Files\Rockwell\VStudio.exe
- C:\Program Files\Common Files\Rockwell\RNADirMultiplexor.exe
- C:\Program Files\CommonFiles\Rockwell\RNADiagnosticsSrv.exe
- C:\Program Files\Rockwell Software\RSLinx Enterprise\RSLinxNG.exe
Before installing or running FactoryTalk View Machine Edition Station, configure your Internet firewall to allow the following .exe files to access the Internet:
- C:\Program Files\Rockwell Software\RSView Enterprise\MEMacroEditor.exe
- C:\Program Files\Rockwell Software\RSView Enterprise\MERuntime.exe
- C:\Program Files\Rockwell Software\RSView Enterprise\TagSrv.exe
After configuring your firewall software to allow these files internet access, restart your computer to apply the changes.
|
Tip:
|
If your computer is running a 64-bit operating system, the files are in \Program Files (x86), instead of \Program Files.
|
User Account Control settings
Constraints when using FactoryTalk View version 6.10.00 or later
- FactoryTalk View Machine Edition version 6.0 and earlier use Watcom database for the tag databases
- FactoryTalk View Machine Edition version 6.10, 7.0, 8.0, 8.10, 8.20, and 9.0 use Microsoft SQL Server 2008 R2 Express for the tag databases
- FactoryTalk View Machine Edition version 10.0 uses Microsoft SQL Server 2014 Express LocalDB for the tag databases
When installing FactoryTalk View Machine Edition version 6.10.00 or later:
- On a 32-bit operating system, Watcom database and SQL Server database will be installed.
- On a 64-bit operating system, only SQL Server database will be installed.
Due to this difference, some constraints with using FactoryTalk View Machine Edition version 6.10.00 or later are introduced on a 64-bit Windows OS.
To open or convert an application created with FactoryTalk View version 10.0 in FactoryTalk View version 9.0 or earlier, see Rockwell Automation Knowledgebase Answer ID 1041447.
For more information about constraints with creating and running MER on a 64-bit Windows operating system, review Appendix D, "Constraints when using FactoryTalk View version 6.10.00 or later" in FactoryTalk View Machine Edition Installation Guide for details.
Component names
- The names for the following FactoryTalk View Studio components do not support extended ASCII characters or UNICODE characters:
- Application
- HMI server
- Data server
- HMI tag
- FactoryTalk Linx shortcut
- design time application file (.med)
- All FactoryTalk View application components, including graphic displays, parameter files, macro files, and data log files
Alarms
- If filtering is set up, when <AllTriggers> is triggered, the <AllTriggers> message will not show in the Alarm Status List.
Application Documenter
- If you restored an application using the Application Manager, the Application Documenter may not be able to detect the restored application or select it for documentation.
To avoid the problem, open the restored application in FactoryTalk View Studio before opening it in the Application Documenter.
Application Manager
- If a FactoryTalk View Machine Edition application is created on a computer whose operating system is in one language, such as the English version of Windows, and is later restored on another operating system that is in another language, such as the German version of Windows, unexpected errors may arise when the application name includes more than 16 characters.
To avoid this problem:
- Open or restore the application on an operating system that is in the original language, English version of Windows in this example.
- On the English version of Windows operating system, use Application Manager to rename the application to 16 characters or less and to back up the application to an APA file.
- Restore the APA file on the operating system that is in another language, German version of Windows in this example.
For updated information, subscribe to Answer ID 42498 in the Rockwell Automation Knowledgebase.
- If a FactoryTalk View Machine Edition application is closed, but FactoryTalk View Studio remains open, the Application Manager cannot delete or copy the closed application. The Application Manager does not recognize the application as being closed.
To avoid this problem, open another application in FactoryTalk View Studio or close FactoryTalk View Studio before deleting or copying the application in Application Manager.
- The existing Application Name dialog box cannot show the .mea application when restoring a legacy .mea application through FactoryTalk View ME directly.
To avoid this problem, use Application Manager to convert the .mea application to an .med application. The .med application can then be imported using FactoryTalk View Machine Edition.
Data logging
- If a FactoryTalk View Machine Edition application running on a Windows desktop platform is logging data to a custom path, attempting to access the log file, (for example, to copy it), while data is being logged will stop the logging process and produce an error.
To avoid this problem, access the log file after the data is logged.
- If the custom path is set as C:\ in FactoryTalk View Machine Edition version 6.0 or later version applications (including the applications migrated from FactoryTalk View Machine Edition version 5.1 or earlier) running on Windows 7 or Windows Server 2008 operating system, the data logging process fails to start and cannot show the trend with historical data.
To avoid this problem, rebuild the application and change the store path to other drives or a subfolder of drive C:, such as "C:\log" or "C\log\data".
- If communication to a custom path fails while data is being written to the data log, data logging will stop.
To resume data logging, shut down and restart the application.
- When FactoryTalk View ME Station is configured to delete log files on startup, it will delete alarm log file, audit log file, data log model, and diagnostics.
Domain controller
- If you set up a primary domain controller with a backup domain controller to authenticate users for a PanelView Plus 7, PanelView Plus 6, PanelView Plus, or PanelView Plus CE terminal and the primary domain controller loses its network connection, the terminal will fail to authenticate through the backup domain controller.
This will not happen if you authenticate domain users for personal computers.
Edit menu
- The Delete Row(s) menu item on the Edit menu does not delete multiple selected rows in certain spreadsheet editors. If you select multiple rows in the Information Messages, Local Messages, Macros, and Alarm Setup (Messages tab) editors, and then select Delete Row(s) from the Edit menu, only one row will be deleted.
To delete multiple rows, right-click in the editor and select Delete Row(s).
Embedded variable
- Embedded variables are not loaded until the text in the graphic object they are associated with is shown. If an object with an embedded variable has visibility animation, the embedded variable will not be activated until the object becomes visible. If the object later becomes invisible, the embedded variable will remain active.
For example, if a display containing an object with both visibility animation and embedded variables opens with the object invisible, and if the connection between the embedded variable and its tag is broken, FactoryTalk Diagnostics will not register communication errors for the object until the object becomes visible. If the object later becomes invisible, the communications errors will still be logged.
This also means that if one or more states of a multistate indicator include embedded variables, the variables will become active when those states are shown.
Firmware Upgrade Package
- For the sake of expediency, we recommend upgrading via Ethernet or Compact Flash. The other protocols will work, however, the upgrade process may be extremely lengthy.
- When upgrading the firmware directly on a PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal, do not remove the Compact Flash card until you see the following message: "The firmware upgrade has been completed. Remove the Firmware Upgrade Card and then press the Exit button." Premature removal of the card will cause the upgrade to fail.
- When the existing Machine Edition software on a PanelView Plus terminal is uninstalled during the upgrade, a multi-language message shows, stating that the software may be corrupted. The message includes two buttons, marked Download and Continue. Ignore this message, and do not press either of these buttons. Pressing either of these buttons will cause the Firmware Upgrade Wizard to become unstable.
- Upgrading the firmware over a direct Ethernet or Serial connection will not work unless the PanelView File Transfer Utility is running on the terminal.
- Files on the network are not available for upgrades. The upgrade files must be on the same computer as the Firmware Upgrade Wizard, otherwise the upgrade cannot be completed.
- The firmware upgrade deletes any files and shortcuts in the startup directory (Storage card\Windows\Startup), including those not related to FactoryTalk View ME Station.
- When you upgrade the firmware using a firmware upgrade (Compact Flash) card, the install procedure does not check the available space on the terminal's storage card. If the upgrade is larger than the existing firmware installation, be sure there is sufficient space available before starting the upgrade.
- When downloading through a local connection, the progress dialog becomes locked and cannot be moved. If another application is opened over the dialog and then removed, the progress dialog does not refresh, but goes blank instead.
- When the PanelView Plus , PanelView Plus Compact, and PanelView Plus CE terminals start, the characters EBC, followed by a letter or a number sequence, are shown on the top right corner of the screen: EBC-M or EBC 2.00.30, for example. If you see an EBC letter version earlier than "M", the Firmware Upgrade Wizard cannot perform the system upgrade.
- Firmware upgrades to PanelView Plus and PanelView Plus Compact 400 and 600 terminals can be performed remotely provided the terminal has sufficient available space. Since the presence of KepServer drivers is the most likely to affect the amount of available memory, if the terminal includes KepServer drivers, or if the upgrade includes KepServer drivers, the download may fail. A Compact Flash card upgrade is recommended.
Global display
- If an object contains undefined strings (for example, Chinese), and you choose to show undefined strings in the default language (for example, English), after you copy and paste the object, the duplicated object always shows the English language when you switch application languages. In this example, if the default language remains English and you did not choose to show undefined strings in the default language, when you change the application's current language to Chinese or French, the duplicated object still shows the English language, instead of a question mark (?).
To avoid this problem, in the Language Configuration dialog box, clear the Display undefined strings using the default language check box before copying and pasting the object.
- Graphic objects that show floating point values, such as numeric displays and input objects, show only five decimal places and the fifth decimal place will be rounded if necessary.
- Graphic displays, images, and graphic libraries that have the same name cannot be opened at the same time.
- Objects that have rounded corners and use a wide line width (greater than 10) will not show the rounded corners on a PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal.
- If you are applying width or vertical position animation to text that uses Courier New font, the text will not animate properly.
To avoid this problem, select a different font.
- Scaled graphic objects add 1 to width or height settings when editing.
To avoid this problem, choose one of the following methods:
- Ungroup the objects before scaling, scale each object individually, and regroup if needed.
- Set the height and width for the objects twice.
Import files
- If you import a tag CSV file that contains large amounts of tags and alarms while a runtime application is running, you will need to wait a few minutes and the Server Busy dialog box may show.
To avoid this problem, stop the runtime application before importing a tag CSV file.
- When a PanelView 1200 project is converted to FactoryTalk View Machine Edition, the character lines are not scaled and some symbol characters may not convert correctly.
To avoid this problem, import the application and then scale the graphics after import.
- When a PanelView 1400 project is converted to FactoryTalk View Machine Edition, the Min and Max value of the Bit position tag may not convert correctly.
Language switching
- Spanish (Traditional Sort) cannot be saved in the Languages field of the Properties dialog box for a language switch button.
To save Spanish (Traditional Sort), make the selection in the Property Panel instead of in the Properties dialog box.
- When FactoryTalk ME Station is running on aPanelView Plus terminal, if the user presses the LS (Language Switch) button with the Start in Last Runtime Language option (Application Settings/Startup Language) selected, language switching is slower than in previous releases.
Memory
- If FactoryTalk View ME is configured to print alarms, and the printer is not connected, the alarms will accumulate in the memory. This can eventually create a low memory available situation.
To clear the accumulated print alarms, connect the configured printers. The memory will be released as each alarm prints.
Navigation
- Users cannot navigate through the Display List Selector by holding the Up or Down key on a terminal running FactoryTalk View Machine Edition Station version 6.10.00.
To avoid this problem, in FactoryTalk View Machine Edition Station, go to Terminal Settings > Input Device > Keyboard/Keypad and change the value for Repeat Rate to 2 or greater.
PanelView Plus 7 Standard application
- In FactoryTalk View Studio version 8.20.00 and earlier, a PanelView Plus 7 Standard application cannot contain more than 25 displays or more than 200 alarms. Starting from FactoryTalk View Studio version 9.00.00, a PanelView Plus 7 Standard application can contain up to 25 On Top displays, 25 Replace displays, and 500 alarms.
Using FactoryTalk View Studio version 9.00.00 or later, you can create a v8.20 or earlier version of PanelView Plus 7 Standard runtime application (.mer) that contains more than 25 displays or more than 200 alarms. The runtime application can be run on a PanelView Plus 7 Standard terminal installed with firmware version 8.20 or earlier, and can be restored to a design time application (.med) using FactoryTalk View Studio version 8.20.00 or earlier. However, from the restored application, you cannot create a PanelView Plus 7 Standard runtime application using FactoryTalk View Studio version 8.20.00 or earlier, because the number of alarms or displays exceeds the restriction defined in FactoryTalk View Studio version 8.20.00 or earlier.
PanelView Plus terminal
- If the AM symbol, PM symbol or Separator contains an ampersand (&), the string in the Time Format window is not shown correctly.
- When a parameter list is used to open a graphic display on a PanelView Plus terminal, it does not show correctly if spaces are part of the string.
To show strings correctly on a PanelView Plus terminal, define all strings without spaces.
Parameter file
- If a parameter file name includes an exclamation point (!), no error message will appear when the parameter file is saved, but it will not be possible to create the run-time file (.mer) for the application.
To avoid this problem, do not include an exclamation point in a parameter file name.
- When you use a parameter file generated from an SE project directly in an ME project, an error message shows.
To avoid this problem, delete "@!=1" from the first line of the parameter file.
- ANSI format parameter file is shown in mess code when opened in FactoryTalk View Studio.
To avoid this problem, convert the parameter file from ANSI to Unicode format, for example, in WordPad.
Runtime
- On a PanelView Plus 7 or PanelView Plus 6 terminal, when saving files that have the same file name extension, and whose names start with the same eight characters on an SD card:
- A maximum of 999 such files can be stored in a folder if the SD card is formatted using FAT32 (File Allocation Table 32).
- More than 999 such files can be stored in a folder if the SD card is formated using exFAT (Extended File Allocation Table). For example, when exporting CSV files (YYYY_MM_DD_HH_mm_ss-<FileLabel>-TYPE.csv), you may need to format the SD card using exFAT to save more files.
For more information about formatting an SD card using exFAT, see Appendix, "Format an SD card using exFAT" in the FactoryTalk View Machine Edition User's Guide.
- On a PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal, selecting the following option produces an error message in red: Terminal settings > Startup options > Startup tests > Select tests > CF External
This message can safely be ignored. It does not indicate that the Compact Flash card has failed. This option is intended for use at time of manufacture only.
- FactoryTalk View ME Station running on a Windows Server 2008 desktop does not save the Startup settings. Settings are not retained after closing the Terminal Settings > FactoryTalk View ME Station Startup dialog box.
- If a Windows-linked user belongs to a Distribution type Windows-linked user group, the user cannot log in to the running application on desktops.
To ensure that the user can log in, change the group type of the Windows-linked user group to Security.
- In Windows 2000 domain, if a user group is added to run-time security, but the group's user is not directly added to run-time security, the user cannot log in on PanelView Plus 7 or PanelView Plus 6 terminals when SSL is enabled.
Shut down an application
- When there are multiple macros running in the application or there are several displays popping up, if you shut down the application, you might experience a crash.
To resolve this issue, reset the terminal.
Tag
- If tag names, device shortcuts, or direct references include spaces, the Tag Substitution tool does not work for the tags in embedded variables.
To avoid this problem, remove spaces in tag names, device shortcuts, and direct references when the tags are in an embedded variable.
- If an HMI tag's Maximum property is increased, the change is not effective immediately.
To apply the changes, close and reopen FactoryTalk View Studio.
- Using a long integer tag with a value of 2,147,483,648 or greater will not allow an application to be validated or a converted MER file to be created from version 5.1 to 6.0. It is because that during the validation and conversion process, a tag is written in the command line (tag=2147483648), macro, or expression.
To avoid this problem, keep the integer tag value less than 2,147,483,648.
- When using tags, the values that are less than 53 bits are not shown correctly or may appear wireframed. It is because LINT, ULINT, or LWORD data types are not fully supported.
Trend
- If trend pens are configured with the maximum buffer size of 32,767 records, the entire allocated program memory on a CE terminal will be consumed in a few hours, resulting in an "out of memory" error. This requires a reboot of the terminal before the application can continue.
To avoid this problem, set the buffer for extra data below the theoretical maximum.
- If you use two or more pens, with the Isolated graphing display option selected, the colors of the pens will no longer match the legend and will appear offset.
To avoid this problem, add and use a Next Pen button to align the legend with the pen.
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Copyright © 2026 Rockwell Automation, Inc. All rights reserved.
Rockwell Automation, Allen-Bradley, and FactoryTalk are trademarks of Rockwell Automation, Inc.
To view a complete list of Rockwell Automation trademarks please
click here.Trademarks not belonging to Rockwell Automation are property of their respective companies.